#define _GNU_SOURCE #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "../../drivers/vhost/test.h" struct vq_info { int kick; int call; int num; int idx; void *ring; /* copy used for control */ struct vring vring; struct virtqueue *vq; }; struct vdev_info { struct virtio_device vdev; int control; struct pollfd fds[1]; struct vq_info vqs[1]; int nvqs; void *buf; size_t buf_size; struct vhost_memory *mem; }; void vq_notify(struct virtqueue *vq) { struct vq_info *info = vq->priv; unsigned long long v = 1; int r; r = write(info->kick, &v, sizeof v); assert(r == sizeof v); } void vq_callback(struct virtqueue *vq) { } void vhost_vq_setup(struct vdev_info *dev, struct vq_info *info) { struct vhost_vring_state state = { .index = info->idx }; struct vhost_vring_file file = { .index = info->idx }; unsigned long long features = dev->vdev.features[0]; struct vhost_vring_addr addr = { .index = info->idx, .desc_user_addr = (uint64_t)(unsigned long)info->vring.desc, .avail_user_addr = (uint64_t)(unsigned long)info->vring.avail, .used_user_addr = (uint64_t)(unsigned long)info->vring.used, }; int r; r = ioctl(dev->control, VHOST_SET_FEATURES, &features); assert(r >= 0); state.num = info->vring.num; r = ioctl(dev->control, VHOST_SET_VRING_NUM, &state); assert(r >= 0); state.num = 0; r = ioctl(dev->control, VHOST_SET_VRING_BASE, &state); assert(r >= 0); r = ioctl(dev->control, VHOST_SET_VRING_ADDR, &addr); assert(r >= 0); file.fd = info->kick; r = ioctl(dev->control, VHOST_SET_VRING_KICK, &file); assert(r >= 0); file.fd = info->call; r = ioctl(dev->control, VHOST_SET_VRING_CALL, &file); assert(r >= 0); } static void vq_info_add(struct vdev_info *dev, int num) { struct vq_info *info = &dev->vqs[dev->nvqs]; int r; info->idx = dev->nvqs; info->kick = eventfd(0, EFD_NONBLOCK); info->call = eventfd(0, EFD_NONBLOCK); r = posix_memalign(&info->ring, 4096, vring_size(num, 4096)); assert(r >= 0); memset(info->ring, 0, vring_size(num, 4096)); vring_init(&info->vring, num, info->ring, 4096); info->vq = vring_new_virtqueue(info->vring.num, 4096, &dev->vdev, info->ring, vq_notify, vq_callback, "test"); assert(info->vq); info->vq->priv = info; vhost_vq_setup(dev, info); dev->fds[info->idx].fd = info->call; dev->fds[info->idx].events = POLLIN; dev->nvqs++; } static void vdev_info_init(struct vdev_info* dev, unsigned long long features) { int r; memset(dev, 0, sizeof *dev); dev->vdev.features[0] = features; dev->vdev.features[1] = features >> 32; dev->buf_size = 1024; dev->buf = malloc(dev->buf_size); assert(dev->buf); dev->control = open("/dev/vhost-test", O_RDWR); assert(dev->control >= 0); r = ioctl(dev->control, VHOST_SET_OWNER, NULL); assert(r >= 0); dev->mem = malloc(offsetof(struct vhost_memory, regions) + sizeof dev->mem->regions[0]); assert(dev->mem); memset(dev->mem, 0, offsetof(struct vhost_memory, regions) + sizeof dev->mem->regions[0]); dev->mem->nregions = 1; dev->mem->regions[0].guest_phys_addr = (long)dev->buf; dev->mem->regions[0].userspace_addr = (long)dev->buf; dev->mem->regions[0].memory_size = dev->buf_size; r = ioctl(dev->control, VHOST_SET_MEM_TABLE, dev->mem); assert(r >= 0); } /* TODO: this is pretty bad: we get a cache line bounce * for the wait queue on poll and another one on read, * plus the read which is there just to clear the * current state. */ static void wait_for_interrupt(struct vdev_info *dev) { int i; unsigned long long val; poll(dev->fds, dev->nvqs, -1); for (i = 0; i < dev->nvqs; ++i) if (dev->fds[i].revents & POLLIN) { read(dev->fds[i].fd, &val, sizeof val); } } static void run_test(struct vdev_info *dev, struct vq_info *vq, int bufs) { struct scatterlist sl; long started = 0, completed = 0; long completed_before; int r, test = 1; unsigned len; long long spurious = 0; r = ioctl(dev->control, VHOST_TEST_RUN, &test); assert(r >= 0); for (;;) { virtqueue_disable_cb(vq->vq); completed_before = completed; do { if (started < bufs) { sg_init_one(&sl, dev->buf, dev->buf_size); r = virtqueue_add_buf(vq->vq, &sl, 1, 0, dev->buf + started); if (likely(r >= 0)) { ++started; virtqueue_kick(vq->vq); } } else r = -1; /* Flush out completed bufs if any */ if (virtqueue_get_buf(vq->vq, &len)) { ++completed; r = 0; } } while (r >= 0); if (completed == completed_before) ++spurious; assert(completed <= bufs); assert(started <= bufs); if (completed == bufs) break; if (virtqueue_enable_cb(vq->vq)) { wait_for_interrupt(dev); } } test = 0; r = ioctl(dev->control, VHOST_TEST_RUN, &test); assert(r >= 0); fprintf(stderr, "spurious wakeus: 0x%llx\n", spurious); } const char optstring[] = "h"; const struct option longopts[] = { { .name = "help", .val = 'h', }, { .name = "event-idx", .val = 'E', }, { .name = "no-event-idx", .val = 'e', }, { .name = "indirect", .val = 'I', }, { .name = "no-indirect", .val = 'i', }, { } }; static void help() { fprintf(stderr, "Usage: virtio_test [--help]" " [--no-indirect]" " [--no-event-idx]" "\n"); } int main(int argc, char **argv) { struct vdev_info dev; unsigned long long features = (1ULL << VIRTIO_RING_F_INDIRECT_DESC) | (1ULL << VIRTIO_RING_F_EVENT_IDX); int o; for (;;) { o = getopt_long(argc, argv, optstring, longopts, NULL); switch (o) { case -1: goto done; case '?': help(); exit(2); case 'e': features &= ~(1ULL << VIRTIO_RING_F_EVENT_IDX); break; case 'h': help(); goto done; case 'i': features &= ~(1ULL << VIRTIO_RING_F_INDIRECT_DESC); break; default: assert(0); break; } } done: vdev_info_init(&dev, features); vq_info_add(&dev, 256); run_test(&dev, &dev.vqs[0], 0x100000); return 0; }