index f02d87f68e5415ddefa5df4b00f0e88d085b4058..fa803c63da8c2185390c3e6a23c4850dfb4915ad 100644 (file)
/*
* OMAP2/3 PRM module functions
*
- * Copyright (C) 2010 Texas Instruments, Inc.
+ * Copyright (C) 2010-2011 Texas Instruments, Inc.
* Copyright (C) 2010 Nokia Corporation
* BenoƮt Cousson
* Paul Walmsley
#include <linux/err.h>
#include <linux/io.h>
-#include <plat/common.h>
+#include "common.h"
#include <plat/cpu.h>
#include <plat/prcm.h>
#include "prm-regbits-24xx.h"
#include "prm-regbits-34xx.h"
+static const struct omap_prcm_irq omap3_prcm_irqs[] = {
+ OMAP_PRCM_IRQ("wkup", 0, 0),
+ OMAP_PRCM_IRQ("io", 9, 1),
+};
+
+static struct omap_prcm_irq_setup omap3_prcm_irq_setup = {
+ .ack = OMAP3_PRM_IRQSTATUS_MPU_OFFSET,
+ .mask = OMAP3_PRM_IRQENABLE_MPU_OFFSET,
+ .nr_regs = 1,
+ .irqs = omap3_prcm_irqs,
+ .nr_irqs = ARRAY_SIZE(omap3_prcm_irqs),
+ .irq = INT_34XX_PRCM_MPU_IRQ,
+ .read_pending_irqs = &omap3xxx_prm_read_pending_irqs,
+ .ocp_barrier = &omap3xxx_prm_ocp_barrier,
+ .save_and_clear_irqen = &omap3xxx_prm_save_and_clear_irqen,
+ .restore_irqen = &omap3xxx_prm_restore_irqen,
+};
+
u32 omap2_prm_read_mod_reg(s16 module, u16 idx)
{
return __raw_readl(prm_base + module + idx);
{
return omap2_prm_rmw_mod_reg_bits(mask, bits, OMAP3430_GR_MOD, offset);
}
+
+/**
+ * omap3xxx_prm_read_pending_irqs - read pending PRM MPU IRQs into @events
+ * @events: ptr to a u32, preallocated by caller
+ *
+ * Read PRM_IRQSTATUS_MPU bits, AND'ed with the currently-enabled PRM
+ * MPU IRQs, and store the result into the u32 pointed to by @events.
+ * No return value.
+ */
+void omap3xxx_prm_read_pending_irqs(unsigned long *events)
+{
+ u32 mask, st;
+
+ /* XXX Can the mask read be avoided (e.g., can it come from RAM?) */
+ mask = omap2_prm_read_mod_reg(OCP_MOD, OMAP3_PRM_IRQENABLE_MPU_OFFSET);
+ st = omap2_prm_read_mod_reg(OCP_MOD, OMAP3_PRM_IRQSTATUS_MPU_OFFSET);
+
+ events[0] = mask & st;
+}
+
+/**
+ * omap3xxx_prm_ocp_barrier - force buffered MPU writes to the PRM to complete
+ *
+ * Force any buffered writes to the PRM IP block to complete. Needed
+ * by the PRM IRQ handler, which reads and writes directly to the IP
+ * block, to avoid race conditions after acknowledging or clearing IRQ
+ * bits. No return value.
+ */
+void omap3xxx_prm_ocp_barrier(void)
+{
+ omap2_prm_read_mod_reg(OCP_MOD, OMAP3_PRM_REVISION_OFFSET);
+}
+
+/**
+ * omap3xxx_prm_save_and_clear_irqen - save/clear PRM_IRQENABLE_MPU reg
+ * @saved_mask: ptr to a u32 array to save IRQENABLE bits
+ *
+ * Save the PRM_IRQENABLE_MPU register to @saved_mask. @saved_mask
+ * must be allocated by the caller. Intended to be used in the PRM
+ * interrupt handler suspend callback. The OCP barrier is needed to
+ * ensure the write to disable PRM interrupts reaches the PRM before
+ * returning; otherwise, spurious interrupts might occur. No return
+ * value.
+ */
+void omap3xxx_prm_save_and_clear_irqen(u32 *saved_mask)
+{
+ saved_mask[0] = omap2_prm_read_mod_reg(OCP_MOD,
+ OMAP3_PRM_IRQENABLE_MPU_OFFSET);
+ omap2_prm_write_mod_reg(0, OCP_MOD, OMAP3_PRM_IRQENABLE_MPU_OFFSET);
+
+ /* OCP barrier */
+ omap2_prm_read_mod_reg(OCP_MOD, OMAP3_PRM_REVISION_OFFSET);
+}
+
+/**
+ * omap3xxx_prm_restore_irqen - set PRM_IRQENABLE_MPU register from args
+ * @saved_mask: ptr to a u32 array of IRQENABLE bits saved previously
+ *
+ * Restore the PRM_IRQENABLE_MPU register from @saved_mask. Intended
+ * to be used in the PRM interrupt handler resume callback to restore
+ * values saved by omap3xxx_prm_save_and_clear_irqen(). No OCP
+ * barrier should be needed here; any pending PRM interrupts will fire
+ * once the writes reach the PRM. No return value.
+ */
+void omap3xxx_prm_restore_irqen(u32 *saved_mask)
+{
+ omap2_prm_write_mod_reg(saved_mask[0], OCP_MOD,
+ OMAP3_PRM_IRQENABLE_MPU_OFFSET);
+}
+
+static int __init omap3xxx_prcm_init(void)
+{
+ if (cpu_is_omap34xx() && !cpu_is_am33xx())
+ return omap_prcm_register_chain_handler(&omap3_prcm_irq_setup);
+ return 0;
+}
+subsys_initcall(omap3xxx_prcm_init);