arm: am33xx: Add CPSW MII mac select support
authorChandan Nath <chandan.nath@ti.com>
Wed, 11 Jan 2012 12:05:47 +0000 (17:35 +0530)
committerVaibhav Hiremath <hvaibhav@ti.com>
Mon, 23 Jan 2012 19:14:47 +0000 (00:44 +0530)
commit06b2d14954e0d9332490413cb9fb377b1c988480
treeea1313d246a0da75a56c2839ccdb821879884e47
parent38f1ae3d786e532574ec3a21e243a72afb54458a
arm: am33xx: Add CPSW MII mac select support

This patch fixes missing configuration for MII interface
configuration in device control register. MII mode selection
should be done depending up on the board/phy type.
This was missing in linux, however without this also it was
working as it was configured in uboot. This is required in
linux also in order to remove any dependency on uboot.

Signed-off-by: Chandan Nath <chandan.nath@ti.com>
arch/arm/mach-omap2/board-am335xevm.c
arch/arm/mach-omap2/devices.c
arch/arm/mach-omap2/include/mach/board-am335xevm.h