arm:omap:am335x: CPSW autonegotiates to 10/100 mbps
authorChandan Nath <chandan.nath@ti.com>
Wed, 5 Oct 2011 10:13:54 +0000 (15:43 +0530)
committerVaibhav Hiremath <hvaibhav@ti.com>
Mon, 23 Jan 2012 19:14:28 +0000 (00:44 +0530)
commit49e3ee1a5943ed402db8e5d381b1db83e04a0c64
tree06cc564921058f74de5aa5535cfd714e141ccc76
parent3e7405c5f4deb13c036c281e9b576f242d83556e
arm:omap:am335x: CPSW autonegotiates to 10/100 mbps

This patch is added as an workaround for cpsw to autonegotiates
to 10/100 mbps speed even if it is connected to 1 Gig link. The reason
for this is to overcome hardware issue of 1 Gig speed. Currently cpsw
is not working at 1 Gig speed and so when ethernet is connected to 1 Gig
link, it will auto negotiates and will fall back 10/100 mbps speed.

Signed-off-by: Chandan Nath <chandan.nath@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
drivers/net/ethernet/ti/cpsw.c