]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/commitdiff
OMAP2+: hwmod: Mark functions used only during initialization with __init
authorBenoit Cousson <b-cousson@ti.com>
Wed, 22 Dec 2010 04:31:28 +0000 (21:31 -0700)
committerPaul Walmsley <paul@pwsan.com>
Wed, 22 Dec 2010 04:31:28 +0000 (21:31 -0700)
_register, _find_mpu_port_index and _find_mpu_rt_base are static APIs
that will be used only during the omap_hwmod initialization phase.
There is no need to keep them for runtime.

Signed-off-by: Benoit Cousson <b-cousson@ti.com>
Signed-off-by: Paul Walmsley <paul@pwsan.com>
Cc: Kevin Hilman <khilman@deeprootsystems.com>
arch/arm/mach-omap2/omap_hwmod.c

index 298fc3b779ecfca0c54c3b4a9918d25f99b02e15..1a0dd5647cf61b7c5157016131c9f00a26f9c6d6 100644 (file)
@@ -673,7 +673,7 @@ static void _disable_optional_clocks(struct omap_hwmod *oh)
  * Returns the array index of the OCP slave port that the MPU
  * addresses the device on, or -EINVAL upon error or not found.
  */
-static int _find_mpu_port_index(struct omap_hwmod *oh)
+static int __init _find_mpu_port_index(struct omap_hwmod *oh)
 {
        int i;
        int found = 0;
@@ -707,7 +707,7 @@ static int _find_mpu_port_index(struct omap_hwmod *oh)
  * Return the virtual address of the base of the register target of
  * device @oh, or NULL on error.
  */
-static void __iomem *_find_mpu_rt_base(struct omap_hwmod *oh, u8 index)
+static void __iomem * __init _find_mpu_rt_base(struct omap_hwmod *oh, u8 index)
 {
        struct omap_hwmod_ocp_if *os;
        struct omap_hwmod_addr_space *mem;
@@ -1435,7 +1435,7 @@ static int _setup(struct omap_hwmod *oh, void *data)
  * that the copy process would be relatively complex due to the large number
  * of substructures.
  */
-static int _register(struct omap_hwmod *oh)
+static int __init _register(struct omap_hwmod *oh)
 {
        int ret, ms_id;
 
@@ -1587,7 +1587,7 @@ int omap_hwmod_for_each(int (*fn)(struct omap_hwmod *oh, void *data),
  * listed in @ohs that are valid for this chip.  Returns -EINVAL if
  * omap_hwmod_init() has already been called or 0 otherwise.
  */
-int omap_hwmod_init(struct omap_hwmod **ohs)
+int __init omap_hwmod_init(struct omap_hwmod **ohs)
 {
        struct omap_hwmod *oh;
        int r;