summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3eb3409)
raw | patch | inline | side by side (parent: 3eb3409)
author | Philip, Avinash <avinashphilip@ti.com> | |
Sun, 11 Mar 2012 08:21:38 +0000 (13:51 +0530) | ||
committer | Philip, Avinash <avinashphilip@ti.com> | |
Tue, 13 Mar 2012 12:40:37 +0000 (18:10 +0530) |
This patch
1. Cleans up actions required to access PWMSS config space. This
involves removal of semaphore, usage of use count values,
config_mem_base, etc. This is legitimate as multiple probe will not
overlap unless we sleep. Also multiple ioremap will succeed on same
address. So we can remap the PWMSS config space from respective drivers.
2. Replaces __raw [read/write] functions with [read/write], as these
functions inserts memory barrier instructions required with ARMv6+
3. Also corrects the coding style for write and read usage for more code
readability by read modify write approach.
5. Removes usage of clk_enabled flag.
6. Fixes the way of handling clock on pwm start and stop. In pwm start
clock should be enabled and disable of the clock should done from stop.
Failure condition added to fail on starting of running pwm device and
stopping of non-running pwm. For other API's, they have to explicitly
handle clock.
7. Adds config_mem_base variable to handle PWMSS config space in
ecap_pwm structure.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
1. Cleans up actions required to access PWMSS config space. This
involves removal of semaphore, usage of use count values,
config_mem_base, etc. This is legitimate as multiple probe will not
overlap unless we sleep. Also multiple ioremap will succeed on same
address. So we can remap the PWMSS config space from respective drivers.
2. Replaces __raw [read/write] functions with [read/write], as these
functions inserts memory barrier instructions required with ARMv6+
3. Also corrects the coding style for write and read usage for more code
readability by read modify write approach.
5. Removes usage of clk_enabled flag.
6. Fixes the way of handling clock on pwm start and stop. In pwm start
clock should be enabled and disable of the clock should done from stop.
Failure condition added to fail on starting of running pwm device and
stopping of non-running pwm. For other API's, they have to explicitly
handle clock.
7. Adds config_mem_base variable to handle PWMSS config space in
ecap_pwm structure.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
drivers/pwm/ecap.c | patch | blob | history |
diff --git a/drivers/pwm/ecap.c b/drivers/pwm/ecap.c
index cc2ed19fbee4531e0f2f8074dc876d8a9e00a769..fb876f1e394de4fe67264e95e4be1a5880f7c78c 100644 (file)
--- a/drivers/pwm/ecap.c
+++ b/drivers/pwm/ecap.c
struct pwm_device_ops ops;
spinlock_t lock;
struct clk *clk;
- int clk_enabled;
void __iomem *mmio_base;
u8 version;
+ void __iomem *config_mem_base;
};
static inline struct ecap_pwm *to_ecap_pwm(const struct pwm_device *p)
static int ecap_pwm_stop(struct pwm_device *p)
{
- unsigned long flags;
+ unsigned long flags, v;
struct ecap_pwm *ep = to_ecap_pwm(p);
- clk_enable(ep->clk);
+ /* Trying to stop a non-running PWM, not allowed */
+ if (!pwm_is_running(p))
+ return -EPERM;
spin_lock_irqsave(&ep->lock, flags);
- __raw_writew(__raw_readw(ep->mmio_base + CAPTURE_CTRL2_REG) &
- ~BIT(4), ep->mmio_base + CAPTURE_CTRL2_REG);
+ v = readw(ep->mmio_base + CAPTURE_CTRL2_REG);
+ v &= ~BIT(4);
+ writew(v, ep->mmio_base + CAPTURE_CTRL2_REG);
spin_unlock_irqrestore(&ep->lock, flags);
+ /* For PWM clock should be disabled on stop */
clk_disable(ep->clk);
- if (ep->clk_enabled) {
- clk_disable(ep->clk);
- ep->clk_enabled = 0;
- }
clear_bit(FLAG_RUNNING, &p->flags);
return 0;
static int ecap_pwm_start(struct pwm_device *p)
{
int ret = 0;
- unsigned long flags;
+ unsigned long flags, v;
struct ecap_pwm *ep = to_ecap_pwm(p);
+ /* Trying to start a running PWM, not allowed */
+ if (pwm_is_running(p))
+ return -EPERM;
+
+ /* For PWM clock should be enabled on start */
clk_enable(ep->clk);
+
spin_lock_irqsave(&ep->lock, flags);
- __raw_writew(__raw_readw(ep->mmio_base + CAPTURE_CTRL2_REG) |
- BIT(4), ep->mmio_base + CAPTURE_CTRL2_REG);
+ v = readw(ep->mmio_base + CAPTURE_CTRL2_REG);
+ v |= BIT(4);
+ writew(v, ep->mmio_base + CAPTURE_CTRL2_REG);
spin_unlock_irqrestore(&ep->lock, flags);
-
- clk_disable(ep->clk);
- if (!ep->clk_enabled) {
- ret = clk_enable(ep->clk);
- if (ret)
- return ret;
- ep->clk_enabled = 1;
- }
set_bit(FLAG_RUNNING, &p->flags);
return ret;
static int ecap_pwm_set_polarity(struct pwm_device *p, char pol)
{
- unsigned long flags;
+ unsigned long flags, v;
struct ecap_pwm *ep = to_ecap_pwm(p);
clk_enable(ep->clk);
spin_lock_irqsave(&ep->lock, flags);
- __raw_writew((__raw_readw(ep->mmio_base + CAPTURE_CTRL2_REG) &
- ~BIT(10)) | (!pol << 10), ep->mmio_base + CAPTURE_CTRL2_REG);
+ v = readw(ep->mmio_base + CAPTURE_CTRL2_REG);
+ v &= ~BIT(10);
+ v |= (!pol << 10);
+ writew(v, ep->mmio_base + CAPTURE_CTRL2_REG);
spin_unlock_irqrestore(&ep->lock, flags);
clk_disable(ep->clk);
clk_enable(ep->clk);
spin_lock_irqsave(&ep->lock, flags);
- __raw_writel((p->period_ticks) - 1, ep->mmio_base + CAPTURE_3_REG);
- __raw_writew(ECTRL2_MDSL_ECAP | ECTRL2_SYNCOSEL_MASK |
- ECTRL2_CTRSTP_FREERUN, ep->mmio_base + CAPTURE_CTRL2_REG);
+ writel((p->period_ticks) - 1, ep->mmio_base + CAPTURE_3_REG);
+ writew(ECTRL2_MDSL_ECAP | ECTRL2_SYNCOSEL_MASK | ECTRL2_CTRSTP_FREERUN,
+ ep->mmio_base + CAPTURE_CTRL2_REG);
spin_unlock_irqrestore(&ep->lock, flags);
clk_disable(ep->clk);
clk_enable(ep->clk);
spin_lock_irqsave(&ep->lock, flags);
- __raw_writew(ECTRL2_MDSL_ECAP | ECTRL2_SYNCOSEL_MASK |
- ECTRL2_CTRSTP_FREERUN, ep->mmio_base + CAPTURE_CTRL2_REG);
+ writew(ECTRL2_MDSL_ECAP | ECTRL2_SYNCOSEL_MASK | ECTRL2_CTRSTP_FREERUN,
+ ep->mmio_base + CAPTURE_CTRL2_REG);
if (p->duty_ticks > 0) {
- __raw_writel(p->duty_ticks, ep->mmio_base + CAPTURE_4_REG);
+ writel(p->duty_ticks, ep->mmio_base + CAPTURE_4_REG);
} else {
- __raw_writel(p->duty_ticks, ep->mmio_base + CAPTURE_2_REG);
- __raw_writel(0, ep->mmio_base + TIMER_CTR_REG);
+ writel(p->duty_ticks, ep->mmio_base + CAPTURE_2_REG);
+ writel(0, ep->mmio_base + TIMER_CTR_REG);
}
spin_unlock_irqrestore(&ep->lock, flags);
if (!ep) {
dev_err(&pdev->dev, "failed to allocate memory\n");
- ret = -ENOMEM;
- goto err_mem_failure;
+ return -ENOMEM;
}
ep->version = pdata->version;
if (IS_ERR(ep->clk)) {
ret = PTR_ERR(ep->clk);
- goto err_clock_failure;
+ goto err_clk_get;
}
if (ep->version == PWM_VERSION_1) {
- down(&pdata->config_semaphore);
r = platform_get_resource(pdev, IORESOURCE_MEM, 0);
if (!r) {
dev_err(&pdev->dev, "no memory resource defined\n");
ret = -ENOMEM;
- up(&pdata->config_semaphore);
- goto err_resource_mem_failure;
- }
-
- r = request_mem_region(r->start, resource_size(r), pdev->name);
-
- if (!r) {
-
- if (pdata->config_mem_base) {
- goto set_bit;
- } else {
- dev_err(&pdev->dev,
- "failed to request memory resource\n");
- ret = -EBUSY;
- up(&pdata->config_semaphore);
- goto err_request_mem_failure;
- }
+ goto err_get_resource;
}
- pdata->config_mem_base = ioremap(r->start, resource_size(r));
+ ep->config_mem_base = ioremap(r->start, resource_size(r));
- if (!pdata->config_mem_base) {
+ if (!ep->config_mem_base) {
dev_err(&pdev->dev, "failed to ioremap() registers\n");
- ret = -ENODEV;
- up(&pdata->config_semaphore);
- goto err_free_mem_config;
+ ret = -ENOMEM;
+ goto err_get_resource;
}
-set_bit:
- pdata->pwmss_module_usage_count++;
clk_enable(ep->clk);
- val = __raw_readw(pdata->config_mem_base + PWMSS_CLKCONFIG);
+ val = readw(ep->config_mem_base + PWMSS_CLKCONFIG);
val |= BIT(ECAP_CLK_EN);
- __raw_writew(val, pdata->config_mem_base + PWMSS_CLKCONFIG);
+ writew(val, ep->config_mem_base + PWMSS_CLKCONFIG);
clk_disable(ep->clk);
- up(&pdata->config_semaphore);
}
spin_lock_init(&ep->lock);
if (!r) {
dev_err(&pdev->dev, "no memory resource defined\n");
ret = -ENODEV;
- goto err_resource_mem2_failiure;
+ goto err_request_mem;
}
r = request_mem_region(r->start, resource_size(r), pdev->name);
if (!r) {
dev_err(&pdev->dev, "failed to request memory resource\n");
ret = -EBUSY;
- goto err_request_mem2_failure;
+ goto err_request_mem;
}
ep->mmio_base = ioremap(r->start, resource_size(r));
if (!ep->mmio_base) {
dev_err(&pdev->dev, "failed to ioremap() registers\n");
ret = -ENODEV;
- goto err_free_mem2;
+ goto err_ioremap;
}
ep->pwm.ops = &ep->ops;
platform_set_drvdata(pdev, ep);
return 0;
-err_free_mem2:
+err_ioremap:
release_mem_region(r->start, resource_size(r));
-err_request_mem2_failure:
-err_resource_mem2_failiure:
- if (ep->version == PWM_VERSION_1) {
- down(&pdata->config_semaphore);
- pdata->pwmss_module_usage_count--;
-
- if (!pdata->pwmss_module_usage_count) {
- iounmap(pdata->config_mem_base);
- pdata->config_mem_base = NULL;
- }
- up(&pdata->config_semaphore);
- }
-err_free_mem_config:
+err_request_mem:
if (ep->version == PWM_VERSION_1) {
- r = platform_get_resource(pdev, IORESOURCE_MEM, 0);
- release_mem_region(r->start, resource_size(r));
+ iounmap(ep->config_mem_base);
+ ep->config_mem_base = NULL;
}
-err_request_mem_failure:
-err_resource_mem_failure:
+err_get_resource:
clk_put(ep->clk);
-err_clock_failure:
+err_clk_get:
kfree(ep);
-err_mem_failure:
return ret;
}
if (ep->version == PWM_VERSION_1) {
pdata = (&pdev->dev)->platform_data;
- down(&pdata->config_semaphore);
- pdata->pwmss_module_usage_count--;
- val = __raw_readw(pdata->config_mem_base + PWMSS_CLKCONFIG);
+ val = readw(ep->config_mem_base + PWMSS_CLKCONFIG);
val &= ~BIT(ECAP_CLK_EN);
- __raw_writew(val, pdata->config_mem_base + PWMSS_CLKCONFIG);
-
- if (!pdata->pwmss_module_usage_count) {
- iounmap(pdata->config_mem_base);
- pdata->config_mem_base = NULL;
- r = platform_get_resource(pdev, IORESOURCE_MEM, 0);
- release_mem_region(r->start, resource_size(r));
- }
- up(&pdata->config_semaphore);
+ writew(val, ep->config_mem_base + PWMSS_CLKCONFIG);
+ iounmap(ep->config_mem_base);
+ ep->config_mem_base = NULL;
}
pwm_unregister(&ep->pwm);