USB: musb: NAK timeout scheme on bulk TX endpoint
authorAjay Kumar Gupta <ajay.gupta@ti.com>
Fri, 31 Dec 2010 07:22:30 +0000 (12:52 +0530)
committerVaibhav Hiremath <hvaibhav@ti.com>
Mon, 23 Jan 2012 19:14:09 +0000 (00:44 +0530)
Fixes endpoint starvation issue when more than one bulk QH is
multiplexed on the reserved bulk TX endpoint.

This patch sets the NAK timeout interval for such QHs, and when
a timeout triggers the next QH will be scheduled.

This scheme doesn't work for devices which are connected to a
high to full speed tree (transaction translator) as there is
no NAK timeout interrupt from the musb controller from such
devices.

Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
drivers/usb/musb/musb_host.c

index 592e1904ceb0de27476a7b0e519741a90c5d52b7..d699b34b32c0fe4208e719d3a09024d585a17d40 100644 (file)
@@ -914,6 +914,73 @@ static void musb_ep_program(struct musb *musb, u8 epnum,
        }
 }
 
        }
 }
 
+/* Schedule next QH from musb->in_bulk/out_bulk and move the current qh to
+ * the end; avoids starvation for other endpoints.
+ */
+static void musb_bulk_nak_timeout(struct musb *musb, struct musb_hw_ep *ep,
+       int is_in)
+{
+       struct dma_channel      *dma;
+       struct urb              *urb;
+       void __iomem            *mbase = musb->mregs;
+       void __iomem            *epio = ep->regs;
+       struct musb_qh          *cur_qh, *next_qh;
+       u16                     rx_csr, tx_csr;
+
+       musb_ep_select(musb, mbase, ep->epnum);
+       if (is_in) {
+               dma = is_dma_capable() ? ep->rx_channel : NULL;
+
+               /* clear nak timeout bit */
+               rx_csr = musb_readw(epio, MUSB_RXCSR);
+               rx_csr |= MUSB_RXCSR_H_WZC_BITS;
+               rx_csr &= ~MUSB_RXCSR_DATAERROR;
+               musb_writew(epio, MUSB_RXCSR, rx_csr);
+
+               cur_qh = first_qh(&musb->in_bulk);
+       } else {
+               dma = is_dma_capable() ? ep->tx_channel : NULL;
+
+               /* clear nak timeout bit */
+               tx_csr = musb_readw(epio, MUSB_TXCSR);
+               tx_csr |= MUSB_TXCSR_H_WZC_BITS;
+               tx_csr &= ~MUSB_TXCSR_H_NAKTIMEOUT;
+               musb_writew(epio, MUSB_TXCSR, tx_csr);
+
+               cur_qh = first_qh(&musb->out_bulk);
+       }
+       if (cur_qh) {
+               urb = next_urb(cur_qh);
+               if (dma_channel_status(dma) == MUSB_DMA_STATUS_BUSY) {
+                       dma->status = MUSB_DMA_STATUS_CORE_ABORT;
+                       musb->dma_controller->channel_abort(dma);
+                       urb->actual_length += dma->actual_len;
+                       dma->actual_len = 0L;
+               }
+               musb_save_toggle(cur_qh, is_in, urb);
+
+               if (is_in) {
+                       /* move cur_qh to end of queue */
+                       list_move_tail(&cur_qh->ring, &musb->in_bulk);
+
+                       /* get the next qh from musb->in_bulk */
+                       next_qh = first_qh(&musb->in_bulk);
+
+                       /* set rx_reinit and schedule the next qh */
+                       ep->rx_reinit = 1;
+               } else {
+                       /* move cur_qh to end of queue */
+                       list_move_tail(&cur_qh->ring, &musb->out_bulk);
+
+                       /* get the next qh from musb->out_bulk */
+                       next_qh = first_qh(&musb->out_bulk);
+
+                       /* set tx_reinit and schedule the next qh */
+                       ep->tx_reinit = 1;
+               }
+               musb_start_urb(musb, is_in, next_qh);
+       }
+}
 
 /*
  * Service the default endpoint (ep0) as host.
 
 /*
  * Service the default endpoint (ep0) as host.
@@ -1176,20 +1243,27 @@ void musb_host_tx(struct musb *musb, u8 epnum)
                status = -ETIMEDOUT;
 
        } else if (tx_csr & MUSB_TXCSR_H_NAKTIMEOUT) {
                status = -ETIMEDOUT;
 
        } else if (tx_csr & MUSB_TXCSR_H_NAKTIMEOUT) {
-               dev_dbg(musb->controller, "TX end=%d device not responding\n", epnum);
+               if (USB_ENDPOINT_XFER_BULK == qh->type && qh->mux == 1
+                               && !list_is_singular(&musb->out_bulk)) {
 
 
-               /* NOTE:  this code path would be a good place to PAUSE a
-                * transfer, if there's some other (nonperiodic) tx urb
-                * that could use this fifo.  (dma complicates it...)
-                * That's already done for bulk RX transfers.
-                *
-                * if (bulk && qh->ring.next != &musb->out_bulk), then
-                * we have a candidate... NAKing is *NOT* an error
-                */
-               musb_ep_select(musb, mbase, epnum);
-               musb_writew(epio, MUSB_TXCSR,
-                               MUSB_TXCSR_H_WZC_BITS
-                               | MUSB_TXCSR_TXPKTRDY);
+                       dev_dbg(musb->controller, "TX end %d NAK timeout\n", epnum);
+                       musb_bulk_nak_timeout(musb, hw_ep, 0);
+               } else {
+                       dev_dbg(musb->controller, "TX end=%d device not responding\n", epnum);
+
+                       /* NOTE: this code path would be a good place to PAUSE a
+                        * transfer, if there's some other (nonperiodic) tx urb
+                        * that could use this fifo.  (dma complicates it...)
+                        * That's already done for bulk RX transfers.
+                        *
+                        * if (bulk && qh->ring.next != &musb->out_bulk), then
+                        * we have a candidate... NAKing is *NOT* an error
+                        */
+                       musb_ep_select(musb, mbase, epnum);
+                       musb_writew(epio, MUSB_TXCSR,
+                                       MUSB_TXCSR_H_WZC_BITS
+                                       | MUSB_TXCSR_TXPKTRDY);
+               }
                return;
        }
 
                return;
        }
 
@@ -1406,50 +1480,6 @@ void musb_host_tx(struct musb *musb, u8 epnum)
  *     last packet of one URB's transfer.
  */
 
  *     last packet of one URB's transfer.
  */
 
-/* Schedule next QH from musb->in_bulk and move the current qh to
- * the end; avoids starvation for other endpoints.
- */
-static void musb_bulk_rx_nak_timeout(struct musb *musb, struct musb_hw_ep *ep)
-{
-       struct dma_channel      *dma;
-       struct urb              *urb;
-       void __iomem            *mbase = musb->mregs;
-       void __iomem            *epio = ep->regs;
-       struct musb_qh          *cur_qh, *next_qh;
-       u16                     rx_csr;
-
-       musb_ep_select(musb, mbase, ep->epnum);
-       dma = is_dma_capable() ? ep->rx_channel : NULL;
-
-       /* clear nak timeout bit */
-       rx_csr = musb_readw(epio, MUSB_RXCSR);
-       rx_csr |= MUSB_RXCSR_H_WZC_BITS;
-       rx_csr &= ~MUSB_RXCSR_DATAERROR;
-       musb_writew(epio, MUSB_RXCSR, rx_csr);
-
-       cur_qh = first_qh(&musb->in_bulk);
-       if (cur_qh) {
-               urb = next_urb(cur_qh);
-               if (dma_channel_status(dma) == MUSB_DMA_STATUS_BUSY) {
-                       dma->status = MUSB_DMA_STATUS_CORE_ABORT;
-                       musb->dma_controller->channel_abort(dma);
-                       urb->actual_length += dma->actual_len;
-                       dma->actual_len = 0L;
-               }
-               musb_save_toggle(cur_qh, 1, urb);
-
-               /* move cur_qh to end of queue */
-               list_move_tail(&cur_qh->ring, &musb->in_bulk);
-
-               /* get the next qh from musb->in_bulk */
-               next_qh = first_qh(&musb->in_bulk);
-
-               /* set rx_reinit and schedule the next qh */
-               ep->rx_reinit = 1;
-               musb_start_urb(musb, 1, next_qh);
-       }
-}
-
 /*
  * Service an RX interrupt for the given IN endpoint; docs cover bulk, iso,
  * and high-bandwidth IN transfer cases.
 /*
  * Service an RX interrupt for the given IN endpoint; docs cover bulk, iso,
  * and high-bandwidth IN transfer cases.
@@ -1526,7 +1556,7 @@ void musb_host_rx(struct musb *musb, u8 epnum)
                        if (usb_pipebulk(urb->pipe)
                                        && qh->mux == 1
                                        && !list_is_singular(&musb->in_bulk)) {
                        if (usb_pipebulk(urb->pipe)
                                        && qh->mux == 1
                                        && !list_is_singular(&musb->in_bulk)) {
-                               musb_bulk_rx_nak_timeout(musb, hw_ep);
+                               musb_bulk_nak_timeout(musb, hw_ep, 1);
                                return;
                        }
                        musb_ep_select(musb, mbase, epnum);
                                return;
                        }
                        musb_ep_select(musb, mbase, epnum);
@@ -1883,14 +1913,14 @@ static int musb_schedule(
                else
                        head = &musb->out_bulk;
 
                else
                        head = &musb->out_bulk;
 
-               /* Enable bulk RX NAK timeout scheme when bulk requests are
+               /* Enable bulk RX/TX NAK timeout scheme when bulk requests are
                 * multiplexed.  This scheme doen't work in high speed to full
                 * speed scenario as NAK interrupts are not coming from a
                 * full speed device connected to a high speed device.
                 * NAK timeout interval is 8 (128 uframe or 16ms) for HS and
                 * 4 (8 frame or 8ms) for FS device.
                 */
                 * multiplexed.  This scheme doen't work in high speed to full
                 * speed scenario as NAK interrupts are not coming from a
                 * full speed device connected to a high speed device.
                 * NAK timeout interval is 8 (128 uframe or 16ms) for HS and
                 * 4 (8 frame or 8ms) for FS device.
                 */
-               if (is_in && qh->dev)
+               if (qh->dev)
                        qh->intv_reg =
                                (USB_SPEED_HIGH == qh->dev->speed) ? 8 : 4;
                goto success;
                        qh->intv_reg =
                                (USB_SPEED_HIGH == qh->dev->speed) ? 8 : 4;
                goto success;