summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: aee48e3)
raw | patch | inline | side by side (parent: aee48e3)
author | Benoit Cousson <b-cousson@ti.com> | |
Tue, 21 Sep 2010 16:57:59 +0000 (18:57 +0200) | ||
committer | Paul Walmsley <paul@pwsan.com> | |
Tue, 21 Sep 2010 21:28:30 +0000 (15:28 -0600) |
In OMAP3 a specific SYSSTATUS register was used to get the softreset status.
Starting in OMAP4, some IPs does not have SYSSTATUS register and instead
use the SYSC softreset bit to provide the status.
Other cases might exist:
- Some IPs like McBSP does have a softreset control but no reset status.
- Some IPs that represent subsystem, like the DSS, can contains
a reset status without softreset control. The status is the aggregation
of all the sub modules reset status.
- Add a new flag (SYSC_HAS_RESET_STATUS) to identify the new programming model
and replace the previous SYSS_MISSING, that was used to flag IP with
softreset control but without the SYSSTATUS register, with a specific
SYSS_HAS_RESET_STATUS flag.
- MCSPI and MMC contains both programming models, so the legacy one
will be prevented by removing the syss offset field that become useless.
Signed-off-by: Benoit Cousson <b-cousson@ti.com>
Signed-off-by: Paul Walmsley <paul@pwsan.com>
Cc: Kevin Hilman <khilman@deeprootsystems.com>
Cc: Rajendra Nayak <rnayak@ti.com>
Starting in OMAP4, some IPs does not have SYSSTATUS register and instead
use the SYSC softreset bit to provide the status.
Other cases might exist:
- Some IPs like McBSP does have a softreset control but no reset status.
- Some IPs that represent subsystem, like the DSS, can contains
a reset status without softreset control. The status is the aggregation
of all the sub modules reset status.
- Add a new flag (SYSC_HAS_RESET_STATUS) to identify the new programming model
and replace the previous SYSS_MISSING, that was used to flag IP with
softreset control but without the SYSSTATUS register, with a specific
SYSS_HAS_RESET_STATUS flag.
- MCSPI and MMC contains both programming models, so the legacy one
will be prevented by removing the syss offset field that become useless.
Signed-off-by: Benoit Cousson <b-cousson@ti.com>
Signed-off-by: Paul Walmsley <paul@pwsan.com>
Cc: Kevin Hilman <khilman@deeprootsystems.com>
Cc: Rajendra Nayak <rnayak@ti.com>
arch/arm/mach-omap2/omap_hwmod.c | patch | blob | history | |
arch/arm/plat-omap/include/plat/omap_hwmod.h | patch | blob | history |
index 8c279235ea8734d16a3d7a59da6fefe10dd23a98..5027879b062fe82e2e4c2eb8def51dc454bb674c 100644 (file)
* enabled for this to work. Returns -EINVAL if the hwmod cannot be
* reset this way or if the hwmod is in the wrong state, -ETIMEDOUT if
* the module did not reset in time, or 0 upon success.
+ *
+ * In OMAP3 a specific SYSSTATUS register is used to get the reset status.
+ * Starting in OMAP4, some IPs does not have SYSSTATUS register and instead
+ * use the SYSCONFIG softreset bit to provide the status.
+ *
+ * Note that some IP like McBSP does have a reset control but no reset status.
*/
static int _reset(struct omap_hwmod *oh)
{
int c = 0;
if (!oh->class->sysc ||
- !(oh->class->sysc->sysc_flags & SYSC_HAS_SOFTRESET) ||
- (oh->class->sysc->sysc_flags & SYSS_MISSING))
+ !(oh->class->sysc->sysc_flags & SYSC_HAS_SOFTRESET))
return -EINVAL;
/* clocks must be on for this operation */
return r;
_write_sysconfig(v, oh);
- omap_test_timeout((omap_hwmod_readl(oh, oh->class->sysc->syss_offs) &
- SYSS_RESETDONE_MASK),
- MAX_MODULE_SOFTRESET_WAIT, c);
+ if (oh->class->sysc->sysc_flags & SYSS_HAS_RESET_STATUS)
+ omap_test_timeout((omap_hwmod_readl(oh,
+ oh->class->sysc->syss_offs)
+ & SYSS_RESETDONE_MASK),
+ MAX_MODULE_SOFTRESET_WAIT, c);
+ else if (oh->class->sysc->sysc_flags & SYSC_HAS_RESET_STATUS)
+ omap_test_timeout(!(omap_hwmod_readl(oh,
+ oh->class->sysc->sysc_offs)
+ & SYSC_TYPE2_SOFTRESET_MASK),
+ MAX_MODULE_SOFTRESET_WAIT, c);
if (c == MAX_MODULE_SOFTRESET_WAIT)
pr_warning("omap_hwmod: %s: softreset failed (waited %d usec)\n",
diff --git a/arch/arm/plat-omap/include/plat/omap_hwmod.h b/arch/arm/plat-omap/include/plat/omap_hwmod.h
index 7fde44d3c2482557c37c35155c4a4c9b8c4ff299..faa08273b1e45b7a6112ddf140ca564384f038b4 100644 (file)
#define SYSC_HAS_CLOCKACTIVITY (1 << 4)
#define SYSC_HAS_SIDLEMODE (1 << 5)
#define SYSC_HAS_MIDLEMODE (1 << 6)
-#define SYSS_MISSING (1 << 7)
+#define SYSS_HAS_RESET_STATUS (1 << 7)
#define SYSC_NO_CACHE (1 << 8) /* XXX SW flag, belongs elsewhere */
+#define SYSC_HAS_RESET_STATUS (1 << 9)
/* omap_hwmod_sysconfig.clockact flags */
#define CLOCKACT_TEST_BOTH 0x0