summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: b4ce6a2)
raw | patch | inline | side by side (parent: b4ce6a2)
author | Florian Tobias Schandinat <FlorianSchandinat@gmx.de> | |
Sat, 23 Apr 2011 22:06:18 +0000 (22:06 +0000) | ||
committer | Florian Tobias Schandinat <FlorianSchandinat@gmx.de> | |
Sat, 23 Apr 2011 22:06:18 +0000 (22:06 +0000) |
This patch fixes the devices connected on OLPC. The OLPC panel seems
to be connected to DVP1 and LVDS2 for some reasons and if not both
are handled correct the display does not work correct or not at all.
This patch prevents regressions on the OLPC where it worked by
accident but would break in future as the driver did not know the
correct devices connected. This might also fix hardware scaling.
Hopefully the OLPC is the only device with such a requirement but it
will be certainly better to actually know what devices are actually
connected and to not work by accident.
Signed-off-by: Florian Tobias Schandinat <FlorianSchandinat@gmx.de>
to be connected to DVP1 and LVDS2 for some reasons and if not both
are handled correct the display does not work correct or not at all.
This patch prevents regressions on the OLPC where it worked by
accident but would break in future as the driver did not know the
correct devices connected. This might also fix hardware scaling.
Hopefully the OLPC is the only device with such a requirement but it
will be certainly better to actually know what devices are actually
connected and to not work by accident.
Signed-off-by: Florian Tobias Schandinat <FlorianSchandinat@gmx.de>
drivers/video/via/hw.c | patch | blob | history |
diff --git a/drivers/video/via/hw.c b/drivers/video/via/hw.c
index 980e263f187550681892f2fc2109ef49134506c1..b8f01103f5c5ae7c498b5ffb33d32fb92cc482ee 100644 (file)
--- a/drivers/video/via/hw.c
+++ b/drivers/video/via/hw.c
*/
#include <linux/via-core.h>
+#include <asm/olpc.h>
#include "global.h"
static struct pll_config cle266_pll_config[] = {
viaparinfo->chip_info->
lvds_chip_info2.output_interface);
}
+
+ /* looks like the OLPC has its display wired to DVP1 and LVDS2 */
+ if (machine_is_olpc())
+ viaparinfo->shared->iga2_devices = VIA_DVP1 | VIA_LVDS2;
}
static void set_color_register(u8 index, u8 red, u8 green, u8 blue)