summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 6aeef6f)
raw | patch | inline | side by side (parent: 6aeef6f)
author | Manjunathappa, Prakash <prakash.pm@ti.com> | |
Tue, 27 Sep 2011 06:01:28 +0000 (11:31 +0530) | ||
committer | Vaibhav Hiremath <hvaibhav@ti.com> | |
Mon, 23 Jan 2012 19:14:26 +0000 (00:44 +0530) |
There is flicker/tearing issue was observed with current FB driver.
Below link to wiki describes the issue and it also has link to
application with which issue can be reproduced.
http://ap-fpdsp-swapps.dal.design.ti.com/index.php/DA8XX_LCDC_Linux_FB_FAQs
Issue is because of 2 active DMA channels ping ponging among them
along with usage of 2 DDR buffer ping pong and application is not
aware of active DMA channel.
Below steps describe issue:
1)Initially assume both buffers FB0 and FB1 are programmed for buffer-0.
2)On EOF0: Program FB0 for buffer-1, indicate(wake up) application
to fill up buffer-0. As FB1 is active and continues to DMA buffer-0
(which is being filled), leading to tearing/flickering issue.
3)On EOF1: Program FB1 for buffer-0, indicate(wake up) application to
fill up buffer-1. As FB0 is active and continues to DMA buffer-1(which
is being filled), leading to tearing/flickering issue.
4)On EOF0: Program FB0 for buffer-1, indicate(wake up) application to fill
up buffer-0. As FB1 is active and continues to DMA buffer-0(which is being
filled), leading to tearing/flickering issue.
...
The above steps also depicts that there is one frame delay for each
frame panned by application.
Patch fixes the issue by keeping track free DMA channel and configures
it in driver PAN callback so that panned frame from application gets
displayed in next frame period.
Signed-off-by: Nellutla, Aditya <aditya.n@ti.com>
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Below link to wiki describes the issue and it also has link to
application with which issue can be reproduced.
http://ap-fpdsp-swapps.dal.design.ti.com/index.php/DA8XX_LCDC_Linux_FB_FAQs
Issue is because of 2 active DMA channels ping ponging among them
along with usage of 2 DDR buffer ping pong and application is not
aware of active DMA channel.
Below steps describe issue:
1)Initially assume both buffers FB0 and FB1 are programmed for buffer-0.
2)On EOF0: Program FB0 for buffer-1, indicate(wake up) application
to fill up buffer-0. As FB1 is active and continues to DMA buffer-0
(which is being filled), leading to tearing/flickering issue.
3)On EOF1: Program FB1 for buffer-0, indicate(wake up) application to
fill up buffer-1. As FB0 is active and continues to DMA buffer-1(which
is being filled), leading to tearing/flickering issue.
4)On EOF0: Program FB0 for buffer-1, indicate(wake up) application to fill
up buffer-0. As FB1 is active and continues to DMA buffer-0(which is being
filled), leading to tearing/flickering issue.
...
The above steps also depicts that there is one frame delay for each
frame panned by application.
Patch fixes the issue by keeping track free DMA channel and configures
it in driver PAN callback so that panned frame from application gets
displayed in next frame period.
Signed-off-by: Nellutla, Aditya <aditya.n@ti.com>
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
drivers/video/da8xx-fb.c | patch | blob | history |
index d6792bd04b5c1eee0ad8f4c78016969b152f1d7a..c3432a8989dbeec57f2a5a63661a4fcd661d3fca 100644 (file)
--- a/drivers/video/da8xx-fb.c
+++ b/drivers/video/da8xx-fb.c
#include <linux/clk.h>
#include <linux/cpufreq.h>
#include <linux/console.h>
+#include <linux/spinlock.h>
#include <linux/slab.h>
#include <video/da8xx-fb.h>
#include <asm/mach-types.h>
wait_queue_head_t vsync_wait;
int vsync_flag;
int vsync_timeout;
+ spinlock_t lock_for_chan_update;
+
+ /*
+ * LCDC has 2 ping pong DMA channels, channel 0
+ * and channel 1.
+ */
+ unsigned int which_dma_channel_done;
#ifdef CONFIG_CPU_FREQ
struct notifier_block freq_transition;
#endif
lcdc_write(stat, LCD_MASKED_STAT_REG);
if (stat & LCD_END_OF_FRAME0) {
+ par->which_dma_channel_done = 0;
lcdc_write(par->dma_start,
LCD_DMA_FRM_BUF_BASE_ADDR_0_REG);
lcdc_write(par->dma_end,
}
if (stat & LCD_END_OF_FRAME1) {
+ par->which_dma_channel_done = 1;
lcdc_write(par->dma_start,
LCD_DMA_FRM_BUF_BASE_ADDR_1_REG);
lcdc_write(par->dma_end,
struct fb_fix_screeninfo *fix = &fbi->fix;
unsigned int end;
unsigned int start;
+ unsigned long irq_flags;
if (var->xoffset != fbi->var.xoffset ||
var->yoffset != fbi->var.yoffset) {
end = start + fbi->var.yres * fix->line_length - 1;
par->dma_start = start;
par->dma_end = end;
+ spin_lock_irqsave(&par->lock_for_chan_update,
+ irq_flags);
+ if (par->which_dma_channel_done == 0) {
+ lcdc_write(par->dma_start,
+ LCD_DMA_FRM_BUF_BASE_ADDR_0_REG);
+ lcdc_write(par->dma_end,
+ LCD_DMA_FRM_BUF_CEILING_ADDR_0_REG);
+ } else if (par->which_dma_channel_done == 1) {
+ lcdc_write(par->dma_start,
+ LCD_DMA_FRM_BUF_BASE_ADDR_1_REG);
+ lcdc_write(par->dma_end,
+ LCD_DMA_FRM_BUF_CEILING_ADDR_1_REG);
+ }
+ spin_unlock_irqrestore(&par->lock_for_chan_update,
+ irq_flags);
}
}
/* initialize the vsync wait queue */
init_waitqueue_head(&par->vsync_wait);
par->vsync_timeout = HZ / 5;
+ par->which_dma_channel_done = -1;
+ spin_lock_init(&par->lock_for_chan_update);
/* Register the Frame Buffer */
if (register_framebuffer(da8xx_fb_info) < 0) {