]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/commitdiff
OMAP4: hwmod: Introduce the module control in hwmod control
authorBenoit Cousson <b-cousson@ti.com>
Sun, 10 Jul 2011 11:56:33 +0000 (05:56 -0600)
committerPaul Walmsley <paul@pwsan.com>
Sun, 10 Jul 2011 11:56:33 +0000 (05:56 -0600)
Take advantage of the explicit modulemode control to fix
the way parents clocks are managed.
A module must be disabled before any parents are disabled.
That programming model was not possible with the previous
implementation that was considering a modulemode as a leaf
clock node managed by the clock fmwk.
This was leading to bad crash upon disable when the parent
clock was gated before the module completed its transition
to idle.

Signed-off-by: Benoit Cousson <b-cousson@ti.com>
Cc: Paul Walmsley <paul@pwsan.com>
Cc: Rajendra Nayak <rnayak@ti.com>
Signed-off-by: Paul Walmsley <paul@pwsan.com>
arch/arm/mach-omap2/omap_hwmod.c

index a0f7d313e69f9ba466accdaa21868e7b637a08d2..4424fee5cd5a071a6df0057113bed37db8a22ef8 100644 (file)
@@ -679,6 +679,56 @@ static void _disable_optional_clocks(struct omap_hwmod *oh)
                }
 }
 
+/**
+ * _enable_module - enable CLKCTRL modulemode on OMAP4
+ * @oh: struct omap_hwmod *
+ *
+ * Enables the PRCM module mode related to the hwmod @oh.
+ * No return value.
+ */
+static void _enable_module(struct omap_hwmod *oh)
+{
+       /* The module mode does not exist prior OMAP4 */
+       if (cpu_is_omap24xx() || cpu_is_omap34xx())
+               return;
+
+       if (!oh->clkdm || !oh->prcm.omap4.modulemode)
+               return;
+
+       pr_debug("omap_hwmod: %s: _enable_module: %d\n",
+                oh->name, oh->prcm.omap4.modulemode);
+
+       omap4_cminst_module_enable(oh->prcm.omap4.modulemode,
+                                  oh->clkdm->prcm_partition,
+                                  oh->clkdm->cm_inst,
+                                  oh->clkdm->clkdm_offs,
+                                  oh->prcm.omap4.clkctrl_offs);
+}
+
+/**
+ * _disable_module - enable CLKCTRL modulemode on OMAP4
+ * @oh: struct omap_hwmod *
+ *
+ * Disable the PRCM module mode related to the hwmod @oh.
+ * No return value.
+ */
+static void _disable_module(struct omap_hwmod *oh)
+{
+       /* The module mode does not exist prior OMAP4 */
+       if (cpu_is_omap24xx() || cpu_is_omap34xx())
+               return;
+
+       if (!oh->clkdm || !oh->prcm.omap4.modulemode)
+               return;
+
+       pr_debug("omap_hwmod: %s: _disable_module\n", oh->name);
+
+       omap4_cminst_module_disable(oh->clkdm->prcm_partition,
+                                   oh->clkdm->cm_inst,
+                                   oh->clkdm->clkdm_offs,
+                                   oh->prcm.omap4.clkctrl_offs);
+}
+
 /**
  * _count_mpu_irqs - count the number of MPU IRQ lines associated with @oh
  * @oh: struct omap_hwmod *oh
@@ -1424,6 +1474,7 @@ static int _enable(struct omap_hwmod *oh)
 
                return r;
        }
+       _enable_module(oh);
 
        oh->_state = _HWMOD_STATE_ENABLED;
 
@@ -1460,11 +1511,18 @@ static int _idle(struct omap_hwmod *oh)
        if (oh->class->sysc)
                _idle_sysc(oh);
        _del_initiator_dep(oh, mpu_oh);
-       _disable_clocks(oh);
+       _disable_module(oh);
        ret = _wait_target_disable(oh);
        if (ret)
                pr_warn("omap_hwmod: %s: _wait_target_disable failed\n",
                        oh->name);
+       /*
+        * The module must be in idle mode before disabling any parents
+        * clocks. Otherwise, the parent clock might be disabled before
+        * the module transition is done, and thus will prevent the
+        * transition to complete properly.
+        */
+       _disable_clocks(oh);
 
        /* Mux pins for device idle if populated */
        if (oh->mux && oh->mux->pads_dynamic)
@@ -1556,11 +1614,12 @@ static int _shutdown(struct omap_hwmod *oh)
        if (oh->_state == _HWMOD_STATE_ENABLED) {
                _del_initiator_dep(oh, mpu_oh);
                /* XXX what about the other system initiators here? dma, dsp */
-               _disable_clocks(oh);
+               _disable_module(oh);
                ret = _wait_target_disable(oh);
                if (ret)
                        pr_warn("omap_hwmod: %s: _wait_target_disable failed\n",
                                oh->name);
+               _disable_clocks(oh);
        }
        /* XXX Should this code also force-disable the optional clocks? */