]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-epos/sitara-epos-kernel.git/history - drivers
video: da8xx-fb: Interrupt configuration of revised LCDC IP
[sitara-epos/sitara-epos-kernel.git] / drivers /
2011-07-13 Manjunathappa, Prakashvideo: da8xx-fb: Interrupt configuration of revised...
2011-07-13 Kristoffer Glembovideo: Add Aeroflex Gaisler GRVGA framebuffer device...
2011-06-24 Jesper JuhlRemove unneeded version.h includes from drivers/video/
2011-06-24 Paul MundtMerge branch 'fbdev/stable-updates'
2011-06-24 Joe Perchesvideo: Fix speficied typo
2011-06-24 Loïc Minierfbdev: amba: Link fb device to its parent
2011-06-24 Timur Tabifsl-diu-fb: remove check for pixel clock ranges
2011-06-24 William Katsakudlfb: Correct sub-optimal resolution selection.
2011-06-24 Paul MundtMerge branch 'common/fbdev-meram' of git://git.kernel...
2011-06-24 Pavel Shvedhecubafb: add module_put on error path in hecubafb_probe()
2011-06-24 Randy Dunlapsm501fb: fix section mismatch warning
2011-06-24 Randy Dunlapgx1fb: Fix section mismatch warnings
2011-06-24 Damian Hobson-Garciafbdev: sh_mobile_meram: Correct pointer check for YCbCr...
2011-06-23 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-23 Linus TorvaldsMerge branch 'pm-fixes' of git://git.kernel.org/pub...
2011-06-22 Linus TorvaldsMerge branch 'bugfixes' of git://git.linux-nfs.org...
2011-06-21 Rafael J. WysockiPCI / PM: Block races between runtime PM and system...
2011-06-21 Rafael J. WysockiPM / Runtime: Handle clocks correctly if CONFIG_PM_RUNT...
2011-06-21 Alan SternPM: Fix async resume following suspend failure
2011-06-21 Alan SternPM: Rename dev_pm_info.in_suspend to is_prepared
2011-06-21 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-21 Linus TorvaldsMerge branch 'for_linus' of git://git.kernel.org/pub...
2011-06-21 Linus TorvaldsMerge branch 'drm-fixes' of git://git.kernel.org/pub...
2011-06-21 Linus TorvaldsMerge branch 'msm-fix' of git://codeaurora.org/quic...
2011-06-21 Linus TorvaldsMerge branch 'for-2.6.40' of git://linux-nfs.org/~bfiel...
2011-06-21 Linus TorvaldsMerge git://git.kernel.org/pub/scm/linux/kernel/git...
2011-06-21 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-20 Alex Deucherdrm/radeon/kms/r6xx+: voltage fixes
2011-06-20 Richard Cochranpxa168_eth: fix race in transmit path.
2011-06-20 Eric Dumazetnetxen: fix race in skb->len access
2011-06-20 Linus TorvaldsMerge branch 'stable/bug.fixes' of git://git.kernel...
2011-06-20 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-20 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-20 Dave Airliedrm/nouveau: drop leftover debugging
2011-06-20 Dave AirlieMerge branch 'drm-nouveau-fixes' of git://anongit.freed...
2011-06-20 Dave Airliedrm/radeon: avoid warnings from r600/eg irq handlers...
2011-06-19 Alex Deucherdrm/radeon/kms: add missing param for dce3.2 DP transmi...
2011-06-19 Alex Deucherdrm/radeon/kms/atom: fix duallink on some early DCE3...
2011-06-19 Eric Dumazetsgi-xp: fix a use after free
2011-06-19 Eric Dumazethp100: fix an skb->len race
2011-06-19 David S. MillerMerge branch 'davem.r8169' of git://git.kernel.org...
2011-06-19 WANG Congnetpoll: copy dev name of slaves to struct netpoll
2011-06-19 Linus TorvaldsMerge branches 'perf-urgent-for-linus', 'sched-urgent...
2011-06-19 Linus TorvaldsMerge branch 'core-urgent-for-linus' of git://git.kerne...
2011-06-19 Linus TorvaldsMerge branch 'hwmon-for-linus' of git://git.kernel...
2011-06-18 Magnus DammInput: sh_keysc - 8x8 MODE_6 fix
2011-06-18 Janusz KrzysztofikInput: omap-keypad - add missing input_sync()
2011-06-18 Dmitry TorokhovInput: evdev - try to wake up readers only if we have...
2011-06-18 Guenter Roeckhwmon: (s3c) Initialize sysfs attributes
2011-06-18 Guenter Roeckhwmon: (ibmpex) Initialize sysfs attributes
2011-06-18 Guenter Roeckhwmon: (ibmaem) Initialize sysfs attributes
2011-06-18 Guenter Roeckhwmon: (asus_atk0110) Consolidate sysfs attribute initi...
2011-06-18 Jean Delvarehwmon: (coretemp) Drop unused struct members
2011-06-18 Ben Skeggsdrm/nouveau: fix assumption that semaphore dmaobj is...
2011-06-18 Ben Skeggsdrm/nv50/disp: fix gamma with page flipping overlay...
2011-06-18 Emil Velikovdrm/nouveau/pm: Prevent overflow in nouveau_perf_init()
2011-06-18 Ben Skeggsdrm/nouveau: fix big-endian switch
2011-06-18 Linus TorvaldsMerge branch 'drm-fixes' of git://git.kernel.org/pub...
2011-06-18 Linus TorvaldsMerge branch 'fixes' of git://git.kernel.org/pub/scm...
2011-06-18 Linus TorvaldsMerge branch 'anon_vma-locking'
2011-06-17 Daniel J Bluemandrm/i915: Fix gen6 (SNB) missed BLT ring interrupts.
2011-06-17 Francois Romieur8169: fix static initializers.
2011-06-17 Pavel Shvedgigaset: call module_put before restart of if_open()
2011-06-17 Pavel Shvedfarsync: add module_put to error path in fst_open()
2011-06-17 Clive Stubbingsfs_enet: fix freescale FCC ethernet dp buffer alignment
2011-06-17 Roland DreierMerge branches 'cxgb4' and 'qib' into for-next
2011-06-17 Mitko HaralanovIB/qib: Ensure that LOS and DFE are being turned off
2011-06-17 Steve WiseRDMA/cxgb4: Couple of abort fixes
2011-06-17 Steve WiseRDMA/cxgb4: Don't truncate MR lengths
2011-06-17 Steve WiseRDMA/cxgb4: Don't exceed hw IQ depth limit for user CQs
2011-06-17 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-17 Linus TorvaldsMerge branch 'for-linus' of git://oss.sgi.com/xfs/xfs
2011-06-17 Linus TorvaldsMerge branch 'for-linus' of git://git.kernel.org/pub...
2011-06-17 Linus TorvaldsMerge branches 'gpio/merge' and 'spi/merge' of git...
2011-06-17 Linus TorvaldsMerge branch 'fixes' of git://git.kernel.org/pub/scm...
2011-06-17 John W. LinvilleMerge branch 'master' of git://git.kernel.org/pub/scm...
2011-06-17 Mike Frysingerspi/bfin_spi: fix handling of default bits per word...
2011-06-17 Sonic Zhangnetdev: bfin_mac: fix memory leak when freeing dma...
2011-06-17 Neil Hormantun: teach the tun/tap driver to support netpoll
2011-06-17 Richard Cochrandp83640: drop PHY status frames in the driver.
2011-06-17 Richard Cochrandp83640: fix phy status frame event parsing
2011-06-17 Ralf Baechlephylib: Allow BCM63XX PHY to be selected only on BCM63XX.
2011-06-17 Changli Gaoppp: use PPP_TRANS instead of the magic number 0x20
2011-06-17 Marius B. Kotsbaknet/usb: Add Samsung Kalmia driver for Samsung GT-B3730
2011-06-17 David S. MillerMerge branch 'master' of git://git.kernel.org/pub/scm...
2011-06-17 Linus TorvaldsMerge branch 'drm-fixes' of git://git.kernel.org/pub...
2011-06-16 Alex Deucherdrm/radeon/kms: use helper functions for fence read...
2011-06-16 Alex Deucherdrm/radeon/kms: set DP link config properly for DP...
2011-06-16 Alex Deucherdrm/radeon/kms/atom: AdjustPixelClock fixes for DP...
2011-06-16 Alex Deucherdrm/radeon/kms: fix handling of DP to LVDS bridges
2011-06-16 Alex Deucherdrm/radeon/kms: issue blank/unblank commands for ext...
2011-06-16 Alex Deucherdrm/radeon/kms: fix support for DDC on dp bridges
2011-06-16 Alex Deucherdrm/radeon/kms: add support for load detection on dp...
2011-06-16 Alex Deucherdrm/radeon/kms: add missing external encoder action
2011-06-16 Alex Deucherdrm/radeon/kms: rework atombios_get_encoder_mode()
2011-06-16 Alex Deucherdrm/radeon/kms: fix num crtcs for Cedar and Caicos
2011-06-16 Jean DelvareRevert "drm/i915: Enable GMBUS for post-gen2 chipsets"
2011-06-16 Linus TorvaldsMerge git://git.kernel.org/pub/scm/linux/kernel/git...
2011-06-16 Konrad Rzeszutek... [CPUFREQ] powernow-k8: Don't try to transition if the...
2011-06-16 Konrad Rzeszutek... [CPUFREQ] powernow-k8: Don't notify of successful trans...
next