musb: adding support for am335x
am335x has two musb interface and uses cppi4.1 dma engine. It's
almost same as ti81xx and so using ti81xx files for am335x.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
am335x has two musb interface and uses cppi4.1 dma engine. It's
almost same as ti81xx and so using ti81xx files for am335x.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
am335x: add musb support
Adding musb support in am335evm board file. Configured for:
- Two instance of musb
- 500mA of power
Also added the pinmux needed for drvvbus pins of each usb interface.
Others usb pins are not multiplexed so no need to setup them.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Adding musb support in am335evm board file. Configured for:
- Two instance of musb
- 500mA of power
Also added the pinmux needed for drvvbus pins of each usb interface.
Others usb pins are not multiplexed so no need to setup them.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: misc fixes for v3.1.0
Changes
- v3.1-rc3 has replaced all DBG to dev_dbg.
- CONFIG_MUSB_DEBUG related cleanups
- drivers always in OTG mode so drop all GADGET or HOST ifdefs
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Changes
- v3.1-rc3 has replaced all DBG to dev_dbg.
- CONFIG_MUSB_DEBUG related cleanups
- drivers always in OTG mode so drop all GADGET or HOST ifdefs
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: gadget: don't allow suspend when connected to host
While the target is connected to host and user has initiated suspend
then we should not allow system suspend as target is acting as slave
in gadget mode and can't suspend the bus without host initiation.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
While the target is connected to host and user has initiated suspend
then we should not allow system suspend as target is acting as slave
in gadget mode and can't suspend the bus without host initiation.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:ti81xx: removed warning while using toolchain arago-gcc-4.5.3
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:cppi41: fix for early tx-dma completion
The tx-dma completion occurs early, while endpoint fifo
is nonempty and transmit is still in progress.
The patch workaround this issue by polling for tx endpoint
fifo in worker thread till last byte from fifo is
transmitted out.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
The tx-dma completion occurs early, while endpoint fifo
is nonempty and transmit is still in progress.
The patch workaround this issue by polling for tx endpoint
fifo in worker thread till last byte from fifo is
transmitted out.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb_host: cppi41 dma fixes for cdc-class
Fixes the cppi41 dma issue while configuring rx dma.
Fixes the bug in rx short pkt completion in
musb-host-rx.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fixes the cppi41 dma issue while configuring rx dma.
Fixes the bug in rx short pkt completion in
musb-host-rx.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:cppi41: Added rx-dma infinite mode for fsg gadget mode
In infinite dma mode the DMA ignores the SOP bit and closes up
a packet after a max_buf_cnt buffer has been filled OR if
the EOP field is set in the info word 0
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
In infinite dma mode the DMA ignores the SOP bit and closes up
a packet after a max_buf_cnt buffer has been filled OR if
the EOP field is set in the info word 0
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:cppi41: The epsize register must be multiple of 64
In generic rnids mode the epsize register must be
receive length multiple of 64 bytes.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
In generic rnids mode the epsize register must be
receive length multiple of 64 bytes.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:cppi41: use GRNDIS mode for rx-dma except file-storage gadget
The cppi41 rx-dma in gadget mode is configured for transparent mode
only for file-storage-gadget driver and GRNDIS mode is used for
other gadget driver.
Also fixes the interrupt out transfer for 1024 bytes in gadget mode,
since the transparent mode does not work for interrupt transfer of
1024 size.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
The cppi41 rx-dma in gadget mode is configured for transparent mode
only for file-storage-gadget driver and GRNDIS mode is used for
other gadget driver.
Also fixes the interrupt out transfer for 1024 bytes in gadget mode,
since the transparent mode does not work for interrupt transfer of
1024 size.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: pm workaround fix in host mode when no device connected to ports
In host mode, the musb does not go to suspend state when no
device connected to port0/port1, only in the otg mode the try
idle function tries to turn off the session when no device is
connected to port.
This patch workaround this issue by clear/set the session bit
when system wide suspend/resume is invoked.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
In host mode, the musb does not go to suspend state when no
device connected to port0/port1, only in the otg mode the try
idle function tries to turn off the session when no device is
connected to port.
This patch workaround this issue by clear/set the session bit
when system wide suspend/resume is invoked.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
ti816x:usb: Added usb hwmod and platform support for ti816x usb
1.Added the hwmod usb support
2.Added the platform driver changes for hwmod
3.The musb_probe function should check for named resource for
dual instance of musb.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
1.Added the hwmod usb support
2.Added the platform driver changes for hwmod
3.The musb_probe function should check for named resource for
dual instance of musb.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Added babble workaround enable/disable control
Added enable/disable babble workaround through procfs entry
to eanble babble workaround
echo 'K' > /proc/driver/musb_hdrc.0 or 1
to disable babble workaround
echo 'k' > /proc/driver/musb_hdrc.0 or 1
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Added enable/disable babble workaround through procfs entry
to eanble babble workaround
echo 'K' > /proc/driver/musb_hdrc.0 or 1
to disable babble workaround
echo 'k' > /proc/driver/musb_hdrc.0 or 1
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: driving usbid pin control through sofware
By default usbid pin is controlled from external through
mini-A or mini-B plug. This patch adds the configuration
of usbid pin through software to force usbid to ground or
open.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
By default usbid pin is controlled from external through
mini-A or mini-B plug. This patch adds the configuration
of usbid pin through software to force usbid to ground or
open.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:ti81x: cppi41dma modular fixes for musb gadget mode
This patch fixes the insmod/rmmod fixes for musb
gadget mode and cppi41dma cleanup.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch fixes the insmod/rmmod fixes for musb
gadget mode and cppi41dma cleanup.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Fix for the test mode feature of musb controller
This patch fixes the generation of test packet when
musb controller enters into test mode.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch fixes the generation of test packet when
musb controller enters into test mode.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: dynamic fifo-mode selection for host/device for ti81xx platform
1. Added mode_6_cfg musb fifo table with double buffer
enabled for musb fifo in gadget mode
2. dynamic fifo mode selection thru platform device
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
1. Added mode_6_cfg musb fifo table with double buffer
enabled for musb fifo in gadget mode
2. dynamic fifo mode selection thru platform device
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb:musb: Fixes for code review of musb for ti81xx platform
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Fix for dma race condition during i/o completion
This patch fixes the cppi41 dma race condition, where software
reads buffer descriptor before being updated by dma as rx/tx
buffer descriptor(BD) writes by dma still pending in
interconnect bridge when traffic on interconnect is high.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch fixes the cppi41 dma race condition, where software
reads buffer descriptor before being updated by dma as rx/tx
buffer descriptor(BD) writes by dma still pending in
interconnect bridge when traffic on interconnect is high.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Workaround for early rx cppi41 dma completion in GRNDIS mode
Fix for device resets during file transfer from one usb stick to other.
Multiple Resets of msc device while transfering file one usb
stick to other. Root caused at CPPI-41 DMA Level. During transfer
of file from one msc-device1 to msc-device2, there is continuous
scsi-read from device-1 and scsi-write to device-2.
After few Mega Bytes of data are transfered, the scsi-read operation
stops and timeout is occuring at scsi layer hence the scsi-subsystem
resets the device-1.
The CATC capture shows that after sending CBW command to read 240
sectors of data, IN tokens are send by controller to receive few
Kilo bytes, further there were no IN-tokens send by controller to
read the data from device-1.
The analysis shows the corresponding rx endpoint-FIFO is full and
XDMA is not moving the data due CPPI-4.1 Rx DMA channel halted.
What exactly happened was, the scsi submitted request to read 28K data,
one rx-bd is queued to rx-free queue of RX-DMA channel configured in
Generic-RNDIS mode and RNDIS-EPSIZE register is set to 28K value.
For some reason the interrupt has occured with 16K data in rx-bd and
the usb driver gives back this request to application layer.
Since this request is abnormally aborted by DMA, there are no free bd
at input queue and transfer DMA has send IN token to receive further data,
the data received is available in FIFO, FIFO is full and there is no rx-bd
the DMA Stalls. This is reason why there are no IN-token seen on the bus
and the request aborted and continuous resets to device is happening
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fix for device resets during file transfer from one usb stick to other.
Multiple Resets of msc device while transfering file one usb
stick to other. Root caused at CPPI-41 DMA Level. During transfer
of file from one msc-device1 to msc-device2, there is continuous
scsi-read from device-1 and scsi-write to device-2.
After few Mega Bytes of data are transfered, the scsi-read operation
stops and timeout is occuring at scsi layer hence the scsi-subsystem
resets the device-1.
The CATC capture shows that after sending CBW command to read 240
sectors of data, IN tokens are send by controller to receive few
Kilo bytes, further there were no IN-tokens send by controller to
read the data from device-1.
The analysis shows the corresponding rx endpoint-FIFO is full and
XDMA is not moving the data due CPPI-4.1 Rx DMA channel halted.
What exactly happened was, the scsi submitted request to read 28K data,
one rx-bd is queued to rx-free queue of RX-DMA channel configured in
Generic-RNDIS mode and RNDIS-EPSIZE register is set to 28K value.
For some reason the interrupt has occured with 16K data in rx-bd and
the usb driver gives back this request to application layer.
Since this request is abnormally aborted by DMA, there are no free bd
at input queue and transfer DMA has send IN token to receive further data,
the data received is available in FIFO, FIFO is full and there is no rx-bd
the DMA Stalls. This is reason why there are no IN-token seen on the bus
and the request aborted and continuous resets to device is happening
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb:cppi41: Fix for modular support issue for TI81XX (DMA mode)
Cleanup of cppi41dma and added un-init routine for
queue manager and dma blocks.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Cleanup of cppi41dma and added un-init routine for
queue manager and dma blocks.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb-musb: Fix for modular support issue for TI81XX (PIO Mode)
This patch fixes the modular support issue for dual
musb instances in ti81xx (for pio mode).
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch fixes the modular support issue for dual
musb instances in ti81xx (for pio mode).
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb-musb: Enabling fifo double buffering for gadget mode
1. Enable the endpoint fifo double buffering for gadget
mode to increase the performance
2. Increase the number of cppidma bd to 128
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
1. Enable the endpoint fifo double buffering for gadget
mode to increase the performance
2. Increase the number of cppidma bd to 128
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Fixes for cppi41 rmmod issue
The cppi41 dma is common module for multi musb instances,
the cppi41 deinitialization will be done as part of
platform exit.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
The cppi41 dma is common module for multi musb instances,
the cppi41 deinitialization will be done as part of
platform exit.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: workaround patch for babble condition
1) During the babble condition occured in host mode
the musb controller removes the session bit and drives
drvvbus to low and musb controller stops working.
2) This patch workaround this issue by restarting the musb
controller by performing usbotgss controller reset, restart
usb phy, enable all interrupts and then starts the musb
session.
3) Since musb controller shutdown during babble, the
disconnect event generated through software to notify
the associated class driver of connected that
musb is not operational.
3) The procfs entry is added to simulate the babble
condition interrupt through software
usage: echo 'b' > /proc/driver/musb_hdrc.0 or 1
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
1) During the babble condition occured in host mode
the musb controller removes the session bit and drives
drvvbus to low and musb controller stops working.
2) This patch workaround this issue by restarting the musb
controller by performing usbotgss controller reset, restart
usb phy, enable all interrupts and then starts the musb
session.
3) Since musb controller shutdown during babble, the
disconnect event generated through software to notify
the associated class driver of connected that
musb is not operational.
3) The procfs entry is added to simulate the babble
condition interrupt through software
usage: echo 'b' > /proc/driver/musb_hdrc.0 or 1
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: CPPI4.1 Tx/Rx DMA Teardown Fixes
This patch fixes the teardown fixes for tx/rx dma channels.
During tx/rx dma channel teardown, the completion BDs from
the tx/rx completion queues must need to removed and recycled
to the BD free pool.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch fixes the teardown fixes for tx/rx dma channels.
During tx/rx dma channel teardown, the completion BDs from
the tx/rx completion queues must need to removed and recycled
to the BD free pool.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Fix multiple define of AUTOREQ and TD reg offset
Fixes multiple definitions of AUTOREQ and TEARDOWN register offset
by adding similar field inside 'struct cppi41'. This is needed as
different platforms has different offsets.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fixes multiple definitions of AUTOREQ and TEARDOWN register offset
by adding similar field inside 'struct cppi41'. This is needed as
different platforms has different offsets.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Adding BD interrupt enable feature
Adding BD interrupt enable feature available in CPPI41 DMA on TI81xx
platform. This feature is not supported in AM35x/DA8x.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Adding BD interrupt enable feature available in CPPI41 DMA on TI81xx
platform. This feature is not supported in AM35x/DA8x.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: teardown descriptor cleanup
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Drop const for rx/tx_comp_q
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Adding support for TI81XX platform
TI81x platform has two musb controller and has CPPI4.1 DMA engine.
Changes:
- Changes done for Kconfig/Makefile for ti81xx usb support
- Adds the ti81xx.c musb platform file
- Multi-musb controller support at usb-musb.c
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
TI81x platform has two musb controller and has CPPI4.1 DMA engine.
Changes:
- Changes done for Kconfig/Makefile for ti81xx usb support
- Adds the ti81xx.c musb platform file
- Multi-musb controller support at usb-musb.c
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: fixes for DBG -> dev_dbg
v3.0 has changed DBG to dev_dbg.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
v3.0 has changed DBG to dev_dbg.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Update usb_cppi41_info to support multi-ctrl
Changed usb_cppi41_info to an array of two such element to support
multi-controller scenarios.
Also updated the required changed in am35x.c
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Changed usb_cppi41_info to an array of two such element to support
multi-controller scenarios.
Also updated the required changed in am35x.c
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Make cppi41_info as a part of struct cppi41
Added cppi41_info in 'struct cppi41' so that each cppi41 instance
can provide their data and thus supporting multi controller.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Added cppi41_info in 'struct cppi41' so that each cppi41 instance
can provide their data and thus supporting multi controller.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: General cleanup
Changes:
- Removed the hard coded constants for size by adding 'size'
field into cppi41 strcuture
- Added q_num and q_mgr as required to support multi-controller
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Changes:
- Removed the hard coded constants for size by adding 'size'
field into cppi41 strcuture
- Added q_num and q_mgr as required to support multi-controller
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: nop: support for multi-nop tranceiver
Modified the nop driver to support multi nop transceiver.
Changes:
- Global xceiv to xceiv[2]
- nop transceiver regiser/deregiser based on musb->id
- Changes to other glue layers
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Modified the nop driver to support multi nop transceiver.
Changes:
- Global xceiv to xceiv[2]
- nop transceiver regiser/deregiser based on musb->id
- Changes to other glue layers
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Changes required in procfs for multi-musb controller
Updated procfs part of code to support multi-musb procfs entries
based on musb->id field.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Updated procfs part of code to support multi-musb procfs entries
based on musb->id field.
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Adding musb->id to support multi-musb controller
Added musb->id field to differenciate two controllers.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Added musb->id field to differenciate two controllers.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: gadget: Read ep0 fifo only if rxcount is non zero
Fixes the read_fifo call with '0' rxcount.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fixes the read_fifo call with '0' rxcount.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: modular fix
Changes:
- Moved global defines to cppi41.c/cppi41_dma.c
- Platform files to fill those global defines.
- Added EXPORT_SYMBOL
- REVISIT: am35x: _put commented
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Changes:
- Moved global defines to cppi41.c/cppi41_dma.c
- Platform files to fill those global defines.
- Added EXPORT_SYMBOL
- REVISIT: am35x: _put commented
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
AM3517: musb: undo pm changes affecting musb
musb becomes unusable due to below pm patch in AM3517.
------------------------------------------------
commit 53f18cf6026bc6a0152ea445f6b54de7fbea1b3c
Author: Tero Kristo <tero.kristo@nokia.com>
OMAP3: PM: Enable system control module autoidle
------------------------------------------------
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb becomes unusable due to below pm patch in AM3517.
------------------------------------------------
commit 53f18cf6026bc6a0152ea445f6b54de7fbea1b3c
Author: Tero Kristo <tero.kristo@nokia.com>
OMAP3: PM: Enable system control module autoidle
------------------------------------------------
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: teardown fix from Ravi
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: device fix from Ravi
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix IO_ADDRESS related issue on AM35x
IO_ADDRESS for AM35x MUSB doesn't work and thus CPPI41 programming
also fails.
Fixing this by ioremapping MUSB complete address space (~32K) and
updating CPPI41 related memory base with this mappings.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
IO_ADDRESS for AM35x MUSB doesn't work and thus CPPI41 programming
also fails.
Fixing this by ioremapping MUSB complete address space (~32K) and
updating CPPI41 related memory base with this mappings.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: AM35x: Add CPPI4.1 DMA support
Adding CPPI4.1 DMA support for musb driver.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Adding CPPI4.1 DMA support for musb driver.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: change number of DMA BLOCK from 4 to 1
Number of DMA block is different for different platforms.
Changing this to '1' for AM3517 platform.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Number of DMA block is different for different platforms.
Changing this to '1' for AM3517 platform.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
AM3517: musb: fix iperf failure issue
As we get DMA completion interrupt even when data is in FIFO.
Fixing the issue by adding delay before calling dma completion.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
As we get DMA completion interrupt even when data is in FIFO.
Fixing the issue by adding delay before calling dma completion.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi: ISO IN fixes for CPPI DMA
ISO doesn't work without this patch as CPPI DMA is not even
programmed for ISO IN transfer.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
ISO doesn't work without this patch as CPPI DMA is not even
programmed for ISO IN transfer.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix MODE_REG compatibility among platforms
AM3517 has seperate Tx and Rx MODE registers whereas OMAPL137/DA8x
has only one registers for both Rx and Tx modes.
Solving this difference by adding TX_MODE and RX_MODE registers
seperately which are actually same in case of OMAPL137/DA8x but
different for AM3517.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
AM3517 has seperate Tx and Rx MODE registers whereas OMAPL137/DA8x
has only one registers for both Rx and Tx modes.
Solving this difference by adding TX_MODE and RX_MODE registers
seperately which are actually same in case of OMAPL137/DA8x but
different for AM3517.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: procfs: add cppi41 related checks
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: Remove platform definitions from cppi41_dma.h
cppi41_dma.h should have common definitions as it would be used
by multiple platforms. As different platform can have different
register layouts so it's better to remove these definitions and
let them come from platform file at plat/usb.h
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41_dma.h should have common definitions as it would be used
by multiple platforms. As different platform can have different
register layouts so it's better to remove these definitions and
let them come from platform file at plat/usb.h
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix channel program for actual len
actual length has to be zero at the start of new dma programming.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
actual length has to be zero at the start of new dma programming.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix macro definition in cppi41.h
Macros definitions for number of queue managers and DMA blocks are
defined in cppi41.h only so use them instead of defining in other
files and using unnecessary extern.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Macros definitions for number of queue managers and DMA blocks are
defined in cppi41.h only so use them instead of defining in other
files and using unnecessary extern.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix scheduler table init in dma_block_init()
scheduler table init programming is unreliable using for loops so
fixing this by using scheduler table entries.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
scheduler table init programming is unreliable using for loops so
fixing this by using scheduler table entries.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: fix RGN0 memory alloc in queue_mgr_init()
queue_mgr_init() is currently allocating memory only for RGN1 and
expecting RGN0 memory to be allocated in platform files.
Normally RGN0 is only used so updating queue_mgr_init() to allocate
RGN0 memory.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
queue_mgr_init() is currently allocating memory only for RGN1 and
expecting RGN0 memory to be allocated in platform files.
Normally RGN0 is only used so updating queue_mgr_init() to allocate
RGN0 memory.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: add cppi41_exit() to free up the memories
Adding cppi41_exit() to free up the allocated memories.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Adding cppi41_exit() to free up the allocated memories.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: fixes to support new musb arch
Changes:
- __init to __devinit
- rename create/destroy functions
- channels maxlen
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Changes:
- __init to __devinit
- rename create/destroy functions
- channels maxlen
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
cppi41: Move CPPI41 core to musb temporarily
This is to ease our development effort and collaboration on Davinci
and OMAP35x family musb drivers.
This would be reverted back once the cppi41 drivers are accepted in
mainline and all confusion are cleared out.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This is to ease our development effort and collaboration on Davinci
and OMAP35x family musb drivers.
This would be reverted back once the cppi41 drivers are accepted in
mainline and all confusion are cleared out.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: cppi41: adding musb CPPI41 DMA support
Texas Instruments CPPI 4.1 DMA support for the MUSBMHRDC driver.
The code makes use of the accelerated "generic RNDIS" DMA mode, falling back to
the transparent (packet per transfer) mode if the hardware restrictions prevent
it from using the accelerated mode.
Update:
- has update for is_cppi41_enabled() due to musb changes
Signed-off-by: Sergei Shtylyov <sshtylyov@ru.mvista.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Texas Instruments CPPI 4.1 DMA support for the MUSBMHRDC driver.
The code makes use of the accelerated "generic RNDIS" DMA mode, falling back to
the transparent (packet per transfer) mode if the hardware restrictions prevent
it from using the accelerated mode.
Update:
- has update for is_cppi41_enabled() due to musb changes
Signed-off-by: Sergei Shtylyov <sshtylyov@ru.mvista.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
cppi41: adding CPPI4.1 DMA support
Add support for Texas Instuments Communication Port Programming Interface 4.1
(CPPI 4.1) used on OMAP-L137/DA830.
At this moment, only the DMA controller and queue manager are supported.
Support for the buffer manager is lacking but this chip doesn't have it anyway.
Signed-off-by: Sergei Shtylyov <sshtylyov@ru.mvista.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Add support for Texas Instuments Communication Port Programming Interface 4.1
(CPPI 4.1) used on OMAP-L137/DA830.
At this moment, only the DMA controller and queue manager are supported.
Support for the buffer manager is lacking but this chip doesn't have it anyway.
Signed-off-by: Sergei Shtylyov <sshtylyov@ru.mvista.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: pm: disbale autosuspend in default mode
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
USB: musb: NAK timeout scheme on bulk TX endpoint
Fixes endpoint starvation issue when more than one bulk QH is
multiplexed on the reserved bulk TX endpoint.
This patch sets the NAK timeout interval for such QHs, and when
a timeout triggers the next QH will be scheduled.
This scheme doesn't work for devices which are connected to a
high to full speed tree (transaction translator) as there is
no NAK timeout interrupt from the musb controller from such
devices.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fixes endpoint starvation issue when more than one bulk QH is
multiplexed on the reserved bulk TX endpoint.
This patch sets the NAK timeout interval for such QHs, and when
a timeout triggers the next QH will be scheduled.
This scheme doesn't work for devices which are connected to a
high to full speed tree (transaction translator) as there is
no NAK timeout interrupt from the musb controller from such
devices.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Add workqueue for URB giveback
Current musb host driver does the giveback of completed urb first and
then start the next request. This is significantly affecting the streaming
from an USB camera wherein we observe huge delay between the two IN tokens
from musb host. This is due to the fact that UVC driver is doing decoding
and further processing in giveback context.
The patch tries to defer the giveback part to a workqueue and continues
with the start of new request in completion path.
the giveback workqueue has only succesfull completed URBs, it is safe to
giveback URBs without taking musb spinlocks.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Current musb host driver does the giveback of completed urb first and
then start the next request. This is significantly affecting the streaming
from an USB camera wherein we observe huge delay between the two IN tokens
from musb host. This is due to the fact that UVC driver is doing decoding
and further processing in giveback context.
The patch tries to defer the giveback part to a workqueue and continues
with the start of new request in completion path.
the giveback workqueue has only succesfull completed URBs, it is safe to
giveback URBs without taking musb spinlocks.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: select fifo_mode at runtime
OMAP35x han an errata restricting active endpoints to use either
first 8K or next 8K of FIFO space while this issue has been
fixed in OMAP3630.
This issue requires the OMAP35x platform to use fifo_mode=5 but
OMAP3630 and AM35x can use fifo_mode=4 which utilises entire 16K
of FIFO.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
OMAP35x han an errata restricting active endpoints to use either
first 8K or next 8K of FIFO space while this issue has been
fixed in OMAP3630.
This issue requires the OMAP35x platform to use fifo_mode=5 but
OMAP3630 and AM35x can use fifo_mode=4 which utilises entire 16K
of FIFO.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Fixes for DTM tests.
Fixes all the DTM tests except mini6sendrecv tests.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Fixes all the DTM tests except mini6sendrecv tests.
Signed-off-by: Ravi B <ravibabu@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: kill unwanted messages
Remives below messages:
musb_bus_suspend 2285: trying to suspend as a_wait_bcon while active
....
....
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Remives below messages:
musb_bus_suspend 2285: trying to suspend as a_wait_bcon while active
....
....
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Add back old musb procfs file
Procfs file is removed from musb and an equivalent debugfs is
expected to replace it.
Adding the old file back to retain the debug functionalities untill
we get debugfs equivalent in mainline.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Procfs file is removed from musb and an equivalent debugfs is
expected to replace it.
Adding the old file back to retain the debug functionalities untill
we get debugfs equivalent in mainline.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: Inform user when gadget cable is disconnected
Currently we don't see any message to inform user that gadget cable is
successfully disconnected leading to suspicion if everything is fine at
driver therefore adding an informative print message in gadget
disconnect path.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Currently we don't see any message to inform user that gadget cable is
successfully disconnected leading to suspicion if everything is fine at
driver therefore adding an informative print message in gadget
disconnect path.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
musb: disable PING on status phase of control transfer
PING token is not mandatory in status phase of control transfer
so some high speed USB sticks doesn't support this.If such devices
are connected to MUSB then they would not respond to PING token
causing delayed or failed enumeration.
Fixing this issue by disabling PING token in status phase of control
transfers.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
PING token is not mandatory in status phase of control transfer
so some high speed USB sticks doesn't support this.If such devices
are connected to MUSB then they would not respond to PING token
causing delayed or failed enumeration.
Fixing this issue by disabling PING token in status phase of control
transfers.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Revert: "musb: otg timer cleanup"
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Revert "musb: make initial HNP roleswitch work (v2)"
This reverts commit 1de00dae8036dfee44ebea2c38f942fb6072e0b7.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This reverts commit 1de00dae8036dfee44ebea2c38f942fb6072e0b7.
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Revert: "musb: support disconnect after HNP roleswitch"
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: implement runtime is_inventra_dma/is_cppi_enabled/tusb_dma_omap
Now we can implement the three helpers below in runtime method:
is_inventra_dma/is_cppi_enabled/tusb_dma_omap
so we can build all hw glue drivers, dma drivers and musb_hdrc into
one single binary image to support musb on mulitple machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Now we can implement the three helpers below in runtime method:
is_inventra_dma/is_cppi_enabled/tusb_dma_omap
so we can build all hw glue drivers, dma drivers and musb_hdrc into
one single binary image to support musb on mulitple machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: pass musb pointer to is_cppi_enabled helper
This patch passes musb pointer to is_cppi_enabled to
prepare for support of runtime is_cppi_enabled.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch passes musb pointer to is_cppi_enabled to
prepare for support of runtime is_cppi_enabled.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: pass musb pointer to tusb_dma_omap helper
This patch passes musb pointer to tusb_dma_omap to
prepare for support of runtime tusb_dma_omap.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch passes musb pointer to tusb_dma_omap to
prepare for support of runtime tusb_dma_omap.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: pass musb pointer to is_inventra_dma helper
This patch passes musb pointer to is_inventra_dma to
prepare for support runtime is_inventra_dma.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch passes musb pointer to is_inventra_dma to
prepare for support runtime is_inventra_dma.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove CONFIG_USB_*_DMA in source code of musb core driver
This patch uses the three helpers below:
is_inventra_dma/is_cppi_enabled/tusb_dma_omap
to replace the options of CONFIG_USB_*_DMA.
The method was applied in musb_host.c before(using
is_cppi_enabled & tusb_dma_omap to replace using
'ifdef CONFIG_USB_*_DMA', and don't introduce any
performance loss since compiler is smart enough to
handle this cases.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch uses the three helpers below:
is_inventra_dma/is_cppi_enabled/tusb_dma_omap
to replace the options of CONFIG_USB_*_DMA.
The method was applied in musb_host.c before(using
is_cppi_enabled & tusb_dma_omap to replace using
'ifdef CONFIG_USB_*_DMA', and don't introduce any
performance loss since compiler is smart enough to
handle this cases.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: introduce is_inventra_dma helper
This patch introduces is_inventra_dma helper, so that
we can remove dependency on CONFIG_USB_INVENTRA_DMA
in source file of musb core driver in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces is_inventra_dma helper, so that
we can remove dependency on CONFIG_USB_INVENTRA_DMA
in source file of musb core driver in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: print dma type in runtime way
We will support multiple dma controller type in one single
musb core driver(binary), so print dma type by the
information from hw glue driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
We will support multiple dma controller type in one single
musb core driver(binary), so print dma type by the
information from hw glue driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove 'ifdef CONFIG_USB_INVENTRA_DMA' for comments only
This comments has said clearly that they are for Mentor(INVENTRA) DMA
controller, so remove this unnecessary ifdef to make code more clean.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This comments has said clearly that they are for Mentor(INVENTRA) DMA
controller, so remove this unnecessary ifdef to make code more clean.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove exit symbol to avoid using of ifdef in musb_g_rx
Remove one 'ifdef' and one 'exit' symbol to make code more cleaner.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Remove one 'ifdef' and one 'exit' symbol to make code more cleaner.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove duplicated define of tusb_dma_omap
tusb_dma_omap is defined in musb_dma.h already and same with
it in tusb6010.h, so remove the definition in tusb6010.h.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
tusb_dma_omap is defined in musb_dma.h already and same with
it in tusb6010.h, so remove the definition in tusb6010.h.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: support each dma controller driver built as module
This patch provides support for building each dma controller driver
as standalone module, and this modules can be built into one same
image and can be used by each hw glue driver.
HW glue driver has the knowledge of which type of dma controller will
be used, and can pass the knowledge into musb core driver via glue ops,
so we can take runtime method to support all hw controller and its dma
controller in one binary musb driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch provides support for building each dma controller driver
as standalone module, and this modules can be built into one same
image and can be used by each hw glue driver.
HW glue driver has the knowledge of which type of dma controller will
be used, and can pass the knowledge into musb core driver via glue ops,
so we can take runtime method to support all hw controller and its dma
controller in one binary musb driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: define DMA controller related flags and callbacks in glue ops
Each musb hw controller may use different DMA controller, so we
introduce dma controller related flags and callbacks in glue ops.
HW glue driver can provide its dma controller information to
musb core with this flags and callbacks, so we can make musb core
more generic and avoid to depend on the ugly macro below as far as
possible:
CONFIG_USB_INVENTRA_DMA
CONFIG_USB_TUSB_OMAP_DMA
CONFIG_USB_TI_CPPI_DMA
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Each musb hw controller may use different DMA controller, so we
introduce dma controller related flags and callbacks in glue ops.
HW glue driver can provide its dma controller information to
musb core with this flags and callbacks, so we can make musb core
more generic and avoid to depend on the ugly macro below as far as
possible:
CONFIG_USB_INVENTRA_DMA
CONFIG_USB_TUSB_OMAP_DMA
CONFIG_USB_TI_CPPI_DMA
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: same MUSB_OFFSET/musb_ep_select for all controller
The patch uses the information about hw endpoint register address
mapping from hw glue driver to implement MUSB_OFFSET/musb_ep_select
for different cases.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
The patch uses the information about hw endpoint register address
mapping from hw glue driver to implement MUSB_OFFSET/musb_ep_select
for different cases.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: pass musb pointer into musb_ep_select & MUSB_EP_OFFSET
This patche adds the paramer of musb pointer to musb_ep_select
and MUSB_EP_OFFSET, then we can pass musb into this two helpers
and can give corresponding implementation for flat mappings and
indexed mappings of hw endpoint register address using the information
from hw glue driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patche adds the paramer of musb pointer to musb_ep_select
and MUSB_EP_OFFSET, then we can pass musb into this two helpers
and can give corresponding implementation for flat mappings and
indexed mappings of hw endpoint register address using the information
from hw glue driver.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: simplify musb_ep_select&MUSB_EP_OFFSET for different hardware
In fact, for tusb, musb_ep_select and MUSB_EP_OFFSET are same with
that for indexed mapping, so merge the two cases to simplify
definition of the two helpers.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
In fact, for tusb, musb_ep_select and MUSB_EP_OFFSET are same with
that for indexed mapping, so merge the two cases to simplify
definition of the two helpers.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: same musb_readb/musb_writeb in single image to support multiple machines
This patch introduces musb_readb/musb_writeb function pointer,
so that we can use same musb_readb/musb_writeb in one single
binary image to help to support multiple machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces musb_readb/musb_writeb function pointer,
so that we can use same musb_readb/musb_writeb in one single
binary image to help to support multiple machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove musb_in_tusb
Remove musb_in_tusb since no one may use it.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Remove musb_in_tusb since no one may use it.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: handle tusb fifo style by runtime method
This patch introduces MUSB_GLUE_TUSB_STYLE flag, which
can be used to handle tusb dependent things by runtime
method instead of previous static method.
This patch handles tusb fifo style according to the flag
of MUSB_GLUE_TUSB_STYLE passed from hw glue drivers.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces MUSB_GLUE_TUSB_STYLE flag, which
can be used to handle tusb dependent things by runtime
method instead of previous static method.
This patch handles tusb fifo style according to the flag
of MUSB_GLUE_TUSB_STYLE passed from hw glue drivers.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: introduce flags field into musb_platform_ops
This patch introduces flags field into musb_platform_ops,
so we can handle hw glue difference in musb core driver
from the information of .flags, then we can remove the
ugly macros of hw glue related to help to make one image
working for multiple machines in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces flags field into musb_platform_ops,
so we can handle hw glue difference in musb core driver
from the information of .flags, then we can remove the
ugly macros of hw glue related to help to make one image
working for multiple machines in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: pass fifo_mode from hw glue driver
Each hw controller may have different fifo configuraion,
so passing fifo_mode from hw glue is very reasonable.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Each hw controller may have different fifo configuraion,
so passing fifo_mode from hw glue is very reasonable.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: use platform_driver_register to register musb_hdrc driver
Since hw glue drivers may depend on musb_hdrc and musb_init will return
failure if no glue device is registered, this patch fixes the issue
by registering musb_hdrc driver first.
Also this patch replaces most of __init with __devinit to support
platform_driver_register.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Since hw glue drivers may depend on musb_hdrc and musb_init will return
failure if no glue device is registered, this patch fixes the issue
by registering musb_hdrc driver first.
Also this patch replaces most of __init with __devinit to support
platform_driver_register.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: use native read_fifo/write_fifo for each hw glue driver
This patch uses native read_fifo/write_fifo for each hw glue driver.
Musb core can always use musb->ops->*_fifo to do PIO, also removes
some ugly ifdef for musb_read_fifo/musb_write_fifo.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch uses native read_fifo/write_fifo for each hw glue driver.
Musb core can always use musb->ops->*_fifo to do PIO, also removes
some ugly ifdef for musb_read_fifo/musb_write_fifo.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: introduce read_fifo/write_fifo callback in glue ops
This patch introduces read_fifo/write_fifo callback in glue ops,
so that we can make musb in one single images working on multiple
boards.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces read_fifo/write_fifo callback in glue ops,
so that we can make musb in one single images working on multiple
boards.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: support to compile hw glue layer driver as module
Obviously hw glue layer driver should be compiled as module,
which can help to build one single image to support multiple machines.
also merged
usb: musb: allow all hw glue modules built into one single image
This patch allows all hw glue drivers to be built into one single
image, so that we can support one single image to be run in multiple
machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Obviously hw glue layer driver should be compiled as module,
which can help to build one single image to support multiple machines.
also merged
usb: musb: allow all hw glue modules built into one single image
This patch allows all hw glue drivers to be built into one single
image, so that we can support one single image to be run in multiple
machines.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: export some symbols for glue driver access
Export this functions so that glue drivers can see them if glue drivers
are built as modules.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Export this functions so that glue drivers can see them if glue drivers
are built as modules.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
usb: musb: introduce get_hw_revision callback in glue ops
This patch introduces get_hw_revision callback in glue_ops,
and implement it in tusb glue driver, so tusb dma code can
get tusb revision via .get_hw_revision callback and we can
make glue drivers built as module easyly in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
This patch introduces get_hw_revision callback in glue_ops,
and implement it in tusb glue driver, so tusb dma code can
get tusb revision via .get_hw_revision callback and we can
make glue drivers built as module easyly in later patches.
Signed-off-by: Ming Lei <tom.leiming@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
Signed-off-by: Ajay Kumar Gupta <ajay.gupta@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
usb: musb: remove extern qualifier from musb_debug.h header
This change removes confusing extern qualifier, which doesn't have any practical
sense there.
Signed-off-by: Vladimir Zapolskiy <vladimir.zapolskiy@nokia.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
This change removes confusing extern qualifier, which doesn't have any practical
sense there.
Signed-off-by: Vladimir Zapolskiy <vladimir.zapolskiy@nokia.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
usb: musb: cleanup kconfig
The whole thing depends on USB_MUSB_HDRC, just add an 'if'.
Signed-off-by: Felipe Contreras <felipe.contreras@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
The whole thing depends on USB_MUSB_HDRC, just add an 'if'.
Signed-off-by: Felipe Contreras <felipe.contreras@gmail.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>