sitara-epos/sitara-epos-kernel.git
10 years agoarm:omap:am33xx: register edma platform
Hebbar, Gururaja [Tue, 4 Oct 2011 12:45:12 +0000 (18:15 +0530)]
arm:omap:am33xx: register edma platform

Chnages
- AM33XX has Three Transfer Controllers. Platform data added for am33xx
- Add xbar mapping for MMCHS2. Since MMCHS edma Event is xbar mapped,
  proper mapping is added when registering xbar structure. This mapping
  uses edma event 12 & 13 which is not used on AM33xx SOC

Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:Kconfig: Add edma option
Vaibhav Hiremath [Thu, 15 Dec 2011 06:16:15 +0000 (11:46 +0530)]
arm:omap:Kconfig: Add edma option

This allows tp enable EDMA support.

Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoTI81xx: (cust) Add SDMA to EDMA wrapper.
Sriramakrishnan [Fri, 11 Feb 2011 06:36:23 +0000 (12:06 +0530)]
TI81xx: (cust) Add SDMA to EDMA wrapper.

Some of the modules are common between OMAP3 and TI81xx. These
modules use SDMA on OMAP3 and EDMA on TI81xx. Add a wrapper for
translating between the SDMA to EDMA API. Need to migrate to a common
DMA interface in the future for co-existence

Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Sriramakrishnan <srk@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add support for EDMA
Sundaram Raju [Tue, 27 Apr 2010 05:49:30 +0000 (11:19 +0530)]
arm:omap:am33xx: Add support for EDMA

Base from
- edma.c is dma.c from arch/arm/mach-davinci
- edma.h is edma.h from arch/arm/mach-davinci/include/mach
- both the files are copied to new locations

Changes
- to account for change in header file location
- added more callback functions to service upto 4 TCs
- Changed edma_init into a subsys call to ensure that edma is registered
  before it is probed
- Code added to support the crossbar
- Certain definitions and functions in edma.c moved to header file
  edma.h so that they can be used in the platform specific file devices.c
- Removed dead code that services non existing TC IRQs

Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Sundaram Raju <sundaram@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: LCD backlight support
Afzal Mohammed [Wed, 21 Dec 2011 08:10:14 +0000 (13:40 +0530)]
arm:omap:am33xx: LCD backlight support

Turn on LCD backlight based on board and
profile detected (i.e if LCD is present)

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
10 years agoarm:omap:am33xx: add CPSW platform hookup support
Chandan Nath [Tue, 4 Oct 2011 11:21:53 +0000 (16:51 +0530)]
arm:omap:am33xx: add CPSW platform hookup support

Signed-off-by: Chandan Nath <chandan.nath@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap2plus: Enable ethernet driver (CPDMA, MDIO and CPSW)
Vaibhav Hiremath [Sat, 26 Nov 2011 10:56:24 +0000 (16:26 +0530)]
arm:omap2plus: Enable ethernet driver (CPDMA, MDIO and CPSW)

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agodriver:ethernet: Add CPSW driver
Vaibhav Hiremath [Sat, 26 Nov 2011 10:54:40 +0000 (16:24 +0530)]
driver:ethernet: Add CPSW driver

This patch adds support for TI's CPSW driver along with
CPSW ALE driver.

Signed-off-by: Chandan Nath <chandan.nath@ti.com>
Signed-off-by: Mugunthan V N <mugunthanvnm@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Update EVM Detection and handling
Vaibhav Hiremath [Sat, 26 Nov 2011 10:34:01 +0000 (16:04 +0530)]
arm:omap:am33xx: Update EVM Detection and handling

AM335X EVM comes in 4 flavours. The type of EVM is encoded in the EEPROM
on the Baseboard.

This patch provides api to read this data from eeprom & setup/configure
the evm/devices accordingly. Also, Profile data is retrieved by reading
the CPLD on the daughter board.

In case the eeprom read fails or if thh data is invalid, the fallback
option selects General Purpose EVM with Daughter board connected in
Profile 0.

Also, This patch adds support for BETA EVM.
BETA EVM is set as the default configuration.
Since the peripherals were supported only in profile 0 for
alpha EVM, It makes use of the exisiting GP EVM structure.

Flag gp_evm_revision can be used to differentiate between the
revisions of the GP EVM.

Also, there exist Alpha EVMs with a version string of 1.0B as
well as 1.0A.
Make our revision detection logic check for just 1.0 and rename
defines to match.

Signed-off-by: Patil, Rachna <rachna@ti.com>
Signed-off-by: Tom Rini <trini@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Afzal Mohammed <afzal@ti.com>
10 years agoarm:omap:am33xx: board_init pin mux initialization
Afzal Mohammed [Tue, 4 Oct 2011 10:06:25 +0000 (15:36 +0530)]
arm:omap:am33xx: board_init pin mux initialization

Configure I2C0 pin mux in board init, required for
board detection (read eeprom). Also add function
for dynamic pin mux.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx:TEMP: Create board support and enable build for AM335XEVM
Vaibhav Hiremath [Sat, 26 Nov 2011 10:28:03 +0000 (15:58 +0530)]
arm:omap:am33xx:TEMP: Create board support and enable build for AM335XEVM

This patch adds minimal support and build configuration for
AM335X EVM.

Also, remove and cleanup AM3517EVM approach, so that we don't end up
polluting board-am3517evm.c file for all AM335x related code.

NOTE: Patch is not for upstream, since upstream approach is completely
      in different direction as far as board changes is concerned.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add pin mux helpers
Afzal Mohammed [Tue, 4 Oct 2011 10:02:45 +0000 (15:32 +0530)]
arm:omap:am33xx: Add pin mux helpers

Add pin mux table, macros for pin mux

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:omap2plus: Enable AT24 EEPROM in defconfig
Vaibhav Hiremath [Sat, 26 Nov 2011 10:35:56 +0000 (16:05 +0530)]
arm:omap:omap2plus: Enable AT24 EEPROM in defconfig

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:clock Remove duplicate macros from DPLL state
Vaibhav Hiremath [Fri, 25 Nov 2011 06:39:37 +0000 (12:09 +0530)]
arm:omap:clock Remove duplicate macros from DPLL state

Irrespective of cpu-type, aren't we supposed to do
same thing for any bypass cases (LPBYPASS/FRBYPASS/MNBYPASS),

     - dpll clock reparenting
     - get dpll rate

This patch cleans up the code and removes the unneccessary cpu check.

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Update defconfig to disable 32K_TIMER and RESET_CLOCKS
Vaibhav Hiremath [Wed, 14 Dec 2011 11:59:49 +0000 (17:29 +0530)]
arm:omap:am33xx: Update defconfig to disable 32K_TIMER and RESET_CLOCKS

Also enable DEBUG_LL option

10 years agoarm:omap:am33xx: SoC type detection
Afzal Mohammed [Tue, 11 Oct 2011 11:54:05 +0000 (17:24 +0530)]
arm:omap:am33xx: SoC type detection

Determine SoC type

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: add control_status register addr & bit offsets
Vaibhav Hiremath [Fri, 18 Nov 2011 14:09:46 +0000 (19:39 +0530)]
arm:omap:am33xx: add control_status register addr & bit offsets

This information is required for clock tree data,
where we need to read the control_status register
to detect the input Osc freq.
Here control_status register is used for .clksel_reg.

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Skip parts where cpu_is_omap34xx() is true but NA for AM33XX
Afzal Mohammed [Thu, 8 Sep 2011 10:59:39 +0000 (16:29 +0530)]
arm:omap:am33xx: Skip parts where cpu_is_omap34xx() is true but NA for AM33XX

Add an explicit check for cpu_is_am33xx() to prevent the block inside
cpu_is_omap34xx() from executing which would otherwise fail/cause
aborts on AM33XX.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add am335x support in generic omap_hwmod
Vaibhav Hiremath [Tue, 4 Oct 2011 12:23:49 +0000 (17:53 +0530)]
arm:omap:am33xx: Add am335x support in generic omap_hwmod

AM335X is bit different than OMAP3/4 architecture when it comes to
PRCM module, for example, the way module is enabled/disabled.
Although it is closer to OMAP4 architecure but the register offset
and PRCM partitions won't match, so we need to seperate API's
for AM335X.

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add clock control api's
Vaibhav Hiremath [Tue, 4 Oct 2011 12:00:35 +0000 (17:30 +0530)]
arm:omap:am33xx: Add clock control api's

Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add HWMOD data
Vaibhav Hiremath [Wed, 14 Dec 2011 11:04:41 +0000 (16:34 +0530)]
arm:omap:am33xx: Add HWMOD data

This patch adds HWMOD data for all the peripherals of AM335X and
also hooks up to the existing OMAP framework.

Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add irq, dma and module base addr to SoC header files
Vaibhav Hiremath [Sun, 20 Nov 2011 09:38:30 +0000 (15:08 +0530)]
arm:omap:am33xx: Add irq, dma and module base addr to SoC header files

This patch creats seperate irq and dma defination header file
and updates the module base addresses required for HWMOD data.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx:CUSTOM: Add CK_AM33XX temporary
Vaibhav Hiremath [Wed, 14 Dec 2011 10:43:21 +0000 (16:13 +0530)]
arm:omap:am33xx:CUSTOM: Add CK_AM33XX temporary

With new clock framework we don't need this, but required now
to get AM335x existing code to build.

10 years agoarm:omap:am33xx: Add Clock & clockdomain data
Vaibhav Hiremath [Wed, 14 Dec 2011 10:41:07 +0000 (16:11 +0530)]
arm:omap:am33xx: Add Clock & clockdomain data

This patch adds support for AM33XX clock & clock domain data,
corresponding API's to access CM module and
CM register offsets & bit fields.

Signed-off-by: Rachna Patil <rachna@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Signed-off-by: Afzal Mohammed <afzal@ti.com>
10 years agoarm:omap:am33xx: Add power domain data
Vaibhav Hiremath [Fri, 9 Dec 2011 11:28:19 +0000 (16:58 +0530)]
arm:omap:am33xx: Add power domain data

This patch adds AM33XX power domain data (powerdomains33xx_data.c),
corresponding API's to access PRM module and
PRM register offsets & bit fields.

Also, hook up AM33XX power domain to OMAP framework.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add voltage domain data
Vaibhav Hiremath [Thu, 1 Dec 2011 13:53:23 +0000 (19:23 +0530)]
arm:omap:am33xx: Add voltage domain data

Currently dummy voltage domain data is being created
in order to succeed boot process.
Nothing has been done w.r.t actual hardware (voltage control).

Also, hook up AM33XX voltage domain to OMAP framework.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoAM335XEVM: Update mach-types
Vaibhav Hiremath [Mon, 7 Nov 2011 11:16:56 +0000 (16:46 +0530)]
AM335XEVM: Update mach-types

New machine-id added, obtained from RMK.

Note: Please note that, the allocated mach-type has typo-mistake
(am335evm => am335xevm) which needs to be corrected. This is going
to be custom patch, since this will get enrolled by Russell automatically.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
10 years agoarm:omap:am33xx: Add low level debugging support
Afzal Mohammed [Fri, 2 Dec 2011 06:14:00 +0000 (11:44 +0530)]
arm:omap:am33xx: Add low level debugging support

Add support for low level debugging on AM335X EVM (AM33XX family).
Currently only support for UART1 console, which is used on AM335X EVM
is added.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
Reviewed-by: Kevin Hilman <khilman@ti.com>
10 years agoarm:omap:am33xx: Add AM335XEVM machine support
Afzal Mohammed [Tue, 9 Aug 2011 08:59:41 +0000 (14:29 +0530)]
arm:omap:am33xx: Add AM335XEVM machine support

This patch adds minimal support for AM335X EVM.
The approach taken here is to add AM335X EVM support
to AM3517EVM, considering the fact that with device tree
developement we will get rid of board-*.c.

Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Vaibhav Hiremath <hvaibhav@ti.com>
[Changed ti816x_init_irq=>ti81xx_init_irq, due to recent acceptance of patches]
Reviewed-by: Kevin Hilman <khilman@ti.com>
10 years agoMerge v3.2 stable kernel here
Vaibhav Hiremath [Mon, 23 Jan 2012 19:08:09 +0000 (00:38 +0530)]
Merge v3.2 stable kernel here

Conflicts:
arch/arm/mach-shmobile/board-kota2.c

10 years agoLinux 3.2 v3.2
Linus Torvalds [Wed, 4 Jan 2012 23:55:44 +0000 (15:55 -0800)]
Linux 3.2

10 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Linus Torvalds [Wed, 4 Jan 2012 23:03:49 +0000 (15:03 -0800)]
Merge git://git./linux/kernel/git/davem/net

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net:
  fix CAN MAINTAINERS SCM tree type
  mwifiex: fix crash during simultaneous scan and connect
  b43: fix regression in PIO case
  ath9k: Fix kernel panic in AR2427 in AP mode
  CAN MAINTAINERS update
  net: fsl: fec: fix build for mx23-only kernel
  sch_qfq: fix overflow in qfq_update_start()
  Revert "Bluetooth: Increase HCI reset timeout in hci_dev_do_close"

10 years agominixfs: misplaced checks lead to dentry leak
Al Viro [Wed, 4 Jan 2012 10:51:03 +0000 (10:51 +0000)]
minixfs: misplaced checks lead to dentry leak

bitmap size sanity checks should be done *before* allocating ->s_root;
there their cleanup on failure would be correct.  As it is, we do iput()
on root inode, but leak the root dentry...

Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
Acked-by: Josh Boyer <jwboyer@redhat.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoptrace: ensure JOBCTL_STOP_SIGMASK is not zero after detach
Oleg Nesterov [Wed, 4 Jan 2012 16:29:20 +0000 (17:29 +0100)]
ptrace: ensure JOBCTL_STOP_SIGMASK is not zero after detach

This is the temporary simple fix for 3.2, we need more changes in this
area.

1. do_signal_stop() assumes that the running untraced thread in the
   stopped thread group is not possible. This was our goal but it is
   not yet achieved: a stopped-but-resumed tracee can clone the running
   thread which can initiate another group-stop.

   Remove WARN_ON_ONCE(!current->ptrace).

2. A new thread always starts with ->jobctl = 0. If it is auto-attached
   and this group is stopped, __ptrace_unlink() sets JOBCTL_STOP_PENDING
   but JOBCTL_STOP_SIGMASK part is zero, this triggers WANR_ON(!signr)
   in do_jobctl_trap() if another debugger attaches.

   Change __ptrace_unlink() to set the artificial SIGSTOP for report.

   Alternatively we could change ptrace_init_task() to copy signr from
   current, but this means we can copy it for no reason and hide the
   possible similar problems.

Acked-by: Tejun Heo <tj@kernel.org>
Cc: <stable@kernel.org> [3.1]
Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoptrace: partially fix the do_wait(WEXITED) vs EXIT_DEAD->EXIT_ZOMBIE race
Oleg Nesterov [Wed, 4 Jan 2012 16:29:02 +0000 (17:29 +0100)]
ptrace: partially fix the do_wait(WEXITED) vs EXIT_DEAD->EXIT_ZOMBIE race

Test-case:

int main(void)
{
int pid, status;

pid = fork();
if (!pid) {
for (;;) {
if (!fork())
return 0;
if (waitpid(-1, &status, 0) < 0) {
printf("ERR!! wait: %m\n");
return 0;
}
}
}

assert(ptrace(PTRACE_ATTACH, pid, 0,0) == 0);
assert(waitpid(-1, NULL, 0) == pid);

assert(ptrace(PTRACE_SETOPTIONS, pid, 0,
PTRACE_O_TRACEFORK) == 0);

do {
ptrace(PTRACE_CONT, pid, 0, 0);
pid = waitpid(-1, NULL, 0);
} while (pid > 0);

return 1;
}

It fails because ->real_parent sees its child in EXIT_DEAD state
while the tracer is going to change the state back to EXIT_ZOMBIE
in wait_task_zombie().

The offending commit is 823b018e which moved the EXIT_DEAD check,
but in fact we should not blame it. The original code was not
correct as well because it didn't take ptrace_reparented() into
account and because we can't really trust ->ptrace.

This patch adds the additional check to close this particular
race but it doesn't solve the whole problem. We simply can't
rely on ->ptrace in this case, it can be cleared if the tracer
is multithreaded by the exiting ->parent.

I think we should kill EXIT_DEAD altogether, we should always
remove the soon-to-be-reaped child from ->children or at least
we should never do the DEAD->ZOMBIE transition. But this is too
complex for 3.2.

Reported-and-tested-by: Denys Vlasenko <vda.linux@googlemail.com>
Tested-by: Lukasz Michalik <lmi@ift.uni.wroc.pl>
Acked-by: Tejun Heo <tj@kernel.org>
Cc: <stable@kernel.org> [3.0+]
Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoMerge git://git.samba.org/sfrench/cifs-2.6
Linus Torvalds [Wed, 4 Jan 2012 22:57:55 +0000 (14:57 -0800)]
Merge git://git.samba.org/sfrench/cifs-2.6

* git://git.samba.org/sfrench/cifs-2.6:
  [CIFS] default ntlmv2 for cifs mount delayed to 3.3
  cifs: fix bad buffer length check in coalesce_t2

10 years agoMerge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/linville/wirel...
John W. Linville [Wed, 4 Jan 2012 16:37:30 +0000 (11:37 -0500)]
Merge branch 'master' of git://git./linux/kernel/git/linville/wireless into for-davem

10 years agoRevert "rtc: Expire alarms after the time is set."
Linus Torvalds [Wed, 4 Jan 2012 15:57:22 +0000 (07:57 -0800)]
Revert "rtc: Expire alarms after the time is set."

This reverts commit 93b2ec0128c431148b216b8f7337c1a52131ef03.

The call to "schedule_work()" in rtc_initialize_alarm() happens too
early, and can cause oopses at bootup

Neil Brown explains why we do it:

  "If you set an alarm in the future, then shutdown and boot again after
   that time, then you will end up with a timer_queue node which is in
   the past.

   When this happens the queue gets stuck.  That entry-in-the-past won't
   get removed until and interrupt happens and an interrupt won't happen
   because the RTC only triggers an interrupt when the alarm is "now".

   So you'll find that e.g.  "hwclock" will always tell you that
   'select' timed out.

   So we force the interrupt work to happen at the start just in case."

and has a patch that convert it to do things in-process rather than with
the worker thread, but right now it's too late to play around with this,
so we just revert the patch that caused problems for now.

Reported-by: Sander Eikelenboom <linux@eikelenboom.it>
Requested-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Requested-by: John Stultz <john.stultz@linaro.org>
Cc: Neil Brown <neilb@suse.de>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years ago[CIFS] default ntlmv2 for cifs mount delayed to 3.3
Steve French [Wed, 4 Jan 2012 05:08:24 +0000 (23:08 -0600)]
[CIFS] default ntlmv2 for cifs mount delayed to 3.3

Turned out the ntlmv2 (default security authentication)
upgrade was harder to test than expected, and we ran
out of time to test against Apple and a few other servers
that we wanted to.  Delay upgrade of default security
from ntlm to ntlmv2 (on mount) to 3.3.  Still works
fine to specify it explicitly via "sec=ntlmv2" so this
should be fine.

Acked-by: Jeff Layton <jlayton@samba.org>
Signed-off-by: Steve French <smfrench@gmail.com>
10 years agocifs: fix bad buffer length check in coalesce_t2
Jeff Layton [Sun, 1 Jan 2012 15:34:39 +0000 (10:34 -0500)]
cifs: fix bad buffer length check in coalesce_t2

The current check looks to see if the RFC1002 length is larger than
CIFSMaxBufSize, and fails if it is. The buffer is actually larger than
that by MAX_CIFS_HDR_SIZE.

This bug has been around for a long time, but the fact that we used to
cap the clients MaxBufferSize at the same level as the server tended
to paper over it. Commit c974befa changed that however and caused this
bug to bite in more cases.

Reported-and-Tested-by: Konstantinos Skarlatos <k.skarlatos@gmail.com>
Tested-by: Shirish Pargaonkar <shirishpargaonkar@gmail.com>
Signed-off-by: Jeff Layton <jlayton@redhat.com>
Signed-off-by: Steve French <smfrench@gmail.com>
10 years agoRevert "rtc: Disable the alarm in the hardware"
Linus Torvalds [Wed, 4 Jan 2012 01:32:13 +0000 (17:32 -0800)]
Revert "rtc: Disable the alarm in the hardware"

This reverts commit c0afabd3d553c521e003779c127143ffde55a16f.

It causes failures on Toshiba laptops - instead of disabling the alarm,
it actually seems to enable it on the affected laptops, resulting in
(for example) the laptop powering on automatically five minutes after
shutdown.

There's a patch for it that appears to work for at least some people,
but it's too late to play around with this, so revert for now and try
again in the next merge window.

See for example

http://bugs.debian.org/652869

Reported-and-bisected-by: Andreas Friedrich <afrie@gmx.net> (Toshiba Tecra)
Reported-by: Antonio-M. Corbi Bellot <antonio.corbi@ua.es> (Toshiba Portege R500)
Reported-by: Marco Santos <marco.santos@waynext.com> (Toshiba Portege Z830)
Reported-by: Christophe Vu-Brugier <cvubrugier@yahoo.fr> (Toshiba Portege R830)
Cc: Jonathan Nieder <jrnieder@gmail.com>
Requested-by: John Stultz <john.stultz@linaro.org>
Cc: stable@kernel.org # for the versions that applied this
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agohung_task: fix false positive during vfork
Mandeep Singh Baines [Tue, 3 Jan 2012 22:41:13 +0000 (14:41 -0800)]
hung_task: fix false positive during vfork

vfork parent uninterruptibly and unkillably waits for its child to
exec/exit. This wait is of unbounded length. Ignore such waits
in the hung_task detector.

Signed-off-by: Mandeep Singh Baines <msb@chromium.org>
Reported-by: Sasha Levin <levinsasha928@gmail.com>
LKML-Reference: <1325344394.28904.43.camel@lappy>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Ingo Molnar <mingo@elte.hu>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: John Kacur <jkacur@redhat.com>
Cc: stable@kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agosecurity: Fix security_old_inode_init_security() when CONFIG_SECURITY is not set
Jan Kara [Tue, 3 Jan 2012 12:14:29 +0000 (13:14 +0100)]
security: Fix security_old_inode_init_security() when CONFIG_SECURITY is not set

Commit 1e39f384bb01 ("evm: fix build problems") makes the stub version
of security_old_inode_init_security() return 0 when CONFIG_SECURITY is
not set.

But that makes callers such as reiserfs_security_init() assume that
security_old_inode_init_security() has set name, value, and len
arguments properly - but security_old_inode_init_security() left them
uninitialized which then results in interesting failures.

Revert security_old_inode_init_security() to the old behavior of
returning EOPNOTSUPP since both callers (reiserfs and ocfs2) handle this
just fine.

[ Also fixed the S_PRIVATE(inode) case of the actual non-stub
  security_old_inode_init_security() function to return EOPNOTSUPP
  for the same reason, as pointed out by Mimi Zohar.

  It got incorrectly changed to match the new function in commit
  fb88c2b6cbb1: "evm: fix security/security_old_init_security return
  code".   - Linus ]

Reported-by: Jorge Bastos <mysql.jorge@decimal.pt>
Acked-by: James Morris <jmorris@namei.org>
Acked-by: Mimi Zohar <zohar@us.ibm.com>
Signed-off-by: Jan Kara <jack@suse.cz>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agofix CAN MAINTAINERS SCM tree type
Oliver Hartkopp [Tue, 3 Jan 2012 19:57:43 +0000 (14:57 -0500)]
fix CAN MAINTAINERS SCM tree type

As pointed out by Joe Perches the SCM tree type was missing in my patch.

Signed-off-by: Oliver Hartkopp <socketcan@hartkopp.net>
CC: Oliver Hartkopp <oliver.hartkopp@volkswagen.de>
CC: Urs Thuermann <urs.thuermann@volkswagen.de>
CC: Wolfgang Grandegger <wg@grandegger.com>
CC: Marc Kleine-Budde <mkl@pengutronix.de>
CC: linux-can@vger.kernel.org
10 years agomwifiex: fix crash during simultaneous scan and connect
Amitkumar Karwar [Tue, 3 Jan 2012 00:18:40 +0000 (16:18 -0800)]
mwifiex: fix crash during simultaneous scan and connect

If 'iw connect' command is fired when driver is already busy in
serving 'iw scan' command, ssid specific scan operation for connect
is skipped. In this case cmd wait queue handler gets called with no
command in queue (i.e. adapter->cmd_queued = NULL).

This patch adds a NULL check in mwifiex_wait_queue_complete()
routine to fix crash observed during simultaneous scan and assoc
operations.

Signed-off-by: Amitkumar Karwar <akarwar@marvell.com>
Signed-off-by: Bing Zhao <bzhao@marvell.com>
Signed-off-by: John W. Linville <linville@tuxdriver.com>
10 years agob43: fix regression in PIO case
Guennadi Liakhovetski [Mon, 26 Dec 2011 17:28:08 +0000 (18:28 +0100)]
b43: fix regression in PIO case

This patch fixes the regression, introduced by

commit 17030f48e31adde5b043741c91ba143f5f7db0fd
From: Rafał Miłecki <zajec5@gmail.com>
Date: Thu, 11 Aug 2011 17:16:27 +0200
Subject: [PATCH] b43: support new RX header, noticed to be used in 598.314+ fw

in PIO case.

Signed-off-by: Guennadi Liakhovetski <g.liakhovetski@gmx.de>
Signed-off-by: John W. Linville <linville@tuxdriver.com>
10 years agoath9k: Fix kernel panic in AR2427 in AP mode
Mohammed Shafi Shajakhan [Mon, 26 Dec 2011 05:12:15 +0000 (10:42 +0530)]
ath9k: Fix kernel panic in AR2427 in AP mode

don't do aggregation related stuff for 'AP mode client power save
handling' if aggregation is not enabled in the driver, otherwise it
will lead to panic because those data structures won't be never
intialized in 'ath_tx_node_init' if aggregation is disabled

EIP is at ath_tx_aggr_wakeup+0x37/0x80 [ath9k]
EAX: e8c09a20 EBX: f2a304e8 ECX: 00000001 EDX: 00000000
ESI: e8c085e0 EDI: f2a304ac EBP: f40e1ca4 ESP: f40e1c8c
DS: 007b ES: 007b FS: 00d8 GS: 00e0 SS: 0068
Process swapper/1 (pid: 0, ti=f40e0000 task=f408e860
task.ti=f40dc000)
Stack:
0001e966 e8c09a20 00000000 f2a304ac e8c085e0 f2a304ac
f40e1cb0 f8186741
f8186700 f40e1d2c f922988d f2a304ac 00000202 00000001
c0b4ba43 00000000
0000000f e8eb75c0 e8c085e0 205b0001 34383220 f2a304ac
f2a30000 00010020
Call Trace:
[<f8186741>] ath9k_sta_notify+0x41/0x50 [ath9k]
[<f8186700>] ? ath9k_get_survey+0x110/0x110 [ath9k]
[<f922988d>] ieee80211_sta_ps_deliver_wakeup+0x9d/0x350
[mac80211]
[<c018dc75>] ? __module_address+0x95/0xb0
[<f92465b3>] ap_sta_ps_end+0x63/0xa0 [mac80211]
[<f9246746>] ieee80211_rx_h_sta_process+0x156/0x2b0
[mac80211]
[<f9247d1e>] ieee80211_rx_handlers+0xce/0x510 [mac80211]
[<c018440b>] ? trace_hardirqs_on+0xb/0x10
[<c056936e>] ? skb_queue_tail+0x3e/0x50
[<f9248271>] ieee80211_prepare_and_rx_handle+0x111/0x750
[mac80211]
[<f9248bf9>] ieee80211_rx+0x349/0xb20 [mac80211]
[<f9248949>] ? ieee80211_rx+0x99/0xb20 [mac80211]
[<f818b0b8>] ath_rx_tasklet+0x818/0x1d00 [ath9k]
[<f8187a75>] ? ath9k_tasklet+0x35/0x1c0 [ath9k]
[<f8187a75>] ? ath9k_tasklet+0x35/0x1c0 [ath9k]
[<f8187b33>] ath9k_tasklet+0xf3/0x1c0 [ath9k]
[<c0151b7e>] tasklet_action+0xbe/0x180

Cc: stable@kernel.org
Cc: Senthil Balasubramanian <senthilb@qca.qualcomm.com>
Cc: Rajkumar Manoharan <rmanohar@qca.qualcomm.com>
Reported-by: Ashwin Mendonca <ashwinloyal@gmail.com>
Tested-by: Ashwin Mendonca <ashwinloyal@gmail.com>
Signed-off-by: Mohammed Shafi Shajakhan <mohammed@qca.qualcomm.com>
Signed-off-by: John W. Linville <linville@tuxdriver.com>
10 years agoMerge branch 'master' of git://git.kernel.org/pub/scm/linux/kernel/git/padovan/bluetooth
John W. Linville [Tue, 3 Jan 2012 19:26:56 +0000 (14:26 -0500)]
Merge branch 'master' of git://git./linux/kernel/git/padovan/bluetooth

10 years agoCAN MAINTAINERS update
Oliver Hartkopp [Tue, 3 Jan 2012 08:40:28 +0000 (08:40 +0000)]
CAN MAINTAINERS update

Update the CAN MAINTAINERS section:

- point out active maintainers
- pull the CAN driver discussion away from netdev ML
- point to the new CAN web site on gitorious.org
- add CAN development git repository URL to submit patches

Signed-off-by: Oliver Hartkopp <socketcan@hartkopp.net>
CC: Oliver Hartkopp <oliver.hartkopp@volkswagen.de>
CC: Urs Thuermann <urs.thuermann@volkswagen.de>
CC: Wolfgang Grandegger <wg@grandegger.com>
CC: Marc Kleine-Budde <mkl@pengutronix.de>
CC: linux-can@vger.kernel.org
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agonet: fsl: fec: fix build for mx23-only kernel
Wolfram Sang [Tue, 3 Jan 2012 03:46:47 +0000 (03:46 +0000)]
net: fsl: fec: fix build for mx23-only kernel

If one only selects mx23-based boards, compile fails:

drivers/net/ethernet/freescale/fec.c:410:2: error: 'FEC_HASH_TABLE_HIGH' undeclared (first use in this function)
drivers/net/ethernet/freescale/fec.c:411:2: error: 'FEC_HASH_TABLE_LOW' undeclared (first use in this function)

This is because fec.h uses CONFIG_SOC_IMX28 to determine the register
layout of the core which makes sense since the MX23 does not have a fec.
However, Kconfig uses the broader ARCH_MXS symbol and this way even
makes the fec-driver default for MX23. Adapt Kconfig to use the more
precise SOC_IMX28 as well.

Signed-off-by: Wolfram Sang <w.sang@pengutronix.de>
Cc: Fabio Estevam <fabio.estevam@freescale.com>
Cc: Uwe Kleine-König <u.kleine-koenig@pengutronix.de>
Cc: Shawn Guo <shawn.guo@linaro.org>
Cc: David S. Miller <davem@davemloft.net>
Acked-by: Fabio Estevam <fabio.estevam@freescale.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agosch_qfq: fix overflow in qfq_update_start()
Eric Dumazet [Mon, 2 Jan 2012 05:47:57 +0000 (05:47 +0000)]
sch_qfq: fix overflow in qfq_update_start()

grp->slot_shift is between 22 and 41, so using 32bit wide variables is
probably a typo.

This could explain QFQ hangs Dave reported to me, after 2^23 packets ?

(23 = 64 - 41)

Reported-by: Dave Taht <dave.taht@gmail.com>
Signed-off-by: Eric Dumazet <eric.dumazet@gmail.com>
CC: Stephen Hemminger <shemminger@vyatta.com>
CC: Dave Taht <dave.taht@gmail.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agodrm/radeon/kms/atom: fix possible segfault in pm setup
Alexander Müller [Fri, 30 Dec 2011 17:55:48 +0000 (12:55 -0500)]
drm/radeon/kms/atom: fix possible segfault in pm setup

If we end up with no power states, don't look up
current vddc.

fixes:
https://bugs.freedesktop.org/show_bug.cgi?id=44130

agd5f: fix patch formatting

Signed-off-by: Alex Deucher <alexander.deucher@amd.com>
Cc: stable@vger.kernel.org
Signed-off-by: Dave Airlie <airlied@redhat.com>
10 years agoMerge branch 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6
Linus Torvalds [Mon, 2 Jan 2012 20:34:03 +0000 (12:34 -0800)]
Merge branch 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6

* 'devicetree/merge' of git://git.secretlab.ca/git/linux-2.6:
  dt/device: Fix auxdata matching to handle entries without a name override

10 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Linus Torvalds [Mon, 2 Jan 2012 03:36:08 +0000 (19:36 -0800)]
Merge git://git./linux/kernel/git/davem/net

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net:
  netfilter: ctnetlink: fix timeout calculation
  ipvs: try also real server with port 0 in backup server
  skge: restore rx multicast filter on resume and after config changes
  mlx4_en: nullify cq->vector field when closing completion queue

10 years agoMerge branch 'fix/asoc' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound
Linus Torvalds [Sat, 31 Dec 2011 19:55:06 +0000 (11:55 -0800)]
Merge branch 'fix/asoc' of git://git./linux/kernel/git/tiwai/sound

* 'fix/asoc' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound:
  ASoC: wm8776: add missing break in sample size switch

10 years agogspca: Fix falling back to lower isoc alt settings
Mauro Carvalho Chehab [Sat, 31 Dec 2011 13:32:03 +0000 (11:32 -0200)]
gspca: Fix falling back to lower isoc alt settings

The current gspca core code has a regression where it no longer properly
falls back to lower alt settings when there is not enough bandwidth.

This causes many iso based usb-1 cameras to not work when plugged into a
usb2 hub or a sandybridge chipset motherboard!

This patch fixes this.

Signed-off-by: Hans de Goede <hdegoede@redhat.com>
Signed-off-by: Mauro Carvalho Chehab <mchehab@redhat.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agofutex: Fix uninterruptible loop due to gate_area
Hugh Dickins [Sat, 31 Dec 2011 19:44:01 +0000 (11:44 -0800)]
futex: Fix uninterruptible loop due to gate_area

It was found (by Sasha) that if you use a futex located in the gate
area we get stuck in an uninterruptible infinite loop, much like the
ZERO_PAGE issue.

While looking at this problem, PeterZ realized you'll get into similar
trouble when hitting any install_special_pages() mapping.  And are there
still drivers setting up their own special mmaps without page->mapping,
and without special VM or pte flags to make get_user_pages fail?

In most cases, if page->mapping is NULL, we do not need to retry at all:
Linus points out that even /proc/sys/vm/drop_caches poses no problem,
because it ends up using remove_mapping(), which takes care not to
interfere when the page reference count is raised.

But there is still one case which does need a retry: if memory pressure
called shmem_writepage in between get_user_pages_fast dropping page
table lock and our acquiring page lock, then the page gets switched from
filecache to swapcache (and ->mapping set to NULL) whatever the refcount.
Fault it back in to get the page->mapping needed for key->shared.inode.

Reported-by: Sasha Levin <levinsasha928@gmail.com>
Signed-off-by: Hugh Dickins <hughd@google.com>
Cc: stable@vger.kernel.org
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agonetfilter: ctnetlink: fix timeout calculation
Xi Wang [Fri, 30 Dec 2011 15:40:17 +0000 (10:40 -0500)]
netfilter: ctnetlink: fix timeout calculation

The sanity check (timeout < 0) never works; the dividend is unsigned
and so is the division, which should have been a signed division.

long timeout = (ct->timeout.expires - jiffies) / HZ;
if (timeout < 0)
timeout = 0;

This patch converts the time values to signed for the division.

Signed-off-by: Xi Wang <xi.wang@gmail.com>
Signed-off-by: Pablo Neira Ayuso <pablo@netfilter.org>
10 years agoipvs: try also real server with port 0 in backup server
Julian Anastasov [Fri, 30 Dec 2011 05:19:02 +0000 (14:19 +0900)]
ipvs: try also real server with port 0 in backup server

We should not forget to try for real server with port 0
in the backup server when processing the sync message. We should
do it in all cases because the backup server can use different
forwarding method.

Signed-off-by: Julian Anastasov <ja@ssi.bg>
Signed-off-by: Simon Horman <horms@verge.net.au>
Signed-off-by: Pablo Neira Ayuso <pablo@netfilter.org>
10 years agoskge: restore rx multicast filter on resume and after config changes
Florian Zumbiehl [Fri, 30 Dec 2011 17:30:09 +0000 (17:30 +0000)]
skge: restore rx multicast filter on resume and after config changes

Restore skge hardware registers for multicast filtering to their
appropriate values after system resume and after hardware restarts
that are done when changing certain settings.

Signed-off-by: Florian Zumbiehl <florz@florz.de>
Acked-by: Stephen Hemminger <shemminger@vyatta.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agomlx4_en: nullify cq->vector field when closing completion queue
Yevgeny Petrilin [Thu, 29 Dec 2011 05:49:58 +0000 (05:49 +0000)]
mlx4_en: nullify cq->vector field when closing completion queue

Caused loss of connectivity when changing ring size.

Signed-off-by: Yevgeny Petrilin <yevgenyp@mellanox.co.il>
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agoMerge branch 'fixes' of http://ftp.arm.linux.org.uk/pub/linux/arm/kernel/git-cur...
Linus Torvalds [Fri, 30 Dec 2011 21:45:34 +0000 (13:45 -0800)]
Merge branch 'fixes' of ftp.arm.linux.org.uk/pub/linux/arm/kernel/git-cur/linux-2.6-arm

* 'fixes' of http://ftp.arm.linux.org.uk/pub/linux/arm/kernel/git-cur/linux-2.6-arm:
  ARM: 7237/1: PL330: Fix driver freeze
  ARM: 7197/1: errata: Remove SMP dependency for erratum 751472
  ARM: 7196/1: errata: Remove SMP dependency for erratum 720789
  ARM: 7220/1: mmc: mmci: Fixup error handling for dma
  ARM: 7214/1: mmc: mmci: Fixup handling of MCI_STARTBITERR

10 years agoMerge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc
Linus Torvalds [Fri, 30 Dec 2011 21:43:45 +0000 (13:43 -0800)]
Merge branch 'fixes' of git://git./linux/kernel/git/arm/arm-soc

* 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/arm/arm-soc:
  ARM: plat-orion: make gpiochip label unique
  enable uncompress log on cpuimx35sd
  cpuimx35: fix touchscreen support
  cpuimx35sd: fix Kconfig
  clock-imx35: fix reboot in internal boot mode
  dma: MX3_IPU fix depends
  imx_v4_v5_defconfig: update default configuration
  cpuimx25sd: fix Kconfig
  arm/imx: fix cpufreq section mismatch
  ARM:imx:fix pwm period value
  ARM: OMAP: hwmod data: fix iva and mailbox hwmods for OMAP 3

10 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input
Linus Torvalds [Fri, 30 Dec 2011 21:42:41 +0000 (13:42 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/dtor/input

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/dtor/input:
  Input: sentelic - fix retrieving number of buttons
  Input: sentelic - release mutex upon register write failure

10 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/sage/ceph...
Linus Torvalds [Fri, 30 Dec 2011 21:34:22 +0000 (13:34 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/sage/ceph-client

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/sage/ceph-client:
  ceph: disable use of dcache for readdir etc.

10 years agoMerge branch 'v3.2-samsung-fixes-4' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Fri, 30 Dec 2011 21:34:00 +0000 (13:34 -0800)]
Merge branch 'v3.2-samsung-fixes-4' of git://git./linux/kernel/git/kgene/linux-samsung

* 'v3.2-samsung-fixes-4' of git://git.kernel.org/pub/scm/linux/kernel/git/kgene/linux-samsung:
  ARM: EXYNOS: Remove duplicated SROMC static memory mapping
  ARM: SAMSUNG: Fix build error when selecting CPU_FREQ_S3C24XX_DEBUGFS on S3C2440

10 years agoRevert "clockevents: Set noop handler in clockevents_exchange_device()"
Linus Torvalds [Fri, 30 Dec 2011 21:24:40 +0000 (13:24 -0800)]
Revert "clockevents: Set noop handler in clockevents_exchange_device()"

This reverts commit de28f25e8244c7353abed8de0c7792f5f883588c.

It results in resume problems for various people. See for example

  http://thread.gmane.org/gmane.linux.kernel/1233033
  http://thread.gmane.org/gmane.linux.kernel/1233389
  http://thread.gmane.org/gmane.linux.kernel/1233159
  http://thread.gmane.org/gmane.linux.kernel/1227868/focus=1230877

and the fedora and ubuntu bug reports

  https://bugzilla.redhat.com/show_bug.cgi?id=767248
  https://bugs.launchpad.net/ubuntu/+source/linux/+bug/904569

which got bisected down to the stable version of this commit.

Reported-by: Jonathan Nieder <jrnieder@gmail.com>
Reported-by: Phil Miller <mille121@illinois.edu>
Reported-by: Philip Langdale <philipl@overt.org>
Reported-by: Tim Gardner <tim.gardner@canonical.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Greg KH <gregkh@suse.de>
Cc: stable@kernel.org # for stable kernels that applied the original
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoMerge git://www.linux-watchdog.org/linux-watchdog
Linus Torvalds [Fri, 30 Dec 2011 20:13:03 +0000 (12:13 -0800)]
Merge git://www.linux-watchdog.org/linux-watchdog

* git://www.linux-watchdog.org/linux-watchdog:
  watchdog: iTCO_wdt.c - problems with newer hardware due to SMI clearing (part 2)
  watchdog: hpwdt: Changes to handle NX secure bit in 32bit path
  watchdog: sp805: Fix section mismatch in ID table.
  watchdog: move coh901327 state holders

10 years agoMerge branch 'iommu/fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/joro...
Linus Torvalds [Fri, 30 Dec 2011 01:36:15 +0000 (17:36 -0800)]
Merge branch 'iommu/fixes' of git://git./linux/kernel/git/joro/iommu

* 'iommu/fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/joro/iommu:
  iommu: Initialize domain->handler in iommu_domain_alloc()

10 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/davem/net
Linus Torvalds [Fri, 30 Dec 2011 01:35:33 +0000 (17:35 -0800)]
Merge git://git./linux/kernel/git/davem/net

* git://git.kernel.org/pub/scm/linux/kernel/git/davem/net:
  packet: fix possible dev refcnt leak when bind fail
  netem: dont call vfree() under spinlock and BH disabled
  netfilter: ctnetlink: fix scheduling while atomic if helper is autoloaded
  netfilter: ctnetlink: fix return value of ctnetlink_get_expect()

10 years agoMerge branch 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Fri, 30 Dec 2011 01:09:16 +0000 (17:09 -0800)]
Merge branch 'perf-urgent-for-linus' of git://git./linux/kernel/git/tip/tip

* 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/tip:
  perf/x86: Fix raw_spin_unlock_irqrestore() usage
  oprofile, arm/sh: Fix oprofile_arch_exit() linkage issue

10 years agoMerge branch 'for-linus' of git://oss.sgi.com/xfs/xfs
Linus Torvalds [Fri, 30 Dec 2011 01:05:45 +0000 (17:05 -0800)]
Merge branch 'for-linus' of git://oss.sgi.com/xfs/xfs

* 'for-linus' of git://oss.sgi.com/xfs/xfs:
  xfs: log all dirty inodes in xfs_fs_sync_fs
  xfs: log the inode in ->write_inode calls for kupdate

10 years agoMerge branch 'for-linus' of git://git.kernel.dk/linux-block
Linus Torvalds [Fri, 30 Dec 2011 00:33:37 +0000 (16:33 -0800)]
Merge branch 'for-linus' of git://git.kernel.dk/linux-block

* 'for-linus' of git://git.kernel.dk/linux-block:
  block: fix blk_queue_end_tag()
  block: re-use existing 'reading' variable instead of checking direction again
  block, cfq: fix empty queue crash caused by request merge

10 years agomm: hugetlb: fix non-atomic enqueue of huge page
Hillf Danton [Wed, 28 Dec 2011 23:57:16 +0000 (15:57 -0800)]
mm: hugetlb: fix non-atomic enqueue of huge page

If a huge page is enqueued under the protection of hugetlb_lock, then the
operation is atomic and safe.

Signed-off-by: Hillf Danton <dhillf@gmail.com>
Reviewed-by: Michal Hocko <mhocko@suse.cz>
Acked-by: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: <stable@vger.kernel.org> [2.6.37+]
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoprocfs: do not confuse jiffies with cputime64_t
Andreas Schwab [Wed, 28 Dec 2011 23:57:15 +0000 (15:57 -0800)]
procfs: do not confuse jiffies with cputime64_t

Commit 2a95ea6c0d129b4 ("procfs: do not overflow get_{idle,iowait}_time
for nohz") did not take into account that one some architectures jiffies
and cputime use different units.

This causes get_idle_time() to return numbers in the wrong units, making
the idle time fields in /proc/stat wrong.

Instead of converting the usec value returned by
get_cpu_{idle,iowait}_time_us to units of jiffies, use the new function
usecs_to_cputime64 to convert it to the correct unit of cputime64_t.

Signed-off-by: Andreas Schwab <schwab@linux-m68k.org>
Acked-by: Michal Hocko <mhocko@suse.cz>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: "Artem S. Tashkinov" <t.artem@mailcity.com>
Cc: Dave Jones <davej@redhat.com>
Cc: Alexey Dobriyan <adobriyan@gmail.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: "Luck, Tony" <tony.luck@intel.com>
Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org>
Cc: Martin Schwidefsky <schwidefsky@de.ibm.com>
Cc: Heiko Carstens <heiko.carstens@de.ibm.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agomm/mempolicy.c: refix mbind_range() vma issue
KOSAKI Motohiro [Wed, 28 Dec 2011 23:57:11 +0000 (15:57 -0800)]
mm/mempolicy.c: refix mbind_range() vma issue

commit 8aacc9f550 ("mm/mempolicy.c: fix pgoff in mbind vma merge") is the
slightly incorrect fix.

Why? Think following case.

1. map 4 pages of a file at offset 0

   [0123]

2. map 2 pages just after the first mapping of the same file but with
   page offset 2

   [0123][23]

3. mbind() 2 pages from the first mapping at offset 2.
   mbind_range() should treat new vma is,

   [0123][23]
     |23|
     mbind vma

   but it does

   [0123][23]
     |01|
     mbind vma

   Oops. then, it makes wrong vma merge and splitting ([01][0123] or similar).

This patch fixes it.

[testcase]
  test result - before the patch

case4: 126: test failed. expect '2,4', actual '2,2,2'
        case5: passed
case6: passed
case7: passed
case8: passed
case_n: 246: test failed. expect '4,2', actual '1,4'

------------[ cut here ]------------
kernel BUG at mm/filemap.c:135!
invalid opcode: 0000 [#4] SMP DEBUG_PAGEALLOC

(snip long bug on messages)

  test result - after the patch

case4: passed
        case5: passed
case6: passed
case7: passed
case8: passed
case_n: passed

  source:  mbind_vma_test.c
============================================================
 #include <numaif.h>
 #include <numa.h>
 #include <sys/mman.h>
 #include <stdio.h>
 #include <unistd.h>
 #include <stdlib.h>
 #include <string.h>

static unsigned long pagesize;
void* mmap_addr;
struct bitmask *nmask;
char buf[1024];
FILE *file;
char retbuf[10240] = "";
int mapped_fd;

char *rubysrc = "ruby -e '\
  pid = %d; \
  vstart = 0x%llx; \
  vend = 0x%llx; \
  s = `pmap -q #{pid}`; \
  rary = []; \
  s.each_line {|line|; \
    ary=line.split(\" \"); \
    addr = ary[0].to_i(16); \
    if(vstart <= addr && addr < vend) then \
      rary.push(ary[1].to_i()/4); \
    end; \
  }; \
  print rary.join(\",\"); \
'";

void init(void)
{
void* addr;
char buf[128];

nmask = numa_allocate_nodemask();
numa_bitmask_setbit(nmask, 0);

pagesize = getpagesize();

sprintf(buf, "%s", "mbind_vma_XXXXXX");
mapped_fd = mkstemp(buf);
if (mapped_fd == -1)
perror("mkstemp "), exit(1);
unlink(buf);

if (lseek(mapped_fd, pagesize*8, SEEK_SET) < 0)
perror("lseek "), exit(1);
if (write(mapped_fd, "\0", 1) < 0)
perror("write "), exit(1);

addr = mmap(NULL, pagesize*8, PROT_NONE,
    MAP_SHARED, mapped_fd, 0);
if (addr == MAP_FAILED)
perror("mmap "), exit(1);

if (mprotect(addr+pagesize, pagesize*6, PROT_READ|PROT_WRITE) < 0)
perror("mprotect "), exit(1);

mmap_addr = addr + pagesize;

/* make page populate */
memset(mmap_addr, 0, pagesize*6);
}

void fin(void)
{
void* addr = mmap_addr - pagesize;
munmap(addr, pagesize*8);

memset(buf, 0, sizeof(buf));
memset(retbuf, 0, sizeof(retbuf));
}

void mem_bind(int index, int len)
{
int err;

err = mbind(mmap_addr+pagesize*index, pagesize*len,
    MPOL_BIND, nmask->maskp, nmask->size, 0);
if (err)
perror("mbind "), exit(err);
}

void mem_interleave(int index, int len)
{
int err;

err = mbind(mmap_addr+pagesize*index, pagesize*len,
    MPOL_INTERLEAVE, nmask->maskp, nmask->size, 0);
if (err)
perror("mbind "), exit(err);
}

void mem_unbind(int index, int len)
{
int err;

err = mbind(mmap_addr+pagesize*index, pagesize*len,
    MPOL_DEFAULT, NULL, 0, 0);
if (err)
perror("mbind "), exit(err);
}

void Assert(char *expected, char *value, char *name, int line)
{
if (strcmp(expected, value) == 0) {
fprintf(stderr, "%s: passed\n", name);
return;
}
else {
fprintf(stderr, "%s: %d: test failed. expect '%s', actual '%s'\n",
name, line,
expected, value);
// exit(1);
}
}

/*
      AAAA
    PPPPPPNNNNNN
    might become
    PPNNNNNNNNNN
    case 4 below
*/
void case4(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

mem_bind(0, 4);
mem_unbind(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("2,4", retbuf, "case4", __LINE__);

fin();
}

/*
       AAAA
 PPPPPPNNNNNN
 might become
 PPPPPPPPPPNN
 case 5 below
*/
void case5(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

mem_bind(0, 2);
mem_bind(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("4,2", retbuf, "case5", __LINE__);

fin();
}

/*
    AAAA
PPPPNNNNXXXX
might become
PPPPPPPPPPPP 6
*/
void case6(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

mem_bind(0, 2);
mem_bind(4, 2);
mem_bind(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("6", retbuf, "case6", __LINE__);

fin();
}

/*
    AAAA
PPPPNNNNXXXX
might become
PPPPPPPPXXXX 7
*/
void case7(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

mem_bind(0, 2);
mem_interleave(4, 2);
mem_bind(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("4,2", retbuf, "case7", __LINE__);

fin();
}

/*
    AAAA
PPPPNNNNXXXX
might become
PPPPNNNNNNNN 8
*/
void case8(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

mem_bind(0, 2);
mem_interleave(4, 2);
mem_interleave(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("2,4", retbuf, "case8", __LINE__);

fin();
}

void case_n(void)
{
init();
sprintf(buf, rubysrc, getpid(), mmap_addr, mmap_addr+pagesize*6);

/* make redundunt mappings [0][1234][34][7] */
mmap(mmap_addr + pagesize*4, pagesize*2, PROT_READ|PROT_WRITE,
     MAP_FIXED|MAP_SHARED, mapped_fd, pagesize*3);

/* Expect to do nothing. */
mem_unbind(2, 2);

file = popen(buf, "r");
fread(retbuf, sizeof(retbuf), 1, file);
Assert("4,2", retbuf, "case_n", __LINE__);

fin();
}

int main(int argc, char** argv)
{
case4();
case5();
case6();
case7();
case8();
case_n();

return 0;
}
=============================================================

Signed-off-by: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com>
Acked-by: Johannes Weiner <hannes@cmpxchg.org>
Cc: Minchan Kim <minchan.kim@gmail.com>
Cc: Caspar Zhang <caspar@casparzhang.com>
Cc: KOSAKI Motohiro <kosaki.motohiro@jp.fujitsu.com>
Cc: Christoph Lameter <cl@linux.com>
Cc: Hugh Dickins <hugh.dickins@tiscali.co.uk>
Cc: Mel Gorman <mel@csn.ul.ie>
Cc: Lee Schermerhorn <lee.schermerhorn@hp.com>
Cc: <stable@vger.kernel.org> [3.1.x]
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agogspca: Fix bulk mode cameras no longer working (regression fix)
Hans de Goede [Thu, 29 Dec 2011 21:09:21 +0000 (19:09 -0200)]
gspca: Fix bulk mode cameras no longer working (regression fix)

The new iso bandwidth calculation code accidentally has broken support
for bulk mode cameras. This has broken the following drivers:
finepix, jeilinj, ovfx2, ov534, ov534_9, se401, sq905, sq905c, sq930x,
stv0680, vicam.

Thix patch fixes this. Fix tested with: se401, sq905, sq905c, stv0680 & vicam
cams.

Signed-off-by: Hans de Goede <hdegoede@redhat.com>
Signed-off-by: Mauro Carvalho Chehab <mchehab@redhat.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoInput: sentelic - fix retrieving number of buttons
Tai-hwa Liang [Thu, 29 Dec 2011 17:47:36 +0000 (09:47 -0800)]
Input: sentelic - fix retrieving number of buttons

Fixing wrong register offset which is used to retrieve the number of buttons
attached to the hardware.

Signed-off-by: Tai-hwa Liang <avatar@sentelic.com>
Signed-off-by: Dmitry Torokhov <dtor@mail.ru>
10 years agoceph: disable use of dcache for readdir etc.
Sage Weil [Thu, 29 Dec 2011 16:05:14 +0000 (08:05 -0800)]
ceph: disable use of dcache for readdir etc.

Ceph attempts to use the dcache to satisfy negative lookups and readdir
when the entire directory contents are in cache.  Disable this behavior
until lingering bugs in this code are shaken out; we'll re-enable these
hooks once things are fully stable.

Signed-off-by: Sage Weil <sage@newdream.net>
10 years agoblock: fix blk_queue_end_tag()
Dan Williams [Thu, 29 Dec 2011 08:16:28 +0000 (09:16 +0100)]
block: fix blk_queue_end_tag()

Commit 5e081591 "block: warn if tag is greater than real_max_depth"
cleaned up blk_queue_end_tag() to warn when the tag is truly invalid
(greater than real_max_depth).  However, it changed behavior in the tag <
max_depth case to not end the request.  Leading to triggering of
BUG_ON(blk_queued_rq(rq)) in the request completion path:

  http://marc.info/?l=linux-kernel&m=132204370518629&w=2

In order to allow blk_queue_resize_tags() to shrink the tag space
blk_queue_end_tag() must always complete tags with a value less than
real_max_depth regardless of the current max_depth.  The comment about
"handling the shrink case" seems to be what prompted changes in this
space, so remove it and BUG on all invalid tags (made even simpler by
Matthew's suggestion to use an unsigned compare).

Signed-off-by: Dan Williams <dan.j.williams@intel.com>
Cc: Tao Ma <boyu.mt@taobao.com>
Cc: Matthew Wilcox <matthew@wil.cx>
Reported-by: Meelis Roos <mroos@ut.ee>
Reported-by: Ed Nadolski <edmund.nadolski@intel.com>
Cc: Tejun Heo <tj@kernel.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Jens Axboe <axboe@kernel.dk>
10 years agoARM: EXYNOS: Remove duplicated SROMC static memory mapping
Thomas Abraham [Wed, 28 Dec 2011 06:07:32 +0000 (15:07 +0900)]
ARM: EXYNOS: Remove duplicated SROMC static memory mapping

SROMC static memory mapping is included in the common s5p initialization
code. Hence, remove the duplicated SROMC static memory mapping for EXYNOS.

Signed-off-by: Thomas Abraham <thomas.abraham@linaro.org>
Cc: stable@kernel.org
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
10 years agoARM: SAMSUNG: Fix build error when selecting CPU_FREQ_S3C24XX_DEBUGFS on S3C2440
Denis Kuzmenko [Wed, 28 Dec 2011 05:04:51 +0000 (14:04 +0900)]
ARM: SAMSUNG: Fix build error when selecting CPU_FREQ_S3C24XX_DEBUGFS on S3C2440

Following is happened when CONFIG_CPU_FREQ_S3C24XX_DEBUGFS
is selected without building of s3c2410-iotiming.c file:

arch/arm/mach-s3c2440/built-in.o:(.data+0x38c): undefined reference to `s3c2410_iotiming_debugfs

Basically, the CONFIG_S3C2410_IOTIMING is not selected for
MACH_MINI2440. Because the s3c2410-iotiming.c is not ever
compiled and enabling CONFIG_CPU_FREQ_S3C24XX_DEBUGFS option
caused undefined reference to s3c2410_iotiming_debugfs()
defined in that file.  The s3c2410_iotiming_debugfs defined
as NULL for this case.

Signed-off-by: Denis Kuzmenko <linux@solonet.org.ua>
Cc: stable@kernel.org
[kgene.kim@samsung.com: removed useless changes]
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
10 years agopacket: fix possible dev refcnt leak when bind fail
Wei Yongjun [Wed, 28 Dec 2011 03:32:41 +0000 (22:32 -0500)]
packet: fix possible dev refcnt leak when bind fail

If bind is fail when bind is called after set PACKET_FANOUT
sock option, the dev refcnt will leak.

Signed-off-by: Wei Yongjun <yongjun_wei@trendmicro.com.cn>
Signed-off-by: David S. Miller <davem@davemloft.net>
10 years agowatchdog: iTCO_wdt.c - problems with newer hardware due to SMI clearing (part 2)
Wim Van Sebroeck [Mon, 26 Dec 2011 14:23:51 +0000 (15:23 +0100)]
watchdog: iTCO_wdt.c - problems with newer hardware due to SMI clearing (part 2)

Redhat Bugzilla: Bug 727875 - TCO_EN bit is disabled by TCO driver

The previous patch breaks reset watchdog behaviour on the older hardware.
It is therefor better to make sure that the behaviour for older hardware (<=ICH5 or
6300ESB) is preserved and that the behaviour for newer hardware is changed.
We therefor use the iTCO_version to see if we need the clearing of the SMI_TCO_EN
bit in the SMI_EN register.

So the new behaviour becomes:
turn_SMI_watchdog_clear_off=0 -> Do not turn off SMI clearing watchdog.
turn_SMI_watchdog_clear_off=1 -> Turn off SMI clearing watchdog when iTCO_version=1
 (ICHO till ICH5 + 6300ESB only)
turn_SMI_watchdog_clear_off=2 -> Turn off SMI clearing watchdog.

Signed-off-by: Wim Van Sebroeck <wim@iguana.be>
10 years agodrm/i915: Disable RC6 on Sandybridge by default
Keith Packard [Tue, 27 Dec 2011 01:02:11 +0000 (17:02 -0800)]
drm/i915: Disable RC6 on Sandybridge by default

RC6 fails again.

> I found my system freeze mostly during starting up X and KDE. Sometimes it
> works for some minutes, sometimes it freezes immediatly. When the freeze
> happens, everything is dead (even the reset button does not work, I need to
> power cycle).

> I disabled RC6, and my system runs wonderfully.

> The system is a Z68 Pro board with Sandybridge i5-2500K processor, 8
> GB of RAM and UEFI firmware.

Reported-by: Kai Krakow <hurikhan77@gmail.com>
Signed-off-by: Keith Packard <keithp@keithp.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agodrm/i915: Disable semaphores by default on SNB
Keith Packard [Tue, 27 Dec 2011 01:02:10 +0000 (17:02 -0800)]
drm/i915: Disable semaphores by default on SNB

Semaphores still cause problems on some machines:

> From Udo Steinberg:
>
> With Linux-3.2-rc6 I'm frequently seeing GPU hangs when large amounts of
> text scroll in an xterm, such as when extracting a tar archive. Such as this
> one (note the timestamps):
>
>  I can reproduce it fairly easily with something
>  as simple as:
>
>   while true; do dmesg; done

This patch turns them off on SNB while leaving them on for IVB.

Reported-by: Udo Steinberg <udo@hypervisor.org>
Cc: Daniel Vetter <daniel@ffwll.ch>
Cc: Eugeni Dodonov <eugeni@dodonov.net>
Signed-off-by: Keith Packard <keithp@keithp.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agoMerge branch 'kvm-updates/3.2' of git://git.kernel.org/pub/scm/virt/kvm/kvm
Linus Torvalds [Mon, 26 Dec 2011 21:17:00 +0000 (13:17 -0800)]
Merge branch 'kvm-updates/3.2' of git://git./virt/kvm/kvm

* 'kvm-updates/3.2' of git://git.kernel.org/pub/scm/virt/kvm/kvm:
  KVM: PPC: e500: include linux/export.h
  KVM: PPC: fix kvmppc_start_thread() for CONFIG_SMP=N
  KVM: PPC: protect use of kvmppc_h_pr
  KVM: PPC: move compute_tlbie_rb to book3s_64 common header
  KVM: Don't automatically expose the TSC deadline timer in cpuid
  KVM: Device assignment permission checks
  KVM: Remove ability to assign a device without iommu support
  KVM: x86: Prevent starting PIT timers in the absence of irqchip support

10 years agoMerge tag 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ieee1394/linux1394
Linus Torvalds [Mon, 26 Dec 2011 20:46:17 +0000 (12:46 -0800)]
Merge tag 'for-linus' of git://git./linux/kernel/git/ieee1394/linux1394

post 3.2-rc7 pull request

* tag 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ieee1394/linux1394:
  MAINTAINERS: firewire git URL update

10 years agovfs: fix handling of lock allocation failure in lease-break case
Linus Torvalds [Mon, 26 Dec 2011 18:25:26 +0000 (10:25 -0800)]
vfs: fix handling of lock allocation failure in lease-break case

Bruce Fields notes that commit 778fc546f749 ("locks: fix tracking of
inprogress lease breaks") introduced a possible error pointer
dereference on failure to allocate memory.  locks_conflict() will
dereference the passed-in new lease lock structure that may be an error pointer.

This means an open (without O_NONBLOCK set) on a file with a lease
applied (generally only done when Samba or nfsd (with v4) is running)
could crash if a kmalloc() fails.

So instead of playing games with IS_ERROR() all over the place, just
check the allocation failure early.  That makes the code more
straightforward, and avoids this possible bad pointer dereference.

Based-on-patch-by: J. Bruce Fields <bfields@redhat.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
10 years agowatchdog: hpwdt: Changes to handle NX secure bit in 32bit path
Mingarelli, Thomas [Mon, 7 Nov 2011 09:59:00 +0000 (10:59 +0100)]
watchdog: hpwdt: Changes to handle NX secure bit in 32bit path

This patch makes use of the set_memory_x() kernel API in order
to make necessary BIOS calls to source NMIs.

This is needed for SLES11 SP2 and the latest upstream kernel as it appears
the NX Execute Disable has grown in its control.

Signed-off by: Thomas Mingarelli <thomas.mingarelli@hp.com>
Signed-off by: Wim Van Sebroeck <wim@iguana.be>
Cc: stable@kernel.org
10 years agowatchdog: sp805: Fix section mismatch in ID table.
Nick Bowler [Mon, 19 Dec 2011 16:22:36 +0000 (11:22 -0500)]
watchdog: sp805: Fix section mismatch in ID table.

The AMBA ID table is marked as __initdata, yet it is referenced by the
driver struct which is not.  This causes a (somewhat unhelpful) section
mismatch warning:

  WARNING: drivers/watchdog/sp805_wdt.o(.data+0x4c): Section mismatch in
           reference from the variable sp805_wdt_driver to the (unknown
           reference) .init.data:(unknown)

Fix this by removing the annotation.

Signed-off-by: Nick Bowler <nbowler@elliptictech.com>
Signed-off-by: Wim Van Sebroeck <wim@iguana.be>
10 years agowatchdog: move coh901327 state holders
Linus Walleij [Mon, 3 Oct 2011 08:52:58 +0000 (10:52 +0200)]
watchdog: move coh901327 state holders

The state holders used in the PM path of the drivers report as
unused variables when compiling without CONFIG_PM so let's
move them inside CONFIG_PM.

Signed-off-by: Linus Walleij <linus.walleij@linaro.org>
Signed-off-by: Wim Van Sebroeck <wim@iguana.be>
10 years agoKVM: PPC: e500: include linux/export.h
Scott Wood [Tue, 20 Dec 2011 14:43:45 +0000 (14:43 +0000)]
KVM: PPC: e500: include linux/export.h

This is required for THIS_MODULE.  We recently stopped acquiring
it via some other header.

Signed-off-by: Scott Wood <scottwood@freescale.com>
Signed-off-by: Alexander Graf <agraf@suse.de>
10 years agoKVM: PPC: fix kvmppc_start_thread() for CONFIG_SMP=N
Michael Neuling [Thu, 10 Nov 2011 16:03:20 +0000 (16:03 +0000)]
KVM: PPC: fix kvmppc_start_thread() for CONFIG_SMP=N

Currently kvmppc_start_thread() tries to wake other SMT threads via
xics_wake_cpu().  Unfortunately xics_wake_cpu only exists when
CONFIG_SMP=Y so when compiling with CONFIG_SMP=N we get:

  arch/powerpc/kvm/built-in.o: In function `.kvmppc_start_thread':
  book3s_hv.c:(.text+0xa1e0): undefined reference to `.xics_wake_cpu'

The following should be fine since kvmppc_start_thread() shouldn't
called to start non-zero threads when SMP=N since threads_per_core=1.

Signed-off-by: Michael Neuling <mikey@neuling.org>
Signed-off-by: Alexander Graf <agraf@suse.de>
10 years agoKVM: PPC: protect use of kvmppc_h_pr
Andreas Schwab [Tue, 8 Nov 2011 07:17:39 +0000 (07:17 +0000)]
KVM: PPC: protect use of kvmppc_h_pr

kvmppc_h_pr is only available if CONFIG_KVM_BOOK3S_64_PR.

Signed-off-by: Andreas Schwab <schwab@linux-m68k.org>
Signed-off-by: Alexander Graf <agraf@suse.de>
10 years agoKVM: PPC: move compute_tlbie_rb to book3s_64 common header
Andreas Schwab [Tue, 8 Nov 2011 07:08:52 +0000 (07:08 +0000)]
KVM: PPC: move compute_tlbie_rb to book3s_64 common header

compute_tlbie_rb is only used on ppc64 and cannot be compiled on ppc32.

Signed-off-by: Andreas Schwab <schwab@linux-m68k.org>
Signed-off-by: Alexander Graf <agraf@suse.de>
10 years agoKVM: Don't automatically expose the TSC deadline timer in cpuid
Jan Kiszka [Wed, 21 Dec 2011 11:28:29 +0000 (12:28 +0100)]
KVM: Don't automatically expose the TSC deadline timer in cpuid

Unlike all of the other cpuid bits, the TSC deadline timer bit is set
unconditionally, regardless of what userspace wants.

This is broken in several ways:
 - if userspace doesn't use KVM_CREATE_IRQCHIP, and doesn't emulate the TSC
   deadline timer feature, a guest that uses the feature will break
 - live migration to older host kernels that don't support the TSC deadline
   timer will cause the feature to be pulled from under the guest's feet;
   breaking it
 - guests that are broken wrt the feature will fail.

Fix by not enabling the feature automatically; instead report it to userspace.
Because the feature depends on KVM_CREATE_IRQCHIP, which we cannot guarantee
will be called, we expose it via a KVM_CAP_TSC_DEADLINE_TIMER and not
KVM_GET_SUPPORTED_CPUID.

Fixes the Illumos guest kernel, which uses the TSC deadline timer feature.

[avi: add the KVM_CAP + documentation]

Reported-by: Alexey Zaytsev <alexey.zaytsev@gmail.com>
Tested-by: Alexey Zaytsev <alexey.zaytsev@gmail.com>
Signed-off-by: Jan Kiszka <jan.kiszka@siemens.com>
Signed-off-by: Avi Kivity <avi@redhat.com>
10 years agoKVM: Device assignment permission checks
Alex Williamson [Wed, 21 Dec 2011 04:59:09 +0000 (21:59 -0700)]
KVM: Device assignment permission checks

Only allow KVM device assignment to attach to devices which:

 - Are not bridges
 - Have BAR resources (assume others are special devices)
 - The user has permissions to use

Assigning a bridge is a configuration error, it's not supported, and
typically doesn't result in the behavior the user is expecting anyway.
Devices without BAR resources are typically chipset components that
also don't have host drivers.  We don't want users to hold such devices
captive or cause system problems by fencing them off into an iommu
domain.  We determine "permission to use" by testing whether the user
has access to the PCI sysfs resource files.  By default a normal user
will not have access to these files, so it provides a good indication
that an administration agent has granted the user access to the device.

[Yang Bai: add missing #include]
[avi: fix comment style]

Signed-off-by: Alex Williamson <alex.williamson@redhat.com>
Signed-off-by: Yang Bai <hamo.by@gmail.com>
Signed-off-by: Marcelo Tosatti <mtosatti@redhat.com>
10 years agoKVM: Remove ability to assign a device without iommu support
Alex Williamson [Wed, 21 Dec 2011 04:59:03 +0000 (21:59 -0700)]
KVM: Remove ability to assign a device without iommu support

This option has no users and it exposes a security hole that we
can allow devices to be assigned without iommu protection.  Make
KVM_DEV_ASSIGN_ENABLE_IOMMU a mandatory option.

Signed-off-by: Alex Williamson <alex.williamson@redhat.com>
Signed-off-by: Marcelo Tosatti <mtosatti@redhat.com>
10 years agoKVM: x86: Prevent starting PIT timers in the absence of irqchip support
Jan Kiszka [Wed, 14 Dec 2011 18:25:13 +0000 (19:25 +0100)]
KVM: x86: Prevent starting PIT timers in the absence of irqchip support

User space may create the PIT and forgets about setting up the irqchips.
In that case, firing PIT IRQs will crash the host:

BUG: unable to handle kernel NULL pointer dereference at 0000000000000128
IP: [<ffffffffa10f6280>] kvm_set_irq+0x30/0x170 [kvm]
...
Call Trace:
 [<ffffffffa11228c1>] pit_do_work+0x51/0xd0 [kvm]
 [<ffffffff81071431>] process_one_work+0x111/0x4d0
 [<ffffffff81071bb2>] worker_thread+0x152/0x340
 [<ffffffff81075c8e>] kthread+0x7e/0x90
 [<ffffffff815a4474>] kernel_thread_helper+0x4/0x10

Prevent this by checking the irqchip mode before starting a timer. We
can't deny creating the PIT if the irqchips aren't set up yet as
current user land expects this order to work.

Signed-off-by: Jan Kiszka <jan.kiszka@siemens.com>
Signed-off-by: Marcelo Tosatti <mtosatti@redhat.com>