ARM: OMAP2+: edma: clear events in edma_start()
This patch fixes an issue where a DMA channel can erroneously process an
event generated by a previous transfer. A failure case is where DMA is
being used for SPI transmit and receive channels on OMAP L138. In this
case there is a single bit that controls all event generation from the
SPI peripheral. Therefore it is possible that between when edma_stop()
has been called for the transmit channel on a previous transfer and
edma_start() is called for the transmit channel on a subsequent
transfer, that a transmit event has been generated.
The fix is to clear events in edma_start(). This prevents false events
from being processed when events are enabled for that channel.
Signed-off-by: Brian Niebuhr <bniebuhr@efjohnson.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
This patch fixes an issue where a DMA channel can erroneously process an
event generated by a previous transfer. A failure case is where DMA is
being used for SPI transmit and receive channels on OMAP L138. In this
case there is a single bit that controls all event generation from the
SPI peripheral. Therefore it is possible that between when edma_stop()
has been called for the transmit channel on a previous transfer and
edma_start() is called for the transmit channel on a subsequent
transfer, that a transmit event has been generated.
The fix is to clear events in edma_start(). This prevents false events
from being processed when events are enabled for that channel.
Signed-off-by: Brian Niebuhr <bniebuhr@efjohnson.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: OMAP2+: edma: clear interrupt status for interrupt enabled channels only
Currently, the ISR in the EDMA driver clears the pending interrupt for all
channels without regard to whether that channel has a registered callback
or not.
This patch fixes the issue by making the ISR clear the interrupts only for
those channels which have interrupt enabled. The channels which are allocated
for the purpose of being polled on by the accelerator will not have a callback
function provided and so will not have IER (interrupt enable register) bits set.
Signed-off-by: Anuj Aggarwal <anuj.aggarwal@ti.com>
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
CC: Archith John Bency <archith@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Currently, the ISR in the EDMA driver clears the pending interrupt for all
channels without regard to whether that channel has a registered callback
or not.
This patch fixes the issue by making the ISR clear the interrupts only for
those channels which have interrupt enabled. The channels which are allocated
for the purpose of being polled on by the accelerator will not have a callback
function provided and so will not have IER (interrupt enable register) bits set.
Signed-off-by: Anuj Aggarwal <anuj.aggarwal@ti.com>
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
CC: Archith John Bency <archith@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: OMAP2+: edma: fix coding style issue related to breaking lines
In the edma driver, most of the long lines in 'if condition' are
broken after the logical operator '&&' except two instances.
This patch fixes that to bring consistency across the file.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
In the edma driver, most of the long lines in 'if condition' are
broken after the logical operator '&&' except two instances.
This patch fixes that to bring consistency across the file.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: OMAP2+: am335x: correct McASP0 pin mux detail
McASP0 AXR3 pin mux-mode was incorrect specified in mux file. This
patch corrects the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
McASP0 AXR3 pin mux-mode was incorrect specified in mux file. This
patch corrects the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: OMAP2+: am335x: Add method to read config data from daughter board
Patch adds support to read config data held in daughter board eeprom
and updates the corresponding sections accordingly.
Signed-off-by: Shankarmurthy, Akshay <akshay.s@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Patch adds support to read config data held in daughter board eeprom
and updates the corresponding sections accordingly.
Signed-off-by: Shankarmurthy, Akshay <akshay.s@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: OMAP2+: am33xx: fix serial mux warnings for am33xx
The patch removes below warning in serial mux setup on AM335x platform
[ 0.162052] _omap_mux_get_by_name: Could not find signal
uart1_cts.uart1_cts
[ 0.169437] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.176384] _omap_mux_get_by_name: Could not find signal
uart2_cts.uart2_cts
[ 0.183735] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.190663] _omap_mux_get_by_name: Could not find signal
uart3_cts_rctx.uart3_cts_rctx
[ 0.198926] omap_hwmod_mux_init: Could not allocate device mux entry
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
The patch removes below warning in serial mux setup on AM335x platform
[ 0.162052] _omap_mux_get_by_name: Could not find signal
uart1_cts.uart1_cts
[ 0.169437] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.176384] _omap_mux_get_by_name: Could not find signal
uart2_cts.uart2_cts
[ 0.183735] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.190663] _omap_mux_get_by_name: Could not find signal
uart3_cts_rctx.uart3_cts_rctx
[ 0.198926] omap_hwmod_mux_init: Could not allocate device mux entry
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
input: TSC: Add suspend/resume feature for TSC
This patch adds support for suspend/resume feature in
touchscreen.
Since touchscreen is in wakeup domain, it can be used
to resume the system.
Signed-off-by: Patil, Rachna <rachna@ti.com>
This patch adds support for suspend/resume feature in
touchscreen.
Since touchscreen is in wakeup domain, it can be used
to resume the system.
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm: omap: am335x:Add ick data in Hwmod for TSC
Add interface clock information pertaining to Touchscreen
in hwmod data.
Signed-off-by: Patil, Rachna <rachna@ti.com>
Add interface clock information pertaining to Touchscreen
in hwmod data.
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm: omap: am335x: Use hwmod data to register TSC
Make changes to register Touchscreen as a platform device
using hwmod data API
Signed-off-by: Patil, Rachna <rachna@ti.com>
Make changes to register Touchscreen as a platform device
using hwmod data API
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:am335x: Correct interrupt signal for TSC
Interrupt signal entry in HwMod data of TSC has been corrected
Signed-off-by: Patil, Rachna <rachna@ti.com>
Interrupt signal entry in HwMod data of TSC has been corrected
Signed-off-by: Patil, Rachna <rachna@ti.com>
pwm:ehrpwm - Fix duty cycle inversion eHRPWM wave.
Patch fixes the ON and OFF period inversion in PWM wave.
Action qualifier register settings causes switching PWM wave to OFF
period when counter reaches zero and to ON period on counter reaches
compare value. Because of this inversion in duty cycle was observed.
Signed-off-by: Shankarmurthy, Akshay <akshay.s@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Patch fixes the ON and OFF period inversion in PWM wave.
Action qualifier register settings causes switching PWM wave to OFF
period when counter reaches zero and to ON period on counter reaches
compare value. Because of this inversion in duty cycle was observed.
Signed-off-by: Shankarmurthy, Akshay <akshay.s@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
pwm: corrects return values to handle error situation
This patch fixes
1. Proper return values for pwm framework API's.
2. Return values for SYSFS interface.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
This patch fixes
1. Proper return values for pwm framework API's.
2. Return values for SYSFS interface.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
pwm: fix division by zero error.
Divisor should be checked before dividing for non-zero value. This patch
fixes the same and added debug messages.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Divisor should be checked before dividing for non-zero value. This patch
fixes the same and added debug messages.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
pwm: Correct the "request" SYSFS interface
This patch changes handling of "request" SYSFS interface
1. Request for PWM device
from "cat request" to "echo 1 > request"
2. Release for PWM device
from "echo 1 > request" to "echo 0 > request"
3.Information on reading "request" SYSFS interface
if pwm device used, "<pwm device> is used by which <application>"
or if pwm device is free, "<pwm device> is free"
Also this patch has the fix for hanging of the system on subsequent
request/release operation after release of unused device. This is
because, release of unused device causes mutex to hold in a locked state
and further request for the mutex would hang.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
This patch changes handling of "request" SYSFS interface
1. Request for PWM device
from "cat request" to "echo 1 > request"
2. Release for PWM device
from "echo 1 > request" to "echo 0 > request"
3.Information on reading "request" SYSFS interface
if pwm device used, "<pwm device> is used by which <application>"
or if pwm device is free, "<pwm device> is free"
Also this patch has the fix for hanging of the system on subsequent
request/release operation after release of unused device. This is
because, release of unused device causes mutex to hold in a locked state
and further request for the mutex would hang.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
usb: defconfig: enable file_storage gadget as module
Enabled file stoarge gadget also as seeing lot of instability with
mass storage gadget.
Enabled file stoarge gadget also as seeing lot of instability with
mass storage gadget.
usb: musb: Let PIO option visible in menuconfig
PIO option is not visible while selecting modules. Fixing the same.
PIO option is not visible while selecting modules. Fixing the same.
usb: musb: cppi41: fall back to pio for interrupt based transfers
System hang is observed as Tx FIFO is never empty for interrupt based transfer
and so system goes into loop checking for txFifo empty.
Fixing by using pio for such transfer where length is less than 128 bytes
System hang is observed as Tx FIFO is never empty for interrupt based transfer
and so system goes into loop checking for txFifo empty.
Fixing by using pio for such transfer where length is less than 128 bytes
Revert "usb: musb_gadget: cppi41: Use pio for interrupt transfer"
This reverts commit fe055e40c74fb24d8d86aae49b0f9a15a25f388b.
This patch is breaking RNDIS ping test with XP PC.
This reverts commit fe055e40c74fb24d8d86aae49b0f9a15a25f388b.
This patch is breaking RNDIS ping test with XP PC.
arm:omap:am33xx: Register SGX device
If SGX is enabled in hardware (information obtained from
device feature register) register SGX platform device.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
If SGX is enabled in hardware (information obtained from
device feature register) register SGX platform device.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: Check device features
Read device feature register and record features
on SOC. Currently only SGX is checked.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Read device feature register and record features
on SOC. Currently only SGX is checked.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
ARM: OMAP: AM33XX: Keep the CLKDIV32K module enabled
One of the 32K clocks for the RTCSS is obtained from
CLKDIV32K module. Till the dependencies are fully sorted
out in the clock tree keep this module enabled.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
One of the 32K clocks for the RTCSS is obtained from
CLKDIV32K module. Till the dependencies are fully sorted
out in the clock tree keep this module enabled.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
arm: omap: am33xx: update TSC hwmod data
Sysconfig register bits are updated for TSC
hwmod. TSC supports idle mode at bit position 2&3,
hence following omap4 IP's.
Signed-off-by: Patil, Rachna <rachna@ti.com>
Sysconfig register bits are updated for TSC
hwmod. TSC supports idle mode at bit position 2&3,
hence following omap4 IP's.
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:am33xx : register i2c2 for beaglebone
Beaglebone uses i2c2 to detect expansion cards. This patch registers
i2c2 device along with setting up pin-muxes
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Beaglebone uses i2c2 to detect expansion cards. This patch registers
i2c2 device along with setting up pin-muxes
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:am33xx - add i2c2 hwmod data
i2c2 buss is used in beaglebone board. Add necessary i2c2 hwmod data
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
i2c2 buss is used in beaglebone board. Add necessary i2c2 hwmod data
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:am33xx - add missing i2c pin mus details
Add all references to i2c pins in mux file. These pins may be used in
different board configurations.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Add all references to i2c pins in mux file. These pins may be used in
different board configurations.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
PWM:eCAP: Reconfigure only if frequency has changed
PWM needs to be reconfigured during cpufreq transition
only if input clock frequency has changed. Change notifier
accrodingly.
This prevents flickering during cpufreq transitions. It is
suspected that as PWM frequency is set to a low value,
reconfiguring PWM is causing flicker observable to naked
eye. Irrespective of this fact, this change removes
unnecessary reconfiguration of PWM.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
PWM needs to be reconfigured during cpufreq transition
only if input clock frequency has changed. Change notifier
accrodingly.
This prevents flickering during cpufreq transitions. It is
suspected that as PWM frequency is set to a low value,
reconfiguring PWM is causing flicker observable to naked
eye. Irrespective of this fact, this change removes
unnecessary reconfiguration of PWM.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm: omap: am335x: corrected mmc1 pin mux naming
Signed-off-by: Patil, Rachna <rachna@ti.com>
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:am335x:remove duplicated code in mux file
GPMC_CLK was declared twice, corrected the same
Signed-off-by: Patil, Rachna <rachna@ti.com>
GPMC_CLK was declared twice, corrected the same
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm: omap: am335x: Add gpio entries in mux file
This pacth adds gpio in mode7 for all
the mux entries of am335x
Signed-off-by: Patil, Rachna <rachna@ti.com>
This pacth adds gpio in mode7 for all
the mux entries of am335x
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:am33xx - drive Haptics motor using eHRPWM's sysfs interface.
Since Haptics doesn't have its own driver(yet), currently Haptics can
be tested using eHRPWM's sysfs interface.
This patch adds support for driving Haptics motor connected to
eHRPWM Instance 2 channel 2.
According to datasheet, the Haptic Motors Max RPM is 15000 RPM. Driving
the Motor above MAX RPM may spoil the Motor.
This patch limits the eHRPWM max freq to 250Hz. This can be changed
from platform data.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Since Haptics doesn't have its own driver(yet), currently Haptics can
be tested using eHRPWM's sysfs interface.
This patch adds support for driving Haptics motor connected to
eHRPWM Instance 2 channel 2.
According to datasheet, the Haptic Motors Max RPM is 15000 RPM. Driving
the Motor above MAX RPM may spoil the Motor.
This patch limits the eHRPWM max freq to 250Hz. This can be changed
from platform data.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
am335x: regulator: tps65217 fix for BeagleBone A3 and greater
This patch fixes the problem that tps65217B regulator support
is applicable only for BeagleBone A3 and greater. And tps65217B
regulator is not applicable for the BeagleBone's whose revision
verion is < A3
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
This patch fixes the problem that tps65217B regulator support
is applicable only for BeagleBone A3 and greater. And tps65217B
regulator is not applicable for the BeagleBone's whose revision
verion is < A3
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
ARM: OMAP: AM33XX: Disable self-refresh upon resume
During suspend, we put the SDRAM in self-refresh mode.
If we don't clear this mode in the resume path SDRAM
can automatically enter self-refresh when the CPU is idle.
While this looks to be right behavior, this causes flickers
on the LCD specifically on ICS. So, when coming out of
suspend disable self-refresh mode.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
During suspend, we put the SDRAM in self-refresh mode.
If we don't clear this mode in the resume path SDRAM
can automatically enter self-refresh when the CPU is idle.
While this looks to be right behavior, this causes flickers
on the LCD specifically on ICS. So, when coming out of
suspend disable self-refresh mode.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
video:da8xx: Reverting patch to use dma_alloc_coherent instead
get_free_pages
Reverting "video:da8xx: Replace dma_alloc_coherent tp get_free_pages
(f482ac5b63e0fc84c546cb463e4dea5e02682516)" as SGX model fails do alloc
of DMA memory using get_free_pages. This patch is dependent on "AM335x:
Add option to configure CONSISTENT_DMA_SIZE" patch to increase
CONSISTENT_DMA_SIZE for successful allocation of memory >2MB.
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
get_free_pages
Reverting "video:da8xx: Replace dma_alloc_coherent tp get_free_pages
(f482ac5b63e0fc84c546cb463e4dea5e02682516)" as SGX model fails do alloc
of DMA memory using get_free_pages. This patch is dependent on "AM335x:
Add option to configure CONSISTENT_DMA_SIZE" patch to increase
CONSISTENT_DMA_SIZE for successful allocation of memory >2MB.
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
AM335x: Add option to configure CONSISTENT_DMA_SIZE
This is temporary workaround patch required for SGX model as it fails to
get DMA memory using get_free_pages. So patch configures CONSISTENT_DMA_SIZE
via configurable option FB_DA8XX_CONSISTENT_DMA_SIZE.
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
This is temporary workaround patch required for SGX model as it fails to
get DMA memory using get_free_pages. So patch configures CONSISTENT_DMA_SIZE
via configurable option FB_DA8XX_CONSISTENT_DMA_SIZE.
Signed-off-by: Manjunathappa, Prakash <prakash.pm@ti.com>
ARM: OMAP: am335xevm: Fix pruss clock alias error
Due to changes in clock tree the name of the clock has
changed, so TEMP create new alias entry for pruss.
NOTE: Revisit this commit/patch, based on final clock tree.
Due to changes in clock tree the name of the clock has
changed, so TEMP create new alias entry for pruss.
NOTE: Revisit this commit/patch, based on final clock tree.
ARM: OMAP: io: Add check_revision/feature calls for am33xx_init
ARM: OMAP: id: Add missing break statement in omap3xxx_check_revision
Add missing break statement, which somehow got removed from
omap3xxx_check_revision function inside AM335x switch case,
resulting into wrong omap/cpu_rev configuration.
Add missing break statement, which somehow got removed from
omap3xxx_check_revision function inside AM335x switch case,
resulting into wrong omap/cpu_rev configuration.
input: touchscreen: fix TSC related build warning
Signed-off-by: Patil, Rachna <rachna@ti.com>
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:am33xx - LCD flicker removed.
Backlight frequency is reduced to remove LCD flicker issue.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Backlight frequency is reduced to remove LCD flicker issue.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:am33xx - update GPMC hwmod data
SOFT_RESET flag is added in GPMC_SYSCONFIG flags in hwmod data.
Resetting the module causes kernel crash on gpmc_init(). To fix the
crash base address and size has been updated for AM33xx SOC.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
SOFT_RESET flag is added in GPMC_SYSCONFIG flags in hwmod data.
Resetting the module causes kernel crash on gpmc_init(). To fix the
crash base address and size has been updated for AM33xx SOC.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:am33xx - GPMC timings
Default timing causes issues with OOB data corruption on reading and
causes UBIFS torture test. To resolve the above issue, NAND was tested
with different timings and optimal timings were adapted after repeated
tests and trials.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Default timing causes issues with OOB data corruption on reading and
causes UBIFS torture test. To resolve the above issue, NAND was tested
with different timings and optimal timings were adapted after repeated
tests and trials.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
NAND : Add data memory barrier to enforce ordering
When using delay loop for wait states, need to ascertain that
the write to OMAP HW register is reflected befor the delay
loop starts. This patch adds a dmb() instruction to this effect.
Without this fix, NAND read failures reported with mtd_oobtests.
Signed-off-by: Sriramakrishnan <srk@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
When using delay loop for wait states, need to ascertain that
the write to OMAP HW register is reflected befor the delay
loop starts. This patch adds a dmb() instruction to this effect.
Without this fix, NAND read failures reported with mtd_oobtests.
Signed-off-by: Sriramakrishnan <srk@ti.com>
Signed-off-by: Sriramakrishnan A G <srk@ti.com>
can: d_can: Suspend resume additions
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
am335x: mpu voltage domain tolerance modification
This patch modifies the mpu tolerance to 4% to provide the maximum
voltage limit while requesting for a new voltage. 4% value is taken
from am33xx datasheet
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
This patch modifies the mpu tolerance to 4% to provide the maximum
voltage limit while requesting for a new voltage. 4% value is taken
from am33xx datasheet
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
am335x: Add tps65217 config to am335x def config
This patch adds the tps65217 configuration to am335x_evm_defconfig
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
This patch adds the tps65217 configuration to am335x_evm_defconfig
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
am335x: regulator: Add tps65217 regulator platform data
This patch adds the tps65217 regulator for AM355X, which
is used by the beaglebone. Mainly adds all the consumers
like mpu, core, ddr, usb, rtc and io's.
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
This patch adds the tps65217 regulator for AM355X, which
is used by the beaglebone. Mainly adds all the consumers
like mpu, core, ddr, usb, rtc and io's.
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
regulator: tps65217: Add tps65217 regulator driver
This patch adds tps65217 PMIC as a regulator
The regulator module consists of 3 DCDCs and 4 LDOs. The output
voltages are configurable and are meant to supply power to the
main processor and other components
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
This patch adds tps65217 PMIC as a regulator
The regulator module consists of 3 DCDCs and 4 LDOs. The output
voltages are configurable and are meant to supply power to the
main processor and other components
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
MFD: TPS65217: Add new mfd device for TPS65217
The TPS65217 chip is a power management IC for Portable Navigation Systems
and Tablet Computing devices. It contains the following components:
- Regulators
- White LED
- USB battery charger
This patch adds support for tps65217 mfd device. At this time only
the regulator functionality is made available.
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
The TPS65217 chip is a power management IC for Portable Navigation Systems
and Tablet Computing devices. It contains the following components:
- Regulators
- White LED
- USB battery charger
This patch adds support for tps65217 mfd device. At this time only
the regulator functionality is made available.
Signed-off-by: AnilKumar Ch <anilkumar@ti.com>
ARM: OMAP: AM33XX: Don't enable suspend by default
Leaving the suspend option enabled in the defconfig
leads to a 60 second timeout if the CM3 binary is not
provided. To avoid this, disable suspend for now.
A better solution for this might be exploring the
usage of nowait version of the request_firmware
interface.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Leaving the suspend option enabled in the defconfig
leads to a 60 second timeout if the CM3 binary is not
provided. To avoid this, disable suspend for now.
A better solution for this might be exploring the
usage of nowait version of the request_firmware
interface.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Update the suspend code for DS1
Put SDRAM in self refresh mode when suspending. For now
the reconfiguration of SDRAM is done using fixed values.
The values used are valid for AM335x EVM with DDR2
running @266MHz.
Note: Optimization of the aseembly code will be done
in subsequent patches.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Put SDRAM in self refresh mode when suspending. For now
the reconfiguration of SDRAM is done using fixed values.
The values used are valid for AM335x EVM with DDR2
running @266MHz.
Note: Optimization of the aseembly code will be done
in subsequent patches.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Add EMIF and DDR PHY register offsets and values
When coming out of low power state, the EMIF and DDR
PHY registers need to be restored to the old value.
A naive approach of storing the DDR PHY register values during
suspend and restoring it back during resume will not work
due to a silicon errata related to readback of the DDR PHY
registers.
EMIF registers values can be readback and stored but for
now we assume that the code is running on AM335x EVM with DDR2
which is configured to run @266MHz.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
When coming out of low power state, the EMIF and DDR
PHY registers need to be restored to the old value.
A naive approach of storing the DDR PHY register values during
suspend and restoring it back during resume will not work
due to a silicon errata related to readback of the DDR PHY
registers.
EMIF registers values can be readback and stored but for
now we assume that the code is running on AM335x EVM with DDR2
which is configured to run @266MHz.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Add an API for obtaining the virt EMIF addr
The low level code for suspend needs the virtual address
of EMIF so that the SDRAM can be put in self-refresh.
Since the emif is ioremapped very early on, add an API
which returns the virtual address of the EMIF address space
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
The low level code for suspend needs the virtual address
of EMIF so that the SDRAM can be put in self-refresh.
Since the emif is ioremapped very early on, add an API
which returns the virtual address of the EMIF address space
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Remove autoidle regs
... since this feature is not supported in the hardware.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
... since this feature is not supported in the hardware.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP3+: dpll: Configure autoidle mode only if its supported
The current DPLL code enables and disables autoidle features
without checking whether the autoidle register is available.
Fix this by putting a check for the existence of the autoidle
register in the DPLL data.
With such a check in place, for DPLLs which do not support this
feature, simply skipping the autoidle_reg entry in the DPLL data
is sufficient.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
The current DPLL code enables and disables autoidle features
without checking whether the autoidle register is available.
Fix this by putting a check for the existence of the autoidle
register in the DPLL data.
With such a check in place, for DPLLs which do not support this
feature, simply skipping the autoidle_reg entry in the DPLL data
is sufficient.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP2: AM33XX: misc hwmod fixes
Some of the hwmods that were initially added to the list
are not complete. Due to missing information like base
address, sysc offset and bitfields definitions, the
registration of these hwmods silently fails.
For now, fix up the hwmods which are needed for proceeding
with system suspend. Note that this file is not complete
at the moment and will most likely require a couple of more
rounds to bring it in line with that has been done for
OMAP3/4.
TODO:
1. Check why RTC requires NO_RESET and NO_IDLE to be set
2. Check why GPMC does not work when SOFTRESET is done
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Some of the hwmods that were initially added to the list
are not complete. Due to missing information like base
address, sysc offset and bitfields definitions, the
registration of these hwmods silently fails.
For now, fix up the hwmods which are needed for proceeding
with system suspend. Note that this file is not complete
at the moment and will most likely require a couple of more
rounds to bring it in line with that has been done for
OMAP3/4.
TODO:
1. Check why RTC requires NO_RESET and NO_IDLE to be set
2. Check why GPMC does not work when SOFTRESET is done
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP2+: hwmod: Add two new sysc_field types
In AM33XX, two new types of SYSCONFIG bitfields are present.
This patch introduces two new sysc_field types to take care
of these new schemes.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
In AM33XX, two new types of SYSCONFIG bitfields are present.
This patch introduces two new sysc_field types to take care
of these new schemes.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP2+: hwmod: Add an API to handle master standby mode
This API is intended to be used by drivers/code that requires
direct manipulation of the MSTANDBY bits in SYSCONFIG registers.
AM33XX low power state transition happens only if some of the
bus masters like EDMA, CPSW and USB have been forced to standby.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
This API is intended to be used by drivers/code that requires
direct manipulation of the MSTANDBY bits in SYSCONFIG registers.
AM33XX low power state transition happens only if some of the
bus masters like EDMA, CPSW and USB have been forced to standby.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP2+: UART: Don't register errata i291 for AM33XX
UART_ERRATA_i291_DMA_FORCEIDLE is not applicable to the
AM33XX family
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
UART_ERRATA_i291_DMA_FORCEIDLE is not applicable to the
AM33XX family
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Fix up header inclusion for baseport patches
cm33xx.h does not need to include any of the kernel headers
and hence remove them.
cminst33xx.c needs to explicitly include common.h to avoid
build breakage
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
cm33xx.h does not need to include any of the kernel headers
and hence remove them.
cminst33xx.c needs to explicitly include common.h to avoid
build breakage
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
ARM: OMAP: AM33XX: Mark the essential clocks as ENABLE_ON_INIT
Some of the clocks will never be disabled from the kernel.
To get an accurate use count for such clocks, mark them
with the ENABLE_ON_INIT flag.
Note: Need to check if there's a better way of doing this.
Maybe there should be a clock_get for such clocks.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Some of the clocks will never be disabled from the kernel.
To get an accurate use count for such clocks, mark them
with the ENABLE_ON_INIT flag.
Note: Need to check if there's a better way of doing this.
Maybe there should be a clock_get for such clocks.
Signed-off-by: Vaibhav Bedia <vaibhav.bedia@ti.com>
Backlight - Brightness scale is changed.
Brightness scale is changed to 0-100, from 0-250.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Brightness scale is changed to 0-100, from 0-250.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Backlight - Removed backlight data related to GPIO
As backlight is enabled through PWM, cleaning up the GPIO based
backlight data.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
As backlight is enabled through PWM, cleaning up the GPIO based
backlight data.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
usb: musb_gadget: cppi41: Use pio for interrupt transfer
Use pio mode for interrupt transfer of size <= 64 byte. We have seen
TxFiFoEmpty workqueue going into infinite loop when a CDC device is
connected to another EVM
Use pio mode for interrupt transfer of size <= 64 byte. We have seen
TxFiFoEmpty workqueue going into infinite loop when a CDC device is
connected to another EVM
arm:omap:pwmss - hwmod data corrected.
HW_MOD data updated for PWMSS
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
HW_MOD data updated for PWMSS
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:elm - hwmod data is corrected
sysconf register details are corrected.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
sysconf register details are corrected.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
pwm-backlight - Enabled in am335x config file
PWM backlight is enabled in am335x defconfig
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
PWM backlight is enabled in am335x defconfig
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:pwm - LCD backlight enabled through PWM.
LCD backlight is provided by PWM signal generated by eCAP. So backlight
brightness can control by changing duty cycle of PWM signal.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
LCD backlight is provided by PWM signal generated by eCAP. So backlight
brightness can control by changing duty cycle of PWM signal.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Backlight: Modify the backlight interface
With the introduction of new PWM Framework, access to any PWM driver
should be done through the Framework. So, Modify the Backlight Interface
to use the PWM Framework APIs.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
With the introduction of new PWM Framework, access to any PWM driver
should be done through the Framework. So, Modify the Backlight Interface
to use the PWM Framework APIs.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:pwm - Platform support for PWMSS
AM335x SOC is having 3 instances of PWMSS, each will be having single
module instances of ePWM, eCAP & eQEP. This patch adds platform support
for ePWM & eCAP modules. Initializes the semaphore for common
configuration space access protection.
Time base module clock enabled for EHRPWM.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
AM335x SOC is having 3 instances of PWMSS, each will be having single
module instances of ePWM, eCAP & eQEP. This patch adds platform support
for ePWM & eCAP modules. Initializes the semaphore for common
configuration space access protection.
Time base module clock enabled for EHRPWM.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:am33xx - enabled PWM in defconfig
eHRPWM and eCAP enabled in am335x config file.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
eHRPWM and eCAP enabled in am335x config file.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:pwm - eCAP & ePWM driver in AM335X
Unline with DA850, where each PWM module has individual clock,
AM335x SOC will be having common clock for ePWM, eCAP & eQEP which comes
under PWMSS instances. Clock gating is happening at configuration space
in PWMSS.
This patch modified eCAP & ePWM driver to support AM335X SOC as follows
1. Updated the clk_get() arguments to access common functional clock in
accordance with platform device id.
2. In AM335X SOC, PWMSS has a common config space for eCAP, ePWM & eQEP.
The clock gating to individual module has done from common config
space.So each module drivers should be able to access the common
configuration space independently. This patch provides a method to
access this common configuration space across each modules
independently. This method involves remapping the common config space
only on the first module in PWMSS. All the other modules in PWMSS uses
this remapped address to access the common configuration space. Clock
gating can be controlled on this common configuration space from
respective module. Protection mechanism is provided by
semaphore. Configuratin space unmapping is happening when the last
module is removed.
3. Config file support added for AM33XX_SOC
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Unline with DA850, where each PWM module has individual clock,
AM335x SOC will be having common clock for ePWM, eCAP & eQEP which comes
under PWMSS instances. Clock gating is happening at configuration space
in PWMSS.
This patch modified eCAP & ePWM driver to support AM335X SOC as follows
1. Updated the clk_get() arguments to access common functional clock in
accordance with platform device id.
2. In AM335X SOC, PWMSS has a common config space for eCAP, ePWM & eQEP.
The clock gating to individual module has done from common config
space.So each module drivers should be able to access the common
configuration space independently. This patch provides a method to
access this common configuration space across each modules
independently. This method involves remapping the common config space
only on the first module in PWMSS. All the other modules in PWMSS uses
this remapped address to access the common configuration space. Clock
gating can be controlled on this common configuration space from
respective module. Protection mechanism is provided by
semaphore. Configuratin space unmapping is happening when the last
module is removed.
3. Config file support added for AM33XX_SOC
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
pwm: - Platform data is placed in common position
Platform_driver_data for eHRPWM module is put to common place to access
the structure irrespective of architecture.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Platform_driver_data for eHRPWM module is put to common place to access
the structure irrespective of architecture.
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
eCAP:PWM: Add device driver support for eCAP module
OMAPL138/DA850 contains three instances of eCAP module.
Each eCAP module has one dedicated pin that can be used either
in capture mode(input) or in PWM mode.
This patch adds eCAP driver support for PWM signal generation.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
OMAPL138/DA850 contains three instances of eCAP module.
Each eCAP module has one dedicated pin that can be used either
in capture mode(input) or in PWM mode.
This patch adds eCAP driver support for PWM signal generation.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
eHRPWM: Add device driver support for ehrpwm module
eHRPWM module can be used to generate wide range of complex
PWM waveforms. Apart from conventional PWM generation, eHRPWM
module supports advanced features such as Trip Zone and Dead Band.
This patch adds device driver support for eHRPWM module.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
eHRPWM module can be used to generate wide range of complex
PWM waveforms. Apart from conventional PWM generation, eHRPWM
module supports advanced features such as Trip Zone and Dead Band.
This patch adds device driver support for eHRPWM module.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
PWM: Add cpu frequency transition support for PWM devices
Implement a generic frequency transition callback for PWM
devices. Generic PWM framework notifies all the PWM devices
currently being used about the frequency transition.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Implement a generic frequency transition callback for PWM
devices. Generic PWM framework notifies all the PWM devices
currently being used about the frequency transition.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
PWM: Add helper APIs and sysfs entries to the PWM Frame Work
1. Add pwm_duty_percent and pwm_frequency attributes to the SYSFS interface
of the PWM Framework. Since, PWM waveform is characterized mainly by
percent duty and the frequency, it is pretty much useful to have these
attributes.
2. Also, period_ns and duty_ns variables have been added to
the pwm_device structure as it might be needed by the PWM driver
functions.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
1. Add pwm_duty_percent and pwm_frequency attributes to the SYSFS interface
of the PWM Framework. Since, PWM waveform is characterized mainly by
percent duty and the frequency, it is pretty much useful to have these
attributes.
2. Also, period_ns and duty_ns variables have been added to
the pwm_device structure as it might be needed by the PWM driver
functions.
Signed-off-by: Natarajan Sugumar <sugumar@ti.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
PWM: Implement a generic PWM framework
Updates the existing PWM-related functions to support multiple and/or
hotplugged PWM devices, and adds a sysfs interface.
spin_lock protection added.
Signed-off-by: Bill Gatliff <bgat@billgatliff.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
Updates the existing PWM-related functions to support multiple and/or
hotplugged PWM devices, and adds a sysfs interface.
spin_lock protection added.
Signed-off-by: Bill Gatliff <bgat@billgatliff.com>
Signed-off-by: Philip, Avinash <avinashphilip@ti.com>
arm:omap:am335x : update MCASP hwmod data
This adds update existing mcasp0 data & adds missing mcasp1 hwmod data
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
This adds update existing mcasp0 data & adds missing mcasp1 hwmod data
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:am335x: correct TPCC hwmod data
This patch adds missing TPTC hwmod data like addr space, 1 mpu irq, etc
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
This patch adds missing TPTC hwmod data like addr space, 1 mpu irq, etc
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
update lpj only if frequency has changed
During scaling up of cpu frequency, loops_per_jiffy
is updated upon invoking PRECHANGE notifier.
If setting to new frequency fails in cpufreq driver,
lpj is left at incorrect value.
Hence update lpj only if cpu frequency is changed,
i.e. upon invoking POSTCHANGE notifier.
Penalty would be that during time period between
changing cpu frequency & invocation of POSTCHANGE
notifier, udelay(x) may not gurantee minimal delay
of 'x' us for frequency scaling up operation.
Perhaps a better solution would be to define
CPUFREQ_ABORTCHANGE & handle accordingly, but then
it would be more intrusive (using ABORTCHANGE may
help drivers also; if any has registered notifier
and expect POST for a PRECHANGE, their needs can
be taken care using ABORT)
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Dave Jones <davej@redhat.com>
During scaling up of cpu frequency, loops_per_jiffy
is updated upon invoking PRECHANGE notifier.
If setting to new frequency fails in cpufreq driver,
lpj is left at incorrect value.
Hence update lpj only if cpu frequency is changed,
i.e. upon invoking POSTCHANGE notifier.
Penalty would be that during time period between
changing cpu frequency & invocation of POSTCHANGE
notifier, udelay(x) may not gurantee minimal delay
of 'x' us for frequency scaling up operation.
Perhaps a better solution would be to define
CPUFREQ_ABORTCHANGE & handle accordingly, but then
it would be more intrusive (using ABORTCHANGE may
help drivers also; if any has registered notifier
and expect POST for a PRECHANGE, their needs can
be taken care using ABORT)
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Dave Jones <davej@redhat.com>
cpufreq:userspace: fix cpu_cur_freq updation
CPU frequency is guranteed to be changed on notifier callback with
CPUFREQ_POSTCHANGE. Notifier callback with CPUFREQ_PRECHANGE does
not gurantee a change in frequency; after it, if cpufreq driver is
unable to change CPU to new frequency. This results in wrong
information being fed to user (if setting CPU frequency fails)
upon doing like,
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
Hence in userspace governer update cpu_cur_freq only if notifier
has been called with POSTCHANGE.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Dave Jones <davej@redhat.com>
CPU frequency is guranteed to be changed on notifier callback with
CPUFREQ_POSTCHANGE. Notifier callback with CPUFREQ_PRECHANGE does
not gurantee a change in frequency; after it, if cpufreq driver is
unable to change CPU to new frequency. This results in wrong
information being fed to user (if setting CPU frequency fails)
upon doing like,
cat /sys/devices/system/cpu/cpu0/cpufreq/scaling_setspeed
Hence in userspace governer update cpu_cur_freq only if notifier
has been called with POSTCHANGE.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Signed-off-by: Dave Jones <davej@redhat.com>
regulator: TPS65910: VDD1 error handling
Proper error handling w.r.t I2C transactions
for setting & getting voltage for VDD1
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Proper error handling w.r.t I2C transactions
for setting & getting voltage for VDD1
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: Enable TPS65910 regulator
Enable TPS65910 regulator
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Enable TPS65910 regulator
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: enable cpufreq
Enable cpufreq by default, also select ondemand and
user space governer, with userspace as default
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Enable cpufreq by default, also select ondemand and
user space governer, with userspace as default
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: dpll mpu clock config helpers
Add set_rate & round_rate for MPU PLL, this is
required to configure MPU PLL for CPUFREQ
Signed-off-by: Afzal Mohammed <afzal@ti.com>
Add set_rate & round_rate for MPU PLL, this is
required to configure MPU PLL for CPUFREQ
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: MPU regulator
TPS65910 VDD1 SMPS is connected to MPU.
Add dummy entries for other regulators.
TODO: Replace dummy regulator entries
with proper ones as required.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
TPS65910 VDD1 SMPS is connected to MPU.
Add dummy entries for other regulators.
TODO: Replace dummy regulator entries
with proper ones as required.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx: OPP table
OPP table for MPU voltage domain
Signed-off-by: Afzal Mohammed <afzal@ti.com>
OPP table for MPU voltage domain
Signed-off-by: Afzal Mohammed <afzal@ti.com>
cpufreq: OMAP: am33xx support
am33xx mpu pll clock name is "dpll_mpu_ck",
same as that of omap44xx()
Signed-off-by: Afzal Mohammed <afzal@ti.com>
am33xx mpu pll clock name is "dpll_mpu_ck",
same as that of omap44xx()
Signed-off-by: Afzal Mohammed <afzal@ti.com>
cpufreq: OMAP: voltage scaling
DVFS capability added, voltage scaled as per the
OPP for new frequency. Increase voltage first for
going to higher OPP, and decrease frequency first
for transition to lower OPP.
If regulator is not found, fail cpufreq init.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
DVFS capability added, voltage scaled as per the
OPP for new frequency. Increase voltage first for
going to higher OPP, and decrease frequency first
for transition to lower OPP.
If regulator is not found, fail cpufreq init.
Signed-off-by: Afzal Mohammed <afzal@ti.com>
arm:omap:am33xx : update TSC hwmod data
This patch adds missing fields of hwmod data for TSC
Signed-off-by: Patil, Rachna <rachna@ti.com>
This patch adds missing fields of hwmod data for TSC
Signed-off-by: Patil, Rachna <rachna@ti.com>
arm:omap:gpio - Handle Clocks properly in Suspend/Resume
Clocks were not enabled/disabled during suspend-resume. This patch
corrects the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Clocks were not enabled/disabled during suspend-resume. This patch
corrects the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:gpio - add proper #if check for am335x
few #if check for am335x were missing. This patch adds the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
few #if check for am335x were missing. This patch adds the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:am33xx : correct gpio hwmod data
GPIO IP in am335x doesnt support Wakeup. Also, fix incorrect prcm
clock entries for GPIO 2 & 3.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
GPIO IP in am335x doesnt support Wakeup. Also, fix incorrect prcm
clock entries for GPIO 2 & 3.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:hsmmc - remove invalid bus power setting
SD bus Power was setup at a wrong sequence inside irq code. This Commit
removes the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
SD bus Power was setup at a wrong sequence inside irq code. This Commit
removes the same.
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm:omap:edma - replace edm_info with more relevant edma_cc
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
ARM: edma: use kzalloc()
Use kzalloc rather than kmalloc followed by memset with 0
This considers some simple cases that are common and easy to validate
Note in particular that there are no ...s in the rule, so all of the
matched code has to be contiguous
The semantic patch that makes this output is available
in scripts/coccinelle/api/alloc/kzalloc-simple.cocci.
More information about semantic patching is available at
http://coccinelle.lip6.fr/
Signed-off-by: Thomas Meyer <thomas@m3y3r.de>
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
Use kzalloc rather than kmalloc followed by memset with 0
This considers some simple cases that are common and easy to validate
Note in particular that there are no ...s in the rule, so all of the
matched code has to be contiguous
The semantic patch that makes this output is available
in scripts/coccinelle/api/alloc/kzalloc-simple.cocci.
More information about semantic patching is available at
http://coccinelle.lip6.fr/
Signed-off-by: Thomas Meyer <thomas@m3y3r.de>
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm: edma: check irq2ctlr() result
If irq2ctlr() fails return IRQ_NONE.
Also as it can fail make 'ctlr' signed.
The semantic patch that finds this problem (many false-positive results):
(http://coccinelle.lip6.fr/)
// <smpl>
@ r1 @
identifier f;
@@
int f(...) { ... }
@@
identifier r1.f;
type T;
unsigned T x;
@@
*x = f(...)
...
*x > 0
Signed-off-by: Kulikov Vasiliy <segooon@gmail.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
If irq2ctlr() fails return IRQ_NONE.
Also as it can fail make 'ctlr' signed.
The semantic patch that finds this problem (many false-positive results):
(http://coccinelle.lip6.fr/)
// <smpl>
@ r1 @
identifier f;
@@
int f(...) { ... }
@@
identifier r1.f;
type T;
unsigned T x;
@@
*x = f(...)
...
*x > 0
Signed-off-by: Kulikov Vasiliy <segooon@gmail.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm: edma: use BIT() wherever possible
This patch replaces occurences of (1 << x) with
BIT(x) as it makes for much better reading.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
This patch replaces occurences of (1 << x) with
BIT(x) as it makes for much better reading.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm: edma: fix coding style issue related to usage of braces
In the edma driver, there are couple of instances where braces
are used for a single statement 'if' construct.
There are other instances where 'else' part of the if-else construct
does not use braces even if the 'if' part is a multi-line statement.
This patch fixes both.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
In the edma driver, there are couple of instances where braces
are used for a single statement 'if' construct.
There are other instances where 'else' part of the if-else construct
does not use braces even if the 'if' part is a multi-line statement.
This patch fixes both.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
arm: edma: use a more intuitive name for edma_info
'edma_info' structure inside the edma driver represents
a single instance of edma channel controller. Call it
'edma_cc' instead. This also avoids readers confusing
it with an instance of edma_soc_info structre which
carries the platform data for a single channel controller
instance.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>
'edma_info' structure inside the edma driver represents
a single instance of edma channel controller. Call it
'edma_cc' instead. This also avoids readers confusing
it with an instance of edma_soc_info structre which
carries the platform data for a single channel controller
instance.
Signed-off-by: Sekhar Nori <nsekhar@ti.com>
Signed-off-by: Kevin Hilman <khilman@deeprootsystems.com>
Signed-off-by: Hebbar, Gururaja <gururaja.hebbar@ti.com>