sitara-epos/sitara-epos-kernel.git
11 years agoASoC: Fix module refcount for auxiliary devices
Jarkko Nikula [Wed, 26 Jan 2011 14:39:37 +0000 (16:39 +0200)]
ASoC: Fix module refcount for auxiliary devices

Commit f6c2ed5 "ASoC: Fix the device references to codec and platform drivers"
moved codec driver refcount increments from soc_bind_dai_link into
soc_probe_codec.

However, the commit didn't remove try_module_get from soc_probe_aux_dev so
the auxiliary device reference counts are incremented twice as the
soc_probe_codec is called from soc_probe_aux_dev too.

Signed-off-by: Jarkko Nikula <jhnikula@gmail.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoASoC: correct link specifications for corgi, poodle and spitz
Dmitry Eremin-Solenikov [Fri, 21 Jan 2011 19:14:17 +0000 (22:14 +0300)]
ASoC: correct link specifications for corgi, poodle and spitz

ASoC DAI link descriptions for Corgi, Poodle and Spitz platforms
contained incorrect names for cpu_dai and codec, which effectievly disabled sound
on theese platforms. Fix that errors.

Signed-off-by: Dmitry Eremin-Solenikov <dbaryshkov@gmail.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: Samsung: Fix outdated cpu_dai_name for s3c24xx i2s
Lars-Peter Clausen [Mon, 24 Jan 2011 21:12:42 +0000 (22:12 +0100)]
ASoC: Samsung: Fix outdated cpu_dai_name for s3c24xx i2s

During the multi-component patch the s3c24xx i2s driver was renamed from
"s3c24xx-i2s" to "s3c24xx-iis", while the sound board drivers were not
updated to reflect this change as well.

As a result there is no match between the dai_link and the i2s driver and no
sound card is instantiated.

This patch fixes the problem by updating the sound board drivers to use
"s3c24xx-iis" for the cpu_dai_name.

Signed-off-by: Lars-Peter Clausen <lars@metafoo.de>
Acked-by: Jassi Brar <jassi.brar@samsung.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: Fix codec device id format used by some dai_links
Lars-Peter Clausen [Mon, 24 Jan 2011 21:09:22 +0000 (22:09 +0100)]
ASoC: Fix codec device id format used by some dai_links

The id part of an I2C device name is created with the "%d-%04x" format string.

So for example for an I2C device which is connected to the adapter with the id 0
and has its address set to 0x1a the id part of the devices name would be
"0-001a".

Currently some sound board drivers have the id part the codec_name field of
their dai_link structures set as if it had been created by a "%d-0x%x" format
string. For example "0-0x1a" instead of "0-001a".

As a result there is no match between the codec device and the dai_link and no
sound card is instantiated.

This patch fixes it.

Signed-off-by: Lars-Peter Clausen <lars@metafoo.de>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: Handle low measured DC offsets for wm_hubs devices
Mark Brown [Fri, 21 Jan 2011 12:47:33 +0000 (12:47 +0000)]
ASoC: Handle low measured DC offsets for wm_hubs devices

The DC servo codes are actually signed numbers so need to be treated as
such.

Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Cc: stable@kernel.org
11 years agoASoC: da8xx/omap-l1xx: match codec_name with i2c ids
Rajashekhara, Sudhakar [Fri, 21 Jan 2011 14:40:01 +0000 (20:10 +0530)]
ASoC: da8xx/omap-l1xx: match codec_name with i2c ids

The codec_name entry for da8xx evm in sound/soc/davinci/davinci-evm.c
is not matching with the i2c ids in the board file. Without this fix the
soundcard does not get detected on da850/omap-l138/am18x evm.

Signed-off-by: Rajashekhara, Sudhakar <sudhakar.raj@ti.com>
Tested-by: Dan Sharon <dansharon@nanometrics.ca>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org (for 2.6.37)
11 years agoASoC: WM8994: fix wrong value in tristate function
Qiao Zhou [Wed, 19 Jan 2011 11:10:47 +0000 (19:10 +0800)]
ASoC: WM8994: fix wrong value in tristate function

fix wrong value in wm8994_set_tristate func. when updating reg bits,
it should use "value", not "reg".

Signed-off-by: Qiao Zhou <zhouqiao@marvell.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: WM8995: Fix incorrect use of snd_soc_update_bits()
Dimitris Papastamos [Wed, 19 Jan 2011 12:55:28 +0000 (12:55 +0000)]
ASoC: WM8995: Fix incorrect use of snd_soc_update_bits()

In the wm8995_set_tristate() function when updating the register
bits use the value and not the register index as the value argument.

Signed-off-by: Dimitris Papastamos <dp@opensource.wolfsonmicro.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoMerge branch 'for-2.6.38' of git://git.kernel.org/pub/scm/linux/kernel/git/broonie...
Mark Brown [Wed, 19 Jan 2011 11:17:12 +0000 (11:17 +0000)]
Merge branch 'for-2.6.38' of git://git./linux/kernel/git/broonie/sound-2.6 into for-2.6.38

11 years agoLinux 2.6.38-rc1 v2.6.38-rc1
Linus Torvalds [Tue, 18 Jan 2011 23:14:02 +0000 (15:14 -0800)]
Linux 2.6.38-rc1

11 years agoMerge branch 'hwmon-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/groec...
Linus Torvalds [Tue, 18 Jan 2011 22:30:00 +0000 (14:30 -0800)]
Merge branch 'hwmon-for-linus' of git://git./linux/kernel/git/groeck/staging

* 'hwmon-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/groeck/staging:
  hwmon: (lm93) Add support for LM94

11 years agoMerge branch 'perf-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Tue, 18 Jan 2011 22:29:37 +0000 (14:29 -0800)]
Merge branch 'perf-fixes-for-linus' of git://git./linux/kernel/git/tip/linux-2.6-tip

* 'perf-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
  perf: Validate cpu early in perf_event_alloc()
  perf: Find_get_context: fix the per-cpu-counter check
  perf: Fix contexted inheritance

11 years agoMerge branch 'x86-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git...
Linus Torvalds [Tue, 18 Jan 2011 22:29:21 +0000 (14:29 -0800)]
Merge branch 'x86-fixes-for-linus' of git://git./linux/kernel/git/tip/linux-2.6-tip

* 'x86-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
  x86: Clear irqstack thread_info
  x86: Make relocatable kernel work with new binutils

11 years agoMerge branch 'upstream' of git://git.linux-mips.org/pub/scm/upstream-linus
Linus Torvalds [Tue, 18 Jan 2011 22:28:48 +0000 (14:28 -0800)]
Merge branch 'upstream' of git://git.linux-mips.org/upstream-linus

* 'upstream' of git://git.linux-mips.org/pub/scm/upstream-linus: (26 commits)
  MIPS: Malta: enable Cirrus FB console
  MIPS: add CONFIG_VIRTUALIZATION for virtio support
  MIPS: Implement __read_mostly
  MIPS: ath79: add common WMAC device for AR913X based boards
  MIPS: ath79: Add initial support for the Atheros AP81 reference board
  MIPS: ath79: add common SPI controller device
  SPI: Add SPI controller driver for the Atheros AR71XX/AR724X/AR913X SoCs
  MIPS: ath79: add common GPIO buttons device
  MIPS: ath79: add common watchdog device
  MIPS: ath79: add common GPIO LEDs device
  MIPS: ath79: add initial support for the Atheros PB44 reference board
  MIPS: ath79: utilize the MIPS multi-machine support
  MIPS: ath79: add GPIOLIB support
  MIPS: Add initial support for the Atheros AR71XX/AR724X/AR931X SoCs
  MIPS: jump label: Add MIPS support.
  MIPS: Use WARN() in uasm for better diagnostics.
  MIPS: Optimize TLB handlers for Octeon CPUs
  MIPS: Add LDX and LWX instructions to uasm.
  MIPS: Use BBIT instructions in TLB handlers
  MIPS: Declare uasm bbit0 and bbit1 functions.
  ...

11 years agohwmon: (lm93) Add support for LM94
Guenter Roeck [Mon, 17 Jan 2011 20:48:20 +0000 (12:48 -0800)]
hwmon: (lm93) Add support for LM94

This patch adds basic support for LM94 to the LM93 driver. LM94 specific
sensors and features are not supported.

Signed-off-by: Guenter Roeck <guenter.roeck@ericsson.com>
Acked-by: Jean Delvare <khali@linux-fr.org>
11 years agoASoC: PXA: Fix codec address on Zipit Z2
Vasily Khoruzhick [Tue, 18 Jan 2011 14:54:25 +0000 (16:54 +0200)]
ASoC: PXA: Fix codec address on Zipit Z2

WM8750 address is 0x1b, not 0x1a. Without this fix ALSA detects no sound
cards on Zipit

Signed-off-by: Vasily Khoruzhick <anarsoul@gmail.com>
Acked-by: Marek Vasut <marek.vasut@gmail.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoASoC: PXA: Fix jack detection on Zipit Z2
Vasily Khoruzhick [Tue, 18 Jan 2011 14:54:24 +0000 (16:54 +0200)]
ASoC: PXA: Fix jack detection on Zipit Z2

Fix jack detection on Zipit Z2, otherwise it
disables headphones output when jack is connected

Signed-off-by: Vasily Khoruzhick <anarsoul@gmail.com>
Acked-by: Marek Vasut <marek.vasut@gmail.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoASoC: Blackfin: fix DAI/SPORT config dependency issues
Barry Song [Wed, 12 Jan 2011 01:04:28 +0000 (20:04 -0500)]
ASoC: Blackfin: fix DAI/SPORT config dependency issues

While I2S/TDM/AC97 DAI is built-in, others are compiled as modules,
SND_BF5XX_SOC_SPORT will be module, then DAI can't get some symbols.
Except that, SND_BF5XX_AC97 depends on SND_BF5XX_SOC_AC97 too.

Signed-off-by: Barry Song <barry.song@analog.com>
Signed-off-by: Mike Frysinger <vapier@gentoo.org>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoASoC: Blackfin TDM: use external frame syncs
Barry Song [Wed, 12 Jan 2011 07:59:55 +0000 (02:59 -0500)]
ASoC: Blackfin TDM: use external frame syncs

We don't want to use internal frame syncs otherwise we sometimes
get out of sync, so don't enable them when setting up the SPORT.

Signed-off-by: Barry Song <barry.song@analog.com>
Signed-off-by: Mike Frysinger <vapier@gentoo.org>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoASoC: Blackfin AC97: fix build error after multi-component update
Mike Frysinger [Wed, 12 Jan 2011 00:57:33 +0000 (19:57 -0500)]
ASoC: Blackfin AC97: fix build error after multi-component update

We need to tweak how we query the active capture/playback state after
the recent overhauls of common code.

Signed-off-by: Mike Frysinger <vapier@gentoo.org>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: Blackfin TDM: fix missed snd_soc_dai_get_drvdata update
Mike Frysinger [Wed, 12 Jan 2011 04:08:19 +0000 (23:08 -0500)]
ASoC: Blackfin TDM: fix missed snd_soc_dai_get_drvdata update

One spot was missed in this driver when converting from
snd_soc_dai.private_data to snd_soc_dai_get_drvdata.

Signed-off-by: Mike Frysinger <vapier@gentoo.org>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
Cc: stable@kernel.org
11 years agoASoC: documentation updates
Seungwhan Youn [Thu, 13 Jan 2011 02:08:21 +0000 (11:08 +0900)]
ASoC: documentation updates

This patch is only for RFC purpose of ASoC documentation updates which
match with current ASoC codes with documents. Mostly modify features
are modified to be sync with changes after multi-component patches.

Signed-off-by: Seungwhan Youn <sw.youn@samsung.com>
Acked-by: Liam Girdwood <lrg@slimlogic.co.uk>
Signed-off-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
11 years agoperf: Validate cpu early in perf_event_alloc()
Oleg Nesterov [Tue, 18 Jan 2011 16:10:32 +0000 (17:10 +0100)]
perf: Validate cpu early in perf_event_alloc()

Starting from perf_event_alloc()->perf_init_event(), the kernel
assumes that event->cpu is either -1 or the valid CPU number.

Change perf_event_alloc() to validate this argument early. This
also means we can remove the similar check in
find_get_context().

Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Acked-by: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Alan Stern <stern@rowland.harvard.edu>
Cc: Arnaldo Carvalho de Melo <acme@redhat.com>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Prasad <prasad@linux.vnet.ibm.com>
Cc: Roland McGrath <roland@redhat.com>
Cc: gregkh@suse.de
Cc: stable@kernel.org
LKML-Reference: <20110118161032.GC693@redhat.com>
Signed-off-by: Ingo Molnar <mingo@elte.hu>
11 years agoperf: Find_get_context: fix the per-cpu-counter check
Oleg Nesterov [Tue, 18 Jan 2011 16:10:08 +0000 (17:10 +0100)]
perf: Find_get_context: fix the per-cpu-counter check

If task == NULL, find_get_context() should always check that cpu
is correct.

Afaics, the bug was introduced by 38a81da2 "perf events: Clean
up pid passing", but even before that commit "&& cpu != -1" was
not exactly right, -ESRCH from find_task_by_vpid() is not
accurate.

Signed-off-by: Oleg Nesterov <oleg@redhat.com>
Acked-by: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Alan Stern <stern@rowland.harvard.edu>
Cc: Arnaldo Carvalho de Melo <acme@redhat.com>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Prasad <prasad@linux.vnet.ibm.com>
Cc: Roland McGrath <roland@redhat.com>
Cc: gregkh@suse.de
Cc: stable@kernel.org
LKML-Reference: <20110118161008.GB693@redhat.com>
Signed-off-by: Ingo Molnar <mingo@elte.hu>
11 years agoMIPS: Malta: enable Cirrus FB console
Aurelien Jarno [Tue, 18 Jan 2011 11:20:45 +0000 (12:20 +0100)]
MIPS: Malta: enable Cirrus FB console

While most users of a physical Malta board are using the serial port
as the console, a lot of QEMU users would prefer to interact with a
graphical console. Enable the Cirrus FB support in the Malta default
configuration to make that possible. Note that the default console will
still be the serial port, users have to pass "console=tty0" to the
kernel to use the Cirrus FB.

Signed-off-by: Aurelien Jarno <aurelien@aurel32.net>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/2001/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: add CONFIG_VIRTUALIZATION for virtio support
Aurelien Jarno [Tue, 18 Jan 2011 11:20:44 +0000 (12:20 +0100)]
MIPS: add CONFIG_VIRTUALIZATION for virtio support

Add CONFIG_VIRTUALIZATION to the MIPS architecture and include the
the virtio code there. Used to enable the virtio drivers under QEMU.

Signed-off-by: Aurelien Jarno <aurelien@aurel32.net>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/2002/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Implement __read_mostly
David Daney [Thu, 14 Oct 2010 19:36:49 +0000 (12:36 -0700)]
MIPS: Implement __read_mostly

Just do what everyone else is doing by placing __read_mostly things in
the .data.read_mostly section.

mips_io_port_base can not be read-only (const) and writable
(__read_mostly) at the same time.  One of them has to go, so I chose
to eliminate the __read_mostly.  It will still get stuck in a portion
of memory that is not adjacent to things that are written, and thus
not be on a dirty cache line, for whatever that is worth.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: http://patchwork.linux-mips.org/patch/1702/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add common WMAC device for AR913X based boards
Gabor Juhos [Tue, 4 Jan 2011 20:28:29 +0000 (21:28 +0100)]
MIPS: ath79: add common WMAC device for AR913X based boards

Add common platform_device and helper code to make the registration
of the built-in wireless MAC easier on the Atheros AR9130/AR9132
based boards. Also register the WMAC device on the AR81 board.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Imre Kaloz <kaloz@openwrt.org>,
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1962/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: Add initial support for the Atheros AP81 reference board
Gabor Juhos [Tue, 4 Jan 2011 20:28:28 +0000 (21:28 +0100)]
MIPS: ath79: Add initial support for the Atheros AP81 reference board

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1952/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add common SPI controller device
Gabor Juhos [Tue, 4 Jan 2011 20:28:23 +0000 (21:28 +0100)]
MIPS: ath79: add common SPI controller device

Several boards are using the built-in SPI controller of the
AR71XX/AR724X/AR913X SoCs. This patch adds common platform_device
and helper code to register it. Additionally, the patch registers
the SPI bus on the PB44 board.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Imre Kaloz <kaloz@openwrt.org>
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1956/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoSPI: Add SPI controller driver for the Atheros AR71XX/AR724X/AR913X SoCs
Gabor Juhos [Tue, 4 Jan 2011 20:28:22 +0000 (21:28 +0100)]
SPI: Add SPI controller driver for the Atheros AR71XX/AR724X/AR913X SoCs

The Atheros AR71XX/AR724X/AR913X SoCs have a built-in SPI controller. This
patch implements a driver for that.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: David Brownell <dbrownell@users.sourceforge.net>
Cc: spi-devel-general@lists.sourceforge.net
Acked-by: Grant Likely <grant.likely@secretlab.ca>
Cc: linux-mips@linux-mips.org
Cc: Imre Kaloz <kaloz@openwrt.org>
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1960/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add common GPIO buttons device
Gabor Juhos [Tue, 4 Jan 2011 20:28:21 +0000 (21:28 +0100)]
MIPS: ath79: add common GPIO buttons device

Almost all boards have one or more push buttons connected to GPIO lines.
This patch adds common code to register a platform_device for them.

The patch also adds support for the buttons on the PB44 board.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1954/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add common watchdog device
Gabor Juhos [Tue, 4 Jan 2011 20:28:20 +0000 (21:28 +0100)]
MIPS: ath79: add common watchdog device

All supported SoCs have a built-in hardware watchdog driver. This patch
registers a platform_device for that to make it usable.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1955/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add common GPIO LEDs device
Gabor Juhos [Tue, 4 Jan 2011 20:28:18 +0000 (21:28 +0100)]
MIPS: ath79: add common GPIO LEDs device

Almost all boards have one or more LEDs connected to GPIO lines. This
patch adds common code to register a platform_device for them.

The patch also adds support for the LEDs on the PB44 board.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1953/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add initial support for the Atheros PB44 reference board
Gabor Juhos [Tue, 4 Jan 2011 20:28:17 +0000 (21:28 +0100)]
MIPS: ath79: add initial support for the Atheros PB44 reference board

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1950/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: utilize the MIPS multi-machine support
Gabor Juhos [Tue, 4 Jan 2011 20:28:16 +0000 (21:28 +0100)]
MIPS: ath79: utilize the MIPS multi-machine support

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1949/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: ath79: add GPIOLIB support
Gabor Juhos [Tue, 4 Jan 2011 20:28:15 +0000 (21:28 +0100)]
MIPS: ath79: add GPIOLIB support

This patch implements generic GPIO routines for the built-in
GPIO controllers of the Atheros AR71XX/AR724X/AR913X SoCs.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: David Brownell <dbrownell@users.sourceforge.net>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1948/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Add initial support for the Atheros AR71XX/AR724X/AR931X SoCs
Gabor Juhos [Tue, 4 Jan 2011 20:28:14 +0000 (21:28 +0100)]
MIPS: Add initial support for the Atheros AR71XX/AR724X/AR931X SoCs

This patch adds initial support for various Atheros SoCs based on the
MIPS 24Kc core. The following models are supported at the moment:

  - AR7130
  - AR7141
  - AR7161
  - AR9130
  - AR9132
  - AR7240
  - AR7241
  - AR7242

The current patch contains minimal support only, but the resulting
kernel can boot into user-space with using of an initramfs image on
various boards which are using these SoCs. Support for more built-in
devices and individual boards will be implemented in further patches.

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Signed-off-by: Imre Kaloz <kaloz@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Cc: Kathy Giori <Kathy.Giori@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1947/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: jump label: Add MIPS support.
David Daney [Tue, 28 Dec 2010 21:26:23 +0000 (13:26 -0800)]
MIPS: jump label: Add MIPS support.

In order not to be left behind, we add jump label support for MIPS.

Tested on 64-bit big endian (Octeon), and 32-bit little endian
(malta/qemu).

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Cc: Steven Rostedt <rostedt@goodmis.org>
Cc: Jason Baron <jbaron@redhat.com>
Patchwork: https://patchwork.linux-mips.org/patch/1923/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Use WARN() in uasm for better diagnostics.
David Daney [Tue, 28 Dec 2010 02:18:29 +0000 (18:18 -0800)]
MIPS: Use WARN() in uasm for better diagnostics.

On the off chance that uasm ever warns about overflow, there is no way
to know what the offending instruction is.

Change the printks to WARNs, so we can get a nice stack trace.  It has
the added benefit of being much more noticeable than the short single
line warning message, so is less likely to be ignored.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1905/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Optimize TLB handlers for Octeon CPUs
David Daney [Tue, 28 Dec 2010 02:07:57 +0000 (18:07 -0800)]
MIPS: Optimize TLB handlers for Octeon CPUs

Octeon can use scratch registers in the TLB handlers.  Octeon II can
use LDX instructions.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1904/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Add LDX and LWX instructions to uasm.
David Daney [Tue, 28 Dec 2010 02:07:56 +0000 (18:07 -0800)]
MIPS: Add LDX and LWX instructions to uasm.

Needed by Octeon II optimized TLB handlers.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Pachwork: https://patchwork.linux-mips.org/patch/1903/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Use BBIT instructions in TLB handlers
David Daney [Mon, 20 Dec 2010 23:54:50 +0000 (15:54 -0800)]
MIPS: Use BBIT instructions in TLB handlers

If the CPU supports BBIT0 and BBIT1, use them in TLB handlers as they
are more efficient than an AND followed by an branch and then
restoring the clobbered register.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1873/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Declare uasm bbit0 and bbit1 functions.
David Daney [Mon, 20 Dec 2010 23:54:49 +0000 (15:54 -0800)]
MIPS: Declare uasm bbit0 and bbit1 functions.

these are already defined, but declaring them allow them to be used
outside of uasm.c.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1872/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Use C0_KScratch (if present) to hold PGD pointer.
David Daney [Tue, 21 Dec 2010 22:19:11 +0000 (14:19 -0800)]
MIPS: Use C0_KScratch (if present) to hold PGD pointer.

Decide at runtime to use either Context or KScratch to hold the PGD
pointer.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1876/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Add DINSM to uasm.
David Daney [Tue, 21 Dec 2010 22:19:10 +0000 (14:19 -0800)]
MIPS: Add DINSM to uasm.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1875/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Probe for presence of KScratch registers.
David Daney [Tue, 21 Dec 2010 22:19:09 +0000 (14:19 -0800)]
MIPS: Probe for presence of KScratch registers.

Probe c0_config4 for KScratch registers and report them in /proc/cpuinfo.

Signed-off-by: David Daney <ddaney@caviumnetworks.com>
To: linux-mips@linux-mips.org
Patchwork: https://patchwork.linux-mips.org/patch/1877/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Add generic support for multiple machines within a single kernel
Gabor Juhos [Tue, 23 Nov 2010 15:06:25 +0000 (16:06 +0100)]
MIPS: Add generic support for multiple machines within a single kernel

This patch adds a generic solution to support multiple machines based on
a given SoC within a single kernel image. It is implemented already for
several other architectures but MIPS has no generic support for that yet.

[Ralf: This competes with DT but DT is a much more complex solution and this
code has been used by OpenWRT for a long time so for now DT is a bad reason
to stop the merge but longer term this should be migrated to DT.]

Signed-off-by: Gabor Juhos <juhosg@openwrt.org>
Cc: linux-mips@linux-mips.org
Cc: kaloz@openwrt.org
Cc: Luis R. Rodriguez <lrodriguez@atheros.com>
Cc: Cliff Holden <Cliff.Holden@Atheros.com>
Patchwork: https://patchwork.linux-mips.org/patch/1814/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Use printf extension %pR for struct resource
Joe Perches [Fri, 12 Nov 2010 21:37:52 +0000 (13:37 -0800)]
MIPS: Use printf extension %pR for struct resource

Using %pR standardizes the struct resource output.

Signed-off-by: Joe Perches <joe@perches.com>
To: Jiri Kosina <trivial@kernel.org>
Cc: linux-mips@linux-mips.org
Cc: linux-kernel@vger.kernel.org
Patchwork: https://patchwork.linux-mips.org/patch/1772/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMIPS: Sibyte: Use vzalloc in sbbus profiler
Joe Perches [Fri, 5 Nov 2010 03:07:26 +0000 (20:07 -0700)]
MIPS: Sibyte: Use vzalloc in sbbus profiler

Signed-off-by: Joe Perches <joe@perches.com>
To: Jiri Kosina <trivial@kernel.org>
Cc: linux-mips@linux-mips.org
Cc: linux-kernel@vger.kernel.org
Patchwork: https://patchwork.linux-mips.org/patch/1756/
Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
11 years agoMerge branch 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/jejb/parisc-2.6
Linus Torvalds [Tue, 18 Jan 2011 18:00:50 +0000 (10:00 -0800)]
Merge branch 'fixes' of git://git./linux/kernel/git/jejb/parisc-2.6

* 'fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/jejb/parisc-2.6:
  parisc: fix compile breakage caused by inlining maybe_mkwrite
  parisc : Remove broken line wrapping handling pdc_iodc_print()

11 years agoMerge branch 'next' of git://git.monstr.eu/linux-2.6-microblaze
Linus Torvalds [Tue, 18 Jan 2011 16:06:22 +0000 (08:06 -0800)]
Merge branch 'next' of git://git.monstr.eu/linux-2.6-microblaze

* 'next' of git://git.monstr.eu/linux-2.6-microblaze:
  microblaze: Fix asm/pgtable.h
  microblaze: Fix missing pagemap.h

11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound-2.6
Linus Torvalds [Tue, 18 Jan 2011 16:05:50 +0000 (08:05 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/tiwai/sound-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tiwai/sound-2.6:
  ALSA: hda - Fix initialization for HP 2011 notebooks
  ALSA: hda - Add support for VMware controller
  ALSA: hda - consitify string arrays
  ALSA: hda - Add add multi-streaming playback for AD1988
  ASoC: EP93xx: fixed LRCLK rate and DMA oper. in I2S code
  ASoC: WM8990: msleep() takes milliseconds not jiffies
  ALSA : au88x0 - Limit number of channels to fix Oops via OSS emu
  ALSA: constify functions in ac97
  ASoC: WL1273 FM radio: Fix breakage with MFD API changes
  ALSA: hda - More coverage for odd-number channels elimination for HDMI
  ALSA: hda - Store PCM parameters properly in HDMI open callback
  ALSA: hda - Rearrange fixup struct in patch_realtek.c
  ALSA: oxygen: Xonar DG: fix CS4245 register writes
  ALSA: hda - Suppress the odd number of channels for HDMI
  ALSA: hda - Add fixup-call in init callback
  ALSA: hda - Reorganize fixup structure for Realtek
  ALSA: hda - Apply Sony VAIO hweq fixup only once
  ALSA: hda - Apply mario fixup only once
  ALSA: hda - Remove unused fixup entry for ALC262

11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gerg/m68knommu
Linus Torvalds [Tue, 18 Jan 2011 16:05:20 +0000 (08:05 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/gerg/m68knommu

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/gerg/m68knommu: (25 commits)
  m68knommu: fix broken setting of irq_chip and handler
  m68knommu: switch to using -mcpu= flags for ColdFire targets
  m68knommu: arch/m68knommu/Kconfig whitespace cleanup
  m68knommu: create optimal separate instruction and data cache for ColdFire
  m68knommu: support ColdFire caches that do copyback and write-through
  m68knommu: support version 2 ColdFire split cache
  m68knommu: make cache push code ColdFire generic
  m68knommu: clean up ColdFire cache control code
  m68knommu: move inclusion of ColdFire v4 cache registers
  m68knommu: merge bit definitions for version 3 ColdFire cache controller
  m68knommu: create bit definitions for the version 2 ColdFire cache controller
  m68knommu: remove empty __iounmap() it is no used
  m68knommu: remove kernel_map() code, it is not used
  m68knommu: remove do_page_fault(), it is not used
  m68knommu: use user stack pointer hardware on some ColdFire cores
  m68knommu: remove command line printing DEBUG
  m68knommu: remove fasthandler interrupt code
  m68knommu: move UART addressing to part specific includes
  m68knommu: fix clock rate value reported for ColdFire 54xx parts
  m68knommu: move ColdFire CPU names into their headers
  ...

11 years agoMerge branch 'perf-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel...
Linus Torvalds [Tue, 18 Jan 2011 16:04:30 +0000 (08:04 -0800)]
Merge branch 'perf-fixes-for-linus' of git://git./linux/kernel/git/tip/linux-2.6-tip

* 'perf-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
  perf tools: Fix tracepoint id to string perf.data header table
  perf tools: Fix handling of wildcards in tracepoint event selectors
  powerpc: perf: Fix frequency calculation for overflowing counters

11 years agoMerge branch 's5p-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git...
Linus Torvalds [Tue, 18 Jan 2011 16:03:55 +0000 (08:03 -0800)]
Merge branch 's5p-fixes-for-linus' of git://git./linux/kernel/git/kgene/linux-samsung

* 's5p-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/kgene/linux-samsung:
  ARM: S5PV310: Add missing virtual ASoC DMA device
  ARM: S5PV210: Add missing virtual ASoC DMA device
  ARM: S5P6450: Add missing virtual ASoC DMA device
  ARM: S5P6440: Add missing virtual ASoC DMA device
  ARM: S5P6442: Enable I2S device to work on SMDK6442

11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6
Linus Torvalds [Tue, 18 Jan 2011 15:58:36 +0000 (07:58 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/viro/vfs-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6:
  autofs4: clean ->d_release() and autofs4_free_ino() up
  autofs4: split autofs4_init_ino()
  autofs4: mkdir and symlink always get a dentry that had passed lookup
  autofs4: autofs4_get_inode() doesn't need autofs_info * argument anymore
  autofs4: kill ->size in autofs_info
  autofs4: pass mode to autofs4_get_inode() explicitly
  autofs4: autofs4_mkroot() is not different from autofs4_init_ino()
  autofs4: keep symlink body in inode->i_private
  autofs4 - fix debug print in autofs4_lookup()
  vfs - fix dentry ref count in do_lookup()
  autofs4 - fix get_next_positive_dentry()

11 years agoperf: Fix contexted inheritance
Peter Zijlstra [Mon, 17 Jan 2011 12:45:37 +0000 (13:45 +0100)]
perf: Fix contexted inheritance

Linus reported that the RCU lockdep annotation bits triggered for this
rcu_dereference() because we're not holding rcu_read_lock().

Going over the code I cannot convince myself its correct:

 - holding a ref on the parent_ctx, doesn't avoid it being uncloned
   concurrently (as the comment says), so we can race with a free.

 - holding parent_ctx->mutex doesn't avoid the above free from taking
   place either, it would at best avoid parent_ctx from being freed.

I.e. the warning is correct. To fix the bug, serialize against the
unclone_ctx() call by extending the reach of the parent_ctx->lock.

Reported-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
LKML-Reference: <new-submission>
Signed-off-by: Ingo Molnar <mingo@elte.hu>
11 years agox86: Clear irqstack thread_info
Brian Gerst [Mon, 17 Jan 2011 12:32:10 +0000 (07:32 -0500)]
x86: Clear irqstack thread_info

Mathias Merz reported that v2.6.37 failed to boot on his
system.

Make sure that the thread_info part of the irqstack is
initialized to zeroes.

Reported-and-Tested-by: Matthias Merz <linux@merz-ka.de>
Signed-off-by: Brian Gerst <brgerst@gmail.com>
Acked-by: Pekka Enberg <penberg@kernel.org>
Cc: Arjan van de Ven <arjan@linux.intel.com>
Cc: Linus Torvalds <torvalds@linux-foundation.org>
LKML-Reference: <AANLkTimyKXfJ1x8tgwrr1hYnNLrPfgE1NTe4z7L6tUDm@mail.gmail.com>
Signed-off-by: Ingo Molnar <mingo@elte.hu>
11 years agoMerge branch 'fix/asoc' into for-linus
Takashi Iwai [Tue, 18 Jan 2011 13:05:44 +0000 (14:05 +0100)]
Merge branch 'fix/asoc' into for-linus

11 years agox86: Make relocatable kernel work with new binutils
Shaohua Li [Tue, 18 Jan 2011 00:57:49 +0000 (08:57 +0800)]
x86: Make relocatable kernel work with new binutils

The CONFIG_RELOCATABLE=y option is broken with new binutils, which will make
boot panic.

According to Lu Hongjiu, the affected binutils are from 2.20.51.0.12 to
2.21.51.0.3, which are release since Oct 22 this year. At least ubuntu 10.10 is
using such binutils. See:

    http://sourceware.org/bugzilla/show_bug.cgi?id=12327

The reason of the boot panic is that we have 'jiffies = jiffies_64;' in
vmlinux.lds.S. The jiffies isn't in any section. In kernel build, there is
warning saying jiffies is an absolute address and can't be relocatable. At
runtime, jiffies will have virtual address 0.

Signed-off-by: Shaohua Li<shaohua.li@intel.com>
Cc: Lu Hongjiu<hongjiu.lu@intel.com>
Cc: Huang Ying <ying.huang@intel.com>
Cc: Sam Ravnborg <sam@ravnborg.org>
LKML-Reference: <1295312269.1949.725.camel@sli10-conroe>
Signed-off-by: Ingo Molnar <mingo@elte.hu>
11 years agoMerge branch 'fix/hda' into for-linus
Takashi Iwai [Tue, 18 Jan 2011 06:44:55 +0000 (07:44 +0100)]
Merge branch 'fix/hda' into for-linus

11 years agoALSA: hda - Fix initialization for HP 2011 notebooks
Vitaliy Kulikov [Fri, 14 Jan 2011 23:21:13 +0000 (17:21 -0600)]
ALSA: hda - Fix initialization for HP 2011 notebooks

Fixes for HP 2011 notebooks: enable dock ports and disable BTL
initialization in the driver.

Signed-off-by: Vitaliy Kulikov <Vitaliy.Kulikov@idt.com>
Signed-off-by: Takashi Iwai <tiwai@suse.de>
11 years agoALSA: hda - Add support for VMware controller
Bankim Bhavsar [Mon, 17 Jan 2011 14:23:21 +0000 (15:23 +0100)]
ALSA: hda - Add support for VMware controller

Add the new PCI ID 0x15ad and device ID 0x1977 for VMware HDAudio
Controller.

[changed to use AZX_DRIVER_GENERIC by tiwai]

Signed-off-by: Bankim Bhavsar <bbhavsar@vmware.com>
Signed-off-by: Takashi Iwai <tiwai@suse.de>
11 years agoALSA: hda - consitify string arrays
Takashi Iwai [Mon, 17 Jan 2011 10:29:34 +0000 (11:29 +0100)]
ALSA: hda - consitify string arrays

Signed-off-by: Takashi Iwai <tiwai@suse.de>
11 years agoALSA: hda - Add add multi-streaming playback for AD1988
Raymond Yau [Mon, 17 Jan 2011 10:19:03 +0000 (11:19 +0100)]
ALSA: hda - Add add multi-streaming playback for AD1988

Attached a patch which add a new model to support multi-streaming
playback for ad1988.

playback another stereo stream through the front panel headphone on
device 2 while playback through the speakers connected to rear panel
on device 0 at the same time.

Tested with ad1988a rev2 codec on asus P5B-V motherboard.

Signed-off-by: Raymond Yau <superquad.vortex2@gmail.com>
Signed-off-by: Takashi Iwai <tiwai@suse.de>
11 years agoautofs4: clean ->d_release() and autofs4_free_ino() up
Al Viro [Mon, 17 Jan 2011 02:42:32 +0000 (21:42 -0500)]
autofs4: clean ->d_release() and autofs4_free_ino() up

The latter is called only when both ino and dentry are about to
be freed, so cleaning ->d_fsdata and ->dentry is pointless.

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: split autofs4_init_ino()
Al Viro [Sun, 16 Jan 2011 23:43:40 +0000 (18:43 -0500)]
autofs4: split autofs4_init_ino()

split init_ino into new_ino and clean_ino; the former is
what used to be init_ino(NULL, sbi), the latter is for cases
where we passed non-NULL ino.  Lose unused arguments.

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: mkdir and symlink always get a dentry that had passed lookup
Al Viro [Sun, 16 Jan 2011 23:29:35 +0000 (18:29 -0500)]
autofs4: mkdir and symlink always get a dentry that had passed lookup

... so ->d_fsdata will have been set up before we get there

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: autofs4_get_inode() doesn't need autofs_info * argument anymore
Al Viro [Sun, 16 Jan 2011 22:43:52 +0000 (17:43 -0500)]
autofs4: autofs4_get_inode() doesn't need autofs_info * argument anymore

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: kill ->size in autofs_info
Al Viro [Sun, 16 Jan 2011 22:39:15 +0000 (17:39 -0500)]
autofs4: kill ->size in autofs_info

It's used only to pass the length of symlink body to
autofs4_get_inode() in autofs4_dir_symlink().  We can
bloody well set inode->i_size in autofs4_dir_symlink()
directly and be done with that.

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: pass mode to autofs4_get_inode() explicitly
Al Viro [Sun, 16 Jan 2011 22:20:23 +0000 (17:20 -0500)]
autofs4: pass mode to autofs4_get_inode() explicitly

In all cases we'd set inf->mode to know value just before
passing it to autofs4_get_inode().  That kills the need
to store it in autofs_info and pass it to autofs_init_ino()

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: autofs4_mkroot() is not different from autofs4_init_ino()
Al Viro [Sun, 16 Jan 2011 22:13:33 +0000 (17:13 -0500)]
autofs4: autofs4_mkroot() is not different from autofs4_init_ino()

Kill it.  Mind you, it's been an obfuscated call of autofs4_init_ino()
ever since 2.3.99pre6-4...

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4: keep symlink body in inode->i_private
Al Viro [Mon, 17 Jan 2011 05:47:38 +0000 (00:47 -0500)]
autofs4: keep symlink body in inode->i_private

gets rid of all ->free()/->u.symlink machinery in autofs; we simply
keep symlink bodies in inode->i_private and free them in ->evict_inode().

Acked-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4 - fix debug print in autofs4_lookup()
Ian Kent [Tue, 18 Jan 2011 04:06:15 +0000 (12:06 +0800)]
autofs4 - fix debug print in autofs4_lookup()

oz_mode isn't defined any more, use autofs4_oz_mode(sbi) instead.

Signed-off-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agovfs - fix dentry ref count in do_lookup()
Ian Kent [Tue, 18 Jan 2011 04:06:10 +0000 (12:06 +0800)]
vfs - fix dentry ref count in do_lookup()

There is a ref count problem in fs/namei.c:do_lookup().

When walking in ref-walk mode, if follow_managed() returns a fail we
need to drop dentry and possibly vfsmount.  Clean up properly,
as we do in the other caller of follow_managed().

Signed-off-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoautofs4 - fix get_next_positive_dentry()
Ian Kent [Tue, 18 Jan 2011 04:06:04 +0000 (12:06 +0800)]
autofs4 - fix get_next_positive_dentry()

The initialization condition in fs/autofs4/expire.c:get_next_positive_dentry()
appears to be incorrect. If prev == NULL I believe that root should be
returned.

Further down, at the current dentry check for it being simple_positive()
it looks like the d_lock for dentry p should be dropped instead of dentry
ret, otherwise when p is assinged to ret we end up with no lock on p and
a lost lock on ret, which leads to a deadlock.

Signed-off-by: Ian Kent <raven@themaw.net>
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
11 years agoARM: S5PV310: Add missing virtual ASoC DMA device
Jassi Brar [Tue, 18 Jan 2011 05:41:43 +0000 (14:41 +0900)]
ARM: S5PV310: Add missing virtual ASoC DMA device

Signed-off-by: Jassi Brar <jassi.brar@samsung.com>
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
11 years agoARM: S5PV210: Add missing virtual ASoC DMA device
Jassi Brar [Thu, 30 Dec 2010 00:13:23 +0000 (09:13 +0900)]
ARM: S5PV210: Add missing virtual ASoC DMA device

Signed-off-by: Jassi Brar <jassi.brar@samsung.com>
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
11 years agoARM: S5P6450: Add missing virtual ASoC DMA device
Jassi Brar [Thu, 30 Dec 2010 00:12:32 +0000 (09:12 +0900)]
ARM: S5P6450: Add missing virtual ASoC DMA device

Signed-off-by: Jassi Brar <jassi.brar@samsung.com>
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
11 years agoARM: S5P6440: Add missing virtual ASoC DMA device
Jassi Brar [Thu, 30 Dec 2010 00:11:10 +0000 (09:11 +0900)]
ARM: S5P6440: Add missing virtual ASoC DMA device

Signed-off-by: Jassi Brar <jassi.brar@samsung.com>
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
11 years agoARM: S5P6442: Enable I2S device to work on SMDK6442
Jassi Brar [Tue, 21 Dec 2010 00:44:33 +0000 (09:44 +0900)]
ARM: S5P6442: Enable I2S device to work on SMDK6442

Add missing virtual ASoC DMA device.

Signed-off-by: Jassi Brar <jassi.brar@samsung.com>
Acked-by: Mark Brown <broonie@opensource.wolfsonmicro.com>
[kgene.kim@samsung.com: minor changed title]
Signed-off-by: Kukjin Kim <kgene.kim@samsung.com>
11 years agostaging: fix build failure in bcm driver
Andres Salomon [Tue, 18 Jan 2011 00:11:12 +0000 (16:11 -0800)]
staging: fix build failure in bcm driver

While building latest Linus git, I hit the following:

    CC [M]  drivers/staging/bcm/Qos.o
  drivers/staging/bcm/Qos.c: In function ‘PruneQueue’:
  drivers/staging/bcm/Qos.c:367: error: ‘struct netdev_queue’ has no member named ‘tx_dropped’
  drivers/staging/bcm/Qos.c: In function ‘flush_all_queues’:
  drivers/staging/bcm/Qos.c:416: error: ‘struct netdev_queue’ has no member named ‘tx_dropped’
  make[5]: *** [drivers/staging/bcm/Qos.o] Error 1
  make[4]: *** [drivers/staging/bcm] Error 2
  make[3]: *** [drivers/staging] Error 2

As well as:

    CC [M]  drivers/staging/bcm/Transmit.o
  drivers/staging/bcm/Transmit.c: In function ‘SetupNextSend’:
  drivers/staging/bcm/Transmit.c:163: error: ‘struct netdev_queue’ has no member named ‘tx_bytes’
  drivers/staging/bcm/Transmit.c:164: error: ‘struct netdev_queue’ has no member named ‘tx_packets’
  make[2]: *** [drivers/staging/bcm/Transmit.o] Error 1

tx_dropped/tx_bytes_tx_packets were removed in commit 1ac9ad13.  This patch
converts bcm to use net_device_stats instead of netdev_queue.

Acked-by: Stephen Hemminger <shemminger@vyatta.com>
Acked-by: Eric Dumazet <eric.dumazet@gmail.com>
Signed-off-by: Andres Salomon <dilinger@queued.net>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/roland...
Linus Torvalds [Mon, 17 Jan 2011 22:45:48 +0000 (14:45 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/roland/infiniband

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/roland/infiniband:
  RDMA: Update workqueue usage
  RDMA/nes: Fix incorrect SFP+ link status detection on driver init
  RDMA/nes: Fix SFP+ link down detection issue with switch port disable
  RDMA/nes: Generate IB_EVENT_PORT_ERR/PORT_ACTIVE events
  RDMA/nes: Fix bonding on iw_nes
  IB/srp: Test only once whether iu allocation succeeded
  IB/mlx4: Handle protocol field in multicast table
  RDMA: Use vzalloc() to replace vmalloc()+memset(0)
  mlx4_{core, ib, en}: Fix driver when sizeof (phys_addr_t) > sizeof (long)
  IB/mthca: Fix driver when sizeof (phys_addr_t) > sizeof (long)

11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/btrfs...
Linus Torvalds [Mon, 17 Jan 2011 22:43:43 +0000 (14:43 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/mason/btrfs-unstable

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mason/btrfs-unstable: (25 commits)
  Btrfs: forced readonly mounts on errors
  btrfs: Require CAP_SYS_ADMIN for filesystem rebalance
  Btrfs: don't warn if we get ENOSPC in btrfs_block_rsv_check
  btrfs: Fix memory leak in btrfs_read_fs_root_no_radix()
  btrfs: check NULL or not
  btrfs: Don't pass NULL ptr to func that may deref it.
  btrfs: mount failure return value fix
  btrfs: Mem leak in btrfs_get_acl()
  btrfs: fix wrong free space information of btrfs
  btrfs: make the chunk allocator utilize the devices better
  btrfs: restructure find_free_dev_extent()
  btrfs: fix wrong calculation of stripe size
  btrfs: try to reclaim some space when chunk allocation fails
  btrfs: fix wrong data space statistics
  fs/btrfs: Fix build of ctree
  Btrfs: fix off by one while setting block groups readonly
  Btrfs: Add BTRFS_IOC_SUBVOL_GETFLAGS/SETFLAGS ioctls
  Btrfs: Add readonly snapshots support
  Btrfs: Refactor btrfs_ioctl_snap_create()
  btrfs: Extract duplicate decompress code
  ...

11 years agoRevert "mm: simplify code of swap.c"
Linus Torvalds [Mon, 17 Jan 2011 22:42:34 +0000 (14:42 -0800)]
Revert "mm: simplify code of swap.c"

This reverts commit d8505dee1a87b8d41b9c4ee1325cd72258226fbc.

Chris Mason ended up chasing down some page allocation errors and pages
stuck waiting on the IO scheduler, and was able to narrow it down to two
commits: commit 744ed1442757 ("mm: batch activate_page() to reduce lock
contention") and d8505dee1a87 ("mm: simplify code of swap.c").

This reverts the second one.

Reported-and-debugged-by: Chris Mason <chris.mason@oracle.com>
Cc: Mel Gorman <mel@csn.ul.ie>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: Jens Axboe <jaxboe@fusionio.com>
Cc: linux-mm <linux-mm@kvack.org>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: Andrea Arcangeli <aarcange@redhat.com>
Cc: Shaohua Li <shaohua.li@intel.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
11 years agoRevert "mm: batch activate_page() to reduce lock contention"
Linus Torvalds [Mon, 17 Jan 2011 22:42:19 +0000 (14:42 -0800)]
Revert "mm: batch activate_page() to reduce lock contention"

This reverts commit 744ed1442757767ffede5008bb13e0805085902e.

Chris Mason ended up chasing down some page allocation errors and pages
stuck waiting on the IO scheduler, and was able to narrow it down to two
commits: commit 744ed1442757 ("mm: batch activate_page() to reduce lock
contention") and d8505dee1a87 ("mm: simplify code of swap.c").

This reverts the first of them.

Reported-and-debugged-by: Chris Mason <chris.mason@oracle.com>
Cc: Mel Gorman <mel@csn.ul.ie>
Cc: Andrew Morton <akpm@linux-foundation.org>
Cc: Jens Axboe <jaxboe@fusionio.com>
Cc: linux-mm <linux-mm@kvack.org>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Cc: Andrea Arcangeli <aarcange@redhat.com>
Cc: Shaohua Li <shaohua.li@intel.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ecryptfs...
Linus Torvalds [Mon, 17 Jan 2011 20:39:57 +0000 (12:39 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/ecryptfs/ecryptfs-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ecryptfs/ecryptfs-2.6:
  ecryptfs: remove unnecessary decrypt when extending a file
  ecryptfs: Fix ecryptfs_printk() size_t warnings
  fs/ecryptfs: Add printf format/argument verification and fix fallout
  ecryptfs: fixed testing of file descriptor flags
  ecryptfs: test lower_file pointer when lower_file_mutex is locked
  ecryptfs: missing initialization of the superblock 'magic' field
  ecryptfs: moved ECRYPTFS_SUPER_MAGIC definition to linux/magic.h
  ecryptfs: fix truncation error in ecryptfs_read_update_atime

11 years agoxfs: Do not name variables "panic"
Geert Uytterhoeven [Mon, 17 Jan 2011 20:21:14 +0000 (21:21 +0100)]
xfs: Do not name variables "panic"

On platforms that call panic() inside their BUG() macro (m68k/sun3, and
all platforms that don't set HAVE_ARCH_BUG), compilation fails with:

| fs/xfs/support/debug.c: In function ‘xfs_cmn_err’:
| fs/xfs/support/debug.c:92: error: called object ‘panic’ is not a function

as the local variable "panic" conflicts with the "panic()" function.
Rename the local variable to resolve this.

Signed-off-by: Geert Uytterhoeven <geert@linux-m68k.org>
Reviewed-by: Christoph Hellwig <hch@lst.de>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
11 years agoperf tools: Fix tracepoint id to string perf.data header table
Arnaldo Carvalho de Melo [Mon, 17 Jan 2011 20:28:13 +0000 (18:28 -0200)]
perf tools: Fix tracepoint id to string perf.data header table

It was broken by f006d25 that passed just the event name, not the complete
sys:event that it expected to open the /sys/.../sys/sys:event/id file to get
the id.

Fix it by moving it to after parse_events in cmd_record, as at that point
we can just traverse the evsel_list and use evsel->attr.config +
event_name(evsel) instead of re-opening the /id file.

Reported-by: Franck Bui-Huu <vagabon.xyz@gmail.com>
Cc: Franck Bui-Huu <vagabon.xyz@gmail.com>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Han Pingtian <phan@redhat.com>
Cc: Ingo Molnar <mingo@elte.hu>
Cc: Mike Galbraith <efault@gmx.de>
Cc: Paul Mackerras <paulus@samba.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Stephane Eranian <eranian@google.com>
Cc: Tom Zanussi <tzanussi@gmail.com>
LKML-Reference: <20110117202801.GG2085@ghostprotocols.net>
Signed-off-by: Arnaldo Carvalho de Melo <acme@redhat.com>
11 years agoBtrfs: forced readonly mounts on errors
liubo [Thu, 6 Jan 2011 11:30:25 +0000 (19:30 +0800)]
Btrfs: forced readonly mounts on errors

This patch comes from "Forced readonly mounts on errors" ideas.

As we know, this is the first step in being more fault tolerant of disk
corruptions instead of just using BUG() statements.

The major content:
- add a framework for generating errors that should result in filesystems
  going readonly.
- keep FS state in disk super block.
- make sure that all of resource will be freed and released at umount time.
- make sure that fter FS is forced readonly on error, there will be no more
  disk change before FS is corrected. For this, we should stop write operation.

After this patch is applied, the conversion from BUG() to such a framework can
happen incrementally.

Signed-off-by: Liu Bo <liubo2009@cn.fujitsu.com>
Signed-off-by: Chris Mason <chris.mason@oracle.com>
11 years agoMerge branch 'next-devicetree' of git://git.secretlab.ca/git/linux-2.6
Linus Torvalds [Mon, 17 Jan 2011 19:18:40 +0000 (11:18 -0800)]
Merge branch 'next-devicetree' of git://git.secretlab.ca/git/linux-2.6

* 'next-devicetree' of git://git.secretlab.ca/git/linux-2.6:
  spi/spi_sh_msiof: fix a wrong free_irq() parameter
  dt/flattree: Return virtual address from early_init_dt_alloc_memory_arch()

11 years agoMerge git://git.kernel.org/pub/scm/linux/kernel/git/sfrench/cifs-2.6
Linus Torvalds [Mon, 17 Jan 2011 19:17:51 +0000 (11:17 -0800)]
Merge git://git./linux/kernel/git/sfrench/cifs-2.6

* git://git.kernel.org/pub/scm/linux/kernel/git/sfrench/cifs-2.6:
  cifs: add cruid= mount option
  cifs: cFYI the entire error code in map_smb_to_linux_error

11 years agoMerge git://git.infradead.org/mtd-2.6
Linus Torvalds [Mon, 17 Jan 2011 19:15:30 +0000 (11:15 -0800)]
Merge git://git.infradead.org/mtd-2.6

* git://git.infradead.org/mtd-2.6: (59 commits)
  mtd: mtdpart: disallow reading OOB past the end of the partition
  mtd: pxa3xx_nand: NULL dereference in pxa3xx_nand_probe
  UBI: use mtd->writebufsize to set minimal I/O unit size
  mtd: initialize writebufsize in the MTD object of a partition
  mtd: onenand: add mtd->writebufsize initialization
  mtd: nand: add mtd->writebufsize initialization
  mtd: cfi: add writebufsize initialization
  mtd: add writebufsize field to mtd_info struct
  mtd: OneNAND: OMAP2/3: prevent regulator sleeping while OneNAND is in use
  mtd: OneNAND: add enable / disable methods to onenand_chip
  mtd: m25p80: Fix JEDEC ID for AT26DF321
  mtd: txx9ndfmc: limit transfer bytes to 512 (ECC provides 6 bytes max)
  mtd: cfi_cmdset_0002: add support for Samsung K8D3x16UxC NOR chips
  mtd: cfi_cmdset_0002: add support for Samsung K8D6x16UxM NOR chips
  mtd: nand: ams-delta: drop omap_read/write, use ioremap
  mtd: m25p80: add debugging trace in sst_write
  mtd: nand: ams-delta: select for built-in by default
  mtd: OneNAND: lighten scary initial bad block messages
  mtd: OneNAND: OMAP2/3: add support for command line partitioning
  mtd: nand: rearrange ONFI revision checking, add ONFI 2.3
  ...

Fix up trivial conflict in drivers/mtd/Kconfig as per DavidW.

11 years agoecryptfs: remove unnecessary decrypt when extending a file
Frank Swiderski [Mon, 15 Nov 2010 18:43:22 +0000 (10:43 -0800)]
ecryptfs: remove unnecessary decrypt when extending a file

Removes an unecessary page decrypt from ecryptfs_begin_write when the
page is beyond the current file size. Previously, the call to
ecryptfs_decrypt_page would result in a read of 0 bytes, but still
attempt to decrypt an entire page. This patch detects that case and
merely zeros the page before marking it up-to-date.

Signed-off-by: Frank Swiderski <fes@chromium.org>
Signed-off-by: Tyler Hicks <tyhicks@linux.vnet.ibm.com>
11 years agoecryptfs: Fix ecryptfs_printk() size_t warnings
Tyler Hicks [Mon, 15 Nov 2010 23:36:38 +0000 (17:36 -0600)]
ecryptfs: Fix ecryptfs_printk() size_t warnings

Commit cb55d21f6fa19d8c6c2680d90317ce88c1f57269 revealed a number of
missing 'z' length modifiers in calls to ecryptfs_printk() when
printing variables of type size_t. This patch fixes those compiler
warnings.

Signed-off-by: Tyler Hicks <tyhicks@linux.vnet.ibm.com>
11 years agofs/ecryptfs: Add printf format/argument verification and fix fallout
Joe Perches [Wed, 10 Nov 2010 23:46:16 +0000 (15:46 -0800)]
fs/ecryptfs: Add printf format/argument verification and fix fallout

Add __attribute__((format... to __ecryptfs_printk
Make formats and arguments match.
Add casts to (unsigned long long) for %llu.

Signed-off-by: Joe Perches <joe@perches.com>
[tyhicks: 80 columns cleanup and fixed typo]
Signed-off-by: Tyler Hicks <tyhicks@linux.vnet.ibm.com>
11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6
Linus Torvalds [Mon, 17 Jan 2011 19:00:09 +0000 (11:00 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/viro/vfs-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6:
  fs: fix address space warnings in ioctl_fiemap()
  aio: check return value of create_workqueue()
  hpfs_setattr error case avoids unlock_kernel
  compat: copy missing fields in compat_statfs64 to user
  compat: update comment of compat statfs syscalls
  compat: remove unnecessary assignment in compat_rw_copy_check_uvector()
  fs: FS_POSIX_ACL does not depend on BLOCK
  fs: Remove unlikely() from fget_light()
  fs: Remove unlikely() from fput_light()
  fallocate should be a file operation
  make the feature checks in ->fallocate future proof
  staging: smbfs building fix
  tidy up around finish_automount()
  don't drop newmnt on error in do_add_mount()
  Take the completion of automount into new helper

11 years agoMerge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mattst88...
Linus Torvalds [Mon, 17 Jan 2011 18:58:44 +0000 (10:58 -0800)]
Merge branch 'for-linus' of git://git./linux/kernel/git/mattst88/alpha-2.6

* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/mattst88/alpha-2.6:
  alpha: fix WARN_ON in __local_bh_enable()
  alpha: fix breakage caused by df9ee29270
  alpha: add GENERIC_HARDIRQS_NO__DO_IRQ to Kconfig
  alpha/osf_sys: remove unused MAX_SELECT_SECONDS
  alpha: change to new Makefile flag variables
  alpha: kill off alpha_do_IRQ
  alpha: irq clean up
  alpha: use set_irq_chip and push down __do_IRQ to the machine types

11 years agoMerge branch 'drm-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/airlied...
Linus Torvalds [Mon, 17 Jan 2011 18:57:59 +0000 (10:57 -0800)]
Merge branch 'drm-fixes' of git://git./linux/kernel/git/airlied/drm-2.6

* 'drm-fixes' of git://git.kernel.org/pub/scm/linux/kernel/git/airlied/drm-2.6:
  drm/radeon/kms: balance asic_reset functions
  drm/radeon/kms: remove duplicate card_posted() functions
  drm/radeon/kms: add module option for pcie gen2
  drm/radeon/kms: fix typo in evergreen safe reg
  drm/nouveau: fix gpu page faults triggered by plymouthd
  drm/nouveau: greatly simplify mm, killing some bugs in the process
  drm/nvc0: enable protection of system-use-only structures in vm
  drm/nv40: initialise 0x17xx on all chipsets that have it
  drm/nv40: make detection of 0x4097-ful chipsets available everywhere