]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - sitara-linux/mmwavegesture-hmi.git/blob - mmwavegesture_hmi.pro
Makefile.build : add Makefile to enable build through SDK
[sitara-linux/mmwavegesture-hmi.git] / mmwavegesture_hmi.pro
1 QT += quick serialport core
3 #QT += quick  core
4 CONFIG += c++11
6 # The following define makes your compiler emit warnings if you use
7 # any feature of Qt which as been marked deprecated (the exact warnings
8 # depend on your compiler). Please consult the documentation of the
9 # deprecated API in order to know how to port your code away from it.
10 DEFINES += QT_DEPRECATED_WARNINGS
12 # You can also make your code fail to compile if you use deprecated APIs.
13 # In order to do so, uncomment the following line.
14 # You can also select to disable deprecated APIs only up to a certain version of Qt.
15 #DEFINES += QT_DISABLE_DEPRECATED_BEFORE=0x060000    # disables all the APIs deprecated before Qt 6.0.0
17 SOURCES += main.cpp  keyword.cpp serialreaderthread.cpp
19 HEADERS +=  keyword.h serialreaderthread.h \
20     mmwgesturein.h
23 RESOURCES += qml.qrc
25 # Additional import path used to resolve QML modules in Qt Creator's code model
26 QML_IMPORT_PATH =
28 # Additional import path used to resolve QML modules just for Qt Quick Designer
29 QML_DESIGNER_IMPORT_PATH =
31 # Default rules for deployment.
32 qnx: target.path = /tmp/$${TARGET}/bin
33 else: unix:!android: target.path = /opt/$${TARGET}/bin
34 !isEmpty(target.path): INSTALLS += target
36 DISTFILES +=