Added Support for Scaling and Stitching New feature added to demonstrate GC320's ability to scale images and stitch images together. Signed-off-by: Krunal Bhargav <a0227568@ti.com>
video graphics test : new demo application This is completly new application sharing the same name video graphcis test. The previous demo application will no longer be supported. eglf_kms QT QPA API has been enhanced to support multiple display and advance Display subsystem capabilities like scaling, aplhablending and overlaying. This application demonstartes - 1. New enhanced QT eglfs_kms QPA capabilties 2. Dual screen display using eglfs_kms 3. Two different graphics content on two screen using QT QML drawning on SGX 4. 90 degree rotation using GC320 5. Two different video source on two screens - one from VIP capture and other from GC320 90 degree rotated content. dual screen display for graphics content drawn using QT QML annd user overlay planes from camera source and GC320 rotation. Signed-off-by: Manisha Agrawal <manisha.agrawal@ti.com>
video : graphics : test : Advance video use case This project is a place holder to demonstrate advance video use cases needing multiple video overlayes using DSS and GC320, multiple video display, same graphics background plane or different, demonstrating advance feature usage of DSS etc on AM57xx platform. To begin with, the project demonstrate video and graphics plane overlay using DSS. eglfs_kms is the special QPA plugin developed that let application control DSS using DRM api along with QT. QT is the master of DRM resource but with special callback handles let the application controls the DSS for video planes. Signed-off-by: Manisha Agrawal <manisha.agrawal@ti.com>