/* ** ============================================================================= ** Copyright (c) 2016 Texas Instruments Inc. ** ** This program is free software; you can redistribute it and/or modify it under ** the terms of the GNU General Public License as published by the Free Software ** Foundation; version 2. ** ** This program is distributed in the hope that it will be useful, but WITHOUT ** ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS ** FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details. ** ** File: ** tiload.c ** ** Description: ** utility for TAS2557 Android in-system tuning ** ** ============================================================================= */ #include #include #include #include #include #include #include #include #include #include #include #include #include #include #include "tiload.h" /* enable debug prints in the driver */ #define DEBUG static struct cdev *tiload_cdev; static int tiload_major; /* Dynamic allocation of Mjr No. */ static int tiload_opened; /* Dynamic allocation of Mjr No. */ static struct tas2557_priv *g_TAS2557; struct class *tiload_class; static unsigned int magic_num; static char gPage; static char gBook; /******************************** Debug section *****************************/ /*---------------------------------------------------------------------------- * Function : tiload_open * * Purpose : open method for tiload programming interface *---------------------------------------------------------------------------- */ static int tiload_open(struct inode *in, struct file *filp) { struct tas2557_priv *pTAS2557 = g_TAS2557; dev_info(pTAS2557->dev, "%s\n", __func__); if (tiload_opened) { dev_info(pTAS2557->dev, "%s device is already opened\n", "tiload"); return -EINVAL; } filp->private_data = (void *)pTAS2557; tiload_opened++; return 0; } /*---------------------------------------------------------------------------- * Function : tiload_release * * Purpose : close method for tiload programming interface *---------------------------------------------------------------------------- */ static int tiload_release(struct inode *in, struct file *filp) { struct tas2557_priv *pTAS2557 = (struct tas2557_priv *)filp->private_data; dev_info(pTAS2557->dev, "%s\n", __func__); filp->private_data = NULL; tiload_opened--; return 0; } #define MAX_LENGTH 128 /*---------------------------------------------------------------------------- * Function : tiload_read * * Purpose : read from codec *---------------------------------------------------------------------------- */ static ssize_t tiload_read(struct file *filp, char __user *buf, size_t count, loff_t *offset) { struct tas2557_priv *pTAS2557 = (struct tas2557_priv *)filp->private_data; static char rd_data[MAX_LENGTH + 1]; unsigned int nCompositeRegister = 0, Value = 0; char reg_addr; size_t size; int ret = 0; #ifdef DEBUG /* int i; */ #endif dev_info(pTAS2557->dev, "%s\n", __func__); if (count > MAX_LENGTH) { dev_err(pTAS2557->dev, "Max %d bytes can be read\n", MAX_LENGTH); return -EINVAL; } /* copy register address from user space */ size = copy_from_user(®_addr, buf, 1); if (size != 0) { dev_err(pTAS2557->dev, "read: copy_from_user failure\n"); return -EINVAL; } size = count; nCompositeRegister = BPR_REG(gBook, gPage, reg_addr); if (count == 1) { ret = pTAS2557->read(pTAS2557, 0x80000000 | nCompositeRegister, &Value); if (ret >= 0) rd_data[0] = (char) Value; } else if (count > 1) { ret = pTAS2557->bulk_read(pTAS2557, 0x80000000 | nCompositeRegister, rd_data, size); } if (ret < 0) dev_err(pTAS2557->dev, "%s, %d, ret=%d, count=%zu error happen!\n", __func__, __LINE__, ret, count); #ifdef DEBUG dev_info(pTAS2557->dev, "read size = %d, reg_addr= %x , count = %d\n", (int) size, reg_addr, (int) count); /* for (i = 0; i < (int) size; i++) { * dev_dbg(pTAS2557->dev, "rd_data[%d]=%x\n", i, rd_data[i]); * } */ #endif if (size != count) dev_err(pTAS2557->dev, "read %d registers from the codec\n", (int) size); if (copy_to_user(buf, rd_data, size) != 0) { dev_err(pTAS2557->dev, "copy_to_user failed\n"); return -EINVAL; } return size; } /* *---------------------------------------------------------------------------- * Function : tiload_write * * Purpose : write to codec *---------------------------------------------------------------------------- */ static ssize_t tiload_write(struct file *filp, const char __user *buf, size_t count, loff_t *offset) { struct tas2557_priv *pTAS2557 = (struct tas2557_priv *)filp->private_data; static char wr_data[MAX_LENGTH + 1]; char *pData = wr_data; size_t size; unsigned int nCompositeRegister = 0; unsigned int nRegister; int ret = 0; #ifdef DEBUG /* int i; */ #endif dev_info(pTAS2557->dev, "%s\n", __func__); if (count > MAX_LENGTH) { dev_err(pTAS2557->dev, "Max %d bytes can be read\n", MAX_LENGTH); return -EINVAL; } /* copy buffer from user space */ size = copy_from_user(wr_data, buf, count); if (size != 0) { dev_err(pTAS2557->dev, "copy_from_user failure %d\n", (int) size); return -EINVAL; } #ifdef DEBUG dev_info(pTAS2557->dev, "write size = %zu\n", count); /* for (i = 0; i < (int) count; i++) { * dev_info(pTAS2557->dev, "wr_data[%d]=%x\n", i, wr_data[i]); * } */ #endif nRegister = wr_data[0]; size = count; if ((nRegister == 127) && (gPage == 0)) { gBook = wr_data[1]; return size; } if (nRegister == 0) { gPage = wr_data[1]; pData++; count--; } nCompositeRegister = BPR_REG(gBook, gPage, nRegister); if (count == 2) { ret = pTAS2557->write(pTAS2557, 0x80000000 | nCompositeRegister, pData[1]); } else if (count > 2) { ret = pTAS2557->bulk_write(pTAS2557, 0x80000000 | nCompositeRegister, &pData[1], count - 1); } if (ret < 0) dev_err(pTAS2557->dev, "%s, %d, ret=%d, count=%zu, ERROR Happen\n", __func__, __LINE__, ret, count); return size; } static void tiload_route_IO(struct tas2557_priv *pTAS2557, unsigned int bLock) { if (bLock) pTAS2557->write(pTAS2557, 0xAFFEAFFE, 0xBABEBABE); else pTAS2557->write(pTAS2557, 0xBABEBABE, 0xAFFEAFFE); } static long tiload_ioctl(struct file *filp, unsigned int cmd, unsigned long arg) { struct tas2557_priv *pTAS2557 = (struct tas2557_priv *)filp->private_data; long num = 0; void __user *argp = (void __user *) arg; int val; struct BPR bpr; dev_info(pTAS2557->dev, "%s, cmd=0x%x\n", __func__, cmd); /* if (_IOC_TYPE(cmd) != TILOAD_IOC_MAGIC) * return -ENOTTY; */ switch (cmd) { case TILOAD_IOMAGICNUM_GET: num = copy_to_user(argp, &magic_num, sizeof(int)); break; case TILOAD_IOMAGICNUM_SET: num = copy_from_user(&magic_num, argp, sizeof(int)); dev_info(pTAS2557->dev, "TILOAD_IOMAGICNUM_SET\n"); tiload_route_IO(pTAS2557, magic_num); break; case TILOAD_BPR_READ: break; case TILOAD_BPR_WRITE: num = copy_from_user(&bpr, argp, sizeof(struct BPR)); dev_info(pTAS2557->dev, "TILOAD_BPR_WRITE: 0x%02X, 0x%02X, 0x%02X\n\r", bpr.nBook, bpr.nPage, bpr.nRegister); break; case TILOAD_IOCTL_SET_CHL: break; case TILOAD_IOCTL_SET_CONFIG: num = copy_from_user(&val, argp, sizeof(val)); pTAS2557->set_config(pTAS2557, val); break; case TILOAD_IOCTL_SET_CALIBRATION: num = copy_from_user(&val, argp, sizeof(val)); pTAS2557->set_calibration(pTAS2557, val); break; default: break; } return num; } #ifdef CONFIG_COMPAT static long tiload_compat_ioctl(struct file *filp, unsigned int cmd, unsigned long arg) { struct tas2557_priv *pTAS2557 = (struct tas2557_priv *)filp->private_data; long nResult = 0; switch (cmd) { case TILOAD_COMPAT_IOMAGICNUM_GET: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_IOMAGICNUM_GET=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_IOMAGICNUM_GET, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_IOMAGICNUM_SET: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_IOMAGICNUM_SET=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_IOMAGICNUM_SET, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_BPR_READ: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_BPR_READ=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_BPR_READ, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_BPR_WRITE: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_BPR_WRITE=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_BPR_WRITE, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_IOCTL_SET_CHL: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_IOCTL_SET_CHL=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_IOCTL_SET_CHL, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_IOCTL_SET_CONFIG: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_IOCTL_SET_CONFIG=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_IOCTL_SET_CONFIG, (unsigned long) compat_ptr(arg)); break; case TILOAD_COMPAT_IOCTL_SET_CALIBRATION: dev_info(pTAS2557->dev, "%s, TILOAD_COMPAT_IOCTL_SET_CALIBRATION=0x%x\n", __func__, cmd); nResult = tiload_ioctl(filp, TILOAD_IOCTL_SET_CALIBRATION, (unsigned long) compat_ptr(arg)); break; default: dev_err(pTAS2557->dev, "%s, unsupport compat ioctl=0x%x\n", __func__, cmd); break; } return nResult; } #endif /*********** File operations structure for tiload *************/ static const struct file_operations tiload_fops = { .owner = THIS_MODULE, .open = tiload_open, .release = tiload_release, .read = tiload_read, .write = tiload_write, .unlocked_ioctl = tiload_ioctl, #ifdef CONFIG_COMPAT .compat_ioctl = tiload_compat_ioctl, #endif }; /*---------------------------------------------------------------------------- * Function : tiload_driver_init * * Purpose : Register a char driver for dynamic tiload programming *---------------------------------------------------------------------------- */ int tiload_driver_init(struct tas2557_priv *pTAS2557) { int result; dev_t dev = MKDEV(tiload_major, 0); g_TAS2557 = pTAS2557; dev_info(pTAS2557->dev, "%s\n", __func__); result = alloc_chrdev_region(&dev, 0, 1, DEVICE_NAME); if (result < 0) { dev_err(pTAS2557->dev, "cannot allocate major number %d\n", tiload_major); return result; } tiload_class = class_create(THIS_MODULE, DEVICE_NAME); tiload_major = MAJOR(dev); dev_info(pTAS2557->dev, "allocated Major Number: %d\n", tiload_major); tiload_cdev = cdev_alloc(); cdev_init(tiload_cdev, &tiload_fops); tiload_cdev->owner = THIS_MODULE; tiload_cdev->ops = &tiload_fops; if (device_create(tiload_class, NULL, dev, NULL, "tiload_node") == NULL) dev_err(pTAS2557->dev, "Device creation failed\n"); if (cdev_add(tiload_cdev, dev, 1) < 0) { dev_err(pTAS2557->dev, "tiload_driver: cdev_add failed\n"); unregister_chrdev_region(dev, 1); tiload_cdev = NULL; return 1; } dev_info(pTAS2557->dev, "Registered TiLoad driver, Major number: %d\n", tiload_major); /* class_device_create(tiload_class, NULL, dev, NULL, DEVICE_NAME, 0); */ return 0; } MODULE_AUTHOR("Texas Instruments Inc."); MODULE_DESCRIPTION("Utility for TAS2557 Android in-system tuning"); MODULE_LICENSE("GPL v2");