update TAS2557 mono FTC
[tas2557sw-android/tas2557-ftc.git] / tas2557_ftc.h
1 /*\r
2 ** =============================================================================\r
3 ** Copyright (c) 2016  Texas Instruments Inc.\r
4 **\r
5 ** This program is free software; you can redistribute it and/or modify it under\r
6 ** the terms of the GNU General Public License as published by the Free Software \r
7 ** Foundation; version 2.\r
8 **\r
9 ** This program is distributed in the hope that it will be useful, but WITHOUT\r
10 ** ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS\r
11 ** FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details.\r
12 **\r
13 ** You should have received a copy of the GNU General Public License along with\r
14 ** this program; if not, write to the Free Software Foundation, Inc., 51 Franklin\r
15 ** Street, Fifth Floor, Boston, MA 02110-1301, USA.\r
16 **\r
17 ** File:\r
18 **     tas2557_ftc.h\r
19 **\r
20 ** Description:\r
21 **     header file for tas2557_ftc.c\r
22 **\r
23 ** =============================================================================\r
24 */\r
25 \r
26 #ifndef TAS2557_FTC_H_\r
27 #define TAS2557_FTC_H_\r
28 \r
29 #include <stdint.h>\r
30 #include <stdbool.h>\r
31 \r
32 struct TSPKCharData {\r
33         double nSpkTMax;\r
34         double nSpkReTolPer;\r
35         double nSpkReAlpha;\r
36 \r
37         double nPPC3_Re0;\r
38         double nPPC3_RTV;\r
39         double nPPC3_RTM;\r
40         double nPPC3_RTVA;\r
41         double nPPC3_SysGain;\r
42         double nPPC3_DevNonlinPer;\r
43 \r
44         double nReHi;\r
45         double nReLo;\r
46 };\r
47 \r
48 struct TFTCConfiguration {\r
49         bool bVerbose;\r
50         bool bLoadCalibration;\r
51         unsigned int nCalibrationTime;\r
52 \r
53         struct TSPKCharData nTSpkCharDevA;\r
54 };\r
55 \r
56 uint32_t tas2557_ftc(double t_cal, struct TFTCConfiguration *pFTCC);\r
57 \r
58 #endif /* TAS2557_FTC_H_ */\r