/* ** ============================================================================= ** Copyright (c) 2016 Texas Instruments Inc. ** ** This program is free software; you can redistribute it and/or modify it under ** the terms of the GNU General Public License as published by the Free Software ** Foundation; version 2. ** ** This program is distributed in the hope that it will be useful, but WITHOUT ** ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS ** FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details. ** ** You should have received a copy of the GNU General Public License along with ** this program; if not, write to the Free Software Foundation, Inc., 51 Franklin ** Street, Fifth Floor, Boston, MA 02110-1301, USA. ** ** File: ** tas2557_lib_ftc.h ** ** Description: ** header file for tas2557_lib_ftc.c ** ** ============================================================================= */ #ifndef TAS2557_LIB_FTC_H_ #define TAS2557_LIB_FTC_H_ #include #include int get_lib_ver(void); void tas2557_ftc_set_PGID(unsigned char nPGID); void tas2557_ftc_start(void); void set_re(double re_ppc3, double re, double alpha); void set_temp_cal(uint32_t prm_pow, uint32_t prm_tlimit); double get_re(double re_ppc3); uint32_t calc_prm_pow(double re, double delta_t_max, double nRTV, double nRTM, double nRTVA, double nSysGain); uint32_t calc_prm_tlimit(double delta_t_max, double alpha, double nDevNonlinPer, double nRTV, double nRTM, double nRTVA); #endif /* TAS2557_LIB_FTC_H_ */