/* ** ============================================================================= ** Copyright (c) 2016 Texas Instruments Inc. ** ** This program is free software; you can redistribute it and/or modify it under ** the terms of the GNU General Public License as published by the Free Software ** Foundation; version 2. ** ** This program is distributed in the hope that it will be useful, but WITHOUT ** ANY WARRANTY; without even the implied warranty of MERCHANTABILITY or FITNESS ** FOR A PARTICULAR PURPOSE. See the GNU General Public License for more details. ** ** You should have received a copy of the GNU General Public License along with ** this program; if not, write to the Free Software Foundation, Inc., 51 Franklin ** Street, Fifth Floor, Boston, MA 02110-1301, USA. ** ** File: ** tas2557_ftc.c ** ** Description: ** factory test program for TAS2557 Android devices ** ** ============================================================================= */ #include #include #include #include #include "system.h" #include "tas2557.h" // TAS2557 Driver #include "tas2557_ftc_lib.h" #include "tas2557_ftc.h" // TAS2557 Factory Test and Calibration Tool #define PI 3.14159 static struct TFTCConfiguration *gpFTCC; // ----------------------------------------------------------------------------- // tas2557_ftc // ----------------------------------------------------------------------------- // Description: // Obtains Re, f0, Q and T_cal from the speaker. This only needs to be // executed once during production line test. // ----------------------------------------------------------------------------- uint32_t tas2557_ftc(double t_cal, struct TFTCConfiguration *pFTCC) { int nResult = 0; double dev_a_re = pFTCC->nTSpkCharDevA.nPPC3_Re0; // Default Re uint32_t dev_a_prm_pow = 0; // Total RMS power coefficient uint32_t dev_a_prm_tlimit = 0; // Delta temperature limit coefficient double dev_b_re = pFTCC->nTSpkCharDevB.nPPC3_Re0; // Default Re uint32_t dev_b_prm_pow = 0; // Total RMS power coefficient uint32_t dev_b_prm_tlimit = 0; // Delta temperature limit coefficient uint8_t nPGID; uint32_t libVersion; uint32_t result = 0; pid_t nPlaybackProcess; gpFTCC = pFTCC; libVersion = get_lib_ver(); printf("libVersion=0x%x\r\n", libVersion); /* get device PGID */ tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); nPGID = tas2557_get_PGID(); printf("PGID=0x%x\r\n", nPGID); /* set device PGID to FTC process */ tas2557_ftc_set_PGID(nPGID); // STEP 1: Play calibration signal tas2557_mixer_command("PRI_MI2S_RX Audio Mixer MultiMedia1", 1); //platform dependent nPlaybackProcess = sys_play_wav("silense.wav", "loop"); // STEP 2: start calibration process tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); tas2557_ftc_start(); tas2557_switch_device(gpFTCC->nTSpkCharDevB.nDevAddr); tas2557_ftc_start(); // STEP 3: Wait for algorithm to converge sys_delay(gpFTCC->nCalibrationTime); // Delay // STEP 4: Get actual Re from TAS2557 tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); dev_a_re = get_re(gpFTCC->nTSpkCharDevA.nPPC3_Re0); tas2557_switch_device(gpFTCC->nTSpkCharDevB.nDevAddr); dev_b_re = get_re(gpFTCC->nTSpkCharDevB.nPPC3_Re0); // STEP 5: check speaker bounds nResult = check_spk_bounds(gpFTCC, dev_a_re, dev_b_re); // STEP 6: Set temperature limit to target TMAX if ((nResult& RE1_CHK_MSK) == RESULT_PASS) { tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); dev_a_prm_pow = calc_prm_pow (dev_a_re, gpFTCC->nTSpkCharDevA.nSpkTMax - t_cal, gpFTCC->nTSpkCharDevA.nPPC3_RTV, gpFTCC->nTSpkCharDevA.nPPC3_RTM, gpFTCC->nTSpkCharDevA.nPPC3_RTVA, gpFTCC->nTSpkCharDevA.nPPC3_SysGain); dev_a_prm_tlimit = calc_prm_tlimit(gpFTCC->nTSpkCharDevA.nSpkTMax - t_cal, gpFTCC->nTSpkCharDevA.nSpkReAlpha, gpFTCC->nTSpkCharDevA.nPPC3_DevNonlinPer, gpFTCC->nTSpkCharDevA.nPPC3_RTV, gpFTCC->nTSpkCharDevA.nPPC3_RTM, gpFTCC->nTSpkCharDevA.nPPC3_RTVA); set_re(gpFTCC->nTSpkCharDevA.nPPC3_Re0, dev_a_re, gpFTCC->nTSpkCharDevA.nSpkReAlpha); set_temp_cal(dev_a_prm_pow, dev_a_prm_tlimit); } if ((nResult& RE2_CHK_MSK) == RESULT_PASS) { tas2557_switch_device(gpFTCC->nTSpkCharDevB.nDevAddr); dev_b_prm_pow = calc_prm_pow (dev_b_re, gpFTCC->nTSpkCharDevB.nSpkTMax - t_cal, gpFTCC->nTSpkCharDevB.nPPC3_RTV, gpFTCC->nTSpkCharDevB.nPPC3_RTM, gpFTCC->nTSpkCharDevB.nPPC3_RTVA, gpFTCC->nTSpkCharDevB.nPPC3_SysGain); dev_b_prm_tlimit = calc_prm_tlimit(gpFTCC->nTSpkCharDevB.nSpkTMax - t_cal, gpFTCC->nTSpkCharDevB.nSpkReAlpha, gpFTCC->nTSpkCharDevB.nPPC3_DevNonlinPer, gpFTCC->nTSpkCharDevB.nPPC3_RTV, gpFTCC->nTSpkCharDevB.nPPC3_RTM, gpFTCC->nTSpkCharDevB.nPPC3_RTVA); set_re(gpFTCC->nTSpkCharDevB.nPPC3_Re0, dev_b_re, gpFTCC->nTSpkCharDevB.nSpkReAlpha); set_temp_cal(dev_b_prm_pow, dev_b_prm_tlimit); } // STEP 7: start calibration process tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); tas2557_ftc_stop(); tas2557_switch_device(gpFTCC->nTSpkCharDevB.nDevAddr); tas2557_ftc_stop(); sys_stop_wav(nPlaybackProcess); // STEP 8: Save Re, and Cal Temp into a file tas2557_save_cal(gpFTCC, dev_a_re, dev_a_prm_pow, dev_a_prm_tlimit, dev_b_re, dev_b_prm_pow, dev_b_prm_tlimit, t_cal, nResult, "tas2557_cal.txt"); // STEP 9: Save .bin file for TAS2555 driver if ((nResult & (RE1_CHK_MSK | RE2_CHK_MSK)) == RESULT_PASS) { tas2557_open_bin("tas2557_cal.bin", gpFTCC->nTSpkCharDevA.nDevAddr, gpFTCC->nTSpkCharDevB.nDevAddr); if ((nResult & RE1_CHK_MSK) == RESULT_PASS) { tas2557_switch_device(gpFTCC->nTSpkCharDevA.nDevAddr); set_re(gpFTCC->nTSpkCharDevA.nPPC3_Re0, dev_a_re, gpFTCC->nTSpkCharDevA.nSpkReAlpha); set_temp_cal(dev_a_prm_pow, dev_a_prm_tlimit); } if ((nResult & RE2_CHK_MSK) == RESULT_PASS) { tas2557_switch_device(gpFTCC->nTSpkCharDevB.nDevAddr); set_re(gpFTCC->nTSpkCharDevB.nPPC3_Re0, dev_b_re, gpFTCC->nTSpkCharDevB.nSpkReAlpha); set_temp_cal(dev_b_prm_pow, dev_b_prm_tlimit); } tas2557_close_bin(); } if (gpFTCC->bLoadCalibration) tas2557_load_calibration(0xFF); tas2557_ftc_release(); return result; }