DoD: get rid of 'integrated'
authorFelipe Balbi <balbi@ti.com>
Tue, 21 May 2013 20:15:09 +0000 (23:15 +0300)
committerFelipe Balbi <balbi@ti.com>
Tue, 21 May 2013 21:16:43 +0000 (00:16 +0300)
We're targetting mainline only development. There
won't be an official TI Integration tree from LCPD,
so that requirement can vanish.

While at that, also make it clear we want automated
test scripts.

Acked-by: Chase Maupin <chase.maupin@ti.com>
Signed-off-by: Felipe Balbi <balbi@ti.com>
definition-of-done.tex

index 21cd29a7c4ec1299e0e1bc12a59b6b7215f69310..85b569166aa0573a2eeadab724d1a6d2819f89f4 100644 (file)
@@ -95,9 +95,6 @@ definition of Done can be broken down into the following main parts
     \item A Backlog item is not Done until it has been Submitted for
            integration upstream.  For more details see section
            \ref{sec:lcpd-definition-submitted}.
-    \item A Backlog item is not Done until it has been Integrated into the
-        TI integration tree for release.  For more details see section
-        \ref{sec:lcpd-definition-integrated}.
 \end{enumerate}
 
 \paragraph{}
@@ -115,7 +112,7 @@ people this section will detail what we mean when we say tested.
 
 \begin{enumerate}
     \item There is a simple piece of code or scripting that will enable
-          validation of the new functionality.
+          automated validation of the new functionality.
     \item Any environment setup required to run the test code is documented
           within the code itself.
     \item The test code has been provided to the system test team so it can
@@ -190,18 +187,6 @@ constantly being pushed upstream.  More information will be given on this,
 including the role of the Product Owner in section \ref{sec:upstreaming}.
 
 
-\subsection{Integrated}
-\label{lcpd-definition-integrated}
-
-\paragraph{}
-In the LCPD definition of Done an item is not considered Done until it has been
-\textbf{Integrated} into the Integration tree.  The purpose is to make sure
-that the work is in a location where it is available for immediate consumption
-by the Business Units to support their customer releases.  There are possible
-exceptions to this as detailed in section \ref{sec:exceptions} but the general
-theme is that work done needs to be both upstreamed as well as made available
-within a release to enable customers.
-
 \section{Exceptions}
 \label{sec:exceptions}