]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-analog-linux-kernel/dmurphy-analog.git/blob - fs/splice.c
defconfig: Enable M_CAN for dra7
[ti-analog-linux-kernel/dmurphy-analog.git] / fs / splice.c
1 /*
2  * "splice": joining two ropes together by interweaving their strands.
3  *
4  * This is the "extended pipe" functionality, where a pipe is used as
5  * an arbitrary in-memory buffer. Think of a pipe as a small kernel
6  * buffer that you can use to transfer data from one end to the other.
7  *
8  * The traditional unix read/write is extended with a "splice()" operation
9  * that transfers data buffers to or from a pipe buffer.
10  *
11  * Named by Larry McVoy, original implementation from Linus, extended by
12  * Jens to support splicing to files, network, direct splicing, etc and
13  * fixing lots of bugs.
14  *
15  * Copyright (C) 2005-2006 Jens Axboe <axboe@kernel.dk>
16  * Copyright (C) 2005-2006 Linus Torvalds <torvalds@osdl.org>
17  * Copyright (C) 2006 Ingo Molnar <mingo@elte.hu>
18  *
19  */
20 #include <linux/bvec.h>
21 #include <linux/fs.h>
22 #include <linux/file.h>
23 #include <linux/pagemap.h>
24 #include <linux/splice.h>
25 #include <linux/memcontrol.h>
26 #include <linux/mm_inline.h>
27 #include <linux/swap.h>
28 #include <linux/writeback.h>
29 #include <linux/export.h>
30 #include <linux/syscalls.h>
31 #include <linux/uio.h>
32 #include <linux/security.h>
33 #include <linux/gfp.h>
34 #include <linux/socket.h>
35 #include <linux/compat.h>
36 #include <linux/sched/signal.h>
38 #include "internal.h"
40 /*
41  * Attempt to steal a page from a pipe buffer. This should perhaps go into
42  * a vm helper function, it's already simplified quite a bit by the
43  * addition of remove_mapping(). If success is returned, the caller may
44  * attempt to reuse this page for another destination.
45  */
46 static int page_cache_pipe_buf_steal(struct pipe_inode_info *pipe,
47                                      struct pipe_buffer *buf)
48 {
49         struct page *page = buf->page;
50         struct address_space *mapping;
52         lock_page(page);
54         mapping = page_mapping(page);
55         if (mapping) {
56                 WARN_ON(!PageUptodate(page));
58                 /*
59                  * At least for ext2 with nobh option, we need to wait on
60                  * writeback completing on this page, since we'll remove it
61                  * from the pagecache.  Otherwise truncate wont wait on the
62                  * page, allowing the disk blocks to be reused by someone else
63                  * before we actually wrote our data to them. fs corruption
64                  * ensues.
65                  */
66                 wait_on_page_writeback(page);
68                 if (page_has_private(page) &&
69                     !try_to_release_page(page, GFP_KERNEL))
70                         goto out_unlock;
72                 /*
73                  * If we succeeded in removing the mapping, set LRU flag
74                  * and return good.
75                  */
76                 if (remove_mapping(mapping, page)) {
77                         buf->flags |= PIPE_BUF_FLAG_LRU;
78                         return 0;
79                 }
80         }
82         /*
83          * Raced with truncate or failed to remove page from current
84          * address space, unlock and return failure.
85          */
86 out_unlock:
87         unlock_page(page);
88         return 1;
89 }
91 static void page_cache_pipe_buf_release(struct pipe_inode_info *pipe,
92                                         struct pipe_buffer *buf)
93 {
94         put_page(buf->page);
95         buf->flags &= ~PIPE_BUF_FLAG_LRU;
96 }
98 /*
99  * Check whether the contents of buf is OK to access. Since the content
100  * is a page cache page, IO may be in flight.
101  */
102 static int page_cache_pipe_buf_confirm(struct pipe_inode_info *pipe,
103                                        struct pipe_buffer *buf)
105         struct page *page = buf->page;
106         int err;
108         if (!PageUptodate(page)) {
109                 lock_page(page);
111                 /*
112                  * Page got truncated/unhashed. This will cause a 0-byte
113                  * splice, if this is the first page.
114                  */
115                 if (!page->mapping) {
116                         err = -ENODATA;
117                         goto error;
118                 }
120                 /*
121                  * Uh oh, read-error from disk.
122                  */
123                 if (!PageUptodate(page)) {
124                         err = -EIO;
125                         goto error;
126                 }
128                 /*
129                  * Page is ok afterall, we are done.
130                  */
131                 unlock_page(page);
132         }
134         return 0;
135 error:
136         unlock_page(page);
137         return err;
140 const struct pipe_buf_operations page_cache_pipe_buf_ops = {
141         .can_merge = 0,
142         .confirm = page_cache_pipe_buf_confirm,
143         .release = page_cache_pipe_buf_release,
144         .steal = page_cache_pipe_buf_steal,
145         .get = generic_pipe_buf_get,
146 };
148 static int user_page_pipe_buf_steal(struct pipe_inode_info *pipe,
149                                     struct pipe_buffer *buf)
151         if (!(buf->flags & PIPE_BUF_FLAG_GIFT))
152                 return 1;
154         buf->flags |= PIPE_BUF_FLAG_LRU;
155         return generic_pipe_buf_steal(pipe, buf);
158 static const struct pipe_buf_operations user_page_pipe_buf_ops = {
159         .can_merge = 0,
160         .confirm = generic_pipe_buf_confirm,
161         .release = page_cache_pipe_buf_release,
162         .steal = user_page_pipe_buf_steal,
163         .get = generic_pipe_buf_get,
164 };
166 static void wakeup_pipe_readers(struct pipe_inode_info *pipe)
168         smp_mb();
169         if (waitqueue_active(&pipe->wait))
170                 wake_up_interruptible(&pipe->wait);
171         kill_fasync(&pipe->fasync_readers, SIGIO, POLL_IN);
174 /**
175  * splice_to_pipe - fill passed data into a pipe
176  * @pipe:       pipe to fill
177  * @spd:        data to fill
178  *
179  * Description:
180  *    @spd contains a map of pages and len/offset tuples, along with
181  *    the struct pipe_buf_operations associated with these pages. This
182  *    function will link that data to the pipe.
183  *
184  */
185 ssize_t splice_to_pipe(struct pipe_inode_info *pipe,
186                        struct splice_pipe_desc *spd)
188         unsigned int spd_pages = spd->nr_pages;
189         int ret = 0, page_nr = 0;
191         if (!spd_pages)
192                 return 0;
194         if (unlikely(!pipe->readers)) {
195                 send_sig(SIGPIPE, current, 0);
196                 ret = -EPIPE;
197                 goto out;
198         }
200         while (pipe->nrbufs < pipe->buffers) {
201                 int newbuf = (pipe->curbuf + pipe->nrbufs) & (pipe->buffers - 1);
202                 struct pipe_buffer *buf = pipe->bufs + newbuf;
204                 buf->page = spd->pages[page_nr];
205                 buf->offset = spd->partial[page_nr].offset;
206                 buf->len = spd->partial[page_nr].len;
207                 buf->private = spd->partial[page_nr].private;
208                 buf->ops = spd->ops;
209                 buf->flags = 0;
211                 pipe->nrbufs++;
212                 page_nr++;
213                 ret += buf->len;
215                 if (!--spd->nr_pages)
216                         break;
217         }
219         if (!ret)
220                 ret = -EAGAIN;
222 out:
223         while (page_nr < spd_pages)
224                 spd->spd_release(spd, page_nr++);
226         return ret;
228 EXPORT_SYMBOL_GPL(splice_to_pipe);
230 ssize_t add_to_pipe(struct pipe_inode_info *pipe, struct pipe_buffer *buf)
232         int ret;
234         if (unlikely(!pipe->readers)) {
235                 send_sig(SIGPIPE, current, 0);
236                 ret = -EPIPE;
237         } else if (pipe->nrbufs == pipe->buffers) {
238                 ret = -EAGAIN;
239         } else {
240                 int newbuf = (pipe->curbuf + pipe->nrbufs) & (pipe->buffers - 1);
241                 pipe->bufs[newbuf] = *buf;
242                 pipe->nrbufs++;
243                 return buf->len;
244         }
245         pipe_buf_release(pipe, buf);
246         return ret;
248 EXPORT_SYMBOL(add_to_pipe);
250 /*
251  * Check if we need to grow the arrays holding pages and partial page
252  * descriptions.
253  */
254 int splice_grow_spd(const struct pipe_inode_info *pipe, struct splice_pipe_desc *spd)
256         unsigned int buffers = READ_ONCE(pipe->buffers);
258         spd->nr_pages_max = buffers;
259         if (buffers <= PIPE_DEF_BUFFERS)
260                 return 0;
262         spd->pages = kmalloc_array(buffers, sizeof(struct page *), GFP_KERNEL);
263         spd->partial = kmalloc_array(buffers, sizeof(struct partial_page),
264                                      GFP_KERNEL);
266         if (spd->pages && spd->partial)
267                 return 0;
269         kfree(spd->pages);
270         kfree(spd->partial);
271         return -ENOMEM;
274 void splice_shrink_spd(struct splice_pipe_desc *spd)
276         if (spd->nr_pages_max <= PIPE_DEF_BUFFERS)
277                 return;
279         kfree(spd->pages);
280         kfree(spd->partial);
283 /**
284  * generic_file_splice_read - splice data from file to a pipe
285  * @in:         file to splice from
286  * @ppos:       position in @in
287  * @pipe:       pipe to splice to
288  * @len:        number of bytes to splice
289  * @flags:      splice modifier flags
290  *
291  * Description:
292  *    Will read pages from given file and fill them into a pipe. Can be
293  *    used as long as it has more or less sane ->read_iter().
294  *
295  */
296 ssize_t generic_file_splice_read(struct file *in, loff_t *ppos,
297                                  struct pipe_inode_info *pipe, size_t len,
298                                  unsigned int flags)
300         struct iov_iter to;
301         struct kiocb kiocb;
302         int idx, ret;
304         iov_iter_pipe(&to, READ, pipe, len);
305         idx = to.idx;
306         init_sync_kiocb(&kiocb, in);
307         kiocb.ki_pos = *ppos;
308         ret = call_read_iter(in, &kiocb, &to);
309         if (ret > 0) {
310                 *ppos = kiocb.ki_pos;
311                 file_accessed(in);
312         } else if (ret < 0) {
313                 to.idx = idx;
314                 to.iov_offset = 0;
315                 iov_iter_advance(&to, 0); /* to free what was emitted */
316                 /*
317                  * callers of ->splice_read() expect -EAGAIN on
318                  * "can't put anything in there", rather than -EFAULT.
319                  */
320                 if (ret == -EFAULT)
321                         ret = -EAGAIN;
322         }
324         return ret;
326 EXPORT_SYMBOL(generic_file_splice_read);
328 const struct pipe_buf_operations default_pipe_buf_ops = {
329         .can_merge = 0,
330         .confirm = generic_pipe_buf_confirm,
331         .release = generic_pipe_buf_release,
332         .steal = generic_pipe_buf_steal,
333         .get = generic_pipe_buf_get,
334 };
336 static int generic_pipe_buf_nosteal(struct pipe_inode_info *pipe,
337                                     struct pipe_buffer *buf)
339         return 1;
342 /* Pipe buffer operations for a socket and similar. */
343 const struct pipe_buf_operations nosteal_pipe_buf_ops = {
344         .can_merge = 0,
345         .confirm = generic_pipe_buf_confirm,
346         .release = generic_pipe_buf_release,
347         .steal = generic_pipe_buf_nosteal,
348         .get = generic_pipe_buf_get,
349 };
350 EXPORT_SYMBOL(nosteal_pipe_buf_ops);
352 static ssize_t kernel_readv(struct file *file, const struct kvec *vec,
353                             unsigned long vlen, loff_t offset)
355         mm_segment_t old_fs;
356         loff_t pos = offset;
357         ssize_t res;
359         old_fs = get_fs();
360         set_fs(get_ds());
361         /* The cast to a user pointer is valid due to the set_fs() */
362         res = vfs_readv(file, (const struct iovec __user *)vec, vlen, &pos, 0);
363         set_fs(old_fs);
365         return res;
368 static ssize_t default_file_splice_read(struct file *in, loff_t *ppos,
369                                  struct pipe_inode_info *pipe, size_t len,
370                                  unsigned int flags)
372         struct kvec *vec, __vec[PIPE_DEF_BUFFERS];
373         struct iov_iter to;
374         struct page **pages;
375         unsigned int nr_pages;
376         size_t offset, base, copied = 0;
377         ssize_t res;
378         int i;
380         if (pipe->nrbufs == pipe->buffers)
381                 return -EAGAIN;
383         /*
384          * Try to keep page boundaries matching to source pagecache ones -
385          * it probably won't be much help, but...
386          */
387         offset = *ppos & ~PAGE_MASK;
389         iov_iter_pipe(&to, READ, pipe, len + offset);
391         res = iov_iter_get_pages_alloc(&to, &pages, len + offset, &base);
392         if (res <= 0)
393                 return -ENOMEM;
395         nr_pages = DIV_ROUND_UP(res + base, PAGE_SIZE);
397         vec = __vec;
398         if (nr_pages > PIPE_DEF_BUFFERS) {
399                 vec = kmalloc_array(nr_pages, sizeof(struct kvec), GFP_KERNEL);
400                 if (unlikely(!vec)) {
401                         res = -ENOMEM;
402                         goto out;
403                 }
404         }
406         pipe->bufs[to.idx].offset = offset;
407         pipe->bufs[to.idx].len -= offset;
409         for (i = 0; i < nr_pages; i++) {
410                 size_t this_len = min_t(size_t, len, PAGE_SIZE - offset);
411                 vec[i].iov_base = page_address(pages[i]) + offset;
412                 vec[i].iov_len = this_len;
413                 len -= this_len;
414                 offset = 0;
415         }
417         res = kernel_readv(in, vec, nr_pages, *ppos);
418         if (res > 0) {
419                 copied = res;
420                 *ppos += res;
421         }
423         if (vec != __vec)
424                 kfree(vec);
425 out:
426         for (i = 0; i < nr_pages; i++)
427                 put_page(pages[i]);
428         kvfree(pages);
429         iov_iter_advance(&to, copied);  /* truncates and discards */
430         return res;
433 /*
434  * Send 'sd->len' bytes to socket from 'sd->file' at position 'sd->pos'
435  * using sendpage(). Return the number of bytes sent.
436  */
437 static int pipe_to_sendpage(struct pipe_inode_info *pipe,
438                             struct pipe_buffer *buf, struct splice_desc *sd)
440         struct file *file = sd->u.file;
441         loff_t pos = sd->pos;
442         int more;
444         if (!likely(file->f_op->sendpage))
445                 return -EINVAL;
447         more = (sd->flags & SPLICE_F_MORE) ? MSG_MORE : 0;
449         if (sd->len < sd->total_len && pipe->nrbufs > 1)
450                 more |= MSG_SENDPAGE_NOTLAST;
452         return file->f_op->sendpage(file, buf->page, buf->offset,
453                                     sd->len, &pos, more);
456 static void wakeup_pipe_writers(struct pipe_inode_info *pipe)
458         smp_mb();
459         if (waitqueue_active(&pipe->wait))
460                 wake_up_interruptible(&pipe->wait);
461         kill_fasync(&pipe->fasync_writers, SIGIO, POLL_OUT);
464 /**
465  * splice_from_pipe_feed - feed available data from a pipe to a file
466  * @pipe:       pipe to splice from
467  * @sd:         information to @actor
468  * @actor:      handler that splices the data
469  *
470  * Description:
471  *    This function loops over the pipe and calls @actor to do the
472  *    actual moving of a single struct pipe_buffer to the desired
473  *    destination.  It returns when there's no more buffers left in
474  *    the pipe or if the requested number of bytes (@sd->total_len)
475  *    have been copied.  It returns a positive number (one) if the
476  *    pipe needs to be filled with more data, zero if the required
477  *    number of bytes have been copied and -errno on error.
478  *
479  *    This, together with splice_from_pipe_{begin,end,next}, may be
480  *    used to implement the functionality of __splice_from_pipe() when
481  *    locking is required around copying the pipe buffers to the
482  *    destination.
483  */
484 static int splice_from_pipe_feed(struct pipe_inode_info *pipe, struct splice_desc *sd,
485                           splice_actor *actor)
487         int ret;
489         while (pipe->nrbufs) {
490                 struct pipe_buffer *buf = pipe->bufs + pipe->curbuf;
492                 sd->len = buf->len;
493                 if (sd->len > sd->total_len)
494                         sd->len = sd->total_len;
496                 ret = pipe_buf_confirm(pipe, buf);
497                 if (unlikely(ret)) {
498                         if (ret == -ENODATA)
499                                 ret = 0;
500                         return ret;
501                 }
503                 ret = actor(pipe, buf, sd);
504                 if (ret <= 0)
505                         return ret;
507                 buf->offset += ret;
508                 buf->len -= ret;
510                 sd->num_spliced += ret;
511                 sd->len -= ret;
512                 sd->pos += ret;
513                 sd->total_len -= ret;
515                 if (!buf->len) {
516                         pipe_buf_release(pipe, buf);
517                         pipe->curbuf = (pipe->curbuf + 1) & (pipe->buffers - 1);
518                         pipe->nrbufs--;
519                         if (pipe->files)
520                                 sd->need_wakeup = true;
521                 }
523                 if (!sd->total_len)
524                         return 0;
525         }
527         return 1;
530 /**
531  * splice_from_pipe_next - wait for some data to splice from
532  * @pipe:       pipe to splice from
533  * @sd:         information about the splice operation
534  *
535  * Description:
536  *    This function will wait for some data and return a positive
537  *    value (one) if pipe buffers are available.  It will return zero
538  *    or -errno if no more data needs to be spliced.
539  */
540 static int splice_from_pipe_next(struct pipe_inode_info *pipe, struct splice_desc *sd)
542         /*
543          * Check for signal early to make process killable when there are
544          * always buffers available
545          */
546         if (signal_pending(current))
547                 return -ERESTARTSYS;
549         while (!pipe->nrbufs) {
550                 if (!pipe->writers)
551                         return 0;
553                 if (!pipe->waiting_writers && sd->num_spliced)
554                         return 0;
556                 if (sd->flags & SPLICE_F_NONBLOCK)
557                         return -EAGAIN;
559                 if (signal_pending(current))
560                         return -ERESTARTSYS;
562                 if (sd->need_wakeup) {
563                         wakeup_pipe_writers(pipe);
564                         sd->need_wakeup = false;
565                 }
567                 pipe_wait(pipe);
568         }
570         return 1;
573 /**
574  * splice_from_pipe_begin - start splicing from pipe
575  * @sd:         information about the splice operation
576  *
577  * Description:
578  *    This function should be called before a loop containing
579  *    splice_from_pipe_next() and splice_from_pipe_feed() to
580  *    initialize the necessary fields of @sd.
581  */
582 static void splice_from_pipe_begin(struct splice_desc *sd)
584         sd->num_spliced = 0;
585         sd->need_wakeup = false;
588 /**
589  * splice_from_pipe_end - finish splicing from pipe
590  * @pipe:       pipe to splice from
591  * @sd:         information about the splice operation
592  *
593  * Description:
594  *    This function will wake up pipe writers if necessary.  It should
595  *    be called after a loop containing splice_from_pipe_next() and
596  *    splice_from_pipe_feed().
597  */
598 static void splice_from_pipe_end(struct pipe_inode_info *pipe, struct splice_desc *sd)
600         if (sd->need_wakeup)
601                 wakeup_pipe_writers(pipe);
604 /**
605  * __splice_from_pipe - splice data from a pipe to given actor
606  * @pipe:       pipe to splice from
607  * @sd:         information to @actor
608  * @actor:      handler that splices the data
609  *
610  * Description:
611  *    This function does little more than loop over the pipe and call
612  *    @actor to do the actual moving of a single struct pipe_buffer to
613  *    the desired destination. See pipe_to_file, pipe_to_sendpage, or
614  *    pipe_to_user.
615  *
616  */
617 ssize_t __splice_from_pipe(struct pipe_inode_info *pipe, struct splice_desc *sd,
618                            splice_actor *actor)
620         int ret;
622         splice_from_pipe_begin(sd);
623         do {
624                 cond_resched();
625                 ret = splice_from_pipe_next(pipe, sd);
626                 if (ret > 0)
627                         ret = splice_from_pipe_feed(pipe, sd, actor);
628         } while (ret > 0);
629         splice_from_pipe_end(pipe, sd);
631         return sd->num_spliced ? sd->num_spliced : ret;
633 EXPORT_SYMBOL(__splice_from_pipe);
635 /**
636  * splice_from_pipe - splice data from a pipe to a file
637  * @pipe:       pipe to splice from
638  * @out:        file to splice to
639  * @ppos:       position in @out
640  * @len:        how many bytes to splice
641  * @flags:      splice modifier flags
642  * @actor:      handler that splices the data
643  *
644  * Description:
645  *    See __splice_from_pipe. This function locks the pipe inode,
646  *    otherwise it's identical to __splice_from_pipe().
647  *
648  */
649 ssize_t splice_from_pipe(struct pipe_inode_info *pipe, struct file *out,
650                          loff_t *ppos, size_t len, unsigned int flags,
651                          splice_actor *actor)
653         ssize_t ret;
654         struct splice_desc sd = {
655                 .total_len = len,
656                 .flags = flags,
657                 .pos = *ppos,
658                 .u.file = out,
659         };
661         pipe_lock(pipe);
662         ret = __splice_from_pipe(pipe, &sd, actor);
663         pipe_unlock(pipe);
665         return ret;
668 /**
669  * iter_file_splice_write - splice data from a pipe to a file
670  * @pipe:       pipe info
671  * @out:        file to write to
672  * @ppos:       position in @out
673  * @len:        number of bytes to splice
674  * @flags:      splice modifier flags
675  *
676  * Description:
677  *    Will either move or copy pages (determined by @flags options) from
678  *    the given pipe inode to the given file.
679  *    This one is ->write_iter-based.
680  *
681  */
682 ssize_t
683 iter_file_splice_write(struct pipe_inode_info *pipe, struct file *out,
684                           loff_t *ppos, size_t len, unsigned int flags)
686         struct splice_desc sd = {
687                 .total_len = len,
688                 .flags = flags,
689                 .pos = *ppos,
690                 .u.file = out,
691         };
692         int nbufs = pipe->buffers;
693         struct bio_vec *array = kcalloc(nbufs, sizeof(struct bio_vec),
694                                         GFP_KERNEL);
695         ssize_t ret;
697         if (unlikely(!array))
698                 return -ENOMEM;
700         pipe_lock(pipe);
702         splice_from_pipe_begin(&sd);
703         while (sd.total_len) {
704                 struct iov_iter from;
705                 size_t left;
706                 int n, idx;
708                 ret = splice_from_pipe_next(pipe, &sd);
709                 if (ret <= 0)
710                         break;
712                 if (unlikely(nbufs < pipe->buffers)) {
713                         kfree(array);
714                         nbufs = pipe->buffers;
715                         array = kcalloc(nbufs, sizeof(struct bio_vec),
716                                         GFP_KERNEL);
717                         if (!array) {
718                                 ret = -ENOMEM;
719                                 break;
720                         }
721                 }
723                 /* build the vector */
724                 left = sd.total_len;
725                 for (n = 0, idx = pipe->curbuf; left && n < pipe->nrbufs; n++, idx++) {
726                         struct pipe_buffer *buf = pipe->bufs + idx;
727                         size_t this_len = buf->len;
729                         if (this_len > left)
730                                 this_len = left;
732                         if (idx == pipe->buffers - 1)
733                                 idx = -1;
735                         ret = pipe_buf_confirm(pipe, buf);
736                         if (unlikely(ret)) {
737                                 if (ret == -ENODATA)
738                                         ret = 0;
739                                 goto done;
740                         }
742                         array[n].bv_page = buf->page;
743                         array[n].bv_len = this_len;
744                         array[n].bv_offset = buf->offset;
745                         left -= this_len;
746                 }
748                 iov_iter_bvec(&from, WRITE, array, n, sd.total_len - left);
749                 ret = vfs_iter_write(out, &from, &sd.pos, 0);
750                 if (ret <= 0)
751                         break;
753                 sd.num_spliced += ret;
754                 sd.total_len -= ret;
755                 *ppos = sd.pos;
757                 /* dismiss the fully eaten buffers, adjust the partial one */
758                 while (ret) {
759                         struct pipe_buffer *buf = pipe->bufs + pipe->curbuf;
760                         if (ret >= buf->len) {
761                                 ret -= buf->len;
762                                 buf->len = 0;
763                                 pipe_buf_release(pipe, buf);
764                                 pipe->curbuf = (pipe->curbuf + 1) & (pipe->buffers - 1);
765                                 pipe->nrbufs--;
766                                 if (pipe->files)
767                                         sd.need_wakeup = true;
768                         } else {
769                                 buf->offset += ret;
770                                 buf->len -= ret;
771                                 ret = 0;
772                         }
773                 }
774         }
775 done:
776         kfree(array);
777         splice_from_pipe_end(pipe, &sd);
779         pipe_unlock(pipe);
781         if (sd.num_spliced)
782                 ret = sd.num_spliced;
784         return ret;
787 EXPORT_SYMBOL(iter_file_splice_write);
789 static int write_pipe_buf(struct pipe_inode_info *pipe, struct pipe_buffer *buf,
790                           struct splice_desc *sd)
792         int ret;
793         void *data;
794         loff_t tmp = sd->pos;
796         data = kmap(buf->page);
797         ret = __kernel_write(sd->u.file, data + buf->offset, sd->len, &tmp);
798         kunmap(buf->page);
800         return ret;
803 static ssize_t default_file_splice_write(struct pipe_inode_info *pipe,
804                                          struct file *out, loff_t *ppos,
805                                          size_t len, unsigned int flags)
807         ssize_t ret;
809         ret = splice_from_pipe(pipe, out, ppos, len, flags, write_pipe_buf);
810         if (ret > 0)
811                 *ppos += ret;
813         return ret;
816 /**
817  * generic_splice_sendpage - splice data from a pipe to a socket
818  * @pipe:       pipe to splice from
819  * @out:        socket to write to
820  * @ppos:       position in @out
821  * @len:        number of bytes to splice
822  * @flags:      splice modifier flags
823  *
824  * Description:
825  *    Will send @len bytes from the pipe to a network socket. No data copying
826  *    is involved.
827  *
828  */
829 ssize_t generic_splice_sendpage(struct pipe_inode_info *pipe, struct file *out,
830                                 loff_t *ppos, size_t len, unsigned int flags)
832         return splice_from_pipe(pipe, out, ppos, len, flags, pipe_to_sendpage);
835 EXPORT_SYMBOL(generic_splice_sendpage);
837 /*
838  * Attempt to initiate a splice from pipe to file.
839  */
840 static long do_splice_from(struct pipe_inode_info *pipe, struct file *out,
841                            loff_t *ppos, size_t len, unsigned int flags)
843         ssize_t (*splice_write)(struct pipe_inode_info *, struct file *,
844                                 loff_t *, size_t, unsigned int);
846         if (out->f_op->splice_write)
847                 splice_write = out->f_op->splice_write;
848         else
849                 splice_write = default_file_splice_write;
851         return splice_write(pipe, out, ppos, len, flags);
854 /*
855  * Attempt to initiate a splice from a file to a pipe.
856  */
857 static long do_splice_to(struct file *in, loff_t *ppos,
858                          struct pipe_inode_info *pipe, size_t len,
859                          unsigned int flags)
861         ssize_t (*splice_read)(struct file *, loff_t *,
862                                struct pipe_inode_info *, size_t, unsigned int);
863         int ret;
865         if (unlikely(!(in->f_mode & FMODE_READ)))
866                 return -EBADF;
868         ret = rw_verify_area(READ, in, ppos, len);
869         if (unlikely(ret < 0))
870                 return ret;
872         if (unlikely(len > MAX_RW_COUNT))
873                 len = MAX_RW_COUNT;
875         if (in->f_op->splice_read)
876                 splice_read = in->f_op->splice_read;
877         else
878                 splice_read = default_file_splice_read;
880         return splice_read(in, ppos, pipe, len, flags);
883 /**
884  * splice_direct_to_actor - splices data directly between two non-pipes
885  * @in:         file to splice from
886  * @sd:         actor information on where to splice to
887  * @actor:      handles the data splicing
888  *
889  * Description:
890  *    This is a special case helper to splice directly between two
891  *    points, without requiring an explicit pipe. Internally an allocated
892  *    pipe is cached in the process, and reused during the lifetime of
893  *    that process.
894  *
895  */
896 ssize_t splice_direct_to_actor(struct file *in, struct splice_desc *sd,
897                                splice_direct_actor *actor)
899         struct pipe_inode_info *pipe;
900         long ret, bytes;
901         umode_t i_mode;
902         size_t len;
903         int i, flags, more;
905         /*
906          * We require the input being a regular file, as we don't want to
907          * randomly drop data for eg socket -> socket splicing. Use the
908          * piped splicing for that!
909          */
910         i_mode = file_inode(in)->i_mode;
911         if (unlikely(!S_ISREG(i_mode) && !S_ISBLK(i_mode)))
912                 return -EINVAL;
914         /*
915          * neither in nor out is a pipe, setup an internal pipe attached to
916          * 'out' and transfer the wanted data from 'in' to 'out' through that
917          */
918         pipe = current->splice_pipe;
919         if (unlikely(!pipe)) {
920                 pipe = alloc_pipe_info();
921                 if (!pipe)
922                         return -ENOMEM;
924                 /*
925                  * We don't have an immediate reader, but we'll read the stuff
926                  * out of the pipe right after the splice_to_pipe(). So set
927                  * PIPE_READERS appropriately.
928                  */
929                 pipe->readers = 1;
931                 current->splice_pipe = pipe;
932         }
934         /*
935          * Do the splice.
936          */
937         ret = 0;
938         bytes = 0;
939         len = sd->total_len;
940         flags = sd->flags;
942         /*
943          * Don't block on output, we have to drain the direct pipe.
944          */
945         sd->flags &= ~SPLICE_F_NONBLOCK;
946         more = sd->flags & SPLICE_F_MORE;
948         WARN_ON_ONCE(pipe->nrbufs != 0);
950         while (len) {
951                 size_t read_len;
952                 loff_t pos = sd->pos, prev_pos = pos;
954                 /* Don't try to read more the pipe has space for. */
955                 read_len = min_t(size_t, len,
956                                  (pipe->buffers - pipe->nrbufs) << PAGE_SHIFT);
957                 ret = do_splice_to(in, &pos, pipe, read_len, flags);
958                 if (unlikely(ret <= 0))
959                         goto out_release;
961                 read_len = ret;
962                 sd->total_len = read_len;
964                 /*
965                  * If more data is pending, set SPLICE_F_MORE
966                  * If this is the last data and SPLICE_F_MORE was not set
967                  * initially, clears it.
968                  */
969                 if (read_len < len)
970                         sd->flags |= SPLICE_F_MORE;
971                 else if (!more)
972                         sd->flags &= ~SPLICE_F_MORE;
973                 /*
974                  * NOTE: nonblocking mode only applies to the input. We
975                  * must not do the output in nonblocking mode as then we
976                  * could get stuck data in the internal pipe:
977                  */
978                 ret = actor(pipe, sd);
979                 if (unlikely(ret <= 0)) {
980                         sd->pos = prev_pos;
981                         goto out_release;
982                 }
984                 bytes += ret;
985                 len -= ret;
986                 sd->pos = pos;
988                 if (ret < read_len) {
989                         sd->pos = prev_pos + ret;
990                         goto out_release;
991                 }
992         }
994 done:
995         pipe->nrbufs = pipe->curbuf = 0;
996         file_accessed(in);
997         return bytes;
999 out_release:
1000         /*
1001          * If we did an incomplete transfer we must release
1002          * the pipe buffers in question:
1003          */
1004         for (i = 0; i < pipe->buffers; i++) {
1005                 struct pipe_buffer *buf = pipe->bufs + i;
1007                 if (buf->ops)
1008                         pipe_buf_release(pipe, buf);
1009         }
1011         if (!bytes)
1012                 bytes = ret;
1014         goto done;
1016 EXPORT_SYMBOL(splice_direct_to_actor);
1018 static int direct_splice_actor(struct pipe_inode_info *pipe,
1019                                struct splice_desc *sd)
1021         struct file *file = sd->u.file;
1023         return do_splice_from(pipe, file, sd->opos, sd->total_len,
1024                               sd->flags);
1027 /**
1028  * do_splice_direct - splices data directly between two files
1029  * @in:         file to splice from
1030  * @ppos:       input file offset
1031  * @out:        file to splice to
1032  * @opos:       output file offset
1033  * @len:        number of bytes to splice
1034  * @flags:      splice modifier flags
1035  *
1036  * Description:
1037  *    For use by do_sendfile(). splice can easily emulate sendfile, but
1038  *    doing it in the application would incur an extra system call
1039  *    (splice in + splice out, as compared to just sendfile()). So this helper
1040  *    can splice directly through a process-private pipe.
1041  *
1042  */
1043 long do_splice_direct(struct file *in, loff_t *ppos, struct file *out,
1044                       loff_t *opos, size_t len, unsigned int flags)
1046         struct splice_desc sd = {
1047                 .len            = len,
1048                 .total_len      = len,
1049                 .flags          = flags,
1050                 .pos            = *ppos,
1051                 .u.file         = out,
1052                 .opos           = opos,
1053         };
1054         long ret;
1056         if (unlikely(!(out->f_mode & FMODE_WRITE)))
1057                 return -EBADF;
1059         if (unlikely(out->f_flags & O_APPEND))
1060                 return -EINVAL;
1062         ret = rw_verify_area(WRITE, out, opos, len);
1063         if (unlikely(ret < 0))
1064                 return ret;
1066         ret = splice_direct_to_actor(in, &sd, direct_splice_actor);
1067         if (ret > 0)
1068                 *ppos = sd.pos;
1070         return ret;
1072 EXPORT_SYMBOL(do_splice_direct);
1074 static int wait_for_space(struct pipe_inode_info *pipe, unsigned flags)
1076         for (;;) {
1077                 if (unlikely(!pipe->readers)) {
1078                         send_sig(SIGPIPE, current, 0);
1079                         return -EPIPE;
1080                 }
1081                 if (pipe->nrbufs != pipe->buffers)
1082                         return 0;
1083                 if (flags & SPLICE_F_NONBLOCK)
1084                         return -EAGAIN;
1085                 if (signal_pending(current))
1086                         return -ERESTARTSYS;
1087                 pipe->waiting_writers++;
1088                 pipe_wait(pipe);
1089                 pipe->waiting_writers--;
1090         }
1093 static int splice_pipe_to_pipe(struct pipe_inode_info *ipipe,
1094                                struct pipe_inode_info *opipe,
1095                                size_t len, unsigned int flags);
1097 /*
1098  * Determine where to splice to/from.
1099  */
1100 static long do_splice(struct file *in, loff_t __user *off_in,
1101                       struct file *out, loff_t __user *off_out,
1102                       size_t len, unsigned int flags)
1104         struct pipe_inode_info *ipipe;
1105         struct pipe_inode_info *opipe;
1106         loff_t offset;
1107         long ret;
1109         ipipe = get_pipe_info(in);
1110         opipe = get_pipe_info(out);
1112         if (ipipe && opipe) {
1113                 if (off_in || off_out)
1114                         return -ESPIPE;
1116                 if (!(in->f_mode & FMODE_READ))
1117                         return -EBADF;
1119                 if (!(out->f_mode & FMODE_WRITE))
1120                         return -EBADF;
1122                 /* Splicing to self would be fun, but... */
1123                 if (ipipe == opipe)
1124                         return -EINVAL;
1126                 return splice_pipe_to_pipe(ipipe, opipe, len, flags);
1127         }
1129         if (ipipe) {
1130                 if (off_in)
1131                         return -ESPIPE;
1132                 if (off_out) {
1133                         if (!(out->f_mode & FMODE_PWRITE))
1134                                 return -EINVAL;
1135                         if (copy_from_user(&offset, off_out, sizeof(loff_t)))
1136                                 return -EFAULT;
1137                 } else {
1138                         offset = out->f_pos;
1139                 }
1141                 if (unlikely(!(out->f_mode & FMODE_WRITE)))
1142                         return -EBADF;
1144                 if (unlikely(out->f_flags & O_APPEND))
1145                         return -EINVAL;
1147                 ret = rw_verify_area(WRITE, out, &offset, len);
1148                 if (unlikely(ret < 0))
1149                         return ret;
1151                 file_start_write(out);
1152                 ret = do_splice_from(ipipe, out, &offset, len, flags);
1153                 file_end_write(out);
1155                 if (!off_out)
1156                         out->f_pos = offset;
1157                 else if (copy_to_user(off_out, &offset, sizeof(loff_t)))
1158                         ret = -EFAULT;
1160                 return ret;
1161         }
1163         if (opipe) {
1164                 if (off_out)
1165                         return -ESPIPE;
1166                 if (off_in) {
1167                         if (!(in->f_mode & FMODE_PREAD))
1168                                 return -EINVAL;
1169                         if (copy_from_user(&offset, off_in, sizeof(loff_t)))
1170                                 return -EFAULT;
1171                 } else {
1172                         offset = in->f_pos;
1173                 }
1175                 pipe_lock(opipe);
1176                 ret = wait_for_space(opipe, flags);
1177                 if (!ret)
1178                         ret = do_splice_to(in, &offset, opipe, len, flags);
1179                 pipe_unlock(opipe);
1180                 if (ret > 0)
1181                         wakeup_pipe_readers(opipe);
1182                 if (!off_in)
1183                         in->f_pos = offset;
1184                 else if (copy_to_user(off_in, &offset, sizeof(loff_t)))
1185                         ret = -EFAULT;
1187                 return ret;
1188         }
1190         return -EINVAL;
1193 static int iter_to_pipe(struct iov_iter *from,
1194                         struct pipe_inode_info *pipe,
1195                         unsigned flags)
1197         struct pipe_buffer buf = {
1198                 .ops = &user_page_pipe_buf_ops,
1199                 .flags = flags
1200         };
1201         size_t total = 0;
1202         int ret = 0;
1203         bool failed = false;
1205         while (iov_iter_count(from) && !failed) {
1206                 struct page *pages[16];
1207                 ssize_t copied;
1208                 size_t start;
1209                 int n;
1211                 copied = iov_iter_get_pages(from, pages, ~0UL, 16, &start);
1212                 if (copied <= 0) {
1213                         ret = copied;
1214                         break;
1215                 }
1217                 for (n = 0; copied; n++, start = 0) {
1218                         int size = min_t(int, copied, PAGE_SIZE - start);
1219                         if (!failed) {
1220                                 buf.page = pages[n];
1221                                 buf.offset = start;
1222                                 buf.len = size;
1223                                 ret = add_to_pipe(pipe, &buf);
1224                                 if (unlikely(ret < 0)) {
1225                                         failed = true;
1226                                 } else {
1227                                         iov_iter_advance(from, ret);
1228                                         total += ret;
1229                                 }
1230                         } else {
1231                                 put_page(pages[n]);
1232                         }
1233                         copied -= size;
1234                 }
1235         }
1236         return total ? total : ret;
1239 static int pipe_to_user(struct pipe_inode_info *pipe, struct pipe_buffer *buf,
1240                         struct splice_desc *sd)
1242         int n = copy_page_to_iter(buf->page, buf->offset, sd->len, sd->u.data);
1243         return n == sd->len ? n : -EFAULT;
1246 /*
1247  * For lack of a better implementation, implement vmsplice() to userspace
1248  * as a simple copy of the pipes pages to the user iov.
1249  */
1250 static long vmsplice_to_user(struct file *file, struct iov_iter *iter,
1251                              unsigned int flags)
1253         struct pipe_inode_info *pipe = get_pipe_info(file);
1254         struct splice_desc sd = {
1255                 .total_len = iov_iter_count(iter),
1256                 .flags = flags,
1257                 .u.data = iter
1258         };
1259         long ret = 0;
1261         if (!pipe)
1262                 return -EBADF;
1264         if (sd.total_len) {
1265                 pipe_lock(pipe);
1266                 ret = __splice_from_pipe(pipe, &sd, pipe_to_user);
1267                 pipe_unlock(pipe);
1268         }
1270         return ret;
1273 /*
1274  * vmsplice splices a user address range into a pipe. It can be thought of
1275  * as splice-from-memory, where the regular splice is splice-from-file (or
1276  * to file). In both cases the output is a pipe, naturally.
1277  */
1278 static long vmsplice_to_pipe(struct file *file, struct iov_iter *iter,
1279                              unsigned int flags)
1281         struct pipe_inode_info *pipe;
1282         long ret = 0;
1283         unsigned buf_flag = 0;
1285         if (flags & SPLICE_F_GIFT)
1286                 buf_flag = PIPE_BUF_FLAG_GIFT;
1288         pipe = get_pipe_info(file);
1289         if (!pipe)
1290                 return -EBADF;
1292         pipe_lock(pipe);
1293         ret = wait_for_space(pipe, flags);
1294         if (!ret)
1295                 ret = iter_to_pipe(iter, pipe, buf_flag);
1296         pipe_unlock(pipe);
1297         if (ret > 0)
1298                 wakeup_pipe_readers(pipe);
1299         return ret;
1302 static int vmsplice_type(struct fd f, int *type)
1304         if (!f.file)
1305                 return -EBADF;
1306         if (f.file->f_mode & FMODE_WRITE) {
1307                 *type = WRITE;
1308         } else if (f.file->f_mode & FMODE_READ) {
1309                 *type = READ;
1310         } else {
1311                 fdput(f);
1312                 return -EBADF;
1313         }
1314         return 0;
1317 /*
1318  * Note that vmsplice only really supports true splicing _from_ user memory
1319  * to a pipe, not the other way around. Splicing from user memory is a simple
1320  * operation that can be supported without any funky alignment restrictions
1321  * or nasty vm tricks. We simply map in the user memory and fill them into
1322  * a pipe. The reverse isn't quite as easy, though. There are two possible
1323  * solutions for that:
1324  *
1325  *      - memcpy() the data internally, at which point we might as well just
1326  *        do a regular read() on the buffer anyway.
1327  *      - Lots of nasty vm tricks, that are neither fast nor flexible (it
1328  *        has restriction limitations on both ends of the pipe).
1329  *
1330  * Currently we punt and implement it as a normal copy, see pipe_to_user().
1331  *
1332  */
1333 static long do_vmsplice(struct file *f, struct iov_iter *iter, unsigned int flags)
1335         if (unlikely(flags & ~SPLICE_F_ALL))
1336                 return -EINVAL;
1338         if (!iov_iter_count(iter))
1339                 return 0;
1341         if (iov_iter_rw(iter) == WRITE)
1342                 return vmsplice_to_pipe(f, iter, flags);
1343         else
1344                 return vmsplice_to_user(f, iter, flags);
1347 SYSCALL_DEFINE4(vmsplice, int, fd, const struct iovec __user *, uiov,
1348                 unsigned long, nr_segs, unsigned int, flags)
1350         struct iovec iovstack[UIO_FASTIOV];
1351         struct iovec *iov = iovstack;
1352         struct iov_iter iter;
1353         long error;
1354         struct fd f;
1355         int type;
1357         f = fdget(fd);
1358         error = vmsplice_type(f, &type);
1359         if (error)
1360                 return error;
1362         error = import_iovec(type, uiov, nr_segs,
1363                              ARRAY_SIZE(iovstack), &iov, &iter);
1364         if (!error) {
1365                 error = do_vmsplice(f.file, &iter, flags);
1366                 kfree(iov);
1367         }
1368         fdput(f);
1369         return error;
1372 #ifdef CONFIG_COMPAT
1373 COMPAT_SYSCALL_DEFINE4(vmsplice, int, fd, const struct compat_iovec __user *, iov32,
1374                     unsigned int, nr_segs, unsigned int, flags)
1376         struct iovec iovstack[UIO_FASTIOV];
1377         struct iovec *iov = iovstack;
1378         struct iov_iter iter;
1379         long error;
1380         struct fd f;
1381         int type;
1383         f = fdget(fd);
1384         error = vmsplice_type(f, &type);
1385         if (error)
1386                 return error;
1388         error = compat_import_iovec(type, iov32, nr_segs,
1389                              ARRAY_SIZE(iovstack), &iov, &iter);
1390         if (!error) {
1391                 error = do_vmsplice(f.file, &iter, flags);
1392                 kfree(iov);
1393         }
1394         fdput(f);
1395         return error;
1397 #endif
1399 SYSCALL_DEFINE6(splice, int, fd_in, loff_t __user *, off_in,
1400                 int, fd_out, loff_t __user *, off_out,
1401                 size_t, len, unsigned int, flags)
1403         struct fd in, out;
1404         long error;
1406         if (unlikely(!len))
1407                 return 0;
1409         if (unlikely(flags & ~SPLICE_F_ALL))
1410                 return -EINVAL;
1412         error = -EBADF;
1413         in = fdget(fd_in);
1414         if (in.file) {
1415                 if (in.file->f_mode & FMODE_READ) {
1416                         out = fdget(fd_out);
1417                         if (out.file) {
1418                                 if (out.file->f_mode & FMODE_WRITE)
1419                                         error = do_splice(in.file, off_in,
1420                                                           out.file, off_out,
1421                                                           len, flags);
1422                                 fdput(out);
1423                         }
1424                 }
1425                 fdput(in);
1426         }
1427         return error;
1430 /*
1431  * Make sure there's data to read. Wait for input if we can, otherwise
1432  * return an appropriate error.
1433  */
1434 static int ipipe_prep(struct pipe_inode_info *pipe, unsigned int flags)
1436         int ret;
1438         /*
1439          * Check ->nrbufs without the inode lock first. This function
1440          * is speculative anyways, so missing one is ok.
1441          */
1442         if (pipe->nrbufs)
1443                 return 0;
1445         ret = 0;
1446         pipe_lock(pipe);
1448         while (!pipe->nrbufs) {
1449                 if (signal_pending(current)) {
1450                         ret = -ERESTARTSYS;
1451                         break;
1452                 }
1453                 if (!pipe->writers)
1454                         break;
1455                 if (!pipe->waiting_writers) {
1456                         if (flags & SPLICE_F_NONBLOCK) {
1457                                 ret = -EAGAIN;
1458                                 break;
1459                         }
1460                 }
1461                 pipe_wait(pipe);
1462         }
1464         pipe_unlock(pipe);
1465         return ret;
1468 /*
1469  * Make sure there's writeable room. Wait for room if we can, otherwise
1470  * return an appropriate error.
1471  */
1472 static int opipe_prep(struct pipe_inode_info *pipe, unsigned int flags)
1474         int ret;
1476         /*
1477          * Check ->nrbufs without the inode lock first. This function
1478          * is speculative anyways, so missing one is ok.
1479          */
1480         if (pipe->nrbufs < pipe->buffers)
1481                 return 0;
1483         ret = 0;
1484         pipe_lock(pipe);
1486         while (pipe->nrbufs >= pipe->buffers) {
1487                 if (!pipe->readers) {
1488                         send_sig(SIGPIPE, current, 0);
1489                         ret = -EPIPE;
1490                         break;
1491                 }
1492                 if (flags & SPLICE_F_NONBLOCK) {
1493                         ret = -EAGAIN;
1494                         break;
1495                 }
1496                 if (signal_pending(current)) {
1497                         ret = -ERESTARTSYS;
1498                         break;
1499                 }
1500                 pipe->waiting_writers++;
1501                 pipe_wait(pipe);
1502                 pipe->waiting_writers--;
1503         }
1505         pipe_unlock(pipe);
1506         return ret;
1509 /*
1510  * Splice contents of ipipe to opipe.
1511  */
1512 static int splice_pipe_to_pipe(struct pipe_inode_info *ipipe,
1513                                struct pipe_inode_info *opipe,
1514                                size_t len, unsigned int flags)
1516         struct pipe_buffer *ibuf, *obuf;
1517         int ret = 0, nbuf;
1518         bool input_wakeup = false;
1521 retry:
1522         ret = ipipe_prep(ipipe, flags);
1523         if (ret)
1524                 return ret;
1526         ret = opipe_prep(opipe, flags);
1527         if (ret)
1528                 return ret;
1530         /*
1531          * Potential ABBA deadlock, work around it by ordering lock
1532          * grabbing by pipe info address. Otherwise two different processes
1533          * could deadlock (one doing tee from A -> B, the other from B -> A).
1534          */
1535         pipe_double_lock(ipipe, opipe);
1537         do {
1538                 if (!opipe->readers) {
1539                         send_sig(SIGPIPE, current, 0);
1540                         if (!ret)
1541                                 ret = -EPIPE;
1542                         break;
1543                 }
1545                 if (!ipipe->nrbufs && !ipipe->writers)
1546                         break;
1548                 /*
1549                  * Cannot make any progress, because either the input
1550                  * pipe is empty or the output pipe is full.
1551                  */
1552                 if (!ipipe->nrbufs || opipe->nrbufs >= opipe->buffers) {
1553                         /* Already processed some buffers, break */
1554                         if (ret)
1555                                 break;
1557                         if (flags & SPLICE_F_NONBLOCK) {
1558                                 ret = -EAGAIN;
1559                                 break;
1560                         }
1562                         /*
1563                          * We raced with another reader/writer and haven't
1564                          * managed to process any buffers.  A zero return
1565                          * value means EOF, so retry instead.
1566                          */
1567                         pipe_unlock(ipipe);
1568                         pipe_unlock(opipe);
1569                         goto retry;
1570                 }
1572                 ibuf = ipipe->bufs + ipipe->curbuf;
1573                 nbuf = (opipe->curbuf + opipe->nrbufs) & (opipe->buffers - 1);
1574                 obuf = opipe->bufs + nbuf;
1576                 if (len >= ibuf->len) {
1577                         /*
1578                          * Simply move the whole buffer from ipipe to opipe
1579                          */
1580                         *obuf = *ibuf;
1581                         ibuf->ops = NULL;
1582                         opipe->nrbufs++;
1583                         ipipe->curbuf = (ipipe->curbuf + 1) & (ipipe->buffers - 1);
1584                         ipipe->nrbufs--;
1585                         input_wakeup = true;
1586                 } else {
1587                         /*
1588                          * Get a reference to this pipe buffer,
1589                          * so we can copy the contents over.
1590                          */
1591                         pipe_buf_get(ipipe, ibuf);
1592                         *obuf = *ibuf;
1594                         /*
1595                          * Don't inherit the gift flag, we need to
1596                          * prevent multiple steals of this page.
1597                          */
1598                         obuf->flags &= ~PIPE_BUF_FLAG_GIFT;
1600                         obuf->len = len;
1601                         opipe->nrbufs++;
1602                         ibuf->offset += obuf->len;
1603                         ibuf->len -= obuf->len;
1604                 }
1605                 ret += obuf->len;
1606                 len -= obuf->len;
1607         } while (len);
1609         pipe_unlock(ipipe);
1610         pipe_unlock(opipe);
1612         /*
1613          * If we put data in the output pipe, wakeup any potential readers.
1614          */
1615         if (ret > 0)
1616                 wakeup_pipe_readers(opipe);
1618         if (input_wakeup)
1619                 wakeup_pipe_writers(ipipe);
1621         return ret;
1624 /*
1625  * Link contents of ipipe to opipe.
1626  */
1627 static int link_pipe(struct pipe_inode_info *ipipe,
1628                      struct pipe_inode_info *opipe,
1629                      size_t len, unsigned int flags)
1631         struct pipe_buffer *ibuf, *obuf;
1632         int ret = 0, i = 0, nbuf;
1634         /*
1635          * Potential ABBA deadlock, work around it by ordering lock
1636          * grabbing by pipe info address. Otherwise two different processes
1637          * could deadlock (one doing tee from A -> B, the other from B -> A).
1638          */
1639         pipe_double_lock(ipipe, opipe);
1641         do {
1642                 if (!opipe->readers) {
1643                         send_sig(SIGPIPE, current, 0);
1644                         if (!ret)
1645                                 ret = -EPIPE;
1646                         break;
1647                 }
1649                 /*
1650                  * If we have iterated all input buffers or ran out of
1651                  * output room, break.
1652                  */
1653                 if (i >= ipipe->nrbufs || opipe->nrbufs >= opipe->buffers)
1654                         break;
1656                 ibuf = ipipe->bufs + ((ipipe->curbuf + i) & (ipipe->buffers-1));
1657                 nbuf = (opipe->curbuf + opipe->nrbufs) & (opipe->buffers - 1);
1659                 /*
1660                  * Get a reference to this pipe buffer,
1661                  * so we can copy the contents over.
1662                  */
1663                 pipe_buf_get(ipipe, ibuf);
1665                 obuf = opipe->bufs + nbuf;
1666                 *obuf = *ibuf;
1668                 /*
1669                  * Don't inherit the gift flag, we need to
1670                  * prevent multiple steals of this page.
1671                  */
1672                 obuf->flags &= ~PIPE_BUF_FLAG_GIFT;
1674                 if (obuf->len > len)
1675                         obuf->len = len;
1677                 opipe->nrbufs++;
1678                 ret += obuf->len;
1679                 len -= obuf->len;
1680                 i++;
1681         } while (len);
1683         /*
1684          * return EAGAIN if we have the potential of some data in the
1685          * future, otherwise just return 0
1686          */
1687         if (!ret && ipipe->waiting_writers && (flags & SPLICE_F_NONBLOCK))
1688                 ret = -EAGAIN;
1690         pipe_unlock(ipipe);
1691         pipe_unlock(opipe);
1693         /*
1694          * If we put data in the output pipe, wakeup any potential readers.
1695          */
1696         if (ret > 0)
1697                 wakeup_pipe_readers(opipe);
1699         return ret;
1702 /*
1703  * This is a tee(1) implementation that works on pipes. It doesn't copy
1704  * any data, it simply references the 'in' pages on the 'out' pipe.
1705  * The 'flags' used are the SPLICE_F_* variants, currently the only
1706  * applicable one is SPLICE_F_NONBLOCK.
1707  */
1708 static long do_tee(struct file *in, struct file *out, size_t len,
1709                    unsigned int flags)
1711         struct pipe_inode_info *ipipe = get_pipe_info(in);
1712         struct pipe_inode_info *opipe = get_pipe_info(out);
1713         int ret = -EINVAL;
1715         /*
1716          * Duplicate the contents of ipipe to opipe without actually
1717          * copying the data.
1718          */
1719         if (ipipe && opipe && ipipe != opipe) {
1720                 /*
1721                  * Keep going, unless we encounter an error. The ipipe/opipe
1722                  * ordering doesn't really matter.
1723                  */
1724                 ret = ipipe_prep(ipipe, flags);
1725                 if (!ret) {
1726                         ret = opipe_prep(opipe, flags);
1727                         if (!ret)
1728                                 ret = link_pipe(ipipe, opipe, len, flags);
1729                 }
1730         }
1732         return ret;
1735 SYSCALL_DEFINE4(tee, int, fdin, int, fdout, size_t, len, unsigned int, flags)
1737         struct fd in;
1738         int error;
1740         if (unlikely(flags & ~SPLICE_F_ALL))
1741                 return -EINVAL;
1743         if (unlikely(!len))
1744                 return 0;
1746         error = -EBADF;
1747         in = fdget(fdin);
1748         if (in.file) {
1749                 if (in.file->f_mode & FMODE_READ) {
1750                         struct fd out = fdget(fdout);
1751                         if (out.file) {
1752                                 if (out.file->f_mode & FMODE_WRITE)
1753                                         error = do_tee(in.file, out.file,
1754                                                         len, flags);
1755                                 fdput(out);
1756                         }
1757                 }
1758                 fdput(in);
1759         }
1761         return error;