]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-analog-linux-kernel/dmurphy-analog.git/blob - fs/stat.c
defconfig: Enable M_CAN for dra7
[ti-analog-linux-kernel/dmurphy-analog.git] / fs / stat.c
1 // SPDX-License-Identifier: GPL-2.0
2 /*
3  *  linux/fs/stat.c
4  *
5  *  Copyright (C) 1991, 1992  Linus Torvalds
6  */
8 #include <linux/export.h>
9 #include <linux/mm.h>
10 #include <linux/errno.h>
11 #include <linux/file.h>
12 #include <linux/highuid.h>
13 #include <linux/fs.h>
14 #include <linux/namei.h>
15 #include <linux/security.h>
16 #include <linux/cred.h>
17 #include <linux/syscalls.h>
18 #include <linux/pagemap.h>
19 #include <linux/compat.h>
21 #include <linux/uaccess.h>
22 #include <asm/unistd.h>
24 /**
25  * generic_fillattr - Fill in the basic attributes from the inode struct
26  * @inode: Inode to use as the source
27  * @stat: Where to fill in the attributes
28  *
29  * Fill in the basic attributes in the kstat structure from data that's to be
30  * found on the VFS inode structure.  This is the default if no getattr inode
31  * operation is supplied.
32  */
33 void generic_fillattr(struct inode *inode, struct kstat *stat)
34 {
35         stat->dev = inode->i_sb->s_dev;
36         stat->ino = inode->i_ino;
37         stat->mode = inode->i_mode;
38         stat->nlink = inode->i_nlink;
39         stat->uid = inode->i_uid;
40         stat->gid = inode->i_gid;
41         stat->rdev = inode->i_rdev;
42         stat->size = i_size_read(inode);
43         stat->atime = inode->i_atime;
44         stat->mtime = inode->i_mtime;
45         stat->ctime = inode->i_ctime;
46         stat->blksize = i_blocksize(inode);
47         stat->blocks = inode->i_blocks;
49         if (IS_NOATIME(inode))
50                 stat->result_mask &= ~STATX_ATIME;
51         if (IS_AUTOMOUNT(inode))
52                 stat->attributes |= STATX_ATTR_AUTOMOUNT;
53 }
54 EXPORT_SYMBOL(generic_fillattr);
56 /**
57  * vfs_getattr_nosec - getattr without security checks
58  * @path: file to get attributes from
59  * @stat: structure to return attributes in
60  * @request_mask: STATX_xxx flags indicating what the caller wants
61  * @query_flags: Query mode (KSTAT_QUERY_FLAGS)
62  *
63  * Get attributes without calling security_inode_getattr.
64  *
65  * Currently the only caller other than vfs_getattr is internal to the
66  * filehandle lookup code, which uses only the inode number and returns no
67  * attributes to any user.  Any other code probably wants vfs_getattr.
68  */
69 int vfs_getattr_nosec(const struct path *path, struct kstat *stat,
70                       u32 request_mask, unsigned int query_flags)
71 {
72         struct inode *inode = d_backing_inode(path->dentry);
74         memset(stat, 0, sizeof(*stat));
75         stat->result_mask |= STATX_BASIC_STATS;
76         request_mask &= STATX_ALL;
77         query_flags &= KSTAT_QUERY_FLAGS;
78         if (inode->i_op->getattr)
79                 return inode->i_op->getattr(path, stat, request_mask,
80                                             query_flags);
82         generic_fillattr(inode, stat);
83         return 0;
84 }
85 EXPORT_SYMBOL(vfs_getattr_nosec);
87 /*
88  * vfs_getattr - Get the enhanced basic attributes of a file
89  * @path: The file of interest
90  * @stat: Where to return the statistics
91  * @request_mask: STATX_xxx flags indicating what the caller wants
92  * @query_flags: Query mode (KSTAT_QUERY_FLAGS)
93  *
94  * Ask the filesystem for a file's attributes.  The caller must indicate in
95  * request_mask and query_flags to indicate what they want.
96  *
97  * If the file is remote, the filesystem can be forced to update the attributes
98  * from the backing store by passing AT_STATX_FORCE_SYNC in query_flags or can
99  * suppress the update by passing AT_STATX_DONT_SYNC.
100  *
101  * Bits must have been set in request_mask to indicate which attributes the
102  * caller wants retrieving.  Any such attribute not requested may be returned
103  * anyway, but the value may be approximate, and, if remote, may not have been
104  * synchronised with the server.
105  *
106  * 0 will be returned on success, and a -ve error code if unsuccessful.
107  */
108 int vfs_getattr(const struct path *path, struct kstat *stat,
109                 u32 request_mask, unsigned int query_flags)
111         int retval;
113         retval = security_inode_getattr(path);
114         if (retval)
115                 return retval;
116         return vfs_getattr_nosec(path, stat, request_mask, query_flags);
118 EXPORT_SYMBOL(vfs_getattr);
120 /**
121  * vfs_statx_fd - Get the enhanced basic attributes by file descriptor
122  * @fd: The file descriptor referring to the file of interest
123  * @stat: The result structure to fill in.
124  * @request_mask: STATX_xxx flags indicating what the caller wants
125  * @query_flags: Query mode (KSTAT_QUERY_FLAGS)
126  *
127  * This function is a wrapper around vfs_getattr().  The main difference is
128  * that it uses a file descriptor to determine the file location.
129  *
130  * 0 will be returned on success, and a -ve error code if unsuccessful.
131  */
132 int vfs_statx_fd(unsigned int fd, struct kstat *stat,
133                  u32 request_mask, unsigned int query_flags)
135         struct fd f;
136         int error = -EBADF;
138         if (query_flags & ~KSTAT_QUERY_FLAGS)
139                 return -EINVAL;
141         f = fdget_raw(fd);
142         if (f.file) {
143                 error = vfs_getattr(&f.file->f_path, stat,
144                                     request_mask, query_flags);
145                 fdput(f);
146         }
147         return error;
149 EXPORT_SYMBOL(vfs_statx_fd);
151 /**
152  * vfs_statx - Get basic and extra attributes by filename
153  * @dfd: A file descriptor representing the base dir for a relative filename
154  * @filename: The name of the file of interest
155  * @flags: Flags to control the query
156  * @stat: The result structure to fill in.
157  * @request_mask: STATX_xxx flags indicating what the caller wants
158  *
159  * This function is a wrapper around vfs_getattr().  The main difference is
160  * that it uses a filename and base directory to determine the file location.
161  * Additionally, the use of AT_SYMLINK_NOFOLLOW in flags will prevent a symlink
162  * at the given name from being referenced.
163  *
164  * 0 will be returned on success, and a -ve error code if unsuccessful.
165  */
166 int vfs_statx(int dfd, const char __user *filename, int flags,
167               struct kstat *stat, u32 request_mask)
169         struct path path;
170         int error = -EINVAL;
171         unsigned int lookup_flags = LOOKUP_FOLLOW | LOOKUP_AUTOMOUNT;
173         if ((flags & ~(AT_SYMLINK_NOFOLLOW | AT_NO_AUTOMOUNT |
174                        AT_EMPTY_PATH | KSTAT_QUERY_FLAGS)) != 0)
175                 return -EINVAL;
177         if (flags & AT_SYMLINK_NOFOLLOW)
178                 lookup_flags &= ~LOOKUP_FOLLOW;
179         if (flags & AT_NO_AUTOMOUNT)
180                 lookup_flags &= ~LOOKUP_AUTOMOUNT;
181         if (flags & AT_EMPTY_PATH)
182                 lookup_flags |= LOOKUP_EMPTY;
184 retry:
185         error = user_path_at(dfd, filename, lookup_flags, &path);
186         if (error)
187                 goto out;
189         error = vfs_getattr(&path, stat, request_mask, flags);
190         path_put(&path);
191         if (retry_estale(error, lookup_flags)) {
192                 lookup_flags |= LOOKUP_REVAL;
193                 goto retry;
194         }
195 out:
196         return error;
198 EXPORT_SYMBOL(vfs_statx);
201 #ifdef __ARCH_WANT_OLD_STAT
203 /*
204  * For backward compatibility?  Maybe this should be moved
205  * into arch/i386 instead?
206  */
207 static int cp_old_stat(struct kstat *stat, struct __old_kernel_stat __user * statbuf)
209         static int warncount = 5;
210         struct __old_kernel_stat tmp;
212         if (warncount > 0) {
213                 warncount--;
214                 printk(KERN_WARNING "VFS: Warning: %s using old stat() call. Recompile your binary.\n",
215                         current->comm);
216         } else if (warncount < 0) {
217                 /* it's laughable, but... */
218                 warncount = 0;
219         }
221         memset(&tmp, 0, sizeof(struct __old_kernel_stat));
222         tmp.st_dev = old_encode_dev(stat->dev);
223         tmp.st_ino = stat->ino;
224         if (sizeof(tmp.st_ino) < sizeof(stat->ino) && tmp.st_ino != stat->ino)
225                 return -EOVERFLOW;
226         tmp.st_mode = stat->mode;
227         tmp.st_nlink = stat->nlink;
228         if (tmp.st_nlink != stat->nlink)
229                 return -EOVERFLOW;
230         SET_UID(tmp.st_uid, from_kuid_munged(current_user_ns(), stat->uid));
231         SET_GID(tmp.st_gid, from_kgid_munged(current_user_ns(), stat->gid));
232         tmp.st_rdev = old_encode_dev(stat->rdev);
233 #if BITS_PER_LONG == 32
234         if (stat->size > MAX_NON_LFS)
235                 return -EOVERFLOW;
236 #endif
237         tmp.st_size = stat->size;
238         tmp.st_atime = stat->atime.tv_sec;
239         tmp.st_mtime = stat->mtime.tv_sec;
240         tmp.st_ctime = stat->ctime.tv_sec;
241         return copy_to_user(statbuf,&tmp,sizeof(tmp)) ? -EFAULT : 0;
244 SYSCALL_DEFINE2(stat, const char __user *, filename,
245                 struct __old_kernel_stat __user *, statbuf)
247         struct kstat stat;
248         int error;
250         error = vfs_stat(filename, &stat);
251         if (error)
252                 return error;
254         return cp_old_stat(&stat, statbuf);
257 SYSCALL_DEFINE2(lstat, const char __user *, filename,
258                 struct __old_kernel_stat __user *, statbuf)
260         struct kstat stat;
261         int error;
263         error = vfs_lstat(filename, &stat);
264         if (error)
265                 return error;
267         return cp_old_stat(&stat, statbuf);
270 SYSCALL_DEFINE2(fstat, unsigned int, fd, struct __old_kernel_stat __user *, statbuf)
272         struct kstat stat;
273         int error = vfs_fstat(fd, &stat);
275         if (!error)
276                 error = cp_old_stat(&stat, statbuf);
278         return error;
281 #endif /* __ARCH_WANT_OLD_STAT */
283 #ifdef __ARCH_WANT_NEW_STAT
285 #if BITS_PER_LONG == 32
286 #  define choose_32_64(a,b) a
287 #else
288 #  define choose_32_64(a,b) b
289 #endif
291 #define valid_dev(x)  choose_32_64(old_valid_dev(x),true)
292 #define encode_dev(x) choose_32_64(old_encode_dev,new_encode_dev)(x)
294 #ifndef INIT_STRUCT_STAT_PADDING
295 #  define INIT_STRUCT_STAT_PADDING(st) memset(&st, 0, sizeof(st))
296 #endif
298 static int cp_new_stat(struct kstat *stat, struct stat __user *statbuf)
300         struct stat tmp;
302         if (!valid_dev(stat->dev) || !valid_dev(stat->rdev))
303                 return -EOVERFLOW;
304 #if BITS_PER_LONG == 32
305         if (stat->size > MAX_NON_LFS)
306                 return -EOVERFLOW;
307 #endif
309         INIT_STRUCT_STAT_PADDING(tmp);
310         tmp.st_dev = encode_dev(stat->dev);
311         tmp.st_ino = stat->ino;
312         if (sizeof(tmp.st_ino) < sizeof(stat->ino) && tmp.st_ino != stat->ino)
313                 return -EOVERFLOW;
314         tmp.st_mode = stat->mode;
315         tmp.st_nlink = stat->nlink;
316         if (tmp.st_nlink != stat->nlink)
317                 return -EOVERFLOW;
318         SET_UID(tmp.st_uid, from_kuid_munged(current_user_ns(), stat->uid));
319         SET_GID(tmp.st_gid, from_kgid_munged(current_user_ns(), stat->gid));
320         tmp.st_rdev = encode_dev(stat->rdev);
321         tmp.st_size = stat->size;
322         tmp.st_atime = stat->atime.tv_sec;
323         tmp.st_mtime = stat->mtime.tv_sec;
324         tmp.st_ctime = stat->ctime.tv_sec;
325 #ifdef STAT_HAVE_NSEC
326         tmp.st_atime_nsec = stat->atime.tv_nsec;
327         tmp.st_mtime_nsec = stat->mtime.tv_nsec;
328         tmp.st_ctime_nsec = stat->ctime.tv_nsec;
329 #endif
330         tmp.st_blocks = stat->blocks;
331         tmp.st_blksize = stat->blksize;
332         return copy_to_user(statbuf,&tmp,sizeof(tmp)) ? -EFAULT : 0;
335 SYSCALL_DEFINE2(newstat, const char __user *, filename,
336                 struct stat __user *, statbuf)
338         struct kstat stat;
339         int error = vfs_stat(filename, &stat);
341         if (error)
342                 return error;
343         return cp_new_stat(&stat, statbuf);
346 SYSCALL_DEFINE2(newlstat, const char __user *, filename,
347                 struct stat __user *, statbuf)
349         struct kstat stat;
350         int error;
352         error = vfs_lstat(filename, &stat);
353         if (error)
354                 return error;
356         return cp_new_stat(&stat, statbuf);
359 #if !defined(__ARCH_WANT_STAT64) || defined(__ARCH_WANT_SYS_NEWFSTATAT)
360 SYSCALL_DEFINE4(newfstatat, int, dfd, const char __user *, filename,
361                 struct stat __user *, statbuf, int, flag)
363         struct kstat stat;
364         int error;
366         error = vfs_fstatat(dfd, filename, &stat, flag);
367         if (error)
368                 return error;
369         return cp_new_stat(&stat, statbuf);
371 #endif
373 SYSCALL_DEFINE2(newfstat, unsigned int, fd, struct stat __user *, statbuf)
375         struct kstat stat;
376         int error = vfs_fstat(fd, &stat);
378         if (!error)
379                 error = cp_new_stat(&stat, statbuf);
381         return error;
383 #endif
385 static int do_readlinkat(int dfd, const char __user *pathname,
386                          char __user *buf, int bufsiz)
388         struct path path;
389         int error;
390         int empty = 0;
391         unsigned int lookup_flags = LOOKUP_EMPTY;
393         if (bufsiz <= 0)
394                 return -EINVAL;
396 retry:
397         error = user_path_at_empty(dfd, pathname, lookup_flags, &path, &empty);
398         if (!error) {
399                 struct inode *inode = d_backing_inode(path.dentry);
401                 error = empty ? -ENOENT : -EINVAL;
402                 /*
403                  * AFS mountpoints allow readlink(2) but are not symlinks
404                  */
405                 if (d_is_symlink(path.dentry) || inode->i_op->readlink) {
406                         error = security_inode_readlink(path.dentry);
407                         if (!error) {
408                                 touch_atime(&path);
409                                 error = vfs_readlink(path.dentry, buf, bufsiz);
410                         }
411                 }
412                 path_put(&path);
413                 if (retry_estale(error, lookup_flags)) {
414                         lookup_flags |= LOOKUP_REVAL;
415                         goto retry;
416                 }
417         }
418         return error;
421 SYSCALL_DEFINE4(readlinkat, int, dfd, const char __user *, pathname,
422                 char __user *, buf, int, bufsiz)
424         return do_readlinkat(dfd, pathname, buf, bufsiz);
427 SYSCALL_DEFINE3(readlink, const char __user *, path, char __user *, buf,
428                 int, bufsiz)
430         return do_readlinkat(AT_FDCWD, path, buf, bufsiz);
434 /* ---------- LFS-64 ----------- */
435 #if defined(__ARCH_WANT_STAT64) || defined(__ARCH_WANT_COMPAT_STAT64)
437 #ifndef INIT_STRUCT_STAT64_PADDING
438 #  define INIT_STRUCT_STAT64_PADDING(st) memset(&st, 0, sizeof(st))
439 #endif
441 static long cp_new_stat64(struct kstat *stat, struct stat64 __user *statbuf)
443         struct stat64 tmp;
445         INIT_STRUCT_STAT64_PADDING(tmp);
446 #ifdef CONFIG_MIPS
447         /* mips has weird padding, so we don't get 64 bits there */
448         tmp.st_dev = new_encode_dev(stat->dev);
449         tmp.st_rdev = new_encode_dev(stat->rdev);
450 #else
451         tmp.st_dev = huge_encode_dev(stat->dev);
452         tmp.st_rdev = huge_encode_dev(stat->rdev);
453 #endif
454         tmp.st_ino = stat->ino;
455         if (sizeof(tmp.st_ino) < sizeof(stat->ino) && tmp.st_ino != stat->ino)
456                 return -EOVERFLOW;
457 #ifdef STAT64_HAS_BROKEN_ST_INO
458         tmp.__st_ino = stat->ino;
459 #endif
460         tmp.st_mode = stat->mode;
461         tmp.st_nlink = stat->nlink;
462         tmp.st_uid = from_kuid_munged(current_user_ns(), stat->uid);
463         tmp.st_gid = from_kgid_munged(current_user_ns(), stat->gid);
464         tmp.st_atime = stat->atime.tv_sec;
465         tmp.st_atime_nsec = stat->atime.tv_nsec;
466         tmp.st_mtime = stat->mtime.tv_sec;
467         tmp.st_mtime_nsec = stat->mtime.tv_nsec;
468         tmp.st_ctime = stat->ctime.tv_sec;
469         tmp.st_ctime_nsec = stat->ctime.tv_nsec;
470         tmp.st_size = stat->size;
471         tmp.st_blocks = stat->blocks;
472         tmp.st_blksize = stat->blksize;
473         return copy_to_user(statbuf,&tmp,sizeof(tmp)) ? -EFAULT : 0;
476 SYSCALL_DEFINE2(stat64, const char __user *, filename,
477                 struct stat64 __user *, statbuf)
479         struct kstat stat;
480         int error = vfs_stat(filename, &stat);
482         if (!error)
483                 error = cp_new_stat64(&stat, statbuf);
485         return error;
488 SYSCALL_DEFINE2(lstat64, const char __user *, filename,
489                 struct stat64 __user *, statbuf)
491         struct kstat stat;
492         int error = vfs_lstat(filename, &stat);
494         if (!error)
495                 error = cp_new_stat64(&stat, statbuf);
497         return error;
500 SYSCALL_DEFINE2(fstat64, unsigned long, fd, struct stat64 __user *, statbuf)
502         struct kstat stat;
503         int error = vfs_fstat(fd, &stat);
505         if (!error)
506                 error = cp_new_stat64(&stat, statbuf);
508         return error;
511 SYSCALL_DEFINE4(fstatat64, int, dfd, const char __user *, filename,
512                 struct stat64 __user *, statbuf, int, flag)
514         struct kstat stat;
515         int error;
517         error = vfs_fstatat(dfd, filename, &stat, flag);
518         if (error)
519                 return error;
520         return cp_new_stat64(&stat, statbuf);
522 #endif /* __ARCH_WANT_STAT64 || __ARCH_WANT_COMPAT_STAT64 */
524 static noinline_for_stack int
525 cp_statx(const struct kstat *stat, struct statx __user *buffer)
527         struct statx tmp;
529         memset(&tmp, 0, sizeof(tmp));
531         tmp.stx_mask = stat->result_mask;
532         tmp.stx_blksize = stat->blksize;
533         tmp.stx_attributes = stat->attributes;
534         tmp.stx_nlink = stat->nlink;
535         tmp.stx_uid = from_kuid_munged(current_user_ns(), stat->uid);
536         tmp.stx_gid = from_kgid_munged(current_user_ns(), stat->gid);
537         tmp.stx_mode = stat->mode;
538         tmp.stx_ino = stat->ino;
539         tmp.stx_size = stat->size;
540         tmp.stx_blocks = stat->blocks;
541         tmp.stx_attributes_mask = stat->attributes_mask;
542         tmp.stx_atime.tv_sec = stat->atime.tv_sec;
543         tmp.stx_atime.tv_nsec = stat->atime.tv_nsec;
544         tmp.stx_btime.tv_sec = stat->btime.tv_sec;
545         tmp.stx_btime.tv_nsec = stat->btime.tv_nsec;
546         tmp.stx_ctime.tv_sec = stat->ctime.tv_sec;
547         tmp.stx_ctime.tv_nsec = stat->ctime.tv_nsec;
548         tmp.stx_mtime.tv_sec = stat->mtime.tv_sec;
549         tmp.stx_mtime.tv_nsec = stat->mtime.tv_nsec;
550         tmp.stx_rdev_major = MAJOR(stat->rdev);
551         tmp.stx_rdev_minor = MINOR(stat->rdev);
552         tmp.stx_dev_major = MAJOR(stat->dev);
553         tmp.stx_dev_minor = MINOR(stat->dev);
555         return copy_to_user(buffer, &tmp, sizeof(tmp)) ? -EFAULT : 0;
558 /**
559  * sys_statx - System call to get enhanced stats
560  * @dfd: Base directory to pathwalk from *or* fd to stat.
561  * @filename: File to stat or "" with AT_EMPTY_PATH
562  * @flags: AT_* flags to control pathwalk.
563  * @mask: Parts of statx struct actually required.
564  * @buffer: Result buffer.
565  *
566  * Note that fstat() can be emulated by setting dfd to the fd of interest,
567  * supplying "" as the filename and setting AT_EMPTY_PATH in the flags.
568  */
569 SYSCALL_DEFINE5(statx,
570                 int, dfd, const char __user *, filename, unsigned, flags,
571                 unsigned int, mask,
572                 struct statx __user *, buffer)
574         struct kstat stat;
575         int error;
577         if (mask & STATX__RESERVED)
578                 return -EINVAL;
579         if ((flags & AT_STATX_SYNC_TYPE) == AT_STATX_SYNC_TYPE)
580                 return -EINVAL;
582         error = vfs_statx(dfd, filename, flags, &stat, mask);
583         if (error)
584                 return error;
586         return cp_statx(&stat, buffer);
589 #ifdef CONFIG_COMPAT
590 static int cp_compat_stat(struct kstat *stat, struct compat_stat __user *ubuf)
592         struct compat_stat tmp;
594         if (!old_valid_dev(stat->dev) || !old_valid_dev(stat->rdev))
595                 return -EOVERFLOW;
597         memset(&tmp, 0, sizeof(tmp));
598         tmp.st_dev = old_encode_dev(stat->dev);
599         tmp.st_ino = stat->ino;
600         if (sizeof(tmp.st_ino) < sizeof(stat->ino) && tmp.st_ino != stat->ino)
601                 return -EOVERFLOW;
602         tmp.st_mode = stat->mode;
603         tmp.st_nlink = stat->nlink;
604         if (tmp.st_nlink != stat->nlink)
605                 return -EOVERFLOW;
606         SET_UID(tmp.st_uid, from_kuid_munged(current_user_ns(), stat->uid));
607         SET_GID(tmp.st_gid, from_kgid_munged(current_user_ns(), stat->gid));
608         tmp.st_rdev = old_encode_dev(stat->rdev);
609         if ((u64) stat->size > MAX_NON_LFS)
610                 return -EOVERFLOW;
611         tmp.st_size = stat->size;
612         tmp.st_atime = stat->atime.tv_sec;
613         tmp.st_atime_nsec = stat->atime.tv_nsec;
614         tmp.st_mtime = stat->mtime.tv_sec;
615         tmp.st_mtime_nsec = stat->mtime.tv_nsec;
616         tmp.st_ctime = stat->ctime.tv_sec;
617         tmp.st_ctime_nsec = stat->ctime.tv_nsec;
618         tmp.st_blocks = stat->blocks;
619         tmp.st_blksize = stat->blksize;
620         return copy_to_user(ubuf, &tmp, sizeof(tmp)) ? -EFAULT : 0;
623 COMPAT_SYSCALL_DEFINE2(newstat, const char __user *, filename,
624                        struct compat_stat __user *, statbuf)
626         struct kstat stat;
627         int error;
629         error = vfs_stat(filename, &stat);
630         if (error)
631                 return error;
632         return cp_compat_stat(&stat, statbuf);
635 COMPAT_SYSCALL_DEFINE2(newlstat, const char __user *, filename,
636                        struct compat_stat __user *, statbuf)
638         struct kstat stat;
639         int error;
641         error = vfs_lstat(filename, &stat);
642         if (error)
643                 return error;
644         return cp_compat_stat(&stat, statbuf);
647 #ifndef __ARCH_WANT_STAT64
648 COMPAT_SYSCALL_DEFINE4(newfstatat, unsigned int, dfd,
649                        const char __user *, filename,
650                        struct compat_stat __user *, statbuf, int, flag)
652         struct kstat stat;
653         int error;
655         error = vfs_fstatat(dfd, filename, &stat, flag);
656         if (error)
657                 return error;
658         return cp_compat_stat(&stat, statbuf);
660 #endif
662 COMPAT_SYSCALL_DEFINE2(newfstat, unsigned int, fd,
663                        struct compat_stat __user *, statbuf)
665         struct kstat stat;
666         int error = vfs_fstat(fd, &stat);
668         if (!error)
669                 error = cp_compat_stat(&stat, statbuf);
670         return error;
672 #endif
674 /* Caller is here responsible for sufficient locking (ie. inode->i_lock) */
675 void __inode_add_bytes(struct inode *inode, loff_t bytes)
677         inode->i_blocks += bytes >> 9;
678         bytes &= 511;
679         inode->i_bytes += bytes;
680         if (inode->i_bytes >= 512) {
681                 inode->i_blocks++;
682                 inode->i_bytes -= 512;
683         }
685 EXPORT_SYMBOL(__inode_add_bytes);
687 void inode_add_bytes(struct inode *inode, loff_t bytes)
689         spin_lock(&inode->i_lock);
690         __inode_add_bytes(inode, bytes);
691         spin_unlock(&inode->i_lock);
694 EXPORT_SYMBOL(inode_add_bytes);
696 void __inode_sub_bytes(struct inode *inode, loff_t bytes)
698         inode->i_blocks -= bytes >> 9;
699         bytes &= 511;
700         if (inode->i_bytes < bytes) {
701                 inode->i_blocks--;
702                 inode->i_bytes += 512;
703         }
704         inode->i_bytes -= bytes;
707 EXPORT_SYMBOL(__inode_sub_bytes);
709 void inode_sub_bytes(struct inode *inode, loff_t bytes)
711         spin_lock(&inode->i_lock);
712         __inode_sub_bytes(inode, bytes);
713         spin_unlock(&inode->i_lock);
716 EXPORT_SYMBOL(inode_sub_bytes);
718 loff_t inode_get_bytes(struct inode *inode)
720         loff_t ret;
722         spin_lock(&inode->i_lock);
723         ret = __inode_get_bytes(inode);
724         spin_unlock(&inode->i_lock);
725         return ret;
728 EXPORT_SYMBOL(inode_get_bytes);
730 void inode_set_bytes(struct inode *inode, loff_t bytes)
732         /* Caller is here responsible for sufficient locking
733          * (ie. inode->i_lock) */
734         inode->i_blocks = bytes >> 9;
735         inode->i_bytes = bytes & 511;
738 EXPORT_SYMBOL(inode_set_bytes);