1 /* SPDX-License-Identifier: GPL-2.0 */
2 #include <linux/device.h>
3 #include <linux/types.h>
4 #include <linux/io.h>
5 #include <linux/mm.h>
7 #ifndef ioremap_cache
8 /* temporary while we convert existing ioremap_cache users to memremap */
9 __weak void __iomem *ioremap_cache(resource_size_t offset, unsigned long size)
10 {
11 return ioremap(offset, size);
12 }
13 #endif
15 #ifndef arch_memremap_wb
16 static void *arch_memremap_wb(resource_size_t offset, unsigned long size)
17 {
18 return (__force void *)ioremap_cache(offset, size);
19 }
20 #endif
22 #ifndef arch_memremap_can_ram_remap
23 static bool arch_memremap_can_ram_remap(resource_size_t offset, size_t size,
24 unsigned long flags)
25 {
26 return true;
27 }
28 #endif
30 static void *try_ram_remap(resource_size_t offset, size_t size,
31 unsigned long flags)
32 {
33 unsigned long pfn = PHYS_PFN(offset);
35 /* In the simple case just return the existing linear address */
36 if (pfn_valid(pfn) && !PageHighMem(pfn_to_page(pfn)) &&
37 arch_memremap_can_ram_remap(offset, size, flags))
38 return __va(offset);
40 return NULL; /* fallback to arch_memremap_wb */
41 }
43 /**
44 * memremap() - remap an iomem_resource as cacheable memory
45 * @offset: iomem resource start address
46 * @size: size of remap
47 * @flags: any of MEMREMAP_WB, MEMREMAP_WT, MEMREMAP_WC,
48 * MEMREMAP_ENC, MEMREMAP_DEC
49 *
50 * memremap() is "ioremap" for cases where it is known that the resource
51 * being mapped does not have i/o side effects and the __iomem
52 * annotation is not applicable. In the case of multiple flags, the different
53 * mapping types will be attempted in the order listed below until one of
54 * them succeeds.
55 *
56 * MEMREMAP_WB - matches the default mapping for System RAM on
57 * the architecture. This is usually a read-allocate write-back cache.
58 * Morever, if MEMREMAP_WB is specified and the requested remap region is RAM
59 * memremap() will bypass establishing a new mapping and instead return
60 * a pointer into the direct map.
61 *
62 * MEMREMAP_WT - establish a mapping whereby writes either bypass the
63 * cache or are written through to memory and never exist in a
64 * cache-dirty state with respect to program visibility. Attempts to
65 * map System RAM with this mapping type will fail.
66 *
67 * MEMREMAP_WC - establish a writecombine mapping, whereby writes may
68 * be coalesced together (e.g. in the CPU's write buffers), but is otherwise
69 * uncached. Attempts to map System RAM with this mapping type will fail.
70 */
71 void *memremap(resource_size_t offset, size_t size, unsigned long flags)
72 {
73 int is_ram = region_intersects(offset, size,
74 IORESOURCE_SYSTEM_RAM, IORES_DESC_NONE);
75 void *addr = NULL;
77 if (!flags)
78 return NULL;
80 if (is_ram == REGION_MIXED) {
81 WARN_ONCE(1, "memremap attempted on mixed range %pa size: %#lx\n",
82 &offset, (unsigned long) size);
83 return NULL;
84 }
86 /* Try all mapping types requested until one returns non-NULL */
87 if (flags & MEMREMAP_WB) {
88 /*
89 * MEMREMAP_WB is special in that it can be satisifed
90 * from the direct map. Some archs depend on the
91 * capability of memremap() to autodetect cases where
92 * the requested range is potentially in System RAM.
93 */
94 if (is_ram == REGION_INTERSECTS)
95 addr = try_ram_remap(offset, size, flags);
96 if (!addr)
97 addr = arch_memremap_wb(offset, size);
98 }
100 /*
101 * If we don't have a mapping yet and other request flags are
102 * present then we will be attempting to establish a new virtual
103 * address mapping. Enforce that this mapping is not aliasing
104 * System RAM.
105 */
106 if (!addr && is_ram == REGION_INTERSECTS && flags != MEMREMAP_WB) {
107 WARN_ONCE(1, "memremap attempted on ram %pa size: %#lx\n",
108 &offset, (unsigned long) size);
109 return NULL;
110 }
112 if (!addr && (flags & MEMREMAP_WT))
113 addr = ioremap_wt(offset, size);
115 if (!addr && (flags & MEMREMAP_WC))
116 addr = ioremap_wc(offset, size);
118 return addr;
119 }
120 EXPORT_SYMBOL(memremap);
122 void memunmap(void *addr)
123 {
124 if (is_vmalloc_addr(addr))
125 iounmap((void __iomem *) addr);
126 }
127 EXPORT_SYMBOL(memunmap);
129 static void devm_memremap_release(struct device *dev, void *res)
130 {
131 memunmap(*(void **)res);
132 }
134 static int devm_memremap_match(struct device *dev, void *res, void *match_data)
135 {
136 return *(void **)res == match_data;
137 }
139 void *devm_memremap(struct device *dev, resource_size_t offset,
140 size_t size, unsigned long flags)
141 {
142 void **ptr, *addr;
144 ptr = devres_alloc_node(devm_memremap_release, sizeof(*ptr), GFP_KERNEL,
145 dev_to_node(dev));
146 if (!ptr)
147 return ERR_PTR(-ENOMEM);
149 addr = memremap(offset, size, flags);
150 if (addr) {
151 *ptr = addr;
152 devres_add(dev, ptr);
153 } else {
154 devres_free(ptr);
155 return ERR_PTR(-ENXIO);
156 }
158 return addr;
159 }
160 EXPORT_SYMBOL(devm_memremap);
162 void devm_memunmap(struct device *dev, void *addr)
163 {
164 WARN_ON(devres_release(dev, devm_memremap_release,
165 devm_memremap_match, addr));
166 }
167 EXPORT_SYMBOL(devm_memunmap);