1 /*
2 * linux/kernel/softirq.c
3 *
4 * Copyright (C) 1992 Linus Torvalds
5 *
6 * Distribute under GPLv2.
7 *
8 * Rewritten. Old one was good in 2.2, but in 2.3 it was immoral. --ANK (990903)
9 */
11 #define pr_fmt(fmt) KBUILD_MODNAME ": " fmt
13 #include <linux/export.h>
14 #include <linux/kernel_stat.h>
15 #include <linux/interrupt.h>
16 #include <linux/init.h>
17 #include <linux/mm.h>
18 #include <linux/notifier.h>
19 #include <linux/percpu.h>
20 #include <linux/cpu.h>
21 #include <linux/freezer.h>
22 #include <linux/kthread.h>
23 #include <linux/rcupdate.h>
24 #include <linux/ftrace.h>
25 #include <linux/smp.h>
26 #include <linux/smpboot.h>
27 #include <linux/tick.h>
28 #include <linux/irq.h>
30 #define CREATE_TRACE_POINTS
31 #include <trace/events/irq.h>
33 /*
34 - No shared variables, all the data are CPU local.
35 - If a softirq needs serialization, let it serialize itself
36 by its own spinlocks.
37 - Even if softirq is serialized, only local cpu is marked for
38 execution. Hence, we get something sort of weak cpu binding.
39 Though it is still not clear, will it result in better locality
40 or will not.
42 Examples:
43 - NET RX softirq. It is multithreaded and does not require
44 any global serialization.
45 - NET TX softirq. It kicks software netdevice queues, hence
46 it is logically serialized per device, but this serialization
47 is invisible to common code.
48 - Tasklets: serialized wrt itself.
49 */
51 #ifndef __ARCH_IRQ_STAT
52 DEFINE_PER_CPU_ALIGNED(irq_cpustat_t, irq_stat);
53 EXPORT_PER_CPU_SYMBOL(irq_stat);
54 #endif
56 static struct softirq_action softirq_vec[NR_SOFTIRQS] __cacheline_aligned_in_smp;
58 DEFINE_PER_CPU(struct task_struct *, ksoftirqd);
60 const char * const softirq_to_name[NR_SOFTIRQS] = {
61 "HI", "TIMER", "NET_TX", "NET_RX", "BLOCK", "IRQ_POLL",
62 "TASKLET", "SCHED", "HRTIMER", "RCU"
63 };
65 /*
66 * we cannot loop indefinitely here to avoid userspace starvation,
67 * but we also don't want to introduce a worst case 1/HZ latency
68 * to the pending events, so lets the scheduler to balance
69 * the softirq load for us.
70 */
71 static void wakeup_softirqd(void)
72 {
73 /* Interrupts are disabled: no need to stop preemption */
74 struct task_struct *tsk = __this_cpu_read(ksoftirqd);
76 if (tsk && tsk->state != TASK_RUNNING)
77 wake_up_process(tsk);
78 }
80 /*
81 * If ksoftirqd is scheduled, we do not want to process pending softirqs
82 * right now. Let ksoftirqd handle this at its own rate, to get fairness,
83 * unless we're doing some of the synchronous softirqs.
84 */
85 #define SOFTIRQ_NOW_MASK ((1 << HI_SOFTIRQ) | (1 << TASKLET_SOFTIRQ))
86 static bool ksoftirqd_running(unsigned long pending)
87 {
88 struct task_struct *tsk = __this_cpu_read(ksoftirqd);
90 if (pending & SOFTIRQ_NOW_MASK)
91 return false;
92 return tsk && (tsk->state == TASK_RUNNING);
93 }
95 /*
96 * preempt_count and SOFTIRQ_OFFSET usage:
97 * - preempt_count is changed by SOFTIRQ_OFFSET on entering or leaving
98 * softirq processing.
99 * - preempt_count is changed by SOFTIRQ_DISABLE_OFFSET (= 2 * SOFTIRQ_OFFSET)
100 * on local_bh_disable or local_bh_enable.
101 * This lets us distinguish between whether we are currently processing
102 * softirq and whether we just have bh disabled.
103 */
105 /*
106 * This one is for softirq.c-internal use,
107 * where hardirqs are disabled legitimately:
108 */
109 #ifdef CONFIG_TRACE_IRQFLAGS
110 void __local_bh_disable_ip(unsigned long ip, unsigned int cnt)
111 {
112 unsigned long flags;
114 WARN_ON_ONCE(in_irq());
116 raw_local_irq_save(flags);
117 /*
118 * The preempt tracer hooks into preempt_count_add and will break
119 * lockdep because it calls back into lockdep after SOFTIRQ_OFFSET
120 * is set and before current->softirq_enabled is cleared.
121 * We must manually increment preempt_count here and manually
122 * call the trace_preempt_off later.
123 */
124 __preempt_count_add(cnt);
125 /*
126 * Were softirqs turned off above:
127 */
128 if (softirq_count() == (cnt & SOFTIRQ_MASK))
129 trace_softirqs_off(ip);
130 raw_local_irq_restore(flags);
132 if (preempt_count() == cnt) {
133 #ifdef CONFIG_DEBUG_PREEMPT
134 current->preempt_disable_ip = get_lock_parent_ip();
135 #endif
136 trace_preempt_off(CALLER_ADDR0, get_lock_parent_ip());
137 }
138 }
139 EXPORT_SYMBOL(__local_bh_disable_ip);
140 #endif /* CONFIG_TRACE_IRQFLAGS */
142 static void __local_bh_enable(unsigned int cnt)
143 {
144 lockdep_assert_irqs_disabled();
146 if (preempt_count() == cnt)
147 trace_preempt_on(CALLER_ADDR0, get_lock_parent_ip());
149 if (softirq_count() == (cnt & SOFTIRQ_MASK))
150 trace_softirqs_on(_RET_IP_);
152 __preempt_count_sub(cnt);
153 }
155 /*
156 * Special-case - softirqs can safely be enabled by __do_softirq(),
157 * without processing still-pending softirqs:
158 */
159 void _local_bh_enable(void)
160 {
161 WARN_ON_ONCE(in_irq());
162 __local_bh_enable(SOFTIRQ_DISABLE_OFFSET);
163 }
164 EXPORT_SYMBOL(_local_bh_enable);
166 void __local_bh_enable_ip(unsigned long ip, unsigned int cnt)
167 {
168 WARN_ON_ONCE(in_irq());
169 lockdep_assert_irqs_enabled();
170 #ifdef CONFIG_TRACE_IRQFLAGS
171 local_irq_disable();
172 #endif
173 /*
174 * Are softirqs going to be turned on now:
175 */
176 if (softirq_count() == SOFTIRQ_DISABLE_OFFSET)
177 trace_softirqs_on(ip);
178 /*
179 * Keep preemption disabled until we are done with
180 * softirq processing:
181 */
182 preempt_count_sub(cnt - 1);
184 if (unlikely(!in_interrupt() && local_softirq_pending())) {
185 /*
186 * Run softirq if any pending. And do it in its own stack
187 * as we may be calling this deep in a task call stack already.
188 */
189 do_softirq();
190 }
192 preempt_count_dec();
193 #ifdef CONFIG_TRACE_IRQFLAGS
194 local_irq_enable();
195 #endif
196 preempt_check_resched();
197 }
198 EXPORT_SYMBOL(__local_bh_enable_ip);
200 /*
201 * We restart softirq processing for at most MAX_SOFTIRQ_RESTART times,
202 * but break the loop if need_resched() is set or after 2 ms.
203 * The MAX_SOFTIRQ_TIME provides a nice upper bound in most cases, but in
204 * certain cases, such as stop_machine(), jiffies may cease to
205 * increment and so we need the MAX_SOFTIRQ_RESTART limit as
206 * well to make sure we eventually return from this method.
207 *
208 * These limits have been established via experimentation.
209 * The two things to balance is latency against fairness -
210 * we want to handle softirqs as soon as possible, but they
211 * should not be able to lock up the box.
212 */
213 #define MAX_SOFTIRQ_TIME msecs_to_jiffies(2)
214 #define MAX_SOFTIRQ_RESTART 10
216 #ifdef CONFIG_TRACE_IRQFLAGS
217 /*
218 * When we run softirqs from irq_exit() and thus on the hardirq stack we need
219 * to keep the lockdep irq context tracking as tight as possible in order to
220 * not miss-qualify lock contexts and miss possible deadlocks.
221 */
223 static inline bool lockdep_softirq_start(void)
224 {
225 bool in_hardirq = false;
227 if (trace_hardirq_context(current)) {
228 in_hardirq = true;
229 trace_hardirq_exit();
230 }
232 lockdep_softirq_enter();
234 return in_hardirq;
235 }
237 static inline void lockdep_softirq_end(bool in_hardirq)
238 {
239 lockdep_softirq_exit();
241 if (in_hardirq)
242 trace_hardirq_enter();
243 }
244 #else
245 static inline bool lockdep_softirq_start(void) { return false; }
246 static inline void lockdep_softirq_end(bool in_hardirq) { }
247 #endif
249 asmlinkage __visible void __softirq_entry __do_softirq(void)
250 {
251 unsigned long end = jiffies + MAX_SOFTIRQ_TIME;
252 unsigned long old_flags = current->flags;
253 int max_restart = MAX_SOFTIRQ_RESTART;
254 struct softirq_action *h;
255 bool in_hardirq;
256 __u32 pending;
257 int softirq_bit;
259 /*
260 * Mask out PF_MEMALLOC as the current task context is borrowed for the
261 * softirq. A softirq handled, such as network RX, might set PF_MEMALLOC
262 * again if the socket is related to swapping.
263 */
264 current->flags &= ~PF_MEMALLOC;
266 pending = local_softirq_pending();
267 account_irq_enter_time(current);
269 __local_bh_disable_ip(_RET_IP_, SOFTIRQ_OFFSET);
270 in_hardirq = lockdep_softirq_start();
272 restart:
273 /* Reset the pending bitmask before enabling irqs */
274 set_softirq_pending(0);
276 local_irq_enable();
278 h = softirq_vec;
280 while ((softirq_bit = ffs(pending))) {
281 unsigned int vec_nr;
282 int prev_count;
284 h += softirq_bit - 1;
286 vec_nr = h - softirq_vec;
287 prev_count = preempt_count();
289 kstat_incr_softirqs_this_cpu(vec_nr);
291 trace_softirq_entry(vec_nr);
292 h->action(h);
293 trace_softirq_exit(vec_nr);
294 if (unlikely(prev_count != preempt_count())) {
295 pr_err("huh, entered softirq %u %s %p with preempt_count %08x, exited with %08x?\n",
296 vec_nr, softirq_to_name[vec_nr], h->action,
297 prev_count, preempt_count());
298 preempt_count_set(prev_count);
299 }
300 h++;
301 pending >>= softirq_bit;
302 }
304 if (__this_cpu_read(ksoftirqd) == current)
305 rcu_softirq_qs();
306 local_irq_disable();
308 pending = local_softirq_pending();
309 if (pending) {
310 if (time_before(jiffies, end) && !need_resched() &&
311 --max_restart)
312 goto restart;
314 wakeup_softirqd();
315 }
317 lockdep_softirq_end(in_hardirq);
318 account_irq_exit_time(current);
319 __local_bh_enable(SOFTIRQ_OFFSET);
320 WARN_ON_ONCE(in_interrupt());
321 current_restore_flags(old_flags, PF_MEMALLOC);
322 }
324 asmlinkage __visible void do_softirq(void)
325 {
326 __u32 pending;
327 unsigned long flags;
329 if (in_interrupt())
330 return;
332 local_irq_save(flags);
334 pending = local_softirq_pending();
336 if (pending && !ksoftirqd_running(pending))
337 do_softirq_own_stack();
339 local_irq_restore(flags);
340 }
342 /*
343 * Enter an interrupt context.
344 */
345 void irq_enter(void)
346 {
347 rcu_irq_enter();
348 if (is_idle_task(current) && !in_interrupt()) {
349 /*
350 * Prevent raise_softirq from needlessly waking up ksoftirqd
351 * here, as softirq will be serviced on return from interrupt.
352 */
353 local_bh_disable();
354 tick_irq_enter();
355 _local_bh_enable();
356 }
358 __irq_enter();
359 }
361 static inline void invoke_softirq(void)
362 {
363 if (ksoftirqd_running(local_softirq_pending()))
364 return;
366 if (!force_irqthreads) {
367 #ifdef CONFIG_HAVE_IRQ_EXIT_ON_IRQ_STACK
368 /*
369 * We can safely execute softirq on the current stack if
370 * it is the irq stack, because it should be near empty
371 * at this stage.
372 */
373 __do_softirq();
374 #else
375 /*
376 * Otherwise, irq_exit() is called on the task stack that can
377 * be potentially deep already. So call softirq in its own stack
378 * to prevent from any overrun.
379 */
380 do_softirq_own_stack();
381 #endif
382 } else {
383 wakeup_softirqd();
384 }
385 }
387 static inline void tick_irq_exit(void)
388 {
389 #ifdef CONFIG_NO_HZ_COMMON
390 int cpu = smp_processor_id();
392 /* Make sure that timer wheel updates are propagated */
393 if ((idle_cpu(cpu) && !need_resched()) || tick_nohz_full_cpu(cpu)) {
394 if (!in_irq())
395 tick_nohz_irq_exit();
396 }
397 #endif
398 }
400 /*
401 * Exit an interrupt context. Process softirqs if needed and possible:
402 */
403 void irq_exit(void)
404 {
405 #ifndef __ARCH_IRQ_EXIT_IRQS_DISABLED
406 local_irq_disable();
407 #else
408 lockdep_assert_irqs_disabled();
409 #endif
410 account_irq_exit_time(current);
411 preempt_count_sub(HARDIRQ_OFFSET);
412 if (!in_interrupt() && local_softirq_pending())
413 invoke_softirq();
415 tick_irq_exit();
416 rcu_irq_exit();
417 trace_hardirq_exit(); /* must be last! */
418 }
420 /*
421 * This function must run with irqs disabled!
422 */
423 inline void raise_softirq_irqoff(unsigned int nr)
424 {
425 __raise_softirq_irqoff(nr);
427 /*
428 * If we're in an interrupt or softirq, we're done
429 * (this also catches softirq-disabled code). We will
430 * actually run the softirq once we return from
431 * the irq or softirq.
432 *
433 * Otherwise we wake up ksoftirqd to make sure we
434 * schedule the softirq soon.
435 */
436 if (!in_interrupt())
437 wakeup_softirqd();
438 }
440 void raise_softirq(unsigned int nr)
441 {
442 unsigned long flags;
444 local_irq_save(flags);
445 raise_softirq_irqoff(nr);
446 local_irq_restore(flags);
447 }
449 void __raise_softirq_irqoff(unsigned int nr)
450 {
451 trace_softirq_raise(nr);
452 or_softirq_pending(1UL << nr);
453 }
455 void open_softirq(int nr, void (*action)(struct softirq_action *))
456 {
457 softirq_vec[nr].action = action;
458 }
460 /*
461 * Tasklets
462 */
463 struct tasklet_head {
464 struct tasklet_struct *head;
465 struct tasklet_struct **tail;
466 };
468 static DEFINE_PER_CPU(struct tasklet_head, tasklet_vec);
469 static DEFINE_PER_CPU(struct tasklet_head, tasklet_hi_vec);
471 static void __tasklet_schedule_common(struct tasklet_struct *t,
472 struct tasklet_head __percpu *headp,
473 unsigned int softirq_nr)
474 {
475 struct tasklet_head *head;
476 unsigned long flags;
478 local_irq_save(flags);
479 head = this_cpu_ptr(headp);
480 t->next = NULL;
481 *head->tail = t;
482 head->tail = &(t->next);
483 raise_softirq_irqoff(softirq_nr);
484 local_irq_restore(flags);
485 }
487 void __tasklet_schedule(struct tasklet_struct *t)
488 {
489 __tasklet_schedule_common(t, &tasklet_vec,
490 TASKLET_SOFTIRQ);
491 }
492 EXPORT_SYMBOL(__tasklet_schedule);
494 void __tasklet_hi_schedule(struct tasklet_struct *t)
495 {
496 __tasklet_schedule_common(t, &tasklet_hi_vec,
497 HI_SOFTIRQ);
498 }
499 EXPORT_SYMBOL(__tasklet_hi_schedule);
501 static void tasklet_action_common(struct softirq_action *a,
502 struct tasklet_head *tl_head,
503 unsigned int softirq_nr)
504 {
505 struct tasklet_struct *list;
507 local_irq_disable();
508 list = tl_head->head;
509 tl_head->head = NULL;
510 tl_head->tail = &tl_head->head;
511 local_irq_enable();
513 while (list) {
514 struct tasklet_struct *t = list;
516 list = list->next;
518 if (tasklet_trylock(t)) {
519 if (!atomic_read(&t->count)) {
520 if (!test_and_clear_bit(TASKLET_STATE_SCHED,
521 &t->state))
522 BUG();
523 t->func(t->data);
524 tasklet_unlock(t);
525 continue;
526 }
527 tasklet_unlock(t);
528 }
530 local_irq_disable();
531 t->next = NULL;
532 *tl_head->tail = t;
533 tl_head->tail = &t->next;
534 __raise_softirq_irqoff(softirq_nr);
535 local_irq_enable();
536 }
537 }
539 static __latent_entropy void tasklet_action(struct softirq_action *a)
540 {
541 tasklet_action_common(a, this_cpu_ptr(&tasklet_vec), TASKLET_SOFTIRQ);
542 }
544 static __latent_entropy void tasklet_hi_action(struct softirq_action *a)
545 {
546 tasklet_action_common(a, this_cpu_ptr(&tasklet_hi_vec), HI_SOFTIRQ);
547 }
549 void tasklet_init(struct tasklet_struct *t,
550 void (*func)(unsigned long), unsigned long data)
551 {
552 t->next = NULL;
553 t->state = 0;
554 atomic_set(&t->count, 0);
555 t->func = func;
556 t->data = data;
557 }
558 EXPORT_SYMBOL(tasklet_init);
560 void tasklet_kill(struct tasklet_struct *t)
561 {
562 if (in_interrupt())
563 pr_notice("Attempt to kill tasklet from interrupt\n");
565 while (test_and_set_bit(TASKLET_STATE_SCHED, &t->state)) {
566 do {
567 yield();
568 } while (test_bit(TASKLET_STATE_SCHED, &t->state));
569 }
570 tasklet_unlock_wait(t);
571 clear_bit(TASKLET_STATE_SCHED, &t->state);
572 }
573 EXPORT_SYMBOL(tasklet_kill);
575 /*
576 * tasklet_hrtimer
577 */
579 /*
580 * The trampoline is called when the hrtimer expires. It schedules a tasklet
581 * to run __tasklet_hrtimer_trampoline() which in turn will call the intended
582 * hrtimer callback, but from softirq context.
583 */
584 static enum hrtimer_restart __hrtimer_tasklet_trampoline(struct hrtimer *timer)
585 {
586 struct tasklet_hrtimer *ttimer =
587 container_of(timer, struct tasklet_hrtimer, timer);
589 tasklet_hi_schedule(&ttimer->tasklet);
590 return HRTIMER_NORESTART;
591 }
593 /*
594 * Helper function which calls the hrtimer callback from
595 * tasklet/softirq context
596 */
597 static void __tasklet_hrtimer_trampoline(unsigned long data)
598 {
599 struct tasklet_hrtimer *ttimer = (void *)data;
600 enum hrtimer_restart restart;
602 restart = ttimer->function(&ttimer->timer);
603 if (restart != HRTIMER_NORESTART)
604 hrtimer_restart(&ttimer->timer);
605 }
607 /**
608 * tasklet_hrtimer_init - Init a tasklet/hrtimer combo for softirq callbacks
609 * @ttimer: tasklet_hrtimer which is initialized
610 * @function: hrtimer callback function which gets called from softirq context
611 * @which_clock: clock id (CLOCK_MONOTONIC/CLOCK_REALTIME)
612 * @mode: hrtimer mode (HRTIMER_MODE_ABS/HRTIMER_MODE_REL)
613 */
614 void tasklet_hrtimer_init(struct tasklet_hrtimer *ttimer,
615 enum hrtimer_restart (*function)(struct hrtimer *),
616 clockid_t which_clock, enum hrtimer_mode mode)
617 {
618 hrtimer_init(&ttimer->timer, which_clock, mode);
619 ttimer->timer.function = __hrtimer_tasklet_trampoline;
620 tasklet_init(&ttimer->tasklet, __tasklet_hrtimer_trampoline,
621 (unsigned long)ttimer);
622 ttimer->function = function;
623 }
624 EXPORT_SYMBOL_GPL(tasklet_hrtimer_init);
626 void __init softirq_init(void)
627 {
628 int cpu;
630 for_each_possible_cpu(cpu) {
631 per_cpu(tasklet_vec, cpu).tail =
632 &per_cpu(tasklet_vec, cpu).head;
633 per_cpu(tasklet_hi_vec, cpu).tail =
634 &per_cpu(tasklet_hi_vec, cpu).head;
635 }
637 open_softirq(TASKLET_SOFTIRQ, tasklet_action);
638 open_softirq(HI_SOFTIRQ, tasklet_hi_action);
639 }
641 static int ksoftirqd_should_run(unsigned int cpu)
642 {
643 return local_softirq_pending();
644 }
646 static void run_ksoftirqd(unsigned int cpu)
647 {
648 local_irq_disable();
649 if (local_softirq_pending()) {
650 /*
651 * We can safely run softirq on inline stack, as we are not deep
652 * in the task stack here.
653 */
654 __do_softirq();
655 local_irq_enable();
656 cond_resched();
657 return;
658 }
659 local_irq_enable();
660 }
662 #ifdef CONFIG_HOTPLUG_CPU
663 /*
664 * tasklet_kill_immediate is called to remove a tasklet which can already be
665 * scheduled for execution on @cpu.
666 *
667 * Unlike tasklet_kill, this function removes the tasklet
668 * _immediately_, even if the tasklet is in TASKLET_STATE_SCHED state.
669 *
670 * When this function is called, @cpu must be in the CPU_DEAD state.
671 */
672 void tasklet_kill_immediate(struct tasklet_struct *t, unsigned int cpu)
673 {
674 struct tasklet_struct **i;
676 BUG_ON(cpu_online(cpu));
677 BUG_ON(test_bit(TASKLET_STATE_RUN, &t->state));
679 if (!test_bit(TASKLET_STATE_SCHED, &t->state))
680 return;
682 /* CPU is dead, so no lock needed. */
683 for (i = &per_cpu(tasklet_vec, cpu).head; *i; i = &(*i)->next) {
684 if (*i == t) {
685 *i = t->next;
686 /* If this was the tail element, move the tail ptr */
687 if (*i == NULL)
688 per_cpu(tasklet_vec, cpu).tail = i;
689 return;
690 }
691 }
692 BUG();
693 }
695 static int takeover_tasklets(unsigned int cpu)
696 {
697 /* CPU is dead, so no lock needed. */
698 local_irq_disable();
700 /* Find end, append list for that CPU. */
701 if (&per_cpu(tasklet_vec, cpu).head != per_cpu(tasklet_vec, cpu).tail) {
702 *__this_cpu_read(tasklet_vec.tail) = per_cpu(tasklet_vec, cpu).head;
703 this_cpu_write(tasklet_vec.tail, per_cpu(tasklet_vec, cpu).tail);
704 per_cpu(tasklet_vec, cpu).head = NULL;
705 per_cpu(tasklet_vec, cpu).tail = &per_cpu(tasklet_vec, cpu).head;
706 }
707 raise_softirq_irqoff(TASKLET_SOFTIRQ);
709 if (&per_cpu(tasklet_hi_vec, cpu).head != per_cpu(tasklet_hi_vec, cpu).tail) {
710 *__this_cpu_read(tasklet_hi_vec.tail) = per_cpu(tasklet_hi_vec, cpu).head;
711 __this_cpu_write(tasklet_hi_vec.tail, per_cpu(tasklet_hi_vec, cpu).tail);
712 per_cpu(tasklet_hi_vec, cpu).head = NULL;
713 per_cpu(tasklet_hi_vec, cpu).tail = &per_cpu(tasklet_hi_vec, cpu).head;
714 }
715 raise_softirq_irqoff(HI_SOFTIRQ);
717 local_irq_enable();
718 return 0;
719 }
720 #else
721 #define takeover_tasklets NULL
722 #endif /* CONFIG_HOTPLUG_CPU */
724 static struct smp_hotplug_thread softirq_threads = {
725 .store = &ksoftirqd,
726 .thread_should_run = ksoftirqd_should_run,
727 .thread_fn = run_ksoftirqd,
728 .thread_comm = "ksoftirqd/%u",
729 };
731 static __init int spawn_ksoftirqd(void)
732 {
733 cpuhp_setup_state_nocalls(CPUHP_SOFTIRQ_DEAD, "softirq:dead", NULL,
734 takeover_tasklets);
735 BUG_ON(smpboot_register_percpu_thread(&softirq_threads));
737 return 0;
738 }
739 early_initcall(spawn_ksoftirqd);
741 /*
742 * [ These __weak aliases are kept in a separate compilation unit, so that
743 * GCC does not inline them incorrectly. ]
744 */
746 int __init __weak early_irq_init(void)
747 {
748 return 0;
749 }
751 int __init __weak arch_probe_nr_irqs(void)
752 {
753 return NR_IRQS_LEGACY;
754 }
756 int __init __weak arch_early_irq_init(void)
757 {
758 return 0;
759 }
761 unsigned int __weak arch_dynirq_lower_bound(unsigned int from)
762 {
763 return from;
764 }