summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 9825bd9)
raw | patch | inline | side by side (parent: 9825bd9)
author | Lu Baolu <baolu.lu@linux.intel.com> | |
Thu, 24 Jan 2019 02:31:32 +0000 (10:31 +0800) | ||
committer | Joerg Roedel <jroedel@suse.de> | |
Wed, 30 Jan 2019 16:23:58 +0000 (17:23 +0100) |
Commit 765b6a98c1de3 ("iommu/vt-d: Enumerate the scalable
mode capability") enables VT-d scalable mode if hardware
advertises the capability. As we will bring up different
features and use cases to upstream in different patch
series, it will leave some intermediate kernel versions
which support partial features. Hence, end user might run
into problems when they use such kernels on bare metals
or virtualization environments.
This leaves scalable mode default off and end users could
turn it on with "intel-iommu=sm_on" only when they have
clear ideas about which scalable features are supported
in the kernel.
Cc: Liu Yi L <yi.l.liu@intel.com>
Cc: Jacob Pan <jacob.jun.pan@linux.intel.com>
Suggested-by: Ashok Raj <ashok.raj@intel.com>
Suggested-by: Kevin Tian <kevin.tian@intel.com>
Signed-off-by: Lu Baolu <baolu.lu@linux.intel.com>
Signed-off-by: Joerg Roedel <jroedel@suse.de>
mode capability") enables VT-d scalable mode if hardware
advertises the capability. As we will bring up different
features and use cases to upstream in different patch
series, it will leave some intermediate kernel versions
which support partial features. Hence, end user might run
into problems when they use such kernels on bare metals
or virtualization environments.
This leaves scalable mode default off and end users could
turn it on with "intel-iommu=sm_on" only when they have
clear ideas about which scalable features are supported
in the kernel.
Cc: Liu Yi L <yi.l.liu@intel.com>
Cc: Jacob Pan <jacob.jun.pan@linux.intel.com>
Suggested-by: Ashok Raj <ashok.raj@intel.com>
Suggested-by: Kevin Tian <kevin.tian@intel.com>
Signed-off-by: Lu Baolu <baolu.lu@linux.intel.com>
Signed-off-by: Joerg Roedel <jroedel@suse.de>
Documentation/admin-guide/kernel-parameters.txt | patch | blob | history | |
drivers/iommu/intel-iommu.c | patch | blob | history |
diff --git a/Documentation/admin-guide/kernel-parameters.txt b/Documentation/admin-guide/kernel-parameters.txt
index b799bcf67d7b5ae080694467442b113b49c92567..858b6c0b9a15ae71853645013c718dc0398804d4 100644 (file)
By default, super page will be supported if Intel IOMMU
has the capability. With this option, super page will
not be supported.
- sm_off [Default Off]
- By default, scalable mode will be supported if the
+ sm_on [Default Off]
+ By default, scalable mode will be disabled even if the
hardware advertises that it has support for the scalable
mode translation. With this option set, scalable mode
- will not be used even on hardware which claims to support
- it.
+ will be used on hardware which claims to support it.
tboot_noforce [Default Off]
Do not force the Intel IOMMU enabled under tboot.
By default, tboot will force Intel IOMMU on, which
index 1457f931218e0bede0c3c34660aaf870afaaa5a7..78188bf7e90d7a42f6dbc263f2e412c77de92e0c 100644 (file)
static int dmar_forcedac;
static int intel_iommu_strict;
static int intel_iommu_superpage = 1;
-static int intel_iommu_sm = 1;
+static int intel_iommu_sm;
static int iommu_identity_mapping;
#define IDENTMAP_ALL 1
} else if (!strncmp(str, "sp_off", 6)) {
pr_info("Disable supported super page\n");
intel_iommu_superpage = 0;
- } else if (!strncmp(str, "sm_off", 6)) {
- pr_info("Intel-IOMMU: disable scalable mode support\n");
- intel_iommu_sm = 0;
+ } else if (!strncmp(str, "sm_on", 5)) {
+ pr_info("Intel-IOMMU: scalable mode supported\n");
+ intel_iommu_sm = 1;
} else if (!strncmp(str, "tboot_noforce", 13)) {
printk(KERN_INFO
"Intel-IOMMU: not forcing on after tboot. This could expose security risk for tboot\n");