summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: e6d4293)
raw | patch | inline | side by side (parent: e6d4293)
author | Tony Luck <tony.luck@intel.com> | |
Fri, 1 Feb 2019 00:33:41 +0000 (16:33 -0800) | ||
committer | Borislav Petkov <bp@suse.de> | |
Sun, 3 Feb 2019 12:24:24 +0000 (13:24 +0100) |
Internal injection testing crashed with a console log that said:
mce: [Hardware Error]: CPU 7: Machine Check Exception: f Bank 0: bd80000000100134
This caused a lot of head scratching because the MCACOD (bits 15:0) of
that status is a signature from an L1 data cache error. But Linux says
that it found it in "Bank 0", which on this model CPU only reports L1
instruction cache errors.
The answer was that Linux doesn't initialize "m->bank" in the case that
it finds a fatal error in the mce_no_way_out() pre-scan of banks. If
this was a local machine check, then this partially initialized struct
mce is being passed to mce_panic().
Fix is simple: just initialize m->bank in the case of a fatal error.
Fixes: 40c36e2741d7 ("x86/mce: Fix incorrect "Machine check from unknown source" message")
Signed-off-by: Tony Luck <tony.luck@intel.com>
Signed-off-by: Borislav Petkov <bp@suse.de>
Cc: "H. Peter Anvin" <hpa@zytor.com>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Vishal Verma <vishal.l.verma@intel.com>
Cc: x86-ml <x86@kernel.org>
Cc: stable@vger.kernel.org # v4.18 Note pre-v5.0 arch/x86/kernel/cpu/mce/core.c was called arch/x86/kernel/cpu/mcheck/mce.c
Link: https://lkml.kernel.org/r/20190201003341.10638-1-tony.luck@intel.com
mce: [Hardware Error]: CPU 7: Machine Check Exception: f Bank 0: bd80000000100134
This caused a lot of head scratching because the MCACOD (bits 15:0) of
that status is a signature from an L1 data cache error. But Linux says
that it found it in "Bank 0", which on this model CPU only reports L1
instruction cache errors.
The answer was that Linux doesn't initialize "m->bank" in the case that
it finds a fatal error in the mce_no_way_out() pre-scan of banks. If
this was a local machine check, then this partially initialized struct
mce is being passed to mce_panic().
Fix is simple: just initialize m->bank in the case of a fatal error.
Fixes: 40c36e2741d7 ("x86/mce: Fix incorrect "Machine check from unknown source" message")
Signed-off-by: Tony Luck <tony.luck@intel.com>
Signed-off-by: Borislav Petkov <bp@suse.de>
Cc: "H. Peter Anvin" <hpa@zytor.com>
Cc: Ingo Molnar <mingo@redhat.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Vishal Verma <vishal.l.verma@intel.com>
Cc: x86-ml <x86@kernel.org>
Cc: stable@vger.kernel.org # v4.18 Note pre-v5.0 arch/x86/kernel/cpu/mce/core.c was called arch/x86/kernel/cpu/mcheck/mce.c
Link: https://lkml.kernel.org/r/20190201003341.10638-1-tony.luck@intel.com
arch/x86/kernel/cpu/mce/core.c | patch | blob | history |
index 672c7225cb1b89426b682f40b4a4b33a73803d89..6ce290c506d93e83318f3b13b95d8f5861e02983 100644 (file)
quirk_no_way_out(i, m, regs);
if (mce_severity(m, mca_cfg.tolerant, &tmp, true) >= MCE_PANIC_SEVERITY) {
+ m->bank = i;
mce_read_aux(m, i);
*msg = tmp;
return 1;