]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-linux-kernel/ti-linux-kernel-next.git/blob - Makefile
Merged TI feature rpmsg_next into ti-linux-5.4.y-next
[ti-linux-kernel/ti-linux-kernel-next.git] / Makefile
1 # SPDX-License-Identifier: GPL-2.0
2 VERSION = 5
3 PATCHLEVEL = 4
4 SUBLEVEL = 0
5 EXTRAVERSION = -rc2
6 NAME = Nesting Opossum
8 # *DOCUMENTATION*
9 # To see a list of typical targets execute "make help"
10 # More info can be located in ./README
11 # Comments in this file are targeted only to the developer, do not
12 # expect to learn how to build the kernel reading this file.
14 # That's our default target when none is given on the command line
15 PHONY := _all
16 _all:
18 # We are using a recursive build, so we need to do a little thinking
19 # to get the ordering right.
20 #
21 # Most importantly: sub-Makefiles should only ever modify files in
22 # their own directory. If in some directory we have a dependency on
23 # a file in another dir (which doesn't happen often, but it's often
24 # unavoidable when linking the built-in.a targets which finally
25 # turn into vmlinux), we will call a sub make in that other dir, and
26 # after that we are sure that everything which is in that other dir
27 # is now up to date.
28 #
29 # The only cases where we need to modify files which have global
30 # effects are thus separated out and done before the recursive
31 # descending is started. They are now explicitly listed as the
32 # prepare rule.
34 ifneq ($(sub_make_done),1)
36 # Do not use make's built-in rules and variables
37 # (this increases performance and avoids hard-to-debug behaviour)
38 MAKEFLAGS += -rR
40 # Avoid funny character set dependencies
41 unexport LC_ALL
42 LC_COLLATE=C
43 LC_NUMERIC=C
44 export LC_COLLATE LC_NUMERIC
46 # Avoid interference with shell env settings
47 unexport GREP_OPTIONS
49 # Beautify output
50 # ---------------------------------------------------------------------------
51 #
52 # Normally, we echo the whole command before executing it. By making
53 # that echo $($(quiet)$(cmd)), we now have the possibility to set
54 # $(quiet) to choose other forms of output instead, e.g.
55 #
56 #         quiet_cmd_cc_o_c = Compiling $(RELDIR)/$@
57 #         cmd_cc_o_c       = $(CC) $(c_flags) -c -o $@ $<
58 #
59 # If $(quiet) is empty, the whole command will be printed.
60 # If it is set to "quiet_", only the short version will be printed.
61 # If it is set to "silent_", nothing will be printed at all, since
62 # the variable $(silent_cmd_cc_o_c) doesn't exist.
63 #
64 # A simple variant is to prefix commands with $(Q) - that's useful
65 # for commands that shall be hidden in non-verbose mode.
66 #
67 #       $(Q)ln $@ :<
68 #
69 # If KBUILD_VERBOSE equals 0 then the above command will be hidden.
70 # If KBUILD_VERBOSE equals 1 then the above command is displayed.
71 #
72 # To put more focus on warnings, be less verbose as default
73 # Use 'make V=1' to see the full commands
75 ifeq ("$(origin V)", "command line")
76   KBUILD_VERBOSE = $(V)
77 endif
78 ifndef KBUILD_VERBOSE
79   KBUILD_VERBOSE = 0
80 endif
82 ifeq ($(KBUILD_VERBOSE),1)
83   quiet =
84   Q =
85 else
86   quiet=quiet_
87   Q = @
88 endif
90 # If the user is running make -s (silent mode), suppress echoing of
91 # commands
93 ifneq ($(findstring s,$(filter-out --%,$(MAKEFLAGS))),)
94   quiet=silent_
95 endif
97 export quiet Q KBUILD_VERBOSE
99 # Kbuild will save output files in the current working directory.
100 # This does not need to match to the root of the kernel source tree.
102 # For example, you can do this:
104 #  cd /dir/to/store/output/files; make -f /dir/to/kernel/source/Makefile
106 # If you want to save output files in a different location, there are
107 # two syntaxes to specify it.
109 # 1) O=
110 # Use "make O=dir/to/store/output/files/"
112 # 2) Set KBUILD_OUTPUT
113 # Set the environment variable KBUILD_OUTPUT to point to the output directory.
114 # export KBUILD_OUTPUT=dir/to/store/output/files/; make
116 # The O= assignment takes precedence over the KBUILD_OUTPUT environment
117 # variable.
119 # Do we want to change the working directory?
120 ifeq ("$(origin O)", "command line")
121   KBUILD_OUTPUT := $(O)
122 endif
124 ifneq ($(KBUILD_OUTPUT),)
125 # Make's built-in functions such as $(abspath ...), $(realpath ...) cannot
126 # expand a shell special character '~'. We use a somewhat tedious way here.
127 abs_objtree := $(shell mkdir -p $(KBUILD_OUTPUT) && cd $(KBUILD_OUTPUT) && pwd)
128 $(if $(abs_objtree),, \
129      $(error failed to create output directory "$(KBUILD_OUTPUT)"))
131 # $(realpath ...) resolves symlinks
132 abs_objtree := $(realpath $(abs_objtree))
133 else
134 abs_objtree := $(CURDIR)
135 endif # ifneq ($(KBUILD_OUTPUT),)
137 ifeq ($(abs_objtree),$(CURDIR))
138 # Suppress "Entering directory ..." unless we are changing the work directory.
139 MAKEFLAGS += --no-print-directory
140 else
141 need-sub-make := 1
142 endif
144 abs_srctree := $(realpath $(dir $(lastword $(MAKEFILE_LIST))))
146 ifneq ($(words $(subst :, ,$(abs_srctree))), 1)
147 $(error source directory cannot contain spaces or colons)
148 endif
150 ifneq ($(abs_srctree),$(abs_objtree))
151 # Look for make include files relative to root of kernel src
153 # This does not become effective immediately because MAKEFLAGS is re-parsed
154 # once after the Makefile is read. We need to invoke sub-make.
155 MAKEFLAGS += --include-dir=$(abs_srctree)
156 need-sub-make := 1
157 endif
159 ifneq ($(filter 3.%,$(MAKE_VERSION)),)
160 # 'MAKEFLAGS += -rR' does not immediately become effective for GNU Make 3.x
161 # We need to invoke sub-make to avoid implicit rules in the top Makefile.
162 need-sub-make := 1
163 # Cancel implicit rules for this Makefile.
164 $(lastword $(MAKEFILE_LIST)): ;
165 endif
167 export abs_srctree abs_objtree
168 export sub_make_done := 1
170 ifeq ($(need-sub-make),1)
172 PHONY += $(MAKECMDGOALS) sub-make
174 $(filter-out _all sub-make $(lastword $(MAKEFILE_LIST)), $(MAKECMDGOALS)) _all: sub-make
175         @:
177 # Invoke a second make in the output directory, passing relevant variables
178 sub-make:
179         $(Q)$(MAKE) -C $(abs_objtree) -f $(abs_srctree)/Makefile $(MAKECMDGOALS)
181 endif # need-sub-make
182 endif # sub_make_done
184 # We process the rest of the Makefile if this is the final invocation of make
185 ifeq ($(need-sub-make),)
187 # Do not print "Entering directory ...",
188 # but we want to display it when entering to the output directory
189 # so that IDEs/editors are able to understand relative filenames.
190 MAKEFLAGS += --no-print-directory
192 # Call a source code checker (by default, "sparse") as part of the
193 # C compilation.
195 # Use 'make C=1' to enable checking of only re-compiled files.
196 # Use 'make C=2' to enable checking of *all* source files, regardless
197 # of whether they are re-compiled or not.
199 # See the file "Documentation/dev-tools/sparse.rst" for more details,
200 # including where to get the "sparse" utility.
202 ifeq ("$(origin C)", "command line")
203   KBUILD_CHECKSRC = $(C)
204 endif
205 ifndef KBUILD_CHECKSRC
206   KBUILD_CHECKSRC = 0
207 endif
209 # Use make M=dir or set the environment variable KBUILD_EXTMOD to specify the
210 # directory of external module to build. Setting M= takes precedence.
211 ifeq ("$(origin M)", "command line")
212   KBUILD_EXTMOD := $(M)
213 endif
215 export KBUILD_CHECKSRC KBUILD_EXTMOD
217 extmod-prefix = $(if $(KBUILD_EXTMOD),$(KBUILD_EXTMOD)/)
219 ifeq ($(abs_srctree),$(abs_objtree))
220         # building in the source tree
221         srctree := .
222         building_out_of_srctree :=
223 else
224         ifeq ($(abs_srctree)/,$(dir $(abs_objtree)))
225                 # building in a subdirectory of the source tree
226                 srctree := ..
227         else
228                 srctree := $(abs_srctree)
229         endif
230         building_out_of_srctree := 1
231 endif
233 ifneq ($(KBUILD_ABS_SRCTREE),)
234 srctree := $(abs_srctree)
235 endif
237 objtree         := .
238 VPATH           := $(srctree)
240 export building_out_of_srctree srctree objtree VPATH
242 # To make sure we do not include .config for any of the *config targets
243 # catch them early, and hand them over to scripts/kconfig/Makefile
244 # It is allowed to specify more targets when calling make, including
245 # mixing *config targets and build targets.
246 # For example 'make oldconfig all'.
247 # Detect when mixed targets is specified, and make a second invocation
248 # of make so .config is not included in this case either (for *config).
250 version_h := include/generated/uapi/linux/version.h
251 old_version_h := include/linux/version.h
253 clean-targets := %clean mrproper cleandocs
254 no-dot-config-targets := $(clean-targets) \
255                          cscope gtags TAGS tags help% %docs check% coccicheck \
256                          $(version_h) headers headers_% archheaders archscripts \
257                          %asm-generic kernelversion %src-pkg
258 no-sync-config-targets := $(no-dot-config-targets) install %install \
259                            kernelrelease
260 single-targets := %.a %.i %.ko %.lds %.ll %.lst %.mod %.o %.s %.symtypes %/
262 config-build    :=
263 mixed-build     :=
264 need-config     := 1
265 may-sync-config := 1
266 single-build    :=
268 ifneq ($(filter $(no-dot-config-targets), $(MAKECMDGOALS)),)
269         ifeq ($(filter-out $(no-dot-config-targets), $(MAKECMDGOALS)),)
270                 need-config :=
271         endif
272 endif
274 ifneq ($(filter $(no-sync-config-targets), $(MAKECMDGOALS)),)
275         ifeq ($(filter-out $(no-sync-config-targets), $(MAKECMDGOALS)),)
276                 may-sync-config :=
277         endif
278 endif
280 ifneq ($(KBUILD_EXTMOD),)
281         may-sync-config :=
282 endif
284 ifeq ($(KBUILD_EXTMOD),)
285         ifneq ($(filter config %config,$(MAKECMDGOALS)),)
286                 config-build := 1
287                 ifneq ($(words $(MAKECMDGOALS)),1)
288                         mixed-build := 1
289                 endif
290         endif
291 endif
293 # We cannot build single targets and the others at the same time
294 ifneq ($(filter $(single-targets), $(MAKECMDGOALS)),)
295         single-build := 1
296         ifneq ($(filter-out $(single-targets), $(MAKECMDGOALS)),)
297                 mixed-build := 1
298         endif
299 endif
301 # For "make -j clean all", "make -j mrproper defconfig all", etc.
302 ifneq ($(filter $(clean-targets),$(MAKECMDGOALS)),)
303         ifneq ($(filter-out $(clean-targets),$(MAKECMDGOALS)),)
304                 mixed-build := 1
305         endif
306 endif
308 # install and modules_install need also be processed one by one
309 ifneq ($(filter install,$(MAKECMDGOALS)),)
310         ifneq ($(filter modules_install,$(MAKECMDGOALS)),)
311                 mixed-build := 1
312         endif
313 endif
315 ifdef mixed-build
316 # ===========================================================================
317 # We're called with mixed targets (*config and build targets).
318 # Handle them one by one.
320 PHONY += $(MAKECMDGOALS) __build_one_by_one
322 $(filter-out __build_one_by_one, $(MAKECMDGOALS)): __build_one_by_one
323         @:
325 __build_one_by_one:
326         $(Q)set -e; \
327         for i in $(MAKECMDGOALS); do \
328                 $(MAKE) -f $(srctree)/Makefile $$i; \
329         done
331 else # !mixed-build
333 include scripts/Kbuild.include
335 # Read KERNELRELEASE from include/config/kernel.release (if it exists)
336 KERNELRELEASE = $(shell cat include/config/kernel.release 2> /dev/null)
337 KERNELVERSION = $(VERSION)$(if $(PATCHLEVEL),.$(PATCHLEVEL)$(if $(SUBLEVEL),.$(SUBLEVEL)))$(EXTRAVERSION)
338 export VERSION PATCHLEVEL SUBLEVEL KERNELRELEASE KERNELVERSION
340 include scripts/subarch.include
342 # Cross compiling and selecting different set of gcc/bin-utils
343 # ---------------------------------------------------------------------------
345 # When performing cross compilation for other architectures ARCH shall be set
346 # to the target architecture. (See arch/* for the possibilities).
347 # ARCH can be set during invocation of make:
348 # make ARCH=ia64
349 # Another way is to have ARCH set in the environment.
350 # The default ARCH is the host where make is executed.
352 # CROSS_COMPILE specify the prefix used for all executables used
353 # during compilation. Only gcc and related bin-utils executables
354 # are prefixed with $(CROSS_COMPILE).
355 # CROSS_COMPILE can be set on the command line
356 # make CROSS_COMPILE=ia64-linux-
357 # Alternatively CROSS_COMPILE can be set in the environment.
358 # Default value for CROSS_COMPILE is not to prefix executables
359 # Note: Some architectures assign CROSS_COMPILE in their arch/*/Makefile
360 ARCH            ?= $(SUBARCH)
362 # Architecture as present in compile.h
363 UTS_MACHINE     := $(ARCH)
364 SRCARCH         := $(ARCH)
366 # Additional ARCH settings for x86
367 ifeq ($(ARCH),i386)
368         SRCARCH := x86
369 endif
370 ifeq ($(ARCH),x86_64)
371         SRCARCH := x86
372 endif
374 # Additional ARCH settings for sparc
375 ifeq ($(ARCH),sparc32)
376        SRCARCH := sparc
377 endif
378 ifeq ($(ARCH),sparc64)
379        SRCARCH := sparc
380 endif
382 # Additional ARCH settings for sh
383 ifeq ($(ARCH),sh64)
384        SRCARCH := sh
385 endif
387 KCONFIG_CONFIG  ?= .config
388 export KCONFIG_CONFIG
390 # SHELL used by kbuild
391 CONFIG_SHELL := sh
393 HOST_LFS_CFLAGS := $(shell getconf LFS_CFLAGS 2>/dev/null)
394 HOST_LFS_LDFLAGS := $(shell getconf LFS_LDFLAGS 2>/dev/null)
395 HOST_LFS_LIBS := $(shell getconf LFS_LIBS 2>/dev/null)
397 HOSTCC       = gcc
398 HOSTCXX      = g++
399 KBUILD_HOSTCFLAGS   := -Wall -Wmissing-prototypes -Wstrict-prototypes -O2 \
400                 -fomit-frame-pointer -std=gnu89 $(HOST_LFS_CFLAGS) \
401                 $(HOSTCFLAGS)
402 KBUILD_HOSTCXXFLAGS := -O2 $(HOST_LFS_CFLAGS) $(HOSTCXXFLAGS)
403 KBUILD_HOSTLDFLAGS  := $(HOST_LFS_LDFLAGS) $(HOSTLDFLAGS)
404 KBUILD_HOSTLDLIBS   := $(HOST_LFS_LIBS) $(HOSTLDLIBS)
406 # Make variables (CC, etc...)
407 AS              = $(CROSS_COMPILE)as
408 LD              = $(CROSS_COMPILE)ld
409 CC              = $(CROSS_COMPILE)gcc
410 CPP             = $(CC) -E
411 AR              = $(CROSS_COMPILE)ar
412 NM              = $(CROSS_COMPILE)nm
413 STRIP           = $(CROSS_COMPILE)strip
414 OBJCOPY         = $(CROSS_COMPILE)objcopy
415 OBJDUMP         = $(CROSS_COMPILE)objdump
416 OBJSIZE         = $(CROSS_COMPILE)size
417 PAHOLE          = pahole
418 LEX             = flex
419 YACC            = bison
420 AWK             = awk
421 INSTALLKERNEL  := installkernel
422 DEPMOD          = /sbin/depmod
423 PERL            = perl
424 PYTHON          = python
425 PYTHON2         = python2
426 PYTHON3         = python3
427 CHECK           = sparse
428 BASH            = bash
430 CHECKFLAGS     := -D__linux__ -Dlinux -D__STDC__ -Dunix -D__unix__ \
431                   -Wbitwise -Wno-return-void -Wno-unknown-attribute $(CF)
432 NOSTDINC_FLAGS :=
433 CFLAGS_MODULE   =
434 AFLAGS_MODULE   =
435 LDFLAGS_MODULE  =
436 CFLAGS_KERNEL   =
437 AFLAGS_KERNEL   =
438 LDFLAGS_vmlinux =
440 # Use USERINCLUDE when you must reference the UAPI directories only.
441 USERINCLUDE    := \
442                 -I$(srctree)/arch/$(SRCARCH)/include/uapi \
443                 -I$(objtree)/arch/$(SRCARCH)/include/generated/uapi \
444                 -I$(srctree)/include/uapi \
445                 -I$(objtree)/include/generated/uapi \
446                 -include $(srctree)/include/linux/kconfig.h
448 # Use LINUXINCLUDE when you must reference the include/ directory.
449 # Needed to be compatible with the O= option
450 LINUXINCLUDE    := \
451                 -I$(srctree)/arch/$(SRCARCH)/include \
452                 -I$(objtree)/arch/$(SRCARCH)/include/generated \
453                 $(if $(building_out_of_srctree),-I$(srctree)/include) \
454                 -I$(objtree)/include \
455                 $(USERINCLUDE)
457 KBUILD_AFLAGS   := -D__ASSEMBLY__ -fno-PIE
458 KBUILD_CFLAGS   := -Wall -Wundef -Werror=strict-prototypes -Wno-trigraphs \
459                    -fno-strict-aliasing -fno-common -fshort-wchar -fno-PIE \
460                    -Werror=implicit-function-declaration -Werror=implicit-int \
461                    -Wno-format-security \
462                    -std=gnu89
463 KBUILD_CPPFLAGS := -D__KERNEL__
464 KBUILD_AFLAGS_KERNEL :=
465 KBUILD_CFLAGS_KERNEL :=
466 KBUILD_AFLAGS_MODULE  := -DMODULE
467 KBUILD_CFLAGS_MODULE  := -DMODULE
468 KBUILD_LDFLAGS_MODULE :=
469 export KBUILD_LDS_MODULE := $(srctree)/scripts/module-common.lds
470 KBUILD_LDFLAGS :=
471 GCC_PLUGINS_CFLAGS :=
472 CLANG_FLAGS :=
474 export ARCH SRCARCH CONFIG_SHELL BASH HOSTCC KBUILD_HOSTCFLAGS CROSS_COMPILE AS LD CC
475 export CPP AR NM STRIP OBJCOPY OBJDUMP OBJSIZE PAHOLE LEX YACC AWK INSTALLKERNEL
476 export PERL PYTHON PYTHON2 PYTHON3 CHECK CHECKFLAGS MAKE UTS_MACHINE HOSTCXX
477 export KBUILD_HOSTCXXFLAGS KBUILD_HOSTLDFLAGS KBUILD_HOSTLDLIBS LDFLAGS_MODULE
479 export KBUILD_CPPFLAGS NOSTDINC_FLAGS LINUXINCLUDE OBJCOPYFLAGS KBUILD_LDFLAGS
480 export KBUILD_CFLAGS CFLAGS_KERNEL CFLAGS_MODULE
481 export CFLAGS_KASAN CFLAGS_KASAN_NOSANITIZE CFLAGS_UBSAN
482 export KBUILD_AFLAGS AFLAGS_KERNEL AFLAGS_MODULE
483 export KBUILD_AFLAGS_MODULE KBUILD_CFLAGS_MODULE KBUILD_LDFLAGS_MODULE
484 export KBUILD_AFLAGS_KERNEL KBUILD_CFLAGS_KERNEL
486 # Files to ignore in find ... statements
488 export RCS_FIND_IGNORE := \( -name SCCS -o -name BitKeeper -o -name .svn -o    \
489                           -name CVS -o -name .pc -o -name .hg -o -name .git \) \
490                           -prune -o
491 export RCS_TAR_IGNORE := --exclude SCCS --exclude BitKeeper --exclude .svn \
492                          --exclude CVS --exclude .pc --exclude .hg --exclude .git
494 # ===========================================================================
495 # Rules shared between *config targets and build targets
497 # Basic helpers built in scripts/basic/
498 PHONY += scripts_basic
499 scripts_basic:
500         $(Q)$(MAKE) $(build)=scripts/basic
501         $(Q)rm -f .tmp_quiet_recordmcount
503 PHONY += outputmakefile
504 # Before starting out-of-tree build, make sure the source tree is clean.
505 # outputmakefile generates a Makefile in the output directory, if using a
506 # separate output directory. This allows convenient use of make in the
507 # output directory.
508 # At the same time when output Makefile generated, generate .gitignore to
509 # ignore whole output directory
510 outputmakefile:
511 ifdef building_out_of_srctree
512         $(Q)if [ -f $(srctree)/.config -o \
513                  -d $(srctree)/include/config -o \
514                  -d $(srctree)/arch/$(SRCARCH)/include/generated ]; then \
515                 echo >&2 "***"; \
516                 echo >&2 "*** The source tree is not clean, please run 'make$(if $(findstring command line, $(origin ARCH)), ARCH=$(ARCH)) mrproper'"; \
517                 echo >&2 "*** in $(abs_srctree)";\
518                 echo >&2 "***"; \
519                 false; \
520         fi
521         $(Q)ln -fsn $(srctree) source
522         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/mkmakefile $(srctree)
523         $(Q)test -e .gitignore || \
524         { echo "# this is build directory, ignore it"; echo "*"; } > .gitignore
525 endif
527 ifneq ($(shell $(CC) --version 2>&1 | head -n 1 | grep clang),)
528 ifneq ($(CROSS_COMPILE),)
529 CLANG_FLAGS     += --target=$(notdir $(CROSS_COMPILE:%-=%))
530 GCC_TOOLCHAIN_DIR := $(dir $(shell which $(CROSS_COMPILE)elfedit))
531 CLANG_FLAGS     += --prefix=$(GCC_TOOLCHAIN_DIR)
532 GCC_TOOLCHAIN   := $(realpath $(GCC_TOOLCHAIN_DIR)/..)
533 endif
534 ifneq ($(GCC_TOOLCHAIN),)
535 CLANG_FLAGS     += --gcc-toolchain=$(GCC_TOOLCHAIN)
536 endif
537 ifeq ($(shell $(AS) --version 2>&1 | head -n 1 | grep clang),)
538 CLANG_FLAGS     += -no-integrated-as
539 endif
540 CLANG_FLAGS     += -Werror=unknown-warning-option
541 KBUILD_CFLAGS   += $(CLANG_FLAGS)
542 KBUILD_AFLAGS   += $(CLANG_FLAGS)
543 export CLANG_FLAGS
544 endif
546 # The expansion should be delayed until arch/$(SRCARCH)/Makefile is included.
547 # Some architectures define CROSS_COMPILE in arch/$(SRCARCH)/Makefile.
548 # CC_VERSION_TEXT is referenced from Kconfig (so it needs export),
549 # and from include/config/auto.conf.cmd to detect the compiler upgrade.
550 CC_VERSION_TEXT = $(shell $(CC) --version 2>/dev/null | head -n 1)
552 ifdef config-build
553 # ===========================================================================
554 # *config targets only - make sure prerequisites are updated, and descend
555 # in scripts/kconfig to make the *config target
557 # Read arch specific Makefile to set KBUILD_DEFCONFIG as needed.
558 # KBUILD_DEFCONFIG may point out an alternative default configuration
559 # used for 'make defconfig'
560 include arch/$(SRCARCH)/Makefile
561 export KBUILD_DEFCONFIG KBUILD_KCONFIG CC_VERSION_TEXT
563 config: outputmakefile scripts_basic FORCE
564         $(Q)$(MAKE) $(build)=scripts/kconfig $@
566 %config: outputmakefile scripts_basic FORCE
567         $(Q)$(MAKE) $(build)=scripts/kconfig $@
569 else #!config-build
570 # ===========================================================================
571 # Build targets only - this includes vmlinux, arch specific targets, clean
572 # targets and others. In general all targets except *config targets.
574 # If building an external module we do not care about the all: rule
575 # but instead _all depend on modules
576 PHONY += all
577 ifeq ($(KBUILD_EXTMOD),)
578 _all: all
579 else
580 _all: modules
581 endif
583 # Decide whether to build built-in, modular, or both.
584 # Normally, just do built-in.
586 KBUILD_MODULES :=
587 KBUILD_BUILTIN := 1
589 # If we have only "make modules", don't compile built-in objects.
590 # When we're building modules with modversions, we need to consider
591 # the built-in objects during the descend as well, in order to
592 # make sure the checksums are up to date before we record them.
594 ifeq ($(MAKECMDGOALS),modules)
595   KBUILD_BUILTIN := $(if $(CONFIG_MODVERSIONS),1)
596 endif
598 # If we have "make <whatever> modules", compile modules
599 # in addition to whatever we do anyway.
600 # Just "make" or "make all" shall build modules as well
602 ifneq ($(filter all _all modules,$(MAKECMDGOALS)),)
603   KBUILD_MODULES := 1
604 endif
606 ifeq ($(MAKECMDGOALS),)
607   KBUILD_MODULES := 1
608 endif
610 export KBUILD_MODULES KBUILD_BUILTIN
612 ifdef need-config
613 include include/config/auto.conf
614 endif
616 ifeq ($(KBUILD_EXTMOD),)
617 # Objects we will link into vmlinux / subdirs we need to visit
618 init-y          := init/
619 drivers-y       := drivers/ sound/
620 drivers-$(CONFIG_SAMPLES) += samples/
621 drivers-$(CONFIG_KERNEL_HEADER_TEST) += include/
622 net-y           := net/
623 libs-y          := lib/
624 core-y          := usr/
625 virt-y          := virt/
626 endif # KBUILD_EXTMOD
628 # The all: target is the default when no target is given on the
629 # command line.
630 # This allow a user to issue only 'make' to build a kernel including modules
631 # Defaults to vmlinux, but the arch makefile usually adds further targets
632 all: vmlinux
634 CFLAGS_GCOV     := -fprofile-arcs -ftest-coverage \
635         $(call cc-option,-fno-tree-loop-im) \
636         $(call cc-disable-warning,maybe-uninitialized,)
637 export CFLAGS_GCOV
639 # The arch Makefiles can override CC_FLAGS_FTRACE. We may also append it later.
640 ifdef CONFIG_FUNCTION_TRACER
641   CC_FLAGS_FTRACE := -pg
642 endif
644 RETPOLINE_CFLAGS_GCC := -mindirect-branch=thunk-extern -mindirect-branch-register
645 RETPOLINE_VDSO_CFLAGS_GCC := -mindirect-branch=thunk-inline -mindirect-branch-register
646 RETPOLINE_CFLAGS_CLANG := -mretpoline-external-thunk
647 RETPOLINE_VDSO_CFLAGS_CLANG := -mretpoline
648 RETPOLINE_CFLAGS := $(call cc-option,$(RETPOLINE_CFLAGS_GCC),$(call cc-option,$(RETPOLINE_CFLAGS_CLANG)))
649 RETPOLINE_VDSO_CFLAGS := $(call cc-option,$(RETPOLINE_VDSO_CFLAGS_GCC),$(call cc-option,$(RETPOLINE_VDSO_CFLAGS_CLANG)))
650 export RETPOLINE_CFLAGS
651 export RETPOLINE_VDSO_CFLAGS
653 include arch/$(SRCARCH)/Makefile
655 ifdef need-config
656 ifdef may-sync-config
657 # Read in dependencies to all Kconfig* files, make sure to run syncconfig if
658 # changes are detected. This should be included after arch/$(SRCARCH)/Makefile
659 # because some architectures define CROSS_COMPILE there.
660 include include/config/auto.conf.cmd
662 $(KCONFIG_CONFIG):
663         @echo >&2 '***'
664         @echo >&2 '*** Configuration file "$@" not found!'
665         @echo >&2 '***'
666         @echo >&2 '*** Please run some configurator (e.g. "make oldconfig" or'
667         @echo >&2 '*** "make menuconfig" or "make xconfig").'
668         @echo >&2 '***'
669         @/bin/false
671 # The actual configuration files used during the build are stored in
672 # include/generated/ and include/config/. Update them if .config is newer than
673 # include/config/auto.conf (which mirrors .config).
675 # This exploits the 'multi-target pattern rule' trick.
676 # The syncconfig should be executed only once to make all the targets.
677 %/auto.conf %/auto.conf.cmd %/tristate.conf: $(KCONFIG_CONFIG)
678         $(Q)$(MAKE) -f $(srctree)/Makefile syncconfig
679 else # !may-sync-config
680 # External modules and some install targets need include/generated/autoconf.h
681 # and include/config/auto.conf but do not care if they are up-to-date.
682 # Use auto.conf to trigger the test
683 PHONY += include/config/auto.conf
685 include/config/auto.conf:
686         $(Q)test -e include/generated/autoconf.h -a -e $@ || (          \
687         echo >&2;                                                       \
688         echo >&2 "  ERROR: Kernel configuration is invalid.";           \
689         echo >&2 "         include/generated/autoconf.h or $@ are missing.";\
690         echo >&2 "         Run 'make oldconfig && make prepare' on kernel src to fix it.";      \
691         echo >&2 ;                                                      \
692         /bin/false)
694 endif # may-sync-config
695 endif # need-config
697 KBUILD_CFLAGS   += $(call cc-option,-fno-delete-null-pointer-checks,)
698 KBUILD_CFLAGS   += $(call cc-disable-warning,frame-address,)
699 KBUILD_CFLAGS   += $(call cc-disable-warning, format-truncation)
700 KBUILD_CFLAGS   += $(call cc-disable-warning, format-overflow)
701 KBUILD_CFLAGS   += $(call cc-disable-warning, address-of-packed-member)
703 ifdef CONFIG_CC_OPTIMIZE_FOR_PERFORMANCE
704 KBUILD_CFLAGS += -O2
705 else ifdef CONFIG_CC_OPTIMIZE_FOR_PERFORMANCE_O3
706 KBUILD_CFLAGS += -O3
707 else ifdef CONFIG_CC_OPTIMIZE_FOR_SIZE
708 KBUILD_CFLAGS += -Os
709 endif
711 ifdef CONFIG_CC_DISABLE_WARN_MAYBE_UNINITIALIZED
712 KBUILD_CFLAGS   += -Wno-maybe-uninitialized
713 endif
715 # Tell gcc to never replace conditional load with a non-conditional one
716 KBUILD_CFLAGS   += $(call cc-option,--param=allow-store-data-races=0)
718 include scripts/Makefile.kcov
719 include scripts/Makefile.gcc-plugins
721 ifdef CONFIG_READABLE_ASM
722 # Disable optimizations that make assembler listings hard to read.
723 # reorder blocks reorders the control in the function
724 # ipa clone creates specialized cloned functions
725 # partial inlining inlines only parts of functions
726 KBUILD_CFLAGS += $(call cc-option,-fno-reorder-blocks,) \
727                  $(call cc-option,-fno-ipa-cp-clone,) \
728                  $(call cc-option,-fno-partial-inlining)
729 endif
731 ifneq ($(CONFIG_FRAME_WARN),0)
732 KBUILD_CFLAGS += $(call cc-option,-Wframe-larger-than=${CONFIG_FRAME_WARN})
733 endif
735 stackp-flags-$(CONFIG_CC_HAS_STACKPROTECTOR_NONE) := -fno-stack-protector
736 stackp-flags-$(CONFIG_STACKPROTECTOR)             := -fstack-protector
737 stackp-flags-$(CONFIG_STACKPROTECTOR_STRONG)      := -fstack-protector-strong
739 KBUILD_CFLAGS += $(stackp-flags-y)
741 ifdef CONFIG_CC_IS_CLANG
742 KBUILD_CPPFLAGS += -Qunused-arguments
743 KBUILD_CFLAGS += -Wno-format-invalid-specifier
744 KBUILD_CFLAGS += -Wno-gnu
745 # Quiet clang warning: comparison of unsigned expression < 0 is always false
746 KBUILD_CFLAGS += -Wno-tautological-compare
747 # CLANG uses a _MergedGlobals as optimization, but this breaks modpost, as the
748 # source of a reference will be _MergedGlobals and not on of the whitelisted names.
749 # See modpost pattern 2
750 KBUILD_CFLAGS += -mno-global-merge
751 else
753 # These warnings generated too much noise in a regular build.
754 # Use make W=1 to enable them (see scripts/Makefile.extrawarn)
755 KBUILD_CFLAGS += -Wno-unused-but-set-variable
757 # Warn about unmarked fall-throughs in switch statement.
758 # Disabled for clang while comment to attribute conversion happens and
759 # https://github.com/ClangBuiltLinux/linux/issues/636 is discussed.
760 KBUILD_CFLAGS += $(call cc-option,-Wimplicit-fallthrough,)
761 endif
763 KBUILD_CFLAGS += $(call cc-disable-warning, unused-const-variable)
764 ifdef CONFIG_FRAME_POINTER
765 KBUILD_CFLAGS   += -fno-omit-frame-pointer -fno-optimize-sibling-calls
766 else
767 # Some targets (ARM with Thumb2, for example), can't be built with frame
768 # pointers.  For those, we don't have FUNCTION_TRACER automatically
769 # select FRAME_POINTER.  However, FUNCTION_TRACER adds -pg, and this is
770 # incompatible with -fomit-frame-pointer with current GCC, so we don't use
771 # -fomit-frame-pointer with FUNCTION_TRACER.
772 ifndef CONFIG_FUNCTION_TRACER
773 KBUILD_CFLAGS   += -fomit-frame-pointer
774 endif
775 endif
777 # Initialize all stack variables with a pattern, if desired.
778 ifdef CONFIG_INIT_STACK_ALL
779 KBUILD_CFLAGS   += -ftrivial-auto-var-init=pattern
780 endif
782 DEBUG_CFLAGS    := $(call cc-option, -fno-var-tracking-assignments)
784 ifdef CONFIG_DEBUG_INFO
785 ifdef CONFIG_DEBUG_INFO_SPLIT
786 DEBUG_CFLAGS    += -gsplit-dwarf
787 else
788 DEBUG_CFLAGS    += -g
789 endif
790 KBUILD_AFLAGS   += -Wa,-gdwarf-2
791 endif
792 ifdef CONFIG_DEBUG_INFO_DWARF4
793 DEBUG_CFLAGS    += -gdwarf-4
794 endif
796 ifdef CONFIG_DEBUG_INFO_REDUCED
797 DEBUG_CFLAGS    += $(call cc-option, -femit-struct-debug-baseonly) \
798                    $(call cc-option,-fno-var-tracking)
799 endif
801 KBUILD_CFLAGS += $(DEBUG_CFLAGS)
802 export DEBUG_CFLAGS
804 ifdef CONFIG_FUNCTION_TRACER
805 ifdef CONFIG_FTRACE_MCOUNT_RECORD
806   # gcc 5 supports generating the mcount tables directly
807   ifeq ($(call cc-option-yn,-mrecord-mcount),y)
808     CC_FLAGS_FTRACE     += -mrecord-mcount
809     export CC_USING_RECORD_MCOUNT := 1
810   endif
811   ifdef CONFIG_HAVE_NOP_MCOUNT
812     ifeq ($(call cc-option-yn, -mnop-mcount),y)
813       CC_FLAGS_FTRACE   += -mnop-mcount
814       CC_FLAGS_USING    += -DCC_USING_NOP_MCOUNT
815     endif
816   endif
817 endif
818 ifdef CONFIG_HAVE_FENTRY
819   ifeq ($(call cc-option-yn, -mfentry),y)
820     CC_FLAGS_FTRACE     += -mfentry
821     CC_FLAGS_USING      += -DCC_USING_FENTRY
822   endif
823 endif
824 export CC_FLAGS_FTRACE
825 KBUILD_CFLAGS   += $(CC_FLAGS_FTRACE) $(CC_FLAGS_USING)
826 KBUILD_AFLAGS   += $(CC_FLAGS_USING)
827 ifdef CONFIG_DYNAMIC_FTRACE
828         ifdef CONFIG_HAVE_C_RECORDMCOUNT
829                 BUILD_C_RECORDMCOUNT := y
830                 export BUILD_C_RECORDMCOUNT
831         endif
832 endif
833 endif
835 # We trigger additional mismatches with less inlining
836 ifdef CONFIG_DEBUG_SECTION_MISMATCH
837 KBUILD_CFLAGS += $(call cc-option, -fno-inline-functions-called-once)
838 endif
840 ifdef CONFIG_LD_DEAD_CODE_DATA_ELIMINATION
841 KBUILD_CFLAGS_KERNEL += -ffunction-sections -fdata-sections
842 LDFLAGS_vmlinux += --gc-sections
843 endif
845 ifdef CONFIG_LIVEPATCH
846 KBUILD_CFLAGS += $(call cc-option, -flive-patching=inline-clone)
847 endif
849 # arch Makefile may override CC so keep this after arch Makefile is included
850 NOSTDINC_FLAGS += -nostdinc -isystem $(shell $(CC) -print-file-name=include)
852 # warn about C99 declaration after statement
853 KBUILD_CFLAGS += -Wdeclaration-after-statement
855 # Variable Length Arrays (VLAs) should not be used anywhere in the kernel
856 KBUILD_CFLAGS += -Wvla
858 # disable pointer signed / unsigned warnings in gcc 4.0
859 KBUILD_CFLAGS += -Wno-pointer-sign
861 # disable stringop warnings in gcc 8+
862 KBUILD_CFLAGS += $(call cc-disable-warning, stringop-truncation)
864 # disable invalid "can't wrap" optimizations for signed / pointers
865 KBUILD_CFLAGS   += $(call cc-option,-fno-strict-overflow)
867 # clang sets -fmerge-all-constants by default as optimization, but this
868 # is non-conforming behavior for C and in fact breaks the kernel, so we
869 # need to disable it here generally.
870 KBUILD_CFLAGS   += $(call cc-option,-fno-merge-all-constants)
872 # for gcc -fno-merge-all-constants disables everything, but it is fine
873 # to have actual conforming behavior enabled.
874 KBUILD_CFLAGS   += $(call cc-option,-fmerge-constants)
876 # Make sure -fstack-check isn't enabled (like gentoo apparently did)
877 KBUILD_CFLAGS  += $(call cc-option,-fno-stack-check,)
879 # conserve stack if available
880 KBUILD_CFLAGS   += $(call cc-option,-fconserve-stack)
882 # Prohibit date/time macros, which would make the build non-deterministic
883 KBUILD_CFLAGS   += $(call cc-option,-Werror=date-time)
885 # enforce correct pointer usage
886 KBUILD_CFLAGS   += $(call cc-option,-Werror=incompatible-pointer-types)
888 # Require designated initializers for all marked structures
889 KBUILD_CFLAGS   += $(call cc-option,-Werror=designated-init)
891 # change __FILE__ to the relative path from the srctree
892 KBUILD_CFLAGS   += $(call cc-option,-fmacro-prefix-map=$(srctree)/=)
894 # ensure -fcf-protection is disabled when using retpoline as it is
895 # incompatible with -mindirect-branch=thunk-extern
896 ifdef CONFIG_RETPOLINE
897 KBUILD_CFLAGS += $(call cc-option,-fcf-protection=none)
898 endif
900 include scripts/Makefile.kasan
901 include scripts/Makefile.extrawarn
902 include scripts/Makefile.ubsan
904 # Add user supplied CPPFLAGS, AFLAGS and CFLAGS as the last assignments
905 KBUILD_CPPFLAGS += $(KCPPFLAGS)
906 KBUILD_AFLAGS   += $(KAFLAGS)
907 KBUILD_CFLAGS   += $(KCFLAGS)
909 KBUILD_LDFLAGS_MODULE += --build-id
910 LDFLAGS_vmlinux += --build-id
912 ifeq ($(CONFIG_STRIP_ASM_SYMS),y)
913 LDFLAGS_vmlinux += $(call ld-option, -X,)
914 endif
916 ifeq ($(CONFIG_RELR),y)
917 LDFLAGS_vmlinux += --pack-dyn-relocs=relr
918 endif
920 # insure the checker run with the right endianness
921 CHECKFLAGS += $(if $(CONFIG_CPU_BIG_ENDIAN),-mbig-endian,-mlittle-endian)
923 # the checker needs the correct machine size
924 CHECKFLAGS += $(if $(CONFIG_64BIT),-m64,-m32)
926 # Default kernel image to build when no specific target is given.
927 # KBUILD_IMAGE may be overruled on the command line or
928 # set in the environment
929 # Also any assignments in arch/$(ARCH)/Makefile take precedence over
930 # this default value
931 export KBUILD_IMAGE ?= vmlinux
934 # INSTALL_PATH specifies where to place the updated kernel and system map
935 # images. Default is /boot, but you can set it to other values
936 export  INSTALL_PATH ?= /boot
939 # INSTALL_DTBS_PATH specifies a prefix for relocations required by build roots.
940 # Like INSTALL_MOD_PATH, it isn't defined in the Makefile, but can be passed as
941 # an argument if needed. Otherwise it defaults to the kernel install path
943 export INSTALL_DTBS_PATH ?= $(INSTALL_PATH)/dtbs/$(KERNELRELEASE)
946 # INSTALL_MOD_PATH specifies a prefix to MODLIB for module directory
947 # relocations required by build roots.  This is not defined in the
948 # makefile but the argument can be passed to make if needed.
951 MODLIB  = $(INSTALL_MOD_PATH)/lib/modules/$(KERNELRELEASE)
952 export MODLIB
955 # INSTALL_MOD_STRIP, if defined, will cause modules to be
956 # stripped after they are installed.  If INSTALL_MOD_STRIP is '1', then
957 # the default option --strip-debug will be used.  Otherwise,
958 # INSTALL_MOD_STRIP value will be used as the options to the strip command.
960 ifdef INSTALL_MOD_STRIP
961 ifeq ($(INSTALL_MOD_STRIP),1)
962 mod_strip_cmd = $(STRIP) --strip-debug
963 else
964 mod_strip_cmd = $(STRIP) $(INSTALL_MOD_STRIP)
965 endif # INSTALL_MOD_STRIP=1
966 else
967 mod_strip_cmd = true
968 endif # INSTALL_MOD_STRIP
969 export mod_strip_cmd
971 # CONFIG_MODULE_COMPRESS, if defined, will cause module to be compressed
972 # after they are installed in agreement with CONFIG_MODULE_COMPRESS_GZIP
973 # or CONFIG_MODULE_COMPRESS_XZ.
975 mod_compress_cmd = true
976 ifdef CONFIG_MODULE_COMPRESS
977   ifdef CONFIG_MODULE_COMPRESS_GZIP
978     mod_compress_cmd = gzip -n -f
979   endif # CONFIG_MODULE_COMPRESS_GZIP
980   ifdef CONFIG_MODULE_COMPRESS_XZ
981     mod_compress_cmd = xz -f
982   endif # CONFIG_MODULE_COMPRESS_XZ
983 endif # CONFIG_MODULE_COMPRESS
984 export mod_compress_cmd
986 ifdef CONFIG_MODULE_SIG_ALL
987 $(eval $(call config_filename,MODULE_SIG_KEY))
989 mod_sign_cmd = scripts/sign-file $(CONFIG_MODULE_SIG_HASH) $(MODULE_SIG_KEY_SRCPREFIX)$(CONFIG_MODULE_SIG_KEY) certs/signing_key.x509
990 else
991 mod_sign_cmd = true
992 endif
993 export mod_sign_cmd
995 HOST_LIBELF_LIBS = $(shell pkg-config libelf --libs 2>/dev/null || echo -lelf)
997 ifdef CONFIG_STACK_VALIDATION
998   has_libelf := $(call try-run,\
999                 echo "int main() {}" | $(HOSTCC) -xc -o /dev/null $(HOST_LIBELF_LIBS) -,1,0)
1000   ifeq ($(has_libelf),1)
1001     objtool_target := tools/objtool FORCE
1002   else
1003     SKIP_STACK_VALIDATION := 1
1004     export SKIP_STACK_VALIDATION
1005   endif
1006 endif
1008 PHONY += prepare0
1010 export MODORDER := $(extmod-prefix)modules.order
1012 ifeq ($(KBUILD_EXTMOD),)
1013 core-y          += kernel/ certs/ mm/ fs/ ipc/ security/ crypto/ block/
1015 vmlinux-dirs    := $(patsubst %/,%,$(filter %/, $(init-y) $(init-m) \
1016                      $(core-y) $(core-m) $(drivers-y) $(drivers-m) \
1017                      $(net-y) $(net-m) $(libs-y) $(libs-m) $(virt-y)))
1019 vmlinux-alldirs := $(sort $(vmlinux-dirs) Documentation \
1020                      $(patsubst %/,%,$(filter %/, $(init-) $(core-) \
1021                         $(drivers-) $(net-) $(libs-) $(virt-))))
1023 build-dirs      := $(vmlinux-dirs)
1024 clean-dirs      := $(vmlinux-alldirs)
1026 init-y          := $(patsubst %/, %/built-in.a, $(init-y))
1027 core-y          := $(patsubst %/, %/built-in.a, $(core-y))
1028 drivers-y       := $(patsubst %/, %/built-in.a, $(drivers-y))
1029 net-y           := $(patsubst %/, %/built-in.a, $(net-y))
1030 libs-y1         := $(patsubst %/, %/lib.a, $(libs-y))
1031 libs-y2         := $(patsubst %/, %/built-in.a, $(filter-out %.a, $(libs-y)))
1032 virt-y          := $(patsubst %/, %/built-in.a, $(virt-y))
1034 # Externally visible symbols (used by link-vmlinux.sh)
1035 export KBUILD_VMLINUX_OBJS := $(head-y) $(init-y) $(core-y) $(libs-y2) \
1036                               $(drivers-y) $(net-y) $(virt-y)
1037 export KBUILD_VMLINUX_LIBS := $(libs-y1)
1038 export KBUILD_LDS          := arch/$(SRCARCH)/kernel/vmlinux.lds
1039 export LDFLAGS_vmlinux
1040 # used by scripts/package/Makefile
1041 export KBUILD_ALLDIRS := $(sort $(filter-out arch/%,$(vmlinux-alldirs)) LICENSES arch include scripts tools)
1043 vmlinux-deps := $(KBUILD_LDS) $(KBUILD_VMLINUX_OBJS) $(KBUILD_VMLINUX_LIBS)
1045 # Recurse until adjust_autoksyms.sh is satisfied
1046 PHONY += autoksyms_recursive
1047 ifdef CONFIG_TRIM_UNUSED_KSYMS
1048 autoksyms_recursive: descend modules.order
1049         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/adjust_autoksyms.sh \
1050           "$(MAKE) -f $(srctree)/Makefile vmlinux"
1051 endif
1053 # For the kernel to actually contain only the needed exported symbols,
1054 # we have to build modules as well to determine what those symbols are.
1055 # (this can be evaluated only once include/config/auto.conf has been included)
1056 ifdef CONFIG_TRIM_UNUSED_KSYMS
1057   KBUILD_MODULES := 1
1058 endif
1060 autoksyms_h := $(if $(CONFIG_TRIM_UNUSED_KSYMS), include/generated/autoksyms.h)
1062 $(autoksyms_h):
1063         $(Q)mkdir -p $(dir $@)
1064         $(Q)touch $@
1066 ARCH_POSTLINK := $(wildcard $(srctree)/arch/$(SRCARCH)/Makefile.postlink)
1068 # Final link of vmlinux with optional arch pass after final link
1069 cmd_link-vmlinux =                                                 \
1070         $(CONFIG_SHELL) $< $(LD) $(KBUILD_LDFLAGS) $(LDFLAGS_vmlinux) ;    \
1071         $(if $(ARCH_POSTLINK), $(MAKE) -f $(ARCH_POSTLINK) $@, true)
1073 vmlinux: scripts/link-vmlinux.sh autoksyms_recursive $(vmlinux-deps) FORCE
1074         +$(call if_changed,link-vmlinux)
1076 targets := vmlinux
1078 # The actual objects are generated when descending,
1079 # make sure no implicit rule kicks in
1080 $(sort $(vmlinux-deps)): descend ;
1082 filechk_kernel.release = \
1083         echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion $(srctree))"
1085 # Store (new) KERNELRELEASE string in include/config/kernel.release
1086 include/config/kernel.release: FORCE
1087         $(call filechk,kernel.release)
1089 # Additional helpers built in scripts/
1090 # Carefully list dependencies so we do not try to build scripts twice
1091 # in parallel
1092 PHONY += scripts
1093 scripts: scripts_basic scripts_dtc
1094         $(Q)$(MAKE) $(build)=$(@)
1096 # Things we need to do before we recursively start building the kernel
1097 # or the modules are listed in "prepare".
1098 # A multi level approach is used. prepareN is processed before prepareN-1.
1099 # archprepare is used in arch Makefiles and when processed asm symlink,
1100 # version.h and scripts_basic is processed / created.
1102 PHONY += prepare archprepare
1104 archprepare: outputmakefile archheaders archscripts scripts include/config/kernel.release \
1105         asm-generic $(version_h) $(autoksyms_h) include/generated/utsrelease.h
1107 prepare0: archprepare
1108         $(Q)$(MAKE) $(build)=scripts/mod
1109         $(Q)$(MAKE) $(build)=.
1111 # All the preparing..
1112 prepare: prepare0 prepare-objtool
1114 # Support for using generic headers in asm-generic
1115 asm-generic := -f $(srctree)/scripts/Makefile.asm-generic obj
1117 PHONY += asm-generic uapi-asm-generic
1118 asm-generic: uapi-asm-generic
1119         $(Q)$(MAKE) $(asm-generic)=arch/$(SRCARCH)/include/generated/asm \
1120         generic=include/asm-generic
1121 uapi-asm-generic:
1122         $(Q)$(MAKE) $(asm-generic)=arch/$(SRCARCH)/include/generated/uapi/asm \
1123         generic=include/uapi/asm-generic
1125 PHONY += prepare-objtool
1126 prepare-objtool: $(objtool_target)
1127 ifeq ($(SKIP_STACK_VALIDATION),1)
1128 ifdef CONFIG_UNWINDER_ORC
1129         @echo "error: Cannot generate ORC metadata for CONFIG_UNWINDER_ORC=y, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
1130         @false
1131 else
1132         @echo "warning: Cannot use CONFIG_STACK_VALIDATION=y, please install libelf-dev, libelf-devel or elfutils-libelf-devel" >&2
1133 endif
1134 endif
1136 # Generate some files
1137 # ---------------------------------------------------------------------------
1139 # KERNELRELEASE can change from a few different places, meaning version.h
1140 # needs to be updated, so this check is forced on all builds
1142 uts_len := 64
1143 define filechk_utsrelease.h
1144         if [ `echo -n "$(KERNELRELEASE)" | wc -c ` -gt $(uts_len) ]; then \
1145           echo '"$(KERNELRELEASE)" exceeds $(uts_len) characters' >&2;    \
1146           exit 1;                                                         \
1147         fi;                                                               \
1148         echo \#define UTS_RELEASE \"$(KERNELRELEASE)\"
1149 endef
1151 define filechk_version.h
1152         echo \#define LINUX_VERSION_CODE $(shell                         \
1153         expr $(VERSION) \* 65536 + 0$(PATCHLEVEL) \* 256 + 0$(SUBLEVEL)); \
1154         echo '#define KERNEL_VERSION(a,b,c) (((a) << 16) + ((b) << 8) + (c))'
1155 endef
1157 $(version_h): FORCE
1158         $(call filechk,version.h)
1159         $(Q)rm -f $(old_version_h)
1161 include/generated/utsrelease.h: include/config/kernel.release FORCE
1162         $(call filechk,utsrelease.h)
1164 PHONY += headerdep
1165 headerdep:
1166         $(Q)find $(srctree)/include/ -name '*.h' | xargs --max-args 1 \
1167         $(srctree)/scripts/headerdep.pl -I$(srctree)/include
1169 # ---------------------------------------------------------------------------
1170 # Kernel headers
1172 #Default location for installed headers
1173 export INSTALL_HDR_PATH = $(objtree)/usr
1175 quiet_cmd_headers_install = INSTALL $(INSTALL_HDR_PATH)/include
1176       cmd_headers_install = \
1177         mkdir -p $(INSTALL_HDR_PATH); \
1178         rsync -mrl --include='*/' --include='*\.h' --exclude='*' \
1179         usr/include $(INSTALL_HDR_PATH)
1181 PHONY += headers_install
1182 headers_install: headers
1183         $(call cmd,headers_install)
1185 PHONY += archheaders archscripts
1187 hdr-inst := -f $(srctree)/scripts/Makefile.headersinst obj
1189 PHONY += headers
1190 headers: $(version_h) scripts_unifdef uapi-asm-generic archheaders archscripts
1191         $(if $(wildcard $(srctree)/arch/$(SRCARCH)/include/uapi/asm/Kbuild),, \
1192           $(error Headers not exportable for the $(SRCARCH) architecture))
1193         $(Q)$(MAKE) $(hdr-inst)=include/uapi
1194         $(Q)$(MAKE) $(hdr-inst)=arch/$(SRCARCH)/include/uapi
1196 PHONY += headers_check
1197 headers_check: headers
1198         $(Q)$(MAKE) $(hdr-inst)=include/uapi HDRCHECK=1
1199         $(Q)$(MAKE) $(hdr-inst)=arch/$(SRCARCH)/include/uapi HDRCHECK=1
1201 ifdef CONFIG_HEADERS_INSTALL
1202 prepare: headers
1203 endif
1205 ifdef CONFIG_HEADERS_CHECK
1206 all: headers_check
1207 endif
1209 PHONY += scripts_unifdef
1210 scripts_unifdef: scripts_basic
1211         $(Q)$(MAKE) $(build)=scripts scripts/unifdef
1213 # ---------------------------------------------------------------------------
1214 # Kernel selftest
1216 PHONY += kselftest
1217 kselftest:
1218         $(Q)$(MAKE) -C $(srctree)/tools/testing/selftests run_tests
1220 PHONY += kselftest-clean
1221 kselftest-clean:
1222         $(Q)$(MAKE) -C $(srctree)/tools/testing/selftests clean
1224 PHONY += kselftest-merge
1225 kselftest-merge:
1226         $(if $(wildcard $(objtree)/.config),, $(error No .config exists, config your kernel first!))
1227         $(Q)find $(srctree)/tools/testing/selftests -name config | \
1228                 xargs $(srctree)/scripts/kconfig/merge_config.sh -m $(objtree)/.config
1229         $(Q)$(MAKE) -f $(srctree)/Makefile olddefconfig
1231 # ---------------------------------------------------------------------------
1232 # Devicetree files
1234 ifneq ($(wildcard $(srctree)/arch/$(SRCARCH)/boot/dts/),)
1235 dtstree := arch/$(SRCARCH)/boot/dts
1236 endif
1238 ifneq ($(dtstree),)
1240 %.dtb: include/config/kernel.release scripts_dtc
1241         $(Q)$(MAKE) $(build)=$(dtstree) $(dtstree)/$@
1243 PHONY += dtbs dtbs_install dt_binding_check
1244 dtbs dtbs_check: include/config/kernel.release scripts_dtc
1245         $(Q)$(MAKE) $(build)=$(dtstree)
1247 dtbs_check: export CHECK_DTBS=1
1248 dtbs_check: dt_binding_check
1250 dtbs_install:
1251         $(Q)$(MAKE) $(dtbinst)=$(dtstree)
1253 ifdef CONFIG_OF_EARLY_FLATTREE
1254 all: dtbs
1255 endif
1257 endif
1259 PHONY += scripts_dtc
1260 scripts_dtc: scripts_basic
1261         $(Q)$(MAKE) $(build)=scripts/dtc
1263 dt_binding_check: scripts_dtc
1264         $(Q)$(MAKE) $(build)=Documentation/devicetree/bindings
1266 # ---------------------------------------------------------------------------
1267 # Modules
1269 ifdef CONFIG_MODULES
1271 # By default, build modules as well
1273 all: modules
1275 # Build modules
1277 # A module can be listed more than once in obj-m resulting in
1278 # duplicate lines in modules.order files.  Those are removed
1279 # using awk while concatenating to the final file.
1281 PHONY += modules
1282 modules: $(if $(KBUILD_BUILTIN),vmlinux) modules.order modules.builtin
1283         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
1284         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/modules-check.sh
1286 modules.order: descend
1287         $(Q)$(AWK) '!x[$$0]++' $(addsuffix /$@, $(build-dirs)) > $@
1289 modbuiltin-dirs := $(addprefix _modbuiltin_, $(build-dirs))
1291 modules.builtin: $(modbuiltin-dirs)
1292         $(Q)$(AWK) '!x[$$0]++' $(addsuffix /$@, $(build-dirs)) > $@
1294 PHONY += $(modbuiltin-dirs)
1295 # tristate.conf is not included from this Makefile. Add it as a prerequisite
1296 # here to make it self-healing in case somebody accidentally removes it.
1297 $(modbuiltin-dirs): include/config/tristate.conf
1298         $(Q)$(MAKE) $(modbuiltin)=$(patsubst _modbuiltin_%,%,$@)
1300 # Target to prepare building external modules
1301 PHONY += modules_prepare
1302 modules_prepare: prepare
1304 # Target to install modules
1305 PHONY += modules_install
1306 modules_install: _modinst_ _modinst_post
1308 PHONY += _modinst_
1309 _modinst_:
1310         @rm -rf $(MODLIB)/kernel
1311         @rm -f $(MODLIB)/source
1312         @mkdir -p $(MODLIB)/kernel
1313         @ln -s $(abspath $(srctree)) $(MODLIB)/source
1314         @if [ ! $(objtree) -ef  $(MODLIB)/build ]; then \
1315                 rm -f $(MODLIB)/build ; \
1316                 ln -s $(CURDIR) $(MODLIB)/build ; \
1317         fi
1318         @sed 's:^:kernel/:' modules.order > $(MODLIB)/modules.order
1319         @sed 's:^:kernel/:' modules.builtin > $(MODLIB)/modules.builtin
1320         @cp -f $(objtree)/modules.builtin.modinfo $(MODLIB)/
1321         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
1323 # This depmod is only for convenience to give the initial
1324 # boot a modules.dep even before / is mounted read-write.  However the
1325 # boot script depmod is the master version.
1326 PHONY += _modinst_post
1327 _modinst_post: _modinst_
1328         $(call cmd,depmod)
1330 ifeq ($(CONFIG_MODULE_SIG), y)
1331 PHONY += modules_sign
1332 modules_sign:
1333         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modsign
1334 endif
1336 else # CONFIG_MODULES
1338 # Modules not configured
1339 # ---------------------------------------------------------------------------
1341 PHONY += modules modules_install
1342 modules modules_install:
1343         @echo >&2
1344         @echo >&2 "The present kernel configuration has modules disabled."
1345         @echo >&2 "Type 'make config' and enable loadable module support."
1346         @echo >&2 "Then build a kernel with module support enabled."
1347         @echo >&2
1348         @exit 1
1350 endif # CONFIG_MODULES
1352 ###
1353 # Cleaning is done on three levels.
1354 # make clean     Delete most generated files
1355 #                Leave enough to build external modules
1356 # make mrproper  Delete the current configuration, and all generated files
1357 # make distclean Remove editor backup files, patch leftover files and the like
1359 # Directories & files removed with 'make clean'
1360 CLEAN_DIRS  += include/ksym
1361 CLEAN_FILES += modules.builtin.modinfo
1363 # Directories & files removed with 'make mrproper'
1364 MRPROPER_DIRS  += include/config include/generated          \
1365                   arch/$(SRCARCH)/include/generated .tmp_objdiff \
1366                   debian/ snap/ tar-install/
1367 MRPROPER_FILES += .config .config.old .version \
1368                   Module.symvers \
1369                   signing_key.pem signing_key.priv signing_key.x509     \
1370                   x509.genkey extra_certificates signing_key.x509.keyid \
1371                   signing_key.x509.signer vmlinux-gdb.py \
1372                   *.spec
1374 # Directories & files removed with 'make distclean'
1375 DISTCLEAN_DIRS  +=
1376 DISTCLEAN_FILES += tags TAGS cscope* GPATH GTAGS GRTAGS GSYMS
1378 # clean - Delete most, but leave enough to build external modules
1380 clean: rm-dirs  := $(CLEAN_DIRS)
1381 clean: rm-files := $(CLEAN_FILES)
1383 PHONY += archclean vmlinuxclean
1385 vmlinuxclean:
1386         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/link-vmlinux.sh clean
1387         $(Q)$(if $(ARCH_POSTLINK), $(MAKE) -f $(ARCH_POSTLINK) clean)
1389 clean: archclean vmlinuxclean
1391 # mrproper - Delete all generated files, including .config
1393 mrproper: rm-dirs  := $(wildcard $(MRPROPER_DIRS))
1394 mrproper: rm-files := $(wildcard $(MRPROPER_FILES))
1395 mrproper-dirs      := $(addprefix _mrproper_,scripts)
1397 PHONY += $(mrproper-dirs) mrproper
1398 $(mrproper-dirs):
1399         $(Q)$(MAKE) $(clean)=$(patsubst _mrproper_%,%,$@)
1401 mrproper: clean $(mrproper-dirs)
1402         $(call cmd,rmdirs)
1403         $(call cmd,rmfiles)
1405 # distclean
1407 distclean: rm-dirs  := $(wildcard $(DISTCLEAN_DIRS))
1408 distclean: rm-files := $(wildcard $(DISTCLEAN_FILES))
1410 PHONY += distclean
1412 distclean: mrproper
1413         $(call cmd,rmdirs)
1414         $(call cmd,rmfiles)
1415         @find $(srctree) $(RCS_FIND_IGNORE) \
1416                 \( -name '*.orig' -o -name '*.rej' -o -name '*~' \
1417                 -o -name '*.bak' -o -name '#*#' -o -name '*%' \
1418                 -o -name 'core' \) \
1419                 -type f -print | xargs rm -f
1422 # Packaging of the kernel to various formats
1423 # ---------------------------------------------------------------------------
1425 %src-pkg: FORCE
1426         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.package $@
1427 %pkg: include/config/kernel.release FORCE
1428         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.package $@
1430 # Brief documentation of the typical targets used
1431 # ---------------------------------------------------------------------------
1433 boards := $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*_defconfig)
1434 boards := $(sort $(notdir $(boards)))
1435 board-dirs := $(dir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/*/*_defconfig))
1436 board-dirs := $(sort $(notdir $(board-dirs:/=)))
1438 PHONY += help
1439 help:
1440         @echo  'Cleaning targets:'
1441         @echo  '  clean           - Remove most generated files but keep the config and'
1442         @echo  '                    enough build support to build external modules'
1443         @echo  '  mrproper        - Remove all generated files + config + various backup files'
1444         @echo  '  distclean       - mrproper + remove editor backup and patch files'
1445         @echo  ''
1446         @echo  'Configuration targets:'
1447         @$(MAKE) -f $(srctree)/scripts/kconfig/Makefile help
1448         @echo  ''
1449         @echo  'Other generic targets:'
1450         @echo  '  all             - Build all targets marked with [*]'
1451         @echo  '* vmlinux         - Build the bare kernel'
1452         @echo  '* modules         - Build all modules'
1453         @echo  '  modules_install - Install all modules to INSTALL_MOD_PATH (default: /)'
1454         @echo  '  dir/            - Build all files in dir and below'
1455         @echo  '  dir/file.[ois]  - Build specified target only'
1456         @echo  '  dir/file.ll     - Build the LLVM assembly file'
1457         @echo  '                    (requires compiler support for LLVM assembly generation)'
1458         @echo  '  dir/file.lst    - Build specified mixed source/assembly target only'
1459         @echo  '                    (requires a recent binutils and recent build (System.map))'
1460         @echo  '  dir/file.ko     - Build module including final link'
1461         @echo  '  modules_prepare - Set up for building external modules'
1462         @echo  '  tags/TAGS       - Generate tags file for editors'
1463         @echo  '  cscope          - Generate cscope index'
1464         @echo  '  gtags           - Generate GNU GLOBAL index'
1465         @echo  '  kernelrelease   - Output the release version string (use with make -s)'
1466         @echo  '  kernelversion   - Output the version stored in Makefile (use with make -s)'
1467         @echo  '  image_name      - Output the image name (use with make -s)'
1468         @echo  '  headers_install - Install sanitised kernel headers to INSTALL_HDR_PATH'; \
1469          echo  '                    (default: $(INSTALL_HDR_PATH))'; \
1470          echo  ''
1471         @echo  'Static analysers:'
1472         @echo  '  checkstack      - Generate a list of stack hogs'
1473         @echo  '  namespacecheck  - Name space analysis on compiled kernel'
1474         @echo  '  versioncheck    - Sanity check on version.h usage'
1475         @echo  '  includecheck    - Check for duplicate included header files'
1476         @echo  '  export_report   - List the usages of all exported symbols'
1477         @echo  '  headers_check   - Sanity check on exported headers'
1478         @echo  '  headerdep       - Detect inclusion cycles in headers'
1479         @echo  '  coccicheck      - Check with Coccinelle'
1480         @echo  ''
1481         @echo  'Tools:'
1482         @echo  '  nsdeps          - Generate missing symbol namespace dependencies'
1483         @echo  ''
1484         @echo  'Kernel selftest:'
1485         @echo  '  kselftest       - Build and run kernel selftest (run as root)'
1486         @echo  '                    Build, install, and boot kernel before'
1487         @echo  '                    running kselftest on it'
1488         @echo  '  kselftest-clean - Remove all generated kselftest files'
1489         @echo  '  kselftest-merge - Merge all the config dependencies of kselftest to existing'
1490         @echo  '                    .config.'
1491         @echo  ''
1492         @$(if $(dtstree), \
1493                 echo 'Devicetree:'; \
1494                 echo '* dtbs             - Build device tree blobs for enabled boards'; \
1495                 echo '  dtbs_install     - Install dtbs to $(INSTALL_DTBS_PATH)'; \
1496                 echo '  dt_binding_check - Validate device tree binding documents'; \
1497                 echo '  dtbs_check       - Validate device tree source files';\
1498                 echo '')
1500         @echo 'Userspace tools targets:'
1501         @echo '  use "make tools/help"'
1502         @echo '  or  "cd tools; make help"'
1503         @echo  ''
1504         @echo  'Kernel packaging:'
1505         @$(MAKE) -f $(srctree)/scripts/Makefile.package help
1506         @echo  ''
1507         @echo  'Documentation targets:'
1508         @$(MAKE) -f $(srctree)/Documentation/Makefile dochelp
1509         @echo  ''
1510         @echo  'Architecture specific targets ($(SRCARCH)):'
1511         @$(if $(archhelp),$(archhelp),\
1512                 echo '  No architecture specific help defined for $(SRCARCH)')
1513         @echo  ''
1514         @$(if $(boards), \
1515                 $(foreach b, $(boards), \
1516                 printf "  %-24s - Build for %s\\n" $(b) $(subst _defconfig,,$(b));) \
1517                 echo '')
1518         @$(if $(board-dirs), \
1519                 $(foreach b, $(board-dirs), \
1520                 printf "  %-16s - Show %s-specific targets\\n" help-$(b) $(b);) \
1521                 printf "  %-16s - Show all of the above\\n" help-boards; \
1522                 echo '')
1524         @echo  '  make V=0|1 [targets] 0 => quiet build (default), 1 => verbose build'
1525         @echo  '  make V=2   [targets] 2 => give reason for rebuild of target'
1526         @echo  '  make O=dir [targets] Locate all output files in "dir", including .config'
1527         @echo  '  make C=1   [targets] Check re-compiled c source with $$CHECK (sparse by default)'
1528         @echo  '  make C=2   [targets] Force check of all c source with $$CHECK'
1529         @echo  '  make RECORDMCOUNT_WARN=1 [targets] Warn about ignored mcount sections'
1530         @echo  '  make W=n   [targets] Enable extra build checks, n=1,2,3 where'
1531         @echo  '                1: warnings which may be relevant and do not occur too often'
1532         @echo  '                2: warnings which occur quite often but may still be relevant'
1533         @echo  '                3: more obscure warnings, can most likely be ignored'
1534         @echo  '                Multiple levels can be combined with W=12 or W=123'
1535         @echo  ''
1536         @echo  'Execute "make" or "make all" to build all targets marked with [*] '
1537         @echo  'For further info see the ./README file'
1540 help-board-dirs := $(addprefix help-,$(board-dirs))
1542 help-boards: $(help-board-dirs)
1544 boards-per-dir = $(sort $(notdir $(wildcard $(srctree)/arch/$(SRCARCH)/configs/$*/*_defconfig)))
1546 $(help-board-dirs): help-%:
1547         @echo  'Architecture specific targets ($(SRCARCH) $*):'
1548         @$(if $(boards-per-dir), \
1549                 $(foreach b, $(boards-per-dir), \
1550                 printf "  %-24s - Build for %s\\n" $*/$(b) $(subst _defconfig,,$(b));) \
1551                 echo '')
1554 # Documentation targets
1555 # ---------------------------------------------------------------------------
1556 DOC_TARGETS := xmldocs latexdocs pdfdocs htmldocs epubdocs cleandocs \
1557                linkcheckdocs dochelp refcheckdocs
1558 PHONY += $(DOC_TARGETS)
1559 $(DOC_TARGETS):
1560         $(Q)$(MAKE) $(build)=Documentation $@
1562 # Misc
1563 # ---------------------------------------------------------------------------
1565 PHONY += scripts_gdb
1566 scripts_gdb: prepare0
1567         $(Q)$(MAKE) $(build)=scripts/gdb
1568         $(Q)ln -fsn $(abspath $(srctree)/scripts/gdb/vmlinux-gdb.py)
1570 ifdef CONFIG_GDB_SCRIPTS
1571 all: scripts_gdb
1572 endif
1574 else # KBUILD_EXTMOD
1576 ###
1577 # External module support.
1578 # When building external modules the kernel used as basis is considered
1579 # read-only, and no consistency checks are made and the make
1580 # system is not used on the basis kernel. If updates are required
1581 # in the basis kernel ordinary make commands (without M=...) must
1582 # be used.
1584 # The following are the only valid targets when building external
1585 # modules.
1586 # make M=dir clean     Delete all automatically generated files
1587 # make M=dir modules   Make all modules in specified dir
1588 # make M=dir           Same as 'make M=dir modules'
1589 # make M=dir modules_install
1590 #                      Install the modules built in the module directory
1591 #                      Assumes install directory is already created
1593 # We are always building modules
1594 KBUILD_MODULES := 1
1596 PHONY += $(objtree)/Module.symvers
1597 $(objtree)/Module.symvers:
1598         @test -e $(objtree)/Module.symvers || ( \
1599         echo; \
1600         echo "  WARNING: Symbol version dump $(objtree)/Module.symvers"; \
1601         echo "           is missing; modules will have no dependencies and modversions."; \
1602         echo )
1604 build-dirs := $(KBUILD_EXTMOD)
1605 PHONY += modules
1606 modules: descend $(objtree)/Module.symvers
1607         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
1609 PHONY += modules_install
1610 modules_install: _emodinst_ _emodinst_post
1612 install-dir := $(if $(INSTALL_MOD_DIR),$(INSTALL_MOD_DIR),extra)
1613 PHONY += _emodinst_
1614 _emodinst_:
1615         $(Q)mkdir -p $(MODLIB)/$(install-dir)
1616         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modinst
1618 PHONY += _emodinst_post
1619 _emodinst_post: _emodinst_
1620         $(call cmd,depmod)
1622 clean-dirs := $(KBUILD_EXTMOD)
1623 clean: rm-files := $(KBUILD_EXTMOD)/Module.symvers
1625 PHONY += /
1626 /:
1627         @echo >&2 '"$(MAKE) /" is no longer supported. Please use "$(MAKE) ./" instead.'
1629 PHONY += help
1630 help:
1631         @echo  '  Building external modules.'
1632         @echo  '  Syntax: make -C path/to/kernel/src M=$$PWD target'
1633         @echo  ''
1634         @echo  '  modules         - default target, build the module(s)'
1635         @echo  '  modules_install - install the module'
1636         @echo  '  clean           - remove generated files in module directory only'
1637         @echo  ''
1639 PHONY += prepare
1640 endif # KBUILD_EXTMOD
1642 # Handle descending into subdirectories listed in $(build-dirs)
1643 # Preset locale variables to speed up the build process. Limit locale
1644 # tweaks to this spot to avoid wrong language settings when running
1645 # make menuconfig etc.
1646 # Error messages still appears in the original language
1647 PHONY += descend $(build-dirs)
1648 descend: $(build-dirs)
1649 $(build-dirs): prepare
1650         $(Q)$(MAKE) $(build)=$@ single-build=$(single-build) need-builtin=1 need-modorder=1
1652 clean-dirs := $(addprefix _clean_, $(clean-dirs))
1653 PHONY += $(clean-dirs) clean
1654 $(clean-dirs):
1655         $(Q)$(MAKE) $(clean)=$(patsubst _clean_%,%,$@)
1657 clean: $(clean-dirs)
1658         $(call cmd,rmdirs)
1659         $(call cmd,rmfiles)
1660         @find $(if $(KBUILD_EXTMOD), $(KBUILD_EXTMOD), .) $(RCS_FIND_IGNORE) \
1661                 \( -name '*.[aios]' -o -name '*.ko' -o -name '.*.cmd' \
1662                 -o -name '*.ko.*' \
1663                 -o -name '*.dtb' -o -name '*.dtb.S' -o -name '*.dt.yaml' \
1664                 -o -name '*.dwo' -o -name '*.lst' \
1665                 -o -name '*.su' -o -name '*.mod' -o -name '*.ns_deps' \
1666                 -o -name '.*.d' -o -name '.*.tmp' -o -name '*.mod.c' \
1667                 -o -name '*.lex.c' -o -name '*.tab.[ch]' \
1668                 -o -name '*.asn1.[ch]' \
1669                 -o -name '*.symtypes' -o -name 'modules.order' \
1670                 -o -name modules.builtin -o -name '.tmp_*.o.*' \
1671                 -o -name '*.c.[012]*.*' \
1672                 -o -name '*.ll' \
1673                 -o -name '*.gcno' \) -type f -print | xargs rm -f
1675 # Generate tags for editors
1676 # ---------------------------------------------------------------------------
1677 quiet_cmd_tags = GEN     $@
1678       cmd_tags = $(BASH) $(srctree)/scripts/tags.sh $@
1680 tags TAGS cscope gtags: FORCE
1681         $(call cmd,tags)
1683 # Script to generate missing namespace dependencies
1684 # ---------------------------------------------------------------------------
1686 PHONY += nsdeps
1688 nsdeps: modules
1689         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost nsdeps
1690         $(Q)$(CONFIG_SHELL) $(srctree)/scripts/$@
1692 # Scripts to check various things for consistency
1693 # ---------------------------------------------------------------------------
1695 PHONY += includecheck versioncheck coccicheck namespacecheck export_report
1697 includecheck:
1698         find $(srctree)/* $(RCS_FIND_IGNORE) \
1699                 -name '*.[hcS]' -type f -print | sort \
1700                 | xargs $(PERL) -w $(srctree)/scripts/checkincludes.pl
1702 versioncheck:
1703         find $(srctree)/* $(RCS_FIND_IGNORE) \
1704                 -name '*.[hcS]' -type f -print | sort \
1705                 | xargs $(PERL) -w $(srctree)/scripts/checkversion.pl
1707 coccicheck:
1708         $(Q)$(BASH) $(srctree)/scripts/$@
1710 namespacecheck:
1711         $(PERL) $(srctree)/scripts/namespace.pl
1713 export_report:
1714         $(PERL) $(srctree)/scripts/export_report.pl
1716 PHONY += checkstack kernelrelease kernelversion image_name
1718 # UML needs a little special treatment here.  It wants to use the host
1719 # toolchain, so needs $(SUBARCH) passed to checkstack.pl.  Everyone
1720 # else wants $(ARCH), including people doing cross-builds, which means
1721 # that $(SUBARCH) doesn't work here.
1722 ifeq ($(ARCH), um)
1723 CHECKSTACK_ARCH := $(SUBARCH)
1724 else
1725 CHECKSTACK_ARCH := $(ARCH)
1726 endif
1727 checkstack:
1728         $(OBJDUMP) -d vmlinux $$(find . -name '*.ko') | \
1729         $(PERL) $(srctree)/scripts/checkstack.pl $(CHECKSTACK_ARCH)
1731 kernelrelease:
1732         @echo "$(KERNELVERSION)$$($(CONFIG_SHELL) $(srctree)/scripts/setlocalversion $(srctree))"
1734 kernelversion:
1735         @echo $(KERNELVERSION)
1737 image_name:
1738         @echo $(KBUILD_IMAGE)
1740 # Clear a bunch of variables before executing the submake
1742 ifeq ($(quiet),silent_)
1743 tools_silent=s
1744 endif
1746 tools/: FORCE
1747         $(Q)mkdir -p $(objtree)/tools
1748         $(Q)$(MAKE) LDFLAGS= MAKEFLAGS="$(tools_silent) $(filter --j% -j,$(MAKEFLAGS))" O=$(abspath $(objtree)) subdir=tools -C $(srctree)/tools/
1750 tools/%: FORCE
1751         $(Q)mkdir -p $(objtree)/tools
1752         $(Q)$(MAKE) LDFLAGS= MAKEFLAGS="$(tools_silent) $(filter --j% -j,$(MAKEFLAGS))" O=$(abspath $(objtree)) subdir=tools -C $(srctree)/tools/ $*
1754 # Single targets
1755 # ---------------------------------------------------------------------------
1756 # To build individual files in subdirectories, you can do like this:
1758 #   make foo/bar/baz.s
1760 # The supported suffixes for single-target are listed in 'single-targets'
1762 # To build only under specific subdirectories, you can do like this:
1764 #   make foo/bar/baz/
1766 ifdef single-build
1768 single-all := $(filter $(single-targets), $(MAKECMDGOALS))
1770 # .ko is special because modpost is needed
1771 single-ko := $(sort $(filter %.ko, $(single-all)))
1772 single-no-ko := $(sort $(patsubst %.ko,%.mod, $(single-all)))
1774 $(single-ko): single_modpost
1775         @:
1776 $(single-no-ko): descend
1777         @:
1779 ifeq ($(KBUILD_EXTMOD),)
1780 # For the single build of in-tree modules, use a temporary file to avoid
1781 # the situation of modules_install installing an invalid modules.order.
1782 MODORDER := .modules.tmp
1783 endif
1785 PHONY += single_modpost
1786 single_modpost: $(single-no-ko)
1787         $(Q){ $(foreach m, $(single-ko), echo $(extmod-prefix)$m;) } > $(MODORDER)
1788         $(Q)$(MAKE) -f $(srctree)/scripts/Makefile.modpost
1790 KBUILD_MODULES := 1
1792 export KBUILD_SINGLE_TARGETS := $(addprefix $(extmod-prefix), $(single-no-ko))
1794 single-build = $(if $(filter-out $@/, $(single-no-ko)),1)
1796 endif
1798 # FIXME Should go into a make.lib or something
1799 # ===========================================================================
1801 quiet_cmd_rmdirs = $(if $(wildcard $(rm-dirs)),CLEAN   $(wildcard $(rm-dirs)))
1802       cmd_rmdirs = rm -rf $(rm-dirs)
1804 quiet_cmd_rmfiles = $(if $(wildcard $(rm-files)),CLEAN   $(wildcard $(rm-files)))
1805       cmd_rmfiles = rm -f $(rm-files)
1807 # Run depmod only if we have System.map and depmod is executable
1808 quiet_cmd_depmod = DEPMOD  $(KERNELRELEASE)
1809       cmd_depmod = $(CONFIG_SHELL) $(srctree)/scripts/depmod.sh $(DEPMOD) \
1810                    $(KERNELRELEASE)
1812 # read saved command lines for existing targets
1813 existing-targets := $(wildcard $(sort $(targets)))
1815 -include $(foreach f,$(existing-targets),$(dir $(f)).$(notdir $(f)).cmd)
1817 endif # config-targets
1818 endif # mixed-build
1819 endif # need-sub-make
1821 PHONY += FORCE
1822 FORCE:
1824 # Declare the contents of the PHONY variable as phony.  We keep that
1825 # information in a variable so we can use it in if_changed and friends.
1826 .PHONY: $(PHONY)