summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 8be7375)
raw | patch | inline | side by side (parent: 8be7375)
author | Ard Biesheuvel <ard.biesheuvel@linaro.org> | |
Mon, 18 Apr 2016 15:09:48 +0000 (17:09 +0200) | ||
committer | Ard Biesheuvel <ard.biesheuvel@linaro.org> | |
Fri, 29 Jul 2016 16:59:49 +0000 (18:59 +0200) |
Currently, our KASLR implementation randomizes the placement of the core
kernel at 2 MB granularity. This is based on the arm64 kernel boot
protocol, which mandates that the kernel is loaded TEXT_OFFSET bytes above
a 2 MB aligned base address. This requirement is a result of the fact that
the block size used by the early mapping code may be 2 MB at the most (for
a 4 KB granule kernel)
But we can do better than that: since a KASLR kernel needs to be relocated
in any case, we can tolerate a physical misalignment as long as the virtual
misalignment relative to this 2 MB block size is equal in size, and code to
deal with this is already in place.
Since we align the kernel segments to 64 KB, let's randomize the physical
offset at 64 KB granularity as well (unless CONFIG_DEBUG_ALIGN_RODATA is
enabled). This way, the page table and TLB footprint is not affected.
The higher granularity allows for 5 bits of additional entropy to be used.
Reviewed-by: Matt Fleming <matt@codeblueprint.co.uk>
Signed-off-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
Signed-off-by: Will Deacon <will.deacon@arm.com>
(cherry picked from commit 6f26b3671184c36d07eb5d61ba9a6d0aeb583c5d)
Signed-off-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
kernel at 2 MB granularity. This is based on the arm64 kernel boot
protocol, which mandates that the kernel is loaded TEXT_OFFSET bytes above
a 2 MB aligned base address. This requirement is a result of the fact that
the block size used by the early mapping code may be 2 MB at the most (for
a 4 KB granule kernel)
But we can do better than that: since a KASLR kernel needs to be relocated
in any case, we can tolerate a physical misalignment as long as the virtual
misalignment relative to this 2 MB block size is equal in size, and code to
deal with this is already in place.
Since we align the kernel segments to 64 KB, let's randomize the physical
offset at 64 KB granularity as well (unless CONFIG_DEBUG_ALIGN_RODATA is
enabled). This way, the page table and TLB footprint is not affected.
The higher granularity allows for 5 bits of additional entropy to be used.
Reviewed-by: Matt Fleming <matt@codeblueprint.co.uk>
Signed-off-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
Signed-off-by: Will Deacon <will.deacon@arm.com>
(cherry picked from commit 6f26b3671184c36d07eb5d61ba9a6d0aeb583c5d)
Signed-off-by: Ard Biesheuvel <ard.biesheuvel@linaro.org>
drivers/firmware/efi/libstub/arm64-stub.c | patch | blob | history |
index e0e6b74fef8f7becdef4c0481919ead298023250..377d935a33803402c0c8a8d1085023e364368713 100644 (file)
kernel_memsize = kernel_size + (_end - _edata);
if (IS_ENABLED(CONFIG_RANDOMIZE_BASE) && phys_seed != 0) {
+ /*
+ * If CONFIG_DEBUG_ALIGN_RODATA is not set, produce a
+ * displacement in the interval [0, MIN_KIMG_ALIGN) that
+ * is a multiple of the minimal segment alignment (SZ_64K)
+ */
+ u32 mask = (MIN_KIMG_ALIGN - 1) & ~(SZ_64K - 1);
+ u32 offset = !IS_ENABLED(CONFIG_DEBUG_ALIGN_RODATA) ?
+ (phys_seed >> 32) & mask : TEXT_OFFSET;
+
/*
* If KASLR is enabled, and we have some randomness available,
* locate the kernel at a randomized offset in physical memory.
*/
- *reserve_size = kernel_memsize + TEXT_OFFSET;
+ *reserve_size = kernel_memsize + offset;
status = efi_random_alloc(sys_table_arg, *reserve_size,
MIN_KIMG_ALIGN, reserve_addr,
- phys_seed);
+ (u32)phys_seed);
- *image_addr = *reserve_addr + TEXT_OFFSET;
+ *image_addr = *reserve_addr + offset;
} else {
/*
* Else, try a straight allocation at the preferred offset.