summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 1c0232f)
raw | patch | inline | side by side (parent: 1c0232f)
author | Lu Baolu <baolu.lu@linux.intel.com> | |
Tue, 26 Jan 2016 15:50:05 +0000 (17:50 +0200) | ||
committer | Sasha Levin <sasha.levin@oracle.com> | |
Mon, 15 Feb 2016 20:45:33 +0000 (15:45 -0500) |
[ Upstream commit fa89537783cb442263fa5a14df6c7693eaf32f11 ]
Commit abce329c27b3 ("xhci: Workaround to get D3 working in Intel xHCI")
adds a workaround for a limitation of PME storm caused by SSIC port in
some Intel SoCs. This commit only handled one SSIC port, while there
are actually two SSIC ports in the chips. This patch handles both SSIC
ports. Without this fix, users still see PME storm.
Cc: stable@vger.kernel.org # v4.2+
Signed-off-by: Zhuang Jin Can <jin.can.zhuang@intel.com>
Signed-off-by: Lu Baolu <baolu.lu@linux.intel.com>
Signed-off-by: Mathias Nyman <mathias.nyman@linux.intel.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Signed-off-by: Sasha Levin <sasha.levin@oracle.com>
Commit abce329c27b3 ("xhci: Workaround to get D3 working in Intel xHCI")
adds a workaround for a limitation of PME storm caused by SSIC port in
some Intel SoCs. This commit only handled one SSIC port, while there
are actually two SSIC ports in the chips. This patch handles both SSIC
ports. Without this fix, users still see PME storm.
Cc: stable@vger.kernel.org # v4.2+
Signed-off-by: Zhuang Jin Can <jin.can.zhuang@intel.com>
Signed-off-by: Lu Baolu <baolu.lu@linux.intel.com>
Signed-off-by: Mathias Nyman <mathias.nyman@linux.intel.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Signed-off-by: Sasha Levin <sasha.levin@oracle.com>
drivers/usb/host/xhci-pci.c | patch | blob | history |
index dd41053afd6fe22286eb66fb095310f6b704da70..0c59cf11d88d318b9cd796479a875564f9f86ab1 100644 (file)
#include "xhci.h"
#include "xhci-trace.h"
-#define PORT2_SSIC_CONFIG_REG2 0x883c
+#define SSIC_PORT_NUM 2
+#define SSIC_PORT_CFG2 0x880c
+#define SSIC_PORT_CFG2_OFFSET 0x30
#define PROG_DONE (1 << 30)
#define SSIC_PORT_UNUSED (1 << 31)
struct pci_dev *pdev = to_pci_dev(hcd->self.controller);
u32 val;
void __iomem *reg;
+ int i;
if (pdev->vendor == PCI_VENDOR_ID_INTEL &&
pdev->device == PCI_DEVICE_ID_INTEL_CHERRYVIEW_XHCI) {
- reg = (void __iomem *) xhci->cap_regs + PORT2_SSIC_CONFIG_REG2;
-
- /* Notify SSIC that SSIC profile programming is not done */
- val = readl(reg) & ~PROG_DONE;
- writel(val, reg);
-
- /* Mark SSIC port as unused(suspend) or used(resume) */
- val = readl(reg);
- if (suspend)
- val |= SSIC_PORT_UNUSED;
- else
- val &= ~SSIC_PORT_UNUSED;
- writel(val, reg);
-
- /* Notify SSIC that SSIC profile programming is done */
- val = readl(reg) | PROG_DONE;
- writel(val, reg);
- readl(reg);
+ for (i = 0; i < SSIC_PORT_NUM; i++) {
+ reg = (void __iomem *) xhci->cap_regs +
+ SSIC_PORT_CFG2 +
+ i * SSIC_PORT_CFG2_OFFSET;
+
+ /*
+ * Notify SSIC that SSIC profile programming
+ * is not done.
+ */
+ val = readl(reg) & ~PROG_DONE;
+ writel(val, reg);
+
+ /* Mark SSIC port as unused(suspend) or used(resume) */
+ val = readl(reg);
+ if (suspend)
+ val |= SSIC_PORT_UNUSED;
+ else
+ val &= ~SSIC_PORT_UNUSED;
+ writel(val, reg);
+
+ /* Notify SSIC that SSIC profile programming is done */
+ val = readl(reg) | PROG_DONE;
+ writel(val, reg);
+ readl(reg);
+ }
}
reg = (void __iomem *) xhci->cap_regs + 0x80a4;