summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 4d5af83)
raw | patch | inline | side by side (parent: 4d5af83)
author | Michael J. Ruhl <michael.j.ruhl@intel.com> | |
Thu, 20 Sep 2018 19:59:14 +0000 (12:59 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Sat, 20 Oct 2018 07:48:54 +0000 (09:48 +0200) |
commit b4a4957d3d1c328b733fce783b7264996f866ad2 upstream.
rvt_destroy_qp() cannot complete until all in process packets have
been released from the underlying hardware. If a link down event
occurs, an application can hang with a kernel stack similar to:
cat /proc/<app PID>/stack
quiesce_qp+0x178/0x250 [hfi1]
rvt_reset_qp+0x23d/0x400 [rdmavt]
rvt_destroy_qp+0x69/0x210 [rdmavt]
ib_destroy_qp+0xba/0x1c0 [ib_core]
nvme_rdma_destroy_queue_ib+0x46/0x80 [nvme_rdma]
nvme_rdma_free_queue+0x3c/0xd0 [nvme_rdma]
nvme_rdma_destroy_io_queues+0x88/0xd0 [nvme_rdma]
nvme_rdma_error_recovery_work+0x52/0xf0 [nvme_rdma]
process_one_work+0x17a/0x440
worker_thread+0x126/0x3c0
kthread+0xcf/0xe0
ret_from_fork+0x58/0x90
0xffffffffffffffff
quiesce_qp() waits until all outstanding packets have been freed.
This wait should be momentary. During a link down event, the cleanup
handling does not ensure that all packets caught by the link down are
flushed properly.
This is caused by the fact that the freeze path and the link down
event is handled the same. This is not correct. The freeze path
waits until the HFI is unfrozen and then restarts PIO. A link down
is not a freeze event. The link down path cannot restart the PIO
until link is restored. If the PIO path is restarted before the link
comes up, the application (QP) using the PIO path will hang (until
link is restored).
Fix by separating the linkdown path from the freeze path and use the
link down path for link down events.
Close a race condition sc_disable() by acquiring both the progress
and release locks.
Close a race condition in sc_stop() by moving the setting of the flag
bits under the alloc lock.
Cc: <stable@vger.kernel.org> # 4.9.x+
Fixes: 7724105686e7 ("IB/hfi1: add driver files")
Reviewed-by: Mike Marciniszyn <mike.marciniszyn@intel.com>
Signed-off-by: Michael J. Ruhl <michael.j.ruhl@intel.com>
Signed-off-by: Dennis Dalessandro <dennis.dalessandro@intel.com>
Signed-off-by: Jason Gunthorpe <jgg@mellanox.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
rvt_destroy_qp() cannot complete until all in process packets have
been released from the underlying hardware. If a link down event
occurs, an application can hang with a kernel stack similar to:
cat /proc/<app PID>/stack
quiesce_qp+0x178/0x250 [hfi1]
rvt_reset_qp+0x23d/0x400 [rdmavt]
rvt_destroy_qp+0x69/0x210 [rdmavt]
ib_destroy_qp+0xba/0x1c0 [ib_core]
nvme_rdma_destroy_queue_ib+0x46/0x80 [nvme_rdma]
nvme_rdma_free_queue+0x3c/0xd0 [nvme_rdma]
nvme_rdma_destroy_io_queues+0x88/0xd0 [nvme_rdma]
nvme_rdma_error_recovery_work+0x52/0xf0 [nvme_rdma]
process_one_work+0x17a/0x440
worker_thread+0x126/0x3c0
kthread+0xcf/0xe0
ret_from_fork+0x58/0x90
0xffffffffffffffff
quiesce_qp() waits until all outstanding packets have been freed.
This wait should be momentary. During a link down event, the cleanup
handling does not ensure that all packets caught by the link down are
flushed properly.
This is caused by the fact that the freeze path and the link down
event is handled the same. This is not correct. The freeze path
waits until the HFI is unfrozen and then restarts PIO. A link down
is not a freeze event. The link down path cannot restart the PIO
until link is restored. If the PIO path is restarted before the link
comes up, the application (QP) using the PIO path will hang (until
link is restored).
Fix by separating the linkdown path from the freeze path and use the
link down path for link down events.
Close a race condition sc_disable() by acquiring both the progress
and release locks.
Close a race condition in sc_stop() by moving the setting of the flag
bits under the alloc lock.
Cc: <stable@vger.kernel.org> # 4.9.x+
Fixes: 7724105686e7 ("IB/hfi1: add driver files")
Reviewed-by: Mike Marciniszyn <mike.marciniszyn@intel.com>
Signed-off-by: Michael J. Ruhl <michael.j.ruhl@intel.com>
Signed-off-by: Dennis Dalessandro <dennis.dalessandro@intel.com>
Signed-off-by: Jason Gunthorpe <jgg@mellanox.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
drivers/infiniband/hw/hfi1/chip.c | patch | blob | history | |
drivers/infiniband/hw/hfi1/pio.c | patch | blob | history | |
drivers/infiniband/hw/hfi1/pio.h | patch | blob | history |
index 33cf1734c4e5d492766aa2a4e5e211a63766c11d..f9faacce925098b61ccae6a6100c1fd0a2beccd7 100644 (file)
struct hfi1_devdata *dd = ppd->dd;
struct send_context *sc;
int i;
+ int sc_flags;
if (flags & FREEZE_SELF)
write_csr(dd, CCE_CTRL, CCE_CTRL_SPC_FREEZE_SMASK);
/* notify all SDMA engines that they are going into a freeze */
sdma_freeze_notify(dd, !!(flags & FREEZE_LINK_DOWN));
+ sc_flags = SCF_FROZEN | SCF_HALTED | (flags & FREEZE_LINK_DOWN ?
+ SCF_LINK_DOWN : 0);
/* do halt pre-handling on all enabled send contexts */
for (i = 0; i < dd->num_send_contexts; i++) {
sc = dd->send_contexts[i].sc;
if (sc && (sc->flags & SCF_ENABLED))
- sc_stop(sc, SCF_FROZEN | SCF_HALTED);
+ sc_stop(sc, sc_flags);
}
/* Send context are frozen. Notify user space */
add_rcvctrl(dd, RCV_CTRL_RCV_PORT_ENABLE_SMASK);
handle_linkup_change(dd, 1);
+ pio_kernel_linkup(dd);
+
ppd->host_link_state = HLS_UP_INIT;
break;
case HLS_UP_ARMED:
index 19a8e6052820fec0344f3b81700017a49f21ab01..07bf282fd8aaf8c8db7f2f21406ddad5d493df6a 100644 (file)
void sc_disable(struct send_context *sc)
{
u64 reg;
- unsigned long flags;
struct pio_buf *pbuf;
if (!sc)
return;
/* do all steps, even if already disabled */
- spin_lock_irqsave(&sc->alloc_lock, flags);
+ spin_lock_irq(&sc->alloc_lock);
reg = read_kctxt_csr(sc->dd, sc->hw_context, SC(CTRL));
reg &= ~SC(CTRL_CTXT_ENABLE_SMASK);
sc->flags &= ~SCF_ENABLED;
sc_wait_for_packet_egress(sc, 1);
write_kctxt_csr(sc->dd, sc->hw_context, SC(CTRL), reg);
- spin_unlock_irqrestore(&sc->alloc_lock, flags);
/*
* Flush any waiters. Once the context is disabled,
* proceed with the flush.
*/
udelay(1);
- spin_lock_irqsave(&sc->release_lock, flags);
+ spin_lock(&sc->release_lock);
if (sc->sr) { /* this context has a shadow ring */
while (sc->sr_tail != sc->sr_head) {
pbuf = &sc->sr[sc->sr_tail].pbuf;
sc->sr_tail = 0;
}
}
- spin_unlock_irqrestore(&sc->release_lock, flags);
+ spin_unlock(&sc->release_lock);
+ spin_unlock_irq(&sc->alloc_lock);
}
/* return SendEgressCtxtStatus.PacketOccupancy */
sc = dd->send_contexts[i].sc;
if (!sc || !(sc->flags & SCF_FROZEN) || sc->type == SC_USER)
continue;
+ if (sc->flags & SCF_LINK_DOWN)
+ continue;
sc_enable(sc); /* will clear the sc frozen flag */
}
}
+/**
+ * pio_kernel_linkup() - Re-enable send contexts after linkup event
+ * @dd: valid devive data
+ *
+ * When the link goes down, the freeze path is taken. However, a link down
+ * event is different from a freeze because if the send context is re-enabled
+ * whowever is sending data will start sending data again, which will hang
+ * any QP that is sending data.
+ *
+ * The freeze path now looks at the type of event that occurs and takes this
+ * path for link down event.
+ */
+void pio_kernel_linkup(struct hfi1_devdata *dd)
+{
+ struct send_context *sc;
+ int i;
+
+ for (i = 0; i < dd->num_send_contexts; i++) {
+ sc = dd->send_contexts[i].sc;
+ if (!sc || !(sc->flags & SCF_LINK_DOWN) || sc->type == SC_USER)
+ continue;
+
+ sc_enable(sc); /* will clear the sc link down flag */
+ }
+}
+
/*
* Wait for the SendPioInitCtxt.PioInitInProgress bit to clear.
* Returns:
{
unsigned long flags;
- /* mark the context */
- sc->flags |= flag;
-
/* stop buffer allocations */
spin_lock_irqsave(&sc->alloc_lock, flags);
+ /* mark the context */
+ sc->flags |= flag;
sc->flags &= ~SCF_ENABLED;
spin_unlock_irqrestore(&sc->alloc_lock, flags);
wake_up(&sc->halt_wait);
index 99ca5edb0b435a3754c03693f779f9b391f7faf4..c7c4e6e5d317437c53a892c7cb50b6157d723290 100644 (file)
#define SCF_IN_FREE 0x02
#define SCF_HALTED 0x04
#define SCF_FROZEN 0x08
+#define SCF_LINK_DOWN 0x10
struct send_context_info {
struct send_context *sc; /* allocated working context */
void pio_reset_all(struct hfi1_devdata *dd);
void pio_freeze(struct hfi1_devdata *dd);
void pio_kernel_unfreeze(struct hfi1_devdata *dd);
+void pio_kernel_linkup(struct hfi1_devdata *dd);
/* global PIO send control operations */
#define PSC_GLOBAL_ENABLE 0