summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: c094e14)
raw | patch | inline | side by side (parent: c094e14)
author | Filipe Manana <fdmanana@suse.com> | |
Wed, 16 Oct 2019 15:28:52 +0000 (16:28 +0100) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Sun, 27 Oct 2019 20:32:33 +0000 (21:32 +0100) |
commit ba0b084ac309283db6e329785c1dc4f45fdbd379 upstream.
We were checking for the full fsync flag in the inode before locking the
inode, which is racy, since at that that time it might not be set but
after we acquire the inode lock some other task set it. One case where
this can happen is on a system low on memory and some concurrent task
failed to allocate an extent map and therefore set the full sync flag on
the inode, to force the next fsync to work in full mode.
A consequence of missing the full fsync flag set is hitting the problems
fixed by commit 0c713cbab620 ("Btrfs: fix race between ranged fsync and
writeback of adjacent ranges"), BUG_ON() when dropping extents from a log
tree, hitting assertion failures at tree-log.c:copy_items() or all sorts
of weird inconsistencies after replaying a log due to file extents items
representing ranges that overlap.
So just move the check such that it's done after locking the inode and
before starting writeback again.
Fixes: 0c713cbab620 ("Btrfs: fix race between ranged fsync and writeback of adjacent ranges")
CC: stable@vger.kernel.org # 5.2+
Signed-off-by: Filipe Manana <fdmanana@suse.com>
Signed-off-by: David Sterba <dsterba@suse.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
We were checking for the full fsync flag in the inode before locking the
inode, which is racy, since at that that time it might not be set but
after we acquire the inode lock some other task set it. One case where
this can happen is on a system low on memory and some concurrent task
failed to allocate an extent map and therefore set the full sync flag on
the inode, to force the next fsync to work in full mode.
A consequence of missing the full fsync flag set is hitting the problems
fixed by commit 0c713cbab620 ("Btrfs: fix race between ranged fsync and
writeback of adjacent ranges"), BUG_ON() when dropping extents from a log
tree, hitting assertion failures at tree-log.c:copy_items() or all sorts
of weird inconsistencies after replaying a log due to file extents items
representing ranges that overlap.
So just move the check such that it's done after locking the inode and
before starting writeback again.
Fixes: 0c713cbab620 ("Btrfs: fix race between ranged fsync and writeback of adjacent ranges")
CC: stable@vger.kernel.org # 5.2+
Signed-off-by: Filipe Manana <fdmanana@suse.com>
Signed-off-by: David Sterba <dsterba@suse.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
fs/btrfs/file.c | patch | blob | history |
diff --git a/fs/btrfs/file.c b/fs/btrfs/file.c
index c84186563c31121c76abf4445f39c7c6f848550d..4870440d6424a826e4e376123b155b641270a60e 100644 (file)
--- a/fs/btrfs/file.c
+++ b/fs/btrfs/file.c
@@ -2056,25 +2056,7 @@ int btrfs_sync_file(struct file *file, loff_t start, loff_t end, int datasync)
struct btrfs_trans_handle *trans;
struct btrfs_log_ctx ctx;
int ret = 0, err;
- u64 len;
- /*
- * If the inode needs a full sync, make sure we use a full range to
- * avoid log tree corruption, due to hole detection racing with ordered
- * extent completion for adjacent ranges, and assertion failures during
- * hole detection.
- */
- if (test_bit(BTRFS_INODE_NEEDS_FULL_SYNC,
- &BTRFS_I(inode)->runtime_flags)) {
- start = 0;
- end = LLONG_MAX;
- }
-
- /*
- * The range length can be represented by u64, we have to do the typecasts
- * to avoid signed overflow if it's [0, LLONG_MAX] eg. from fsync()
- */
- len = (u64)end - (u64)start + 1;
trace_btrfs_sync_file(file, datasync);
btrfs_init_log_ctx(&ctx, inode);
@@ -2100,6 +2082,19 @@ int btrfs_sync_file(struct file *file, loff_t start, loff_t end, int datasync)
atomic_inc(&root->log_batch);
+ /*
+ * If the inode needs a full sync, make sure we use a full range to
+ * avoid log tree corruption, due to hole detection racing with ordered
+ * extent completion for adjacent ranges, and assertion failures during
+ * hole detection. Do this while holding the inode lock, to avoid races
+ * with other tasks.
+ */
+ if (test_bit(BTRFS_INODE_NEEDS_FULL_SYNC,
+ &BTRFS_I(inode)->runtime_flags)) {
+ start = 0;
+ end = LLONG_MAX;
+ }
+
/*
* Before we acquired the inode's lock, someone may have dirtied more
* pages in the target range. We need to make sure that writeback for
@@ -2127,8 +2122,11 @@ int btrfs_sync_file(struct file *file, loff_t start, loff_t end, int datasync)
/*
* We have to do this here to avoid the priority inversion of waiting on
* IO of a lower priority task while holding a transaciton open.
+ *
+ * Also, the range length can be represented by u64, we have to do the
+ * typecasts to avoid signed overflow if it's [0, LLONG_MAX].
*/
- ret = btrfs_wait_ordered_range(inode, start, len);
+ ret = btrfs_wait_ordered_range(inode, start, (u64)end - (u64)start + 1);
if (ret) {
up_write(&BTRFS_I(inode)->dio_sem);
inode_unlock(inode);