summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 3b73a0e)
raw | patch | inline | side by side (parent: 3b73a0e)
author | Johan Hovold <johan@kernel.org> | |
Fri, 18 Oct 2019 15:19:54 +0000 (17:19 +0200) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Tue, 29 Oct 2019 08:19:47 +0000 (09:19 +0100) |
commit 7a6f22d7479b7a0b68eadd308a997dd64dda7dae upstream.
Fix broken read implementation, which could be used to trigger slab info
leaks.
The driver failed to check if the custom ring buffer was still empty
when waking up after having waited for more data. This would happen on
every interrupt-in completion, even if no data had been added to the
ring buffer (e.g. on disconnect events).
Due to missing sanity checks and uninitialised (kmalloced) ring-buffer
entries, this meant that huge slab info leaks could easily be triggered.
Note that the empty-buffer check after wakeup is enough to fix the info
leak on disconnect, but let's clear the buffer on allocation and add a
sanity check to read() to prevent further leaks.
Fixes: 2824bd250f0b ("[PATCH] USB: add ldusb driver")
Cc: stable <stable@vger.kernel.org> # 2.6.13
Reported-by: syzbot+6fe95b826644f7f12b0b@syzkaller.appspotmail.com
Signed-off-by: Johan Hovold <johan@kernel.org>
Link: https://lore.kernel.org/r/20191018151955.25135-2-johan@kernel.org
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Fix broken read implementation, which could be used to trigger slab info
leaks.
The driver failed to check if the custom ring buffer was still empty
when waking up after having waited for more data. This would happen on
every interrupt-in completion, even if no data had been added to the
ring buffer (e.g. on disconnect events).
Due to missing sanity checks and uninitialised (kmalloced) ring-buffer
entries, this meant that huge slab info leaks could easily be triggered.
Note that the empty-buffer check after wakeup is enough to fix the info
leak on disconnect, but let's clear the buffer on allocation and add a
sanity check to read() to prevent further leaks.
Fixes: 2824bd250f0b ("[PATCH] USB: add ldusb driver")
Cc: stable <stable@vger.kernel.org> # 2.6.13
Reported-by: syzbot+6fe95b826644f7f12b0b@syzkaller.appspotmail.com
Signed-off-by: Johan Hovold <johan@kernel.org>
Link: https://lore.kernel.org/r/20191018151955.25135-2-johan@kernel.org
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
drivers/usb/misc/ldusb.c | patch | blob | history |
index c59a1a48260c8b7cb99809e382ab9ea208d67989..6b3a6fd7d271dd021fb3cac3dccfe7938c3c604f 100644 (file)
--- a/drivers/usb/misc/ldusb.c
+++ b/drivers/usb/misc/ldusb.c
@@ -464,7 +464,7 @@ static ssize_t ld_usb_read(struct file *file, char __user *buffer, size_t count,
/* wait for data */
spin_lock_irq(&dev->rbsl);
- if (dev->ring_head == dev->ring_tail) {
+ while (dev->ring_head == dev->ring_tail) {
dev->interrupt_in_done = 0;
spin_unlock_irq(&dev->rbsl);
if (file->f_flags & O_NONBLOCK) {
@@ -474,12 +474,17 @@ static ssize_t ld_usb_read(struct file *file, char __user *buffer, size_t count,
retval = wait_event_interruptible(dev->read_wait, dev->interrupt_in_done);
if (retval < 0)
goto unlock_exit;
- } else {
- spin_unlock_irq(&dev->rbsl);
+
+ spin_lock_irq(&dev->rbsl);
}
+ spin_unlock_irq(&dev->rbsl);
/* actual_buffer contains actual_length + interrupt_in_buffer */
actual_buffer = (size_t *)(dev->ring_buffer + dev->ring_tail * (sizeof(size_t)+dev->interrupt_in_endpoint_size));
+ if (*actual_buffer > dev->interrupt_in_endpoint_size) {
+ retval = -EIO;
+ goto unlock_exit;
+ }
bytes_to_read = min(count, *actual_buffer);
if (bytes_to_read < *actual_buffer)
dev_warn(&dev->intf->dev, "Read buffer overflow, %zd bytes dropped\n",
@@ -690,10 +695,9 @@ static int ld_usb_probe(struct usb_interface *intf, const struct usb_device_id *
dev_warn(&intf->dev, "Interrupt out endpoint not found (using control endpoint instead)\n");
dev->interrupt_in_endpoint_size = usb_endpoint_maxp(dev->interrupt_in_endpoint);
- dev->ring_buffer =
- kmalloc_array(ring_buffer_size,
- sizeof(size_t) + dev->interrupt_in_endpoint_size,
- GFP_KERNEL);
+ dev->ring_buffer = kcalloc(ring_buffer_size,
+ sizeof(size_t) + dev->interrupt_in_endpoint_size,
+ GFP_KERNEL);
if (!dev->ring_buffer)
goto error;
dev->interrupt_in_buffer = kmalloc(dev->interrupt_in_endpoint_size, GFP_KERNEL);