summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 5b67a47)
raw | patch | inline | side by side (parent: 5b67a47)
author | Vincent Chen <vincent.chen@sifive.com> | |
Mon, 16 Sep 2019 08:47:41 +0000 (16:47 +0800) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Fri, 11 Oct 2019 16:21:29 +0000 (18:21 +0200) |
[ Upstream commit c82dd6d078a2bb29d41eda032bb96d05699a524d ]
When the handle_exception function addresses an exception, the interrupts
will be unconditionally enabled after finishing the context save. However,
It may erroneously enable the interrupts if the interrupts are disabled
before entering the handle_exception.
For example, one of the WARN_ON() condition is satisfied in the scheduling
where the interrupt is disabled and rq.lock is locked. The WARN_ON will
trigger a break exception and the handle_exception function will enable the
interrupts before entering do_trap_break function. During the procedure, if
a timer interrupt is pending, it will be taken when interrupts are enabled.
In this case, it may cause a deadlock problem if the rq.lock is locked
again in the timer ISR.
Hence, the handle_exception() can only enable interrupts when the state of
sstatus.SPIE is 1.
This patch is tested on HiFive Unleashed board.
Signed-off-by: Vincent Chen <vincent.chen@sifive.com>
Reviewed-by: Palmer Dabbelt <palmer@sifive.com>
[paul.walmsley@sifive.com: updated to apply]
Fixes: bcae803a21317 ("RISC-V: Enable IRQ during exception handling")
Cc: David Abdurachmanov <david.abdurachmanov@sifive.com>
Cc: stable@vger.kernel.org
Signed-off-by: Paul Walmsley <paul.walmsley@sifive.com>
Signed-off-by: Sasha Levin <sashal@kernel.org>
When the handle_exception function addresses an exception, the interrupts
will be unconditionally enabled after finishing the context save. However,
It may erroneously enable the interrupts if the interrupts are disabled
before entering the handle_exception.
For example, one of the WARN_ON() condition is satisfied in the scheduling
where the interrupt is disabled and rq.lock is locked. The WARN_ON will
trigger a break exception and the handle_exception function will enable the
interrupts before entering do_trap_break function. During the procedure, if
a timer interrupt is pending, it will be taken when interrupts are enabled.
In this case, it may cause a deadlock problem if the rq.lock is locked
again in the timer ISR.
Hence, the handle_exception() can only enable interrupts when the state of
sstatus.SPIE is 1.
This patch is tested on HiFive Unleashed board.
Signed-off-by: Vincent Chen <vincent.chen@sifive.com>
Reviewed-by: Palmer Dabbelt <palmer@sifive.com>
[paul.walmsley@sifive.com: updated to apply]
Fixes: bcae803a21317 ("RISC-V: Enable IRQ during exception handling")
Cc: David Abdurachmanov <david.abdurachmanov@sifive.com>
Cc: stable@vger.kernel.org
Signed-off-by: Paul Walmsley <paul.walmsley@sifive.com>
Signed-off-by: Sasha Levin <sashal@kernel.org>
arch/riscv/kernel/entry.S | patch | blob | history |
index fa2c08e3c05e6ee74ea0258b62cdf6580f98a385..a03821b2656aa80d8879ae614ce67ae47b40ad04 100644 (file)
move a1, s4 /* scause */
tail do_IRQ
1:
- /* Exceptions run with interrupts enabled */
+ /* Exceptions run with interrupts enabled or disabled
+ depending on the state of sstatus.SR_SPIE */
+ andi t0, s1, SR_SPIE
+ beqz t0, 1f
csrs sstatus, SR_SIE
+1:
/* Handle syscalls */
li t0, EXC_SYSCALL
beq s4, t0, handle_syscall