]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-linux-kernel/ti-linux-kernel-next.git/commit
dmaengine: Add transfer termination synchronization support
authorLars-Peter Clausen <lars@metafoo.de>
Tue, 20 Oct 2015 09:46:28 +0000 (11:46 +0200)
committerVinod Koul <vinod.koul@intel.com>
Mon, 16 Nov 2015 02:58:52 +0000 (08:28 +0530)
commitb36f09c3c441a6e59eab9315032e7d546571de3f
tree10d0bed70e0ea6086ce00f94162c2e02dc8b4221
parent8005c49d9aea74d382f474ce11afbbc7d7130bec
dmaengine: Add transfer termination synchronization support

The DMAengine API has a long standing race condition that is inherent to
the API itself. Calling dmaengine_terminate_all() is supposed to stop and
abort any pending or active transfers that have previously been submitted.
Unfortunately it is possible that this operation races against a currently
running (or with some drivers also scheduled) completion callback.

Since the API allows dmaengine_terminate_all() to be called from atomic
context as well as from within a completion callback it is not possible to
synchronize to the execution of the completion callback from within
dmaengine_terminate_all() itself.

This means that a user of the DMAengine API does not know when it is safe
to free resources used in the completion callback, which can result in a
use-after-free race condition.

This patch addresses the issue by introducing an explicit synchronization
primitive to the DMAengine API called dmaengine_synchronize().

The existing dmaengine_terminate_all() is deprecated in favor of
dmaengine_terminate_sync() and dmaengine_terminate_async(). The former
aborts all pending and active transfers and synchronizes to the current
context, meaning it will wait until all running completion callbacks have
finished. This means it is only possible to call this function from
non-atomic context. The later function does not synchronize, but can still
be used in atomic context or from within a complete callback. It has to be
followed up by dmaengine_synchronize() before a client can free the
resources used in a completion callback.

In addition to this the semantics of the device_terminate_all() callback
are slightly relaxed by this patch. It is now OK for a driver to only
schedule the termination of the active transfer, but does not necessarily
have to wait until the DMA controller has completely stopped. The driver
must ensure though that the controller has stopped and no longer accesses
any memory when the device_synchronize() callback returns.

This was in part done since most drivers do not pay attention to this
anyway at the moment and to emphasize that this needs to be done when the
device_synchronize() callback is implemented. But it also helps with
implementing support for devices where stopping the controller can require
operations that may sleep.

Signed-off-by: Lars-Peter Clausen <lars@metafoo.de>
Signed-off-by: Vinod Koul <vinod.koul@intel.com>
Documentation/dmaengine/client.txt
Documentation/dmaengine/provider.txt
drivers/dma/dmaengine.c
include/linux/dmaengine.h