]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-linux-kernel/ti-linux-kernel-next.git/shortlog
ti-linux-kernel/ti-linux-kernel-next.git
2018-11-20 LCPD Auto MergerMerge branch 'linux-4.19.y' of http://git.kernel.org... ti-linux-4.14.y-next-20181120 ti-linux-4.19.y-next-20181120
2018-11-19 Greg Kroah... Linux 4.19.3-rc1
2018-11-19 Stefano StabelliniCONFIG_XEN_PV breaks xen_create_contiguous_region on ARM
2018-11-19 Ville Syrjälädrm/i915: Fix hpd handling for pins with two encoders
2018-11-19 Lyude Pauldrm/i915: Fix NULL deref when re-enabling HPD IRQs...
2018-11-19 Lyude Pauldrm/i915: Fix possible race in intel_dp_add_mst_connector()
2018-11-19 Chris Wilsondrm/i915/execlists: Force write serialisation into...
2018-11-19 Chris Wilsondrm/i915/ringbuffer: Delay after EMIT_INVALIDATE for...
2018-11-19 Chris Wilsondrm/i915: Mark pin flags as u64
2018-11-19 Ville Syrjälädrm/i915: Don't oops during modeset shutdown after...
2018-11-19 Chris Wilsondrm/i915: Compare user's 64b GTT offset even on 32b
2018-11-19 Ville Syrjälädrm/i915: Fix ilk+ watermarks when disabling pipes
2018-11-19 Ville Syrjälädrm/i915: Fix error handling for the NV12 fb dimensions...
2018-11-19 Chris Wilsondrm/i915: Mark up GTT sizes as u64
2018-11-19 Clint Taylordrm/i915/hdmi: Add HDMI 2.0 audio clock recovery N...
2018-11-19 Manasi Navaredrm/i915/icl: Fix the macros for DFLEXDPMLE register...
2018-11-19 Dhinakaran... drm/i915/dp: Restrict link retrain workaround to extern...
2018-11-19 Dhinakaran... drm/i915/dp: Fix link retraining comment in intel_dp_lo...
2018-11-19 Chris Wilsondrm/i915: Large page offsets for pread/pwrite
2018-11-19 Lyude Pauldrm/i915: Skip vcpi allocation for MSTB ports that...
2018-11-19 Lyude Pauldrm/i915: Don't unset intel_connector->mst_port
2018-11-19 Ville Syrjälädrm/i915: Restore vblank interrupts earlier
2018-11-19 Ville Syrjälädrm/i915: Use the correct crtc when sanitizing plane...
2018-11-19 Manasi Navaredrm/i915/dp: Link train Fallback on eDP only if fallbac...
2018-11-19 Hans de Goededrm: panel-orientation-quirks: Add quirk for Acer One...
2018-11-19 Lyude Pauldrm/atomic_helper: Disallow new modesets on unregistere...
2018-11-19 Stanislav Lisovskiydrm/dp_mst: Check if primary mstb is null
2018-11-19 Lucas Stachdrm/etnaviv: fix bogus fence complete check in timeout...
2018-11-19 Akshu Agrawaldrm/amd/powerplay: Enable/Disable NBPSTATE on On/OFF...
2018-11-19 Lyude Pauldrm/nouveau: Fix nv50_mstc->best_encoder()
2018-11-19 Lyude Pauldrm/nouveau: Check backlight IDs are >= 0, not > 0
2018-11-19 Lyude Pauldrm/amdgpu: Suppress keypresses from ACPI_VIDEO events
2018-11-19 Alex Deucherdrm/amdgpu: add missing CHIP_HAINAN in amdgpu_ucode_get...
2018-11-19 Rex Zhudrm/amdgpu: Fix typo in amdgpu_vmid_mgr_init
2018-11-19 Marc Zyngierdrm/rockchip: Allow driver to be shutdown on reboot...
2018-11-19 Uwe Kleine... scripts/spdxcheck.py: make python3 compliant
2018-11-19 Roman Gushchinmm: don't reclaim inodes with many attached pages
2018-11-19 Ard Biesheuvelefi/arm/libstub: Pack FDT after populating it
2018-11-19 Vasily Averinmm/swapfile.c: use kvzalloc for swap_info_struct allocation
2018-11-19 Mike Kravetzhugetlbfs: fix kernel BUG at fs/hugetlbfs/inode.c:444!
2018-11-19 Arnd Bergmannlib/ubsan.c: don't mark __ubsan_handle_builtin_unreacha...
2018-11-19 Eric Biggerscrypto: user - fix leaking uninitialized memory to...
2018-11-19 Diego Violalibata: blacklist SAMSUNG MZ7TD256HAFV-000L9 SSD
2018-11-19 Andreas Gruenbachergfs2: Fix metadata read-ahead during truncate (2)
2018-11-19 Andreas Gruenbachergfs2: Put bitmap buffers in put_super
2018-11-19 Ondrej Mosnacekselinux: check length properly in SCTP bind hook
2018-11-19 Miklos Szeredifuse: fix possibly missed wake-up after abort
2018-11-19 Miklos Szeredifuse: fix leaked notify reply
2018-11-19 Lukas Czernerfuse: fix use-after-free in fuse_direct_IO()
2018-11-19 Maciej W. Rozyckirtc: hctosys: Add missing range error reporting
2018-11-19 Scott Mayhewnfsd: COPY and CLONE operations require the saved fileh...
2018-11-19 Trond MyklebustNFSv4: Don't exit the state manager without clearing...
2018-11-19 Frank Sorensonsunrpc: correct the computation for page_ptr when trunc...
2018-11-19 Christophe... kdb: print real address of pointers instead of hashed...
2018-11-19 Christophe... kdb: use correct pointer when 'btc' calls 'btt'
2018-11-19 Ulf HanssonARM: cpuidle: Don't register the driver when back-end...
2018-11-19 Dmitry V. Levinuapi: fix linux/kfd_ioctl.h userspace compilation errors
2018-11-19 Benjamin Coddingtonmnt: fix __detach_mounts infinite loop
2018-11-19 Eric W. Biedermanmount: Prevent MNT_DETACH from disconnecting locked...
2018-11-19 Eric W. Biedermanmount: Don't allow copying MNT_UNBINDABLE|MNT_LOCKED...
2018-11-19 Eric W. Biedermanmount: Retest MNT_LOCKED in do_umount
2018-11-19 Vasily Averinext4: fix buffer leak in __ext4_read_dirblock() on...
2018-11-19 Vasily Averinext4: fix buffer leak in ext4_expand_extra_isize_ea...
2018-11-19 Vasily Averinext4: fix buffer leak in ext4_xattr_move_to_block(...
2018-11-19 Vasily Averinext4: release bs.bh before re-using in ext4_xattr_block...
2018-11-19 Vasily Averinext4: fix buffer leak in ext4_xattr_get_block() on...
2018-11-19 Vasily Averinext4: fix possible leak of s_journal_flag_rwsem in...
2018-11-19 Theodore Ts'oext4: fix possible leak of sbi->s_group_desc_leak in...
2018-11-19 Theodore Ts'oext4: avoid possible double brelse() in add_new_gdb...
2018-11-19 Vasily Averinext4: fix missing cleanup if ext4_alloc_flex_bg_array...
2018-11-19 Vasily Averinext4: avoid buffer leak in ext4_orphan_add() after...
2018-11-19 Vasily Averinext4: avoid buffer leak on shutdown in ext4_mark_iloc_d...
2018-11-19 Vasily Averinext4: fix possible inode leak in the retry loop of...
2018-11-19 Vasily Averinext4: missing !bh check in ext4_xattr_inode_write()
2018-11-19 Vasily Averinext4: avoid potential extra brelse in setup_new_flex_gr...
2018-11-19 Vasily Averinext4: add missing brelse() add_new_gdb_meta_bg()'s...
2018-11-19 Vasily Averinext4: add missing brelse() in set_flexbg_block_bitmap...
2018-11-19 Vasily Averinext4: add missing brelse() update_backups()'s error...
2018-11-19 Michael Kelleyclockevents/drivers/i8253: Add support for PIT shutdown...
2018-11-19 Shaokun Zhangbtrfs: tree-checker: Fix misleading group system inform...
2018-11-19 Filipe MananaBtrfs: fix data corruption due to cloning of eof block
2018-11-19 Filipe MananaBtrfs: fix infinite loop on inode eviction after dedupl...
2018-11-19 Robbie KoBtrfs: fix cur_offset in the error case for nocow
2018-11-19 Filipe MananaBtrfs: fix missing data checksums after a ranged fsync...
2018-11-19 Lu Fengqibtrfs: fix pinned underflow after transaction aborted
2018-11-19 Mathieu Malaterrewatchdog/core: Add missing prototypes for weak functions
2018-11-19 H. Peter Anvin... arch/alpha, termios: implement BOTHER, IBSHIFT and...
2018-11-19 H. Peter Anvintermios, tty/tty_baudrate.c: fix buffer overrun
2018-11-19 Michael Kelleyx86/hyper-v: Enable PIT shutdown quirk
2018-11-19 Steven Rostedt... x86/cpu/vmware: Do not trace vmware_sched_clock()
2018-11-19 John Garryof, numa: Validate some distance map rules
2018-11-19 Adrian Hunterperf intel-pt: Insert callchain context into synthesize...
2018-11-19 Adrian Hunterperf intel-pt/bts: Calculate cpumode for synthesized...
2018-11-19 David S. Millerperf callchain: Honour the ordering of PERF_CONTEXT_...
2018-11-19 Thomas Richterperf stat: Handle different PMU names with common prefix
2018-11-19 Leo Yanperf cs-etm: Correct CPU mode for samples
2018-11-19 Dmitry Osipenkohwmon: (core) Fix double-free in __hwmon_device_register()
2018-11-19 Arnd Bergmannmtd: docg3: don't set conflicting BCH_CONST_PARAMS...
2018-11-19 Boris Brezillonmtd: nand: Fix nanddev_neraseblocks()
2018-11-19 Christophe... mtd: spi-nor: cadence-quadspi: Return error code in...
next