]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-linux-kernel/ti-linux-kernel-next.git/shortlog
ti-linux-kernel/ti-linux-kernel-next.git
2018-04-11 LCPD Auto MergerMerge branch 'ti-linux-4.14.y-next' of git.ti.com:ti... ti-rt-linux-4.14.y-next-20180411
2018-04-11 LCPD Auto MergerMerge branch 'ti-linux-4.14.y-for-next' of git://git... ti-linux-4.14.y-next-20180411
2018-04-11 LCPD Auto MergerMerge branch 'ti-linux-4.14.y-for-next' of git://git...
2018-04-11 LCPD Auto MergerMerge branch 'rpmsg-ti-linux-4.14.y-next' of git:/...
2018-04-11 LCPD Auto MergerMerge branch 'linux-4.14.y' of http://git.kernel.org...
2018-04-10 Greg Kroah... Linux 4.14.34-rc1
2018-04-10 Moshe Shemeshnet/mlx4_core: Fix memory leak while delete slave's...
2018-04-10 Jason Wangvhost_net: add missing lock nesting notation
2018-04-10 Xin Longteam: move dev_mc_sync after master_upper_dev_link...
2018-04-10 Xin Longroute: check sysctl_fib_multipath_use_neigh earlier...
2018-04-10 Jason Wangvhost: validate log when IOTLB is enabled
2018-04-10 Roi Dayannet/mlx5e: Fix traffic being dropped on VF representor
2018-04-10 Eran Ben Elishanet/mlx4_en: Fix mixed PFC and Global pause user contro...
2018-04-10 Dave Watsonstrparser: Fix sign of err codes
2018-04-10 Davide Carattinet/sched: fix NULL dereference on the error path of...
2018-04-10 Davide Carattinet/sched: fix NULL dereference in the error path of...
2018-04-10 Shahar Kleinnet/mlx5e: Sync netdev vxlan ports at open
2018-04-10 Jianbo Liunet/mlx5e: Don't override vport admin link state in...
2018-04-10 David Lebrunipv6: sr: fix seg6 encap performances with TSO enabled
2018-04-10 Dirk van der... nfp: use full 40 bits of the NSP buffer address
2018-04-10 Jianbo Liunet/mlx5e: Fix memory usage issues in offloading TC...
2018-04-10 Or Gerlitznet/mlx5e: Avoid using the ipv6 stub in the TC offload...
2018-04-10 Eric Dumazetvti6: better validate user provided tunnel names
2018-04-10 Eric Dumazetip6_tunnel: better validate user provided tunnel names
2018-04-10 Eric Dumazetip6_gre: better validate user provided tunnel names
2018-04-10 Eric Dumazetipv6: sit: better validate user provided tunnel names
2018-04-10 Eric Dumazetip_tunnel: better validate user provided tunnel names
2018-04-10 Eric Dumazetnet: fool proof dev_valid_name()
2018-04-10 Xin Longbonding: process the err returned by dev_set_allmulti...
2018-04-10 Xin Longbonding: move dev_mc_sync after master_upper_dev_link...
2018-04-10 Xin Longbonding: fix the err path for dev hwaddr sync in bond_e...
2018-04-10 David Ahernvrf: Fix use after free and double free in vrf_finish_o...
2018-04-10 Hangbin Liuvlan: also check phy_driver ts_info for vlan's real...
2018-04-10 Jason Wangvhost: correctly remove wait queue during poll failure
2018-04-10 Kai-Heng Fengsky2: Increase D3 delay to sky2 stops working after...
2018-04-10 Eric Dumazetsctp: sctp_sockaddr_af must check minimal addr length...
2018-04-10 Eric Dumazetsctp: do not leak kernel memory to user space
2018-04-10 Heiner Kallweitr8169: fix setting driver_data after register_netdev
2018-04-10 Eric Dumazetpptp: remove a buggy dst release in pptp_connect()
2018-04-10 Davide Carattinet/sched: fix NULL dereference in the error path of...
2018-04-10 Craig Dillabaughnet sched actions: fix dumping which requires several...
2018-04-10 Alexander Potapenkonetlink: make sure nladdr has correct size in netlink_c...
2018-04-10 Jeff Barnhillnet/ipv6: Increment OUTxxx counters after netfilter...
2018-04-10 David Ahernnet/ipv6: Fix route leaking between VRFs
2018-04-10 Eric Dumazetnet: fix possible out-of-bound read in skb_network_prot...
2018-04-10 Raghuram Chary Jlan78xx: Crash in lan78xx_writ_reg (Workqueue: events...
2018-04-10 Paolo Abeniipv6: the entire IPv6 header chain must fit the first...
2018-04-10 Miguel Fadon... arp: fix arp_filter on l3slave devices
2018-04-10 Borislav Petkovx86/microcode: Fix CPU synchronization routine
2018-04-10 Borislav Petkovx86/microcode: Attempt late loading only when new micro...
2018-04-10 Ashok Rajx86/microcode: Synchronize late microcode loading
2018-04-10 Borislav Petkovx86/microcode: Request microcode on the BSP
2018-04-10 Borislav Petkovx86/microcode/intel: Look into the patch cache first
2018-04-10 Ashok Rajx86/microcode: Do not upload microcode if CPUs are...
2018-04-10 Ashok Rajx86/microcode/intel: Writeback and invalidate caches...
2018-04-10 Ashok Rajx86/microcode/intel: Check microcode revision before...
2018-04-10 Borislav Petkovx86/microcode: Get rid of struct apply_microcode_ctx
2018-04-10 Borislav Petkovx86/CPU: Check CPU feature bits after microcode upgrade
2018-04-10 Borislav Petkovx86/CPU: Add a microcode loader callback
2018-04-10 Borislav Petkovx86/microcode: Propagate return value from updating...
2018-04-10 Ard Biesheuvelcrypto: arm64/aes-ce-cipher - move assembler code to...
2018-04-10 Josh Poimboeufobjtool: Add Clang support
2018-04-10 Alexey Khoroshilovthermal: int3400_thermal: fix error handling in int3400...
2018-04-10 Mike Christietcmu: release blocks for partially setup cmds
2018-04-10 Jiri Olsaperf tools: Fix copyfile_offset update of output offset
2018-04-10 Arnd Bergmanncrypto: aes-generic - build with -Os on gcc-7+
2018-04-10 Miquel Raynalmtd: mtd_oobtest: Handle bitflips during reads
2018-04-10 Hans de GoedeInput: goodix - disable IRQs while suspended
2018-04-10 Nathan Fontenotibmvnic: Don't handle RX interrupts when not up.
2018-04-10 Andy Shevchenkosdhci: Advertise 2.0v supply on SDIO host controller
2018-04-10 Jiri Bohacx86/gart: Exclude GART aperture from vmcore
2018-04-10 Wei Yongjungpio: thunderx: fix error return code in thunderx_gpio_...
2018-04-10 Parav PanditRDMA/cma: Fix rdma_cm path querying for RoCE
2018-04-10 Shivasharan Sscsi: megaraid_sas: unload flag should be set after...
2018-04-10 Shivasharan Sscsi: megaraid_sas: Error handling for invalid ldcount...
2018-04-10 Arjun Vynipadathcxgb4vf: Fix SGE FL buffer initialization logic for...
2018-04-10 Jacob Kelleri40evf: don't rely on netif_running() outside rtnl_lock()
2018-04-10 Stephen Hemmingeruio_hv_generic: check that host supports monitor page
2018-04-10 Christophe... EDAC, mv64x60: Fix an error handling path
2018-04-10 Paolo Valenteblock, bfq: put async queues for root bfq groups too
2018-04-10 Tony Lindgrentty: n_gsm: Allow ADM response in addition to UA for...
2018-04-10 Ming Leiblk-mq: fix kernel oops in blk_mq_tag_idle()
2018-04-10 chenxiangscsi: libsas: initialize sas_phy status according to...
2018-04-10 Jason Yanscsi: libsas: fix error when getting phy events
2018-04-10 Jason Yanscsi: libsas: fix memory leak in sas_smp_get_phy_events()
2018-04-10 Tang Junhuibcache: segregate flash only volume write streams
2018-04-10 Tang Junhuibcache: stop writeback thread after detaching
2018-04-10 Rui Huabcache: ret IOERR when read meets metadata error
2018-04-10 Fuyun Liangnet: hns3: fix for changing MTU
2018-04-10 Jian Shennet: hns3: Fix an error macro definition of HNS3_TQP_STAT
2018-04-10 Jian Shennet: hns3: Fix a loop index error of tqp statistics...
2018-04-10 Jian Shennet: hns3: Fix an error of total drop packet statistics
2018-04-10 Daniel Jurgensnet/mlx5: Fix race for multiple RoCE enable
2018-04-10 Colin Ian Kingwl1251: check return from call to wl1251_acx_arp_ip_filter
2018-04-10 Stanislaw Gruszkart2x00: do not pause queue unconditionally on error...
2018-04-10 Hans de Goedepower: supply: axp288_charger: Properly stop work on...
2018-04-10 Christophe... ASoC: Intel: sst: Fix the return value of 'sst_send_byt...
2018-04-10 NeilBrownstaging: lustre: disable preempt while sampling process...
2018-04-10 Jin Yaoperf report: Fix a no annotate browser displayed issue
2018-04-10 Javier Martinez... tpm: return a TPM_RC_COMMAND_CODE response if command...
next