summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: 7764ed0)
raw | patch | inline | side by side (parent: 7764ed0)
author | Heiko Carstens <heiko.carstens@de.ibm.com> | |
Sun, 17 Nov 2019 13:55:38 +0000 (14:55 +0100) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Thu, 9 Jan 2020 09:19:09 +0000 (10:19 +0100) |
[ Upstream commit 72a81ad9d6d62dcb79f7e8ad66ffd1c768b72026 ]
If an SMT capable system is not IPL'ed from the first CPU the setup of
the physical to logical CPU mapping is broken: the IPL core gets CPU
number 0, but then the next core gets CPU number 1. Correct would be
that all SMT threads of CPU 0 get the subsequent logical CPU numbers.
This is important since a lot of code (like e.g. the CPU topology
code) assumes that CPU maps are setup like this. If the mapping is
broken the system will not IPL due to broken topology masks:
[ 1.716341] BUG: arch topology broken
[ 1.716342] the SMT domain not a subset of the MC domain
[ 1.716343] BUG: arch topology broken
[ 1.716344] the MC domain not a subset of the BOOK domain
This scenario can usually not happen since LPARs are always IPL'ed
from CPU 0 and also re-IPL is intiated from CPU 0. However older
kernels did initiate re-IPL on an arbitrary CPU. If therefore a re-IPL
from an old kernel into a new kernel is initiated this may lead to
crash.
Fix this by setting up the physical to logical CPU mapping correctly.
Signed-off-by: Heiko Carstens <heiko.carstens@de.ibm.com>
Signed-off-by: Vasily Gorbik <gor@linux.ibm.com>
Signed-off-by: Sasha Levin <sashal@kernel.org>
If an SMT capable system is not IPL'ed from the first CPU the setup of
the physical to logical CPU mapping is broken: the IPL core gets CPU
number 0, but then the next core gets CPU number 1. Correct would be
that all SMT threads of CPU 0 get the subsequent logical CPU numbers.
This is important since a lot of code (like e.g. the CPU topology
code) assumes that CPU maps are setup like this. If the mapping is
broken the system will not IPL due to broken topology masks:
[ 1.716341] BUG: arch topology broken
[ 1.716342] the SMT domain not a subset of the MC domain
[ 1.716343] BUG: arch topology broken
[ 1.716344] the MC domain not a subset of the BOOK domain
This scenario can usually not happen since LPARs are always IPL'ed
from CPU 0 and also re-IPL is intiated from CPU 0. However older
kernels did initiate re-IPL on an arbitrary CPU. If therefore a re-IPL
from an old kernel into a new kernel is initiated this may lead to
crash.
Fix this by setting up the physical to logical CPU mapping correctly.
Signed-off-by: Heiko Carstens <heiko.carstens@de.ibm.com>
Signed-off-by: Vasily Gorbik <gor@linux.ibm.com>
Signed-off-by: Sasha Levin <sashal@kernel.org>
arch/s390/kernel/smp.c | patch | blob | history |
diff --git a/arch/s390/kernel/smp.c b/arch/s390/kernel/smp.c
index df2413f26a8f2397a6cdb9970e8ad9042a916adb..ecd24711f3aa9caa137544b0434f23e29797c144 100644 (file)
--- a/arch/s390/kernel/smp.c
+++ b/arch/s390/kernel/smp.c
static int smp_add_present_cpu(int cpu);
-static int __smp_rescan_cpus(struct sclp_core_info *info, int sysfs_add)
+static int smp_add_core(struct sclp_core_entry *core, cpumask_t *avail,
+ bool configured, bool early)
{
struct pcpu *pcpu;
- cpumask_t avail;
- int cpu, nr, i, j;
+ int cpu, nr, i;
u16 address;
nr = 0;
- cpumask_xor(&avail, cpu_possible_mask, cpu_present_mask);
- cpu = cpumask_first(&avail);
- for (i = 0; (i < info->combined) && (cpu < nr_cpu_ids); i++) {
- if (sclp.has_core_type && info->core[i].type != boot_core_type)
+ if (sclp.has_core_type && core->type != boot_core_type)
+ return nr;
+ cpu = cpumask_first(avail);
+ address = core->core_id << smp_cpu_mt_shift;
+ for (i = 0; (i <= smp_cpu_mtid) && (cpu < nr_cpu_ids); i++) {
+ if (pcpu_find_address(cpu_present_mask, address + i))
continue;
- address = info->core[i].core_id << smp_cpu_mt_shift;
- for (j = 0; j <= smp_cpu_mtid; j++) {
- if (pcpu_find_address(cpu_present_mask, address + j))
- continue;
- pcpu = pcpu_devices + cpu;
- pcpu->address = address + j;
- pcpu->state =
- (cpu >= info->configured*(smp_cpu_mtid + 1)) ?
- CPU_STATE_STANDBY : CPU_STATE_CONFIGURED;
- smp_cpu_set_polarization(cpu, POLARIZATION_UNKNOWN);
- set_cpu_present(cpu, true);
- if (sysfs_add && smp_add_present_cpu(cpu) != 0)
- set_cpu_present(cpu, false);
- else
- nr++;
- cpu = cpumask_next(cpu, &avail);
- if (cpu >= nr_cpu_ids)
+ pcpu = pcpu_devices + cpu;
+ pcpu->address = address + i;
+ if (configured)
+ pcpu->state = CPU_STATE_CONFIGURED;
+ else
+ pcpu->state = CPU_STATE_STANDBY;
+ smp_cpu_set_polarization(cpu, POLARIZATION_UNKNOWN);
+ set_cpu_present(cpu, true);
+ if (!early && smp_add_present_cpu(cpu) != 0)
+ set_cpu_present(cpu, false);
+ else
+ nr++;
+ cpumask_clear_cpu(cpu, avail);
+ cpu = cpumask_next(cpu, avail);
+ }
+ return nr;
+}
+
+static int __smp_rescan_cpus(struct sclp_core_info *info, bool early)
+{
+ struct sclp_core_entry *core;
+ cpumask_t avail;
+ bool configured;
+ u16 core_id;
+ int nr, i;
+
+ nr = 0;
+ cpumask_xor(&avail, cpu_possible_mask, cpu_present_mask);
+ /*
+ * Add IPL core first (which got logical CPU number 0) to make sure
+ * that all SMT threads get subsequent logical CPU numbers.
+ */
+ if (early) {
+ core_id = pcpu_devices[0].address >> smp_cpu_mt_shift;
+ for (i = 0; i < info->configured; i++) {
+ core = &info->core[i];
+ if (core->core_id == core_id) {
+ nr += smp_add_core(core, &avail, true, early);
break;
+ }
}
}
+ for (i = 0; i < info->combined; i++) {
+ configured = i < info->configured;
+ nr += smp_add_core(&info->core[i], &avail, configured, early);
+ }
return nr;
}
/* Add CPUs present at boot */
get_online_cpus();
- __smp_rescan_cpus(info, 0);
+ __smp_rescan_cpus(info, true);
put_online_cpus();
memblock_free_early((unsigned long)info, sizeof(*info));
}
smp_get_core_info(info, 0);
get_online_cpus();
mutex_lock(&smp_cpu_state_mutex);
- nr = __smp_rescan_cpus(info, 1);
+ nr = __smp_rescan_cpus(info, false);
mutex_unlock(&smp_cpu_state_mutex);
put_online_cpus();
kfree(info);