]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-linux-kernel/ti-linux-kernel.git/commitdiff
fs/seq_file: fix out-of-bounds read
authorVegard Nossum <vegard.nossum@oracle.com>
Thu, 25 Aug 2016 22:17:11 +0000 (15:17 -0700)
committerGreg Kroah-Hartman <gregkh@linuxfoundation.org>
Wed, 7 Sep 2016 06:30:00 +0000 (08:30 +0200)
commit 088bf2ff5d12e2e32ee52a4024fec26e582f44d3 upstream.

seq_read() is a nasty piece of work, not to mention buggy.

It has (I think) an old bug which allows unprivileged userspace to read
beyond the end of m->buf.

I was getting these:

    BUG: KASAN: slab-out-of-bounds in seq_read+0xcd2/0x1480 at addr ffff880116889880
    Read of size 2713 by task trinity-c2/1329
    CPU: 2 PID: 1329 Comm: trinity-c2 Not tainted 4.8.0-rc1+ #96
    Hardware name: QEMU Standard PC (i440FX + PIIX, 1996), BIOS rel-1.9.3-0-ge2fc41e-prebuilt.qemu-project.org 04/01/2014
    Call Trace:
      kasan_object_err+0x1c/0x80
      kasan_report_error+0x2cb/0x7e0
      kasan_report+0x4e/0x80
      check_memory_region+0x13e/0x1a0
      kasan_check_read+0x11/0x20
      seq_read+0xcd2/0x1480
      proc_reg_read+0x10b/0x260
      do_loop_readv_writev.part.5+0x140/0x2c0
      do_readv_writev+0x589/0x860
      vfs_readv+0x7b/0xd0
      do_readv+0xd8/0x2c0
      SyS_readv+0xb/0x10
      do_syscall_64+0x1b3/0x4b0
      entry_SYSCALL64_slow_path+0x25/0x25
    Object at ffff880116889100, in cache kmalloc-4096 size: 4096
    Allocated:
    PID = 1329
      save_stack_trace+0x26/0x80
      save_stack+0x46/0xd0
      kasan_kmalloc+0xad/0xe0
      __kmalloc+0x1aa/0x4a0
      seq_buf_alloc+0x35/0x40
      seq_read+0x7d8/0x1480
      proc_reg_read+0x10b/0x260
      do_loop_readv_writev.part.5+0x140/0x2c0
      do_readv_writev+0x589/0x860
      vfs_readv+0x7b/0xd0
      do_readv+0xd8/0x2c0
      SyS_readv+0xb/0x10
      do_syscall_64+0x1b3/0x4b0
      return_from_SYSCALL_64+0x0/0x6a
    Freed:
    PID = 0
    (stack is not available)
    Memory state around the buggy address:
     ffff88011688a000: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
     ffff88011688a080: 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00 00
    >ffff88011688a100: fc fc fc fc fc fc fc fc fc fc fc fc fc fc fc fc
       ^
     ffff88011688a180: fc fc fc fc fc fc fc fc fc fc fc fc fc fc fc fc
     ffff88011688a200: fb fb fb fb fb fb fb fb fb fb fb fb fb fb fb fb
    ==================================================================
    Disabling lock debugging due to kernel taint

This seems to be the same thing that Dave Jones was seeing here:

  https://lkml.org/lkml/2016/8/12/334

There are multiple issues here:

  1) If we enter the function with a non-empty buffer, there is an attempt
     to flush it. But it was not clearing m->from after doing so, which
     means that if we try to do this flush twice in a row without any call
     to traverse() in between, we are going to be reading from the wrong
     place -- the splat above, fixed by this patch.

  2) If there's a short write to userspace because of page faults, the
     buffer may already contain multiple lines (i.e. pos has advanced by
     more than 1), but we don't save the progress that was made so the
     next call will output what we've already returned previously. Since
     that is a much less serious issue (and I have a headache after
     staring at seq_read() for the past 8 hours), I'll leave that for now.

Link: http://lkml.kernel.org/r/1471447270-32093-1-git-send-email-vegard.nossum@oracle.com
Signed-off-by: Vegard Nossum <vegard.nossum@oracle.com>
Reported-by: Dave Jones <davej@codemonkey.org.uk>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
fs/seq_file.c

index 1d641bb108d239f2476d862f0ce9e366c299762c..d88584c61c1e2e5a497451c788bb43a9416d21d6 100644 (file)
@@ -207,8 +207,10 @@ ssize_t seq_read(struct file *file, char __user *buf, size_t size, loff_t *ppos)
                size -= n;
                buf += n;
                copied += n;
-               if (!m->count)
+               if (!m->count) {
+                       m->from = 0;
                        m->index++;
+               }
                if (!size)
                        goto Done;
        }