summary | shortlog | log | commit | commitdiff | tree
raw | patch | inline | side by side (parent: d9a58c4)
raw | patch | inline | side by side (parent: d9a58c4)
author | David Woodhouse <dwmw@amazon.co.uk> | |
Sat, 14 Jul 2018 09:35:12 +0000 (02:35 -0700) | ||
committer | Greg Kroah-Hartman <gregkh@linuxfoundation.org> | |
Wed, 25 Jul 2018 08:18:25 +0000 (10:18 +0200) |
commit 764f3c21588a059cd783c6ba0734d4db2d72822d upstream
AMD does not need the Speculative Store Bypass mitigation to be enabled.
The parameters for this are already available and can be done via MSR
C001_1020. Each family uses a different bit in that MSR for this.
[ tglx: Expose the bit mask via a variable and move the actual MSR fiddling
into the bugs code as that's the right thing to do and also required
to prepare for dynamic enable/disable ]
[ Srivatsa: Removed __ro_after_init for 4.4.y ]
Suggested-by: Borislav Petkov <bp@suse.de>
Signed-off-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Reviewed-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: David Woodhouse <dwmw@amazon.co.uk>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Signed-off-by: Srivatsa S. Bhat <srivatsa@csail.mit.edu>
Reviewed-by: Matt Helsley (VMware) <matt.helsley@gmail.com>
Reviewed-by: Alexey Makhalov <amakhalov@vmware.com>
Reviewed-by: Bo Gan <ganb@vmware.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
AMD does not need the Speculative Store Bypass mitigation to be enabled.
The parameters for this are already available and can be done via MSR
C001_1020. Each family uses a different bit in that MSR for this.
[ tglx: Expose the bit mask via a variable and move the actual MSR fiddling
into the bugs code as that's the right thing to do and also required
to prepare for dynamic enable/disable ]
[ Srivatsa: Removed __ro_after_init for 4.4.y ]
Suggested-by: Borislav Petkov <bp@suse.de>
Signed-off-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Reviewed-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: David Woodhouse <dwmw@amazon.co.uk>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Signed-off-by: Srivatsa S. Bhat <srivatsa@csail.mit.edu>
Reviewed-by: Matt Helsley (VMware) <matt.helsley@gmail.com>
Reviewed-by: Alexey Makhalov <amakhalov@vmware.com>
Reviewed-by: Bo Gan <ganb@vmware.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
index 9510f5f075c667265e934bd401ba7741a2c2d139..b7cdd1c0513262ad47206156d4d0cd2c3314577c 100644 (file)
#define X86_FEATURE_USE_IBPB ( 7*32+21) /* "" Indirect Branch Prediction Barrier enabled*/
#define X86_FEATURE_USE_IBRS_FW ( 7*32+22) /* "" Use IBRS during runtime firmware calls */
#define X86_FEATURE_SPEC_STORE_BYPASS_DISABLE ( 7*32+23) /* "" Disable Speculative Store Bypass. */
+#define X86_FEATURE_AMD_RDS (7*32+24) /* "" AMD RDS implementation */
/* Virtualization flags: Linux defined, word 8 */
#define X86_FEATURE_TPR_SHADOW ( 8*32+ 0) /* Intel TPR Shadow */
index c786d01faf5162acf04c3eb08312c8fb86c05c30..ac2fdc9666e4a2eb04e02b4c17ed3a9eff3f7f19 100644 (file)
SPEC_STORE_BYPASS_DISABLE,
};
+/* AMD specific Speculative Store Bypass MSR data */
+extern u64 x86_amd_ls_cfg_base;
+extern u64 x86_amd_ls_cfg_rds_mask;
+
extern char __indirect_thunk_start[];
extern char __indirect_thunk_end[];
index 9b2941422b68a37690bc293f7a4ca5de3a420078..4452f387ed32ebdfbddb423c20f91654394fcd50 100644 (file)
#include <asm/processor.h>
#include <asm/apic.h>
#include <asm/cpu.h>
+#include <asm/nospec-branch.h>
#include <asm/smp.h>
#include <asm/pci-direct.h>
#include <asm/delay.h>
if (cpu_has(c, X86_FEATURE_MWAITX))
use_mwaitx_delay();
+
+ if (c->x86 >= 0x15 && c->x86 <= 0x17) {
+ unsigned int bit;
+
+ switch (c->x86) {
+ case 0x15: bit = 54; break;
+ case 0x16: bit = 33; break;
+ case 0x17: bit = 10; break;
+ default: return;
+ }
+ /*
+ * Try to cache the base value so further operations can
+ * avoid RMW. If that faults, do not enable RDS.
+ */
+ if (!rdmsrl_safe(MSR_AMD64_LS_CFG, &x86_amd_ls_cfg_base)) {
+ setup_force_cpu_cap(X86_FEATURE_RDS);
+ setup_force_cpu_cap(X86_FEATURE_AMD_RDS);
+ x86_amd_ls_cfg_rds_mask = 1ULL << bit;
+ }
+ }
}
static void early_init_amd(struct cpuinfo_x86 *c)
/* AMD CPUs don't reset SS attributes on SYSRET, Xen does. */
if (!cpu_has(c, X86_FEATURE_XENPV))
set_cpu_bug(c, X86_BUG_SYSRET_SS_ATTRS);
+
+ if (boot_cpu_has(X86_FEATURE_AMD_RDS)) {
+ set_cpu_cap(c, X86_FEATURE_RDS);
+ set_cpu_cap(c, X86_FEATURE_AMD_RDS);
+ }
}
#ifdef CONFIG_X86_32
index c37e2110d383c37d0e23131b6888e0e43391481d..b8911afbd6b89e32db9513bdf26badb605ad6209 100644 (file)
*/
static u64 x86_spec_ctrl_mask = ~SPEC_CTRL_IBRS;
+/*
+ * AMD specific MSR info for Speculative Store Bypass control.
+ * x86_amd_ls_cfg_rds_mask is initialized in identify_boot_cpu().
+ */
+u64 x86_amd_ls_cfg_base;
+u64 x86_amd_ls_cfg_rds_mask;
+
void __init check_bugs(void)
{
identify_boot_cpu();
/*
* Read the SPEC_CTRL MSR to account for reserved bits which may
- * have unknown values.
+ * have unknown values. AMD64_LS_CFG MSR is cached in the early AMD
+ * init code as it is not enumerated and depends on the family.
*/
if (boot_cpu_has(X86_FEATURE_IBRS))
rdmsrl(MSR_IA32_SPEC_CTRL, x86_spec_ctrl_base);
}
EXPORT_SYMBOL_GPL(x86_spec_ctrl_restore_host);
+static void x86_amd_rds_enable(void)
+{
+ u64 msrval = x86_amd_ls_cfg_base | x86_amd_ls_cfg_rds_mask;
+
+ if (boot_cpu_has(X86_FEATURE_AMD_RDS))
+ wrmsrl(MSR_AMD64_LS_CFG, msrval);
+}
+
#ifdef RETPOLINE
static bool spectre_v2_bad_module;
switch (cmd) {
case SPEC_STORE_BYPASS_CMD_AUTO:
+ /*
+ * AMD platforms by default don't need SSB mitigation.
+ */
+ if (boot_cpu_data.x86_vendor == X86_VENDOR_AMD)
+ break;
case SPEC_STORE_BYPASS_CMD_ON:
mode = SPEC_STORE_BYPASS_DISABLE;
break;
x86_spec_ctrl_set(SPEC_CTRL_RDS);
break;
case X86_VENDOR_AMD:
+ x86_amd_rds_enable();
break;
}
}
{
if (boot_cpu_has(X86_FEATURE_IBRS))
x86_spec_ctrl_set(x86_spec_ctrl_base & ~x86_spec_ctrl_mask);
+
+ if (ssb_mode == SPEC_STORE_BYPASS_DISABLE)
+ x86_amd_rds_enable();
}
#ifdef CONFIG_SYSFS
index 2f1d403cb0ea3d93bac378be11496460ba35ccb5..7405c8653f7ae8022a33e1c27695be8badb4aff4 100644 (file)
{ X86_VENDOR_CENTAUR, 5, },
{ X86_VENDOR_INTEL, 5, },
{ X86_VENDOR_NSC, 5, },
+ { X86_VENDOR_AMD, 0x12, },
+ { X86_VENDOR_AMD, 0x11, },
+ { X86_VENDOR_AMD, 0x10, },
+ { X86_VENDOR_AMD, 0xf, },
{ X86_VENDOR_ANY, 4, },
{}
};