1 #
2 # For a description of the syntax of this configuration file,
3 # see the file Documentation/kbuild/kconfig-language.txt in the
4 # Linux kernel source tree.
5 #
6 mainmenu "U-Boot $(UBOOTVERSION) Configuration"
8 # Allow defaults in arch-specific code to override any given here
9 source "arch/Kconfig"
11 menu "General setup"
13 config BROKEN
14 bool
15 help
16 This option cannot be enabled. It is used as dependency
17 for broken and incomplete features.
19 config DEPRECATED
20 bool
21 help
22 This option cannot be enabled. It it used as a dependency for
23 code that relies on deprecated features that will be removed and
24 the conversion deadline has passed.
26 config LOCALVERSION
27 string "Local version - append to U-Boot release"
28 help
29 Append an extra string to the end of your U-Boot version.
30 This will show up in your boot log, for example.
31 The string you set here will be appended after the contents of
32 any files with a filename matching localversion* in your
33 object and source tree, in that order. Your total string can
34 be a maximum of 64 characters.
36 config LOCALVERSION_AUTO
37 bool "Automatically append version information to the version string"
38 default y
39 help
40 This will try to automatically determine if the current tree is a
41 release tree by looking for Git tags that belong to the current
42 top of tree revision.
44 A string of the format -gxxxxxxxx will be added to the localversion
45 if a Git-based tree is found. The string generated by this will be
46 appended after any matching localversion* files, and after the value
47 set in CONFIG_LOCALVERSION.
49 (The actual string used here is the first eight characters produced
50 by running the command:
52 $ git rev-parse --verify HEAD
54 which is done within the script "scripts/setlocalversion".)
56 config CC_OPTIMIZE_FOR_SIZE
57 bool "Optimize for size"
58 default y
59 help
60 Enabling this option will pass "-Os" instead of "-O2" to gcc
61 resulting in a smaller U-Boot image.
63 This option is enabled by default for U-Boot.
65 config CC_COVERAGE
66 bool "Enable code coverage analysis"
67 depends on SANDBOX
68 help
69 Enabling this option will pass "--coverage" to gcc to compile
70 and link code instrumented for coverage analysis.
72 config DISTRO_DEFAULTS
73 bool "Select defaults suitable for booting general purpose Linux distributions"
74 select AUTO_COMPLETE
75 select CMDLINE_EDITING
76 select CMD_BOOTI if ARM64
77 select CMD_BOOTZ if ARM && !ARM64
78 select CMD_DHCP if CMD_NET
79 select CMD_ENV_EXISTS
80 select CMD_EXT2
81 select CMD_EXT4
82 select CMD_FAT
83 select CMD_FS_GENERIC
84 select CMD_PART if PARTITIONS
85 select CMD_PING if CMD_NET
86 select CMD_PXE if NET
87 select CMD_SYSBOOT
88 select ENV_VARS_UBOOT_CONFIG
89 select HUSH_PARSER
90 select SUPPORT_RAW_INITRD
91 select SYS_LONGHELP
92 imply CMD_MII if NET
93 imply USB_STORAGE
94 imply USE_BOOTCOMMAND
95 help
96 Select this to enable various options and commands which are suitable
97 for building u-boot for booting general purpose Linux distributions.
99 config ENV_VARS_UBOOT_CONFIG
100 bool "Add arch, board, vendor and soc variables to default environment"
101 help
102 Define this in order to add variables describing the
103 U-Boot build configuration to the default environment.
104 These will be named arch, cpu, board, vendor, and soc.
105 Enabling this option will cause the following to be defined:
106 - CONFIG_SYS_ARCH
107 - CONFIG_SYS_CPU
108 - CONFIG_SYS_BOARD
109 - CONFIG_SYS_VENDOR
110 - CONFIG_SYS_SOC
112 config NR_DRAM_BANKS
113 int "Number of DRAM banks"
114 default 1 if ARCH_SUNXI || ARCH_OWL
115 default 4
116 help
117 This defines the number of DRAM banks.
119 config SYS_BOOT_GET_CMDLINE
120 bool "Enable kernel command line setup"
121 help
122 Enables allocating and saving kernel cmdline in space between
123 "bootm_low" and "bootm_low" + BOOTMAPSZ.
125 config SYS_BOOT_GET_KBD
126 bool "Enable kernel board information setup"
127 help
128 Enables allocating and saving a kernel copy of the bd_info in
129 space between "bootm_low" and "bootm_low" + BOOTMAPSZ.
131 config SYS_MALLOC_F
132 bool "Enable malloc() pool before relocation"
133 default y if DM
135 help
136 Before relocation, memory is very limited on many platforms. Still,
137 we can provide a small malloc() pool if needed. Driver model in
138 particular needs this to operate, so that it can allocate the
139 initial serial device and any others that are needed.
141 config SYS_MALLOC_F_LEN
142 hex "Size of malloc() pool before relocation"
143 depends on SYS_MALLOC_F
144 default 0x1000 if AM33XX
145 default 0x2800 if SANDBOX
146 default 0x2000 if (ARCH_IMX8 || ARCH_IMX8M || ARCH_MX7 || \
147 ARCH_MX7ULP || ARCH_MX6 || ARCH_MX5 || \
148 ARCH_LS1012A || ARCH_LS1021A || ARCH_LS1043A || \
149 ARCH_LS1046A || ARCH_QEMU)
150 default 0x400
151 help
152 Before relocation, memory is very limited on many platforms. Still,
153 we can provide a small malloc() pool if needed. Driver model in
154 particular needs this to operate, so that it can allocate the
155 initial serial device and any others that are needed.
157 config SYS_MALLOC_LEN
158 hex "Define memory for Dynamic allocation"
159 depends on ARCH_ZYNQ || ARCH_VERSAL || ARCH_STM32MP || ARCH_ROCKCHIP
160 default 0x2000000 if ARCH_ROCKCHIP
161 help
162 This defines memory to be allocated for Dynamic allocation
163 TODO: Use for other architectures
165 config SPL_SYS_MALLOC_F_LEN
166 hex "Size of malloc() pool in SPL before relocation"
167 depends on SYS_MALLOC_F && SPL
168 default 0x2800 if RCAR_GEN3
169 default SYS_MALLOC_F_LEN
170 help
171 Before relocation, memory is very limited on many platforms. Still,
172 we can provide a small malloc() pool if needed. Driver model in
173 particular needs this to operate, so that it can allocate the
174 initial serial device and any others that are needed.
176 config TPL_SYS_MALLOC_F_LEN
177 hex "Size of malloc() pool in TPL before relocation"
178 depends on SYS_MALLOC_F && TPL
179 default SYS_MALLOC_F_LEN
180 help
181 Before relocation, memory is very limited on many platforms. Still,
182 we can provide a small malloc() pool if needed. Driver model in
183 particular needs this to operate, so that it can allocate the
184 initial serial device and any others that are needed.
186 menuconfig EXPERT
187 bool "Configure standard U-Boot features (expert users)"
188 default y
189 help
190 This option allows certain base U-Boot options and settings
191 to be disabled or tweaked. This is for specialized
192 environments which can tolerate a "non-standard" U-Boot.
193 Use this only if you really know what you are doing.
195 if EXPERT
196 config SYS_MALLOC_CLEAR_ON_INIT
197 bool "Init with zeros the memory reserved for malloc (slow)"
198 default y
199 help
200 This setting is enabled by default. The reserved malloc
201 memory is initialized with zeros, so first malloc calls
202 will return the pointer to the zeroed memory. But this
203 slows the boot time.
205 It is recommended to disable it, when CONFIG_SYS_MALLOC_LEN
206 value, has more than few MiB, e.g. when uses bzip2 or bmp logo.
207 Then the boot time can be significantly reduced.
208 Warning:
209 When disabling this, please check if malloc calls, maybe
210 should be replaced by calloc - if one expects zeroed memory.
212 config SYS_MALLOC_DEFAULT_TO_INIT
213 bool "Default malloc to init while reserving the memory for it"
214 default n
215 help
216 It may happen that one needs to move the dynamic allocation
217 from one to another memory range, eg. when moving the malloc
218 from the limited static to a potentially large dynamic (DDR)
219 memory.
221 If so then on top of setting the updated memory aside one
222 needs to bring the malloc init.
224 If such a scenario is sought choose yes.
226 config TOOLS_DEBUG
227 bool "Enable debug information for tools"
228 help
229 Enable generation of debug information for tools such as mkimage.
230 This can be used for debugging purposes. With debug information
231 it is possible to set breakpoints on particular lines, single-step
232 debug through the source code, etc.
234 endif # EXPERT
236 config PHYS_64BIT
237 bool "64bit physical address support"
238 help
239 Say Y here to support 64bit physical memory address.
240 This can be used not only for 64bit SoCs, but also for
241 large physical address extension on 32bit SoCs.
243 config BUILD_ROM
244 bool "Build U-Boot as BIOS replacement"
245 depends on X86
246 help
247 This option allows to build a ROM version of U-Boot.
248 The build process generally requires several binary blobs
249 which are not shipped in the U-Boot source tree.
250 Please, see doc/arch/x86.rst for details.
252 config SPL_IMAGE
253 string "SPL image used in the combined SPL+U-Boot image"
254 default "spl/boot.bin" if ARCH_AT91 && SPL_NAND_SUPPORT
255 default "spl/u-boot-spl.bin"
256 depends on SPL
257 help
258 Select the SPL build target that shall be generated by the SPL
259 build process (default spl/u-boot-spl.bin). This image will be
260 used to generate a combined image with SPL and main U-Boot
261 proper as one single image.
263 config BUILD_TARGET
264 string "Build target special images"
265 default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_ARRIA10
266 default "u-boot-with-spl.sfp" if TARGET_SOCFPGA_GEN5
267 default "u-boot-spl.kwb" if ARCH_MVEBU && SPL
268 default "u-boot-elf.srec" if RCAR_GEN3
269 default "u-boot.itb" if SPL_LOAD_FIT && (ARCH_ROCKCHIP || \
270 ARCH_SUNXI || RISCV || ARCH_ZYNQMP)
271 default "u-boot.kwb" if ARCH_KIRKWOOD
272 default "u-boot-with-spl.bin" if ARCH_AT91 && SPL_NAND_SUPPORT
273 default "u-boot-with-spl.imx" if ARCH_MX6 && SPL
274 help
275 Some SoCs need special image types (e.g. U-Boot binary
276 with a special header) as build targets. By defining
277 CONFIG_BUILD_TARGET in the SoC / board header, this
278 special image will be automatically built upon calling
279 make / buildman.
281 config SYS_CUSTOM_LDSCRIPT
282 bool "Use a custom location for the U-Boot linker script"
283 help
284 Normally when linking U-Boot we will look in the board directory,
285 the CPU directory and finally the "cpu" directory of the architecture
286 for the ile "u-boot.lds" and use that as our linker. However, in
287 some cases we need to provide a different linker script. To do so,
288 enable this option and then provide the location under
289 CONFIG_SYS_LDSCRIPT.
291 config SYS_LDSCRIPT
292 depends on SYS_CUSTOM_LDSCRIPT
293 string "Custom ldscript location"
294 help
295 Path within the source tree to the linker script to use for the
296 main U-Boot binary.
298 config ERR_PTR_OFFSET
299 hex
300 default 0x0
301 help
302 Some U-Boot pointers have redundant information, so we can use a
303 scheme where we can return either an error code or a pointer with the
304 same return value. The default implementation just casts the pointer
305 to a number, however, this may fail on platforms where the end of the
306 address range is used for valid pointers (e.g. 0xffffff00 is a valid
307 heap pointer in socfpga SPL).
308 For such platforms, this value provides an upper range of those error
309 pointer values - up to 'MAX_ERRNO' bytes below this value must be
310 unused/invalid addresses.
312 config PLATFORM_ELFENTRY
313 string
314 default "__start" if MIPS
315 default "_start"
317 endmenu # General setup
319 menu "Boot images"
321 config ANDROID_BOOT_IMAGE
322 bool "Enable support for Android Boot Images"
323 default y if FASTBOOT
324 help
325 This enables support for booting images which use the Android
326 image format header.
328 config FIT
329 bool "Support Flattened Image Tree"
330 select MD5
331 select SHA1
332 help
333 This option allows you to boot the new uImage structure,
334 Flattened Image Tree. FIT is formally a FDT, which can include
335 images of various types (kernel, FDT blob, ramdisk, etc.)
336 in a single blob. To boot this new uImage structure,
337 pass the address of the blob to the "bootm" command.
338 FIT is very flexible, supporting compression, multiple images,
339 multiple configurations, verification through hashing and also
340 verified boot (secure boot using RSA).
342 if FIT
344 config FIT_EXTERNAL_OFFSET
345 hex "FIT external data offset"
346 default 0x0
347 help
348 This specifies a data offset in fit image.
349 The offset is from data payload offset to the beginning of
350 fit image header. When specifies a offset, specific data
351 could be put in the hole between data payload and fit image
352 header, such as CSF data on i.MX platform.
354 config FIT_ENABLE_SHA256_SUPPORT
355 bool "Support SHA256 checksum of FIT image contents"
356 default y
357 select SHA256
358 help
359 Enable this to support SHA256 checksum of FIT image contents. A
360 SHA256 checksum is a 256-bit (32-byte) hash value used to check that
361 the image contents have not been corrupted. SHA256 is recommended
362 for use in secure applications since (as at 2016) there is no known
363 feasible attack that could produce a 'collision' with differing
364 input data. Use this for the highest security. Note that only the
365 SHA256 variant is supported: SHA512 and others are not currently
366 supported in U-Boot.
368 config FIT_SIGNATURE
369 bool "Enable signature verification of FIT uImages"
370 depends on DM
371 select HASH
372 select RSA
373 select RSA_VERIFY
374 select IMAGE_SIGN_INFO
375 help
376 This option enables signature verification of FIT uImages,
377 using a hash signed and verified using RSA. If
378 CONFIG_SHA_PROG_HW_ACCEL is defined, i.e support for progressive
379 hashing is available using hardware, then the RSA library will use
380 it. See doc/uImage.FIT/signature.txt for more details.
382 WARNING: When relying on signed FIT images with a required signature
383 check the legacy image format is disabled by default, so that
384 unsigned images cannot be loaded. If a board needs the legacy image
385 format support in this case, enable it using
386 CONFIG_LEGACY_IMAGE_FORMAT.
388 config FIT_SIGNATURE_MAX_SIZE
389 hex "Max size of signed FIT structures"
390 depends on FIT_SIGNATURE
391 default 0x10000000
392 help
393 This option sets a max size in bytes for verified FIT uImages.
394 A sane value of 256MB protects corrupted DTB structures from overlapping
395 device memory. Assure this size does not extend past expected storage
396 space.
398 config FIT_ENABLE_RSASSA_PSS_SUPPORT
399 bool "Support rsassa-pss signature scheme of FIT image contents"
400 depends on FIT_SIGNATURE
401 default n
402 help
403 Enable this to support the pss padding algorithm as described
404 in the rfc8017 (https://tools.ietf.org/html/rfc8017).
406 config FIT_CIPHER
407 bool "Enable ciphering data in a FIT uImages"
408 depends on DM
409 select AES
410 help
411 Enable the feature of data ciphering/unciphering in the tool mkimage
412 and in the u-boot support of the FIT image.
414 config FIT_VERBOSE
415 bool "Show verbose messages when FIT images fail"
416 help
417 Generally a system will have valid FIT images so debug messages
418 are a waste of code space. If you are debugging your images then
419 you can enable this option to get more verbose information about
420 failures.
422 config FIT_BEST_MATCH
423 bool "Select the best match for the kernel device tree"
424 help
425 When no configuration is explicitly selected, default to the
426 one whose fdt's compatibility field best matches that of
427 U-Boot itself. A match is considered "best" if it matches the
428 most specific compatibility entry of U-Boot's fdt's root node.
429 The order of entries in the configuration's fdt is ignored.
431 config FIT_IMAGE_POST_PROCESS
432 bool "Enable post-processing of FIT artifacts after loading by U-Boot"
433 depends on TI_SECURE_DEVICE
434 help
435 Allows doing any sort of manipulation to blobs after they got extracted
436 from FIT images like stripping off headers or modifying the size of the
437 blob, verification, authentication, decryption etc. in a platform or
438 board specific way. In order to use this feature a platform or board-
439 specific implementation of board_fit_image_post_process() must be
440 provided. Also, anything done during this post-processing step would
441 need to be comprehended in how the images were prepared before being
442 injected into the FIT creation (i.e. the blobs would have been pre-
443 processed before being added to the FIT image).
445 if SPL
447 config SPL_FIT
448 bool "Support Flattened Image Tree within SPL"
449 depends on SPL
450 select SPL_OF_LIBFDT
452 config SPL_FIT_PRINT
453 bool "Support FIT printing within SPL"
454 depends on SPL_FIT
455 help
456 Support printing the content of the fitImage in a verbose manner in SPL.
458 config SPL_FIT_SIGNATURE
459 bool "Enable signature verification of FIT firmware within SPL"
460 depends on SPL_DM
461 select SPL_FIT
462 select SPL_RSA
463 select SPL_RSA_VERIFY
464 select SPL_IMAGE_SIGN_INFO
466 config SPL_LOAD_FIT
467 bool "Enable SPL loading U-Boot as a FIT (basic fitImage features)"
468 select SPL_FIT
469 help
470 Normally with the SPL framework a legacy image is generated as part
471 of the build. This contains U-Boot along with information as to
472 where it should be loaded. This option instead enables generation
473 of a FIT (Flat Image Tree) which provides more flexibility. In
474 particular it can handle selecting from multiple device tree
475 and passing the correct one to U-Boot.
477 config SPL_LOAD_FIT_APPLY_OVERLAY
478 bool "Enable SPL applying DT overlays from FIT"
479 depends on SPL_LOAD_FIT
480 select OF_LIBFDT_OVERLAY
481 help
482 The device tree is loaded from the FIT image. Allow the SPL is to
483 also load device-tree overlays from the FIT image an apply them
484 over the device tree.
486 config SPL_LOAD_FIT_APPLY_OVERLAY_BUF_SZ
487 depends on SPL_LOAD_FIT_APPLY_OVERLAY
488 default 0x10000
489 hex "size of temporary buffer used to load the overlays"
490 help
491 The size of the area where the overlays will be loaded and
492 uncompress. Must be at least as large as biggest overlay
493 (uncompressed)
495 config SPL_LOAD_FIT_FULL
496 bool "Enable SPL loading U-Boot as a FIT (full fitImage features)"
497 select SPL_FIT
498 help
499 Normally with the SPL framework a legacy image is generated as part
500 of the build. This contains U-Boot along with information as to
501 where it should be loaded. This option instead enables generation
502 of a FIT (Flat Image Tree) which provides more flexibility. In
503 particular it can handle selecting from multiple device tree
504 and passing the correct one to U-Boot.
506 config SPL_FIT_IMAGE_POST_PROCESS
507 bool "Enable post-processing of FIT artifacts after loading by the SPL"
508 depends on SPL_LOAD_FIT
509 help
510 Allows doing any sort of manipulation to blobs after they got extracted
511 from the U-Boot FIT image like stripping off headers or modifying the
512 size of the blob, verification, authentication, decryption etc. in a
513 platform or board specific way. In order to use this feature a platform
514 or board-specific implementation of board_fit_image_post_process() must
515 be provided. Also, anything done during this post-processing step would
516 need to be comprehended in how the images were prepared before being
517 injected into the FIT creation (i.e. the blobs would have been pre-
518 processed before being added to the FIT image).
520 config SPL_FIT_SOURCE
521 string ".its source file for U-Boot FIT image"
522 depends on SPL_FIT
523 help
524 Specifies a (platform specific) FIT source file to generate the
525 U-Boot FIT image. This could specify further image to load and/or
526 execute.
528 config SPL_FIT_GENERATOR
529 string ".its file generator script for U-Boot FIT image"
530 depends on SPL_FIT
531 default "board/sunxi/mksunxi_fit_atf.sh" if SPL_LOAD_FIT && ARCH_SUNXI
532 default "arch/arm/mach-rockchip/make_fit_atf.py" if SPL_LOAD_FIT && ARCH_ROCKCHIP
533 default "arch/arm/mach-zynqmp/mkimage_fit_atf.sh" if SPL_LOAD_FIT && ARCH_ZYNQMP
534 default "arch/riscv/lib/mkimage_fit_opensbi.sh" if SPL_LOAD_FIT && RISCV
535 help
536 Specifies a (platform specific) script file to generate the FIT
537 source file used to build the U-Boot FIT image file. This gets
538 passed a list of supported device tree file stub names to
539 include in the generated image.
541 endif # SPL
543 endif # FIT
545 config LEGACY_IMAGE_FORMAT
546 bool "Enable support for the legacy image format"
547 default y if !FIT_SIGNATURE
548 help
549 This option enables the legacy image format. It is enabled by
550 default for backward compatibility, unless FIT_SIGNATURE is
551 set where it is disabled so that unsigned images cannot be
552 loaded. If a board needs the legacy image format support in this
553 case, enable it here.
555 config OF_BOARD_SETUP
556 bool "Set up board-specific details in device tree before boot"
557 depends on OF_LIBFDT
558 help
559 This causes U-Boot to call ft_board_setup() before booting into
560 the Operating System. This function can set up various
561 board-specific information in the device tree for use by the OS.
562 The device tree is then passed to the OS.
564 config OF_SYSTEM_SETUP
565 bool "Set up system-specific details in device tree before boot"
566 depends on OF_LIBFDT
567 help
568 This causes U-Boot to call ft_system_setup() before booting into
569 the Operating System. This function can set up various
570 system-specific information in the device tree for use by the OS.
571 The device tree is then passed to the OS.
573 config OF_STDOUT_VIA_ALIAS
574 bool "Update the device-tree stdout alias from U-Boot"
575 depends on OF_LIBFDT
576 help
577 This uses U-Boot's serial alias from the aliases node to update
578 the device tree passed to the OS. The "linux,stdout-path" property
579 in the chosen node is set to point to the correct serial node.
580 This option currently references CONFIG_CONS_INDEX, which is
581 incorrect when used with device tree as this option does not
582 exist / should not be used.
584 config SYS_EXTRA_OPTIONS
585 string "Extra Options (DEPRECATED)"
586 help
587 The old configuration infrastructure (= mkconfig + boards.cfg)
588 provided the extra options field. If you have something like
589 "HAS_BAR,BAZ=64", the optional options
590 #define CONFIG_HAS
591 #define CONFIG_BAZ 64
592 will be defined in include/config.h.
593 This option was prepared for the smooth migration from the old
594 configuration to Kconfig. Since this option will be removed sometime,
595 new boards should not use this option.
597 config HAVE_SYS_TEXT_BASE
598 bool
599 depends on !NIOS2 && !XTENSA
600 depends on !EFI_APP
601 default y
603 config SYS_TEXT_BASE
604 depends on HAVE_SYS_TEXT_BASE
605 default 0x80800000 if ARCH_OMAP2PLUS || ARCH_K3
606 default 0x4a000000 if ARCH_SUNXI && !MACH_SUN9I && !MACH_SUN8I_V3S
607 default 0x2a000000 if ARCH_SUNXI && MACH_SUN9I
608 default 0x42e00000 if ARCH_SUNXI && MACH_SUN8I_V3S
609 hex "Text Base"
610 help
611 The address in memory that U-Boot will be running from, initially.
613 config SYS_CLK_FREQ
614 depends on ARC || ARCH_SUNXI || MPC83xx
615 int "CPU clock frequency"
616 help
617 TODO: Move CONFIG_SYS_CLK_FREQ for all the architecture
619 config ARCH_FIXUP_FDT_MEMORY
620 bool "Enable arch_fixup_memory_banks() call"
621 default y
622 help
623 Enable FDT memory map syncup before OS boot. This feature can be
624 used for booting OS with different memory setup where the part of
625 the memory location should be used for different purpose.
627 endmenu # Boot images
629 source "api/Kconfig"
631 source "common/Kconfig"
633 source "cmd/Kconfig"
635 source "disk/Kconfig"
637 source "dts/Kconfig"
639 source "env/Kconfig"
641 source "net/Kconfig"
643 source "drivers/Kconfig"
645 source "fs/Kconfig"
647 source "lib/Kconfig"
649 source "test/Kconfig"