1 Note that this license is not endorsed by the Free Software Foundation.
2 It is available here as a convenience to readers of [1]the license
3 list.
5 The eCos license version 2.0
7 This file is part of eCos, the Embedded Configurable Operating System.
8 Copyright (C) 1998, 1999, 2000, 2001, 2002 Red Hat, Inc.
10 eCos is free software; you can redistribute it and/or modify it under
11 the terms of the GNU General Public License as published by the Free
12 Software Foundation; either version 2 or (at your option) any later
13 version.
15 eCos is distributed in the hope that it will be useful, but WITHOUT ANY
16 WARRANTY; without even the implied warranty of MERCHANTABILITY or
17 FITNESS FOR A PARTICULAR PURPOSE. See the GNU General Public License
18 for more details.
20 You should have received a copy of the GNU General Public License along
21 with eCos; if not, write to the Free Software Foundation, Inc., 51
22 Franklin St, Fifth Floor, Boston, MA 02110-1301 USA.
24 As a special exception, if other files instantiate templates or use
25 macros or inline functions from this file, or you compile this file and
26 link it with other works to produce a work based on this file, this
27 file does not by itself cause the resulting work to be covered by the
28 GNU General Public License. However the source code for this file must
29 still be made available in accordance with section (3) of the GNU
30 General Public License.
32 This exception does not invalidate any other reasons why a work based
33 on this file might be covered by the GNU General Public License.
35 Alternative licenses for eCos may be arranged by contacting Red Hat,
36 Inc. at http://sources.redhat.com/ecos/ecos-license/
37 -------------------------------------------
39 ####ECOSGPLCOPYRIGHTEND####
41 References
43 1. http://www.gnu.org/licenses/license-list.html