1 CONFIG_MIPS=y
2 CONFIG_SYS_TEXT_BASE=0x80010000
3 CONFIG_NR_DRAM_BANKS=1
4 CONFIG_ENV_SIZE=0x2000
5 CONFIG_DM_GPIO=y
6 CONFIG_ARCH_BMIPS=y
7 CONFIG_SOC_BMIPS_BCM6368=y
8 CONFIG_DEFAULT_DEVICE_TREE="comtrend,wap-5813n"
9 # CONFIG_MIPS_BOOT_CMDLINE_LEGACY is not set
10 # CONFIG_MIPS_BOOT_ENV_LEGACY is not set
11 CONFIG_MIPS_BOOT_FDT=y
12 # CONFIG_SYS_MALLOC_CLEAR_ON_INIT is not set
13 CONFIG_OF_STDOUT_VIA_ALIAS=y
14 CONFIG_DISPLAY_CPUINFO=y
15 CONFIG_HUSH_PARSER=y
16 CONFIG_SYS_PROMPT="WAP-5813n # "
17 CONFIG_CMD_CPU=y
18 CONFIG_CMD_LICENSE=y
19 # CONFIG_CMD_BOOTD is not set
20 # CONFIG_CMD_ELF is not set
21 # CONFIG_CMD_XIMG is not set
22 # CONFIG_CMD_EXPORTENV is not set
23 # CONFIG_CMD_IMPORTENV is not set
24 # CONFIG_CMD_EDITENV is not set
25 # CONFIG_CMD_SAVEENV is not set
26 # CONFIG_CMD_ENV_EXISTS is not set
27 # CONFIG_CMD_CRC32 is not set
28 CONFIG_CMD_MEMINFO=y
29 # CONFIG_CMD_LOADS is not set
30 CONFIG_CMD_USB=y
31 CONFIG_CMD_MII=y
32 CONFIG_CMD_PING=y
33 # CONFIG_CMD_SLEEP is not set
34 CONFIG_SYS_RELOC_GD_ENV_ADDR=y
35 CONFIG_NET_RANDOM_ETHADDR=y
36 # CONFIG_DM_DEVICE_REMOVE is not set
37 CONFIG_BCM6348_IUDMA=y
38 CONFIG_BCM6345_GPIO=y
39 CONFIG_LED=y
40 CONFIG_LED_GPIO=y
41 CONFIG_DM_MTD=y
42 CONFIG_MTD_NOR_FLASH=y
43 CONFIG_FLASH_CFI_DRIVER=y
44 CONFIG_CFI_FLASH=y
45 CONFIG_SYS_FLASH_PROTECTION=y
46 CONFIG_SYS_FLASH_CFI=y
47 CONFIG_DM_ETH=y
48 CONFIG_PHY_GIGE=y
49 CONFIG_BCM6368_ETH=y
50 CONFIG_PHY=y
51 CONFIG_BCM6368_USBH_PHY=y
52 CONFIG_DM_RESET=y
53 CONFIG_RESET_BCM6345=y
54 CONFIG_DM_SERIAL=y
55 CONFIG_BCM6345_SERIAL=y
56 CONFIG_USB=y
57 CONFIG_DM_USB=y
58 CONFIG_USB_EHCI_HCD=y
59 CONFIG_USB_EHCI_GENERIC=y
60 CONFIG_USB_OHCI_HCD=y
61 CONFIG_USB_OHCI_GENERIC=y