]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-u-boot/ti-u-boot.git/blob - doc/README.generic_usb_ohci
Prepare v2024.04
[ti-u-boot/ti-u-boot.git] / doc / README.generic_usb_ohci
1 Notes on the the generic USB-OHCI driver
2 ========================================
4 This driver (drivers/usb/usb_ohci.[ch]) is the result of the merge of
5 various existing OHCI drivers that were basically identical beside
6 cpu/board dependant initalization. This initalization has been moved
7 into cpu/board directories and are called via the hooks below.
9 Configuration options
10 ----------------------
12         CONFIG_USB_OHCI_NEW: enable the new OHCI driver
14         CONFIG_SYS_USB_OHCI_BOARD_INIT: call the board dependant hooks:
16                   - extern int board_usb_init(void);
17                   - extern int usb_board_stop(void);
18                   - extern int usb_cpu_init_fail(void);
20         CONFIG_SYS_USB_OHCI_CPU_INIT: call the cpu dependant hooks:
22                   - extern int usb_cpu_init(void);
23                   - extern int usb_cpu_stop(void);
24                   - extern int usb_cpu_init_fail(void);
26         CONFIG_SYS_USB_OHCI_REGS_BASE: defines the base address of the OHCI
27                                 registers
29         CONFIG_SYS_USB_OHCI_SLOT_NAME: slot name
31         CONFIG_SYS_USB_OHCI_MAX_ROOT_PORTS: maximal number of ports of the
32                                      root hub.
35 Endianness issues
36 ------------------
38 The USB bus operates in little endian, but unfortunately there are
39 OHCI controllers that operate in big endian such as ppc4xx. For these the
40 config option
42         CONFIG_SYS_OHCI_BE_CONTROLLER
44 needs to be defined.
47 PCI Controllers
48 ----------------
50 You'll need to define
52         CONFIG_PCI_OHCI
54 If you have several USB PCI controllers, define
56         CONFIG_PCI_OHCI_DEVNO: number of the OHCI device in PCI list
58 If undefined, the first instance found in PCI space will be used.
60 PCI Controllers need to do byte swapping on register accesses, so they
61 should to define:
63         CONFIG_SYS_OHCI_SWAP_REG_ACCESS