1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3 * This file implements recording of each stage of the boot process. It is
4 * intended to implement timing of each stage, reporting this information
5 * to the user and passing it to the OS for logging / further analysis.
6 * Note that it requires timer_get_boot_us() to be defined by the board
7 *
8 * Copyright (c) 2011 The Chromium OS Authors.
9 */
11 #ifndef _BOOTSTAGE_H
12 #define _BOOTSTAGE_H
14 /* Flags for each bootstage record */
15 enum bootstage_flags {
16 BOOTSTAGEF_ERROR = 1 << 0, /* Error record */
17 BOOTSTAGEF_ALLOC = 1 << 1, /* Allocate an id */
18 };
20 /* bootstate sub-IDs used for kernel and ramdisk ranges */
21 enum {
22 BOOTSTAGE_SUB_FORMAT,
23 BOOTSTAGE_SUB_FORMAT_OK,
24 BOOTSTAGE_SUB_NO_UNIT_NAME,
25 BOOTSTAGE_SUB_UNIT_NAME,
26 BOOTSTAGE_SUB_SUBNODE,
28 BOOTSTAGE_SUB_CHECK,
29 BOOTSTAGE_SUB_HASH = 5,
30 BOOTSTAGE_SUB_CHECK_ARCH = 5,
31 BOOTSTAGE_SUB_CHECK_ALL,
32 BOOTSTAGE_SUB_GET_DATA,
33 BOOTSTAGE_SUB_CHECK_ALL_OK = 7,
34 BOOTSTAGE_SUB_GET_DATA_OK,
35 BOOTSTAGE_SUB_LOAD,
36 };
38 /*
39 * A list of boot stages that we know about. Each of these indicates the
40 * state that we are at, and the action that we are about to perform. For
41 * errors, we issue an error for an item when it fails. Therefore the
42 * normal sequence is:
43 *
44 * progress action1
45 * progress action2
46 * progress action3
47 *
48 * and an error condition where action 3 failed would be:
49 *
50 * progress action1
51 * progress action2
52 * progress action3
53 * error on action3
54 */
55 enum bootstage_id {
56 BOOTSTAGE_ID_START = 0,
57 BOOTSTAGE_ID_CHECK_MAGIC, /* Checking image magic */
58 BOOTSTAGE_ID_CHECK_HEADER, /* Checking image header */
59 BOOTSTAGE_ID_CHECK_CHECKSUM, /* Checking image checksum */
60 BOOTSTAGE_ID_CHECK_ARCH, /* Checking architecture */
62 BOOTSTAGE_ID_CHECK_IMAGETYPE = 5,/* Checking image type */
63 BOOTSTAGE_ID_DECOMP_IMAGE, /* Decompressing image */
64 BOOTSTAGE_ID_KERNEL_LOADED, /* Kernel has been loaded */
65 BOOTSTAGE_ID_DECOMP_UNIMPL = 7, /* Odd decompression algorithm */
66 BOOTSTAGE_ID_CHECK_BOOT_OS, /* Calling OS-specific boot function */
67 BOOTSTAGE_ID_BOOT_OS_RETURNED, /* Tried to boot OS, but it returned */
68 BOOTSTAGE_ID_CHECK_RAMDISK = 9, /* Checking ram disk */
70 BOOTSTAGE_ID_RD_MAGIC, /* Checking ram disk magic */
71 BOOTSTAGE_ID_RD_HDR_CHECKSUM, /* Checking ram disk heder checksum */
72 BOOTSTAGE_ID_RD_CHECKSUM, /* Checking ram disk checksum */
73 BOOTSTAGE_ID_COPY_RAMDISK = 12, /* Copying ram disk into place */
74 BOOTSTAGE_ID_RAMDISK, /* Checking for valid ramdisk */
75 BOOTSTAGE_ID_NO_RAMDISK, /* No ram disk found (not an error) */
77 BOOTSTAGE_ID_RUN_OS = 15, /* Exiting U-Boot, entering OS */
79 BOOTSTAGE_ID_NEED_RESET = 30,
80 BOOTSTAGE_ID_POST_FAIL, /* Post failure */
81 BOOTSTAGE_ID_POST_FAIL_R, /* Post failure reported after reloc */
83 /*
84 * This set is reported only by x86, and the meaning is different. In
85 * this case we are reporting completion of a particular stage.
86 * This should probably change in the x86 code (which doesn't report
87 * errors in any case), but discussion this can perhaps wait until we
88 * have a generic board implementation.
89 */
90 BOOTSTAGE_ID_BOARD_INIT_R, /* We have relocated */
91 BOOTSTAGE_ID_BOARD_GLOBAL_DATA, /* Global data is set up */
93 BOOTSTAGE_ID_BOARD_INIT_SEQ, /* We completed the init sequence */
94 BOOTSTAGE_ID_BOARD_FLASH, /* We have configured flash banks */
95 BOOTSTAGE_ID_BOARD_FLASH_37, /* In case you didn't hear... */
96 BOOTSTAGE_ID_BOARD_ENV, /* Environment is relocated & ready */
97 BOOTSTAGE_ID_BOARD_PCI, /* PCI is up */
99 BOOTSTAGE_ID_BOARD_INTERRUPTS, /* Exceptions / interrupts ready */
100 BOOTSTAGE_ID_BOARD_DONE, /* Board init done, off to main loop */
101 /* ^^^ here ends the x86 sequence */
103 /* Boot stages related to loading a kernel from an IDE device */
104 BOOTSTAGE_ID_IDE_START = 41,
105 BOOTSTAGE_ID_IDE_ADDR,
106 BOOTSTAGE_ID_IDE_BOOT_DEVICE,
107 BOOTSTAGE_ID_IDE_TYPE,
109 BOOTSTAGE_ID_IDE_PART,
110 BOOTSTAGE_ID_IDE_PART_INFO,
111 BOOTSTAGE_ID_IDE_PART_TYPE,
112 BOOTSTAGE_ID_IDE_PART_READ,
113 BOOTSTAGE_ID_IDE_FORMAT,
115 BOOTSTAGE_ID_IDE_CHECKSUM, /* 50 */
116 BOOTSTAGE_ID_IDE_READ,
118 /* Boot stages related to loading a kernel from an NAND device */
119 BOOTSTAGE_ID_NAND_PART,
120 BOOTSTAGE_ID_NAND_SUFFIX,
121 BOOTSTAGE_ID_NAND_BOOT_DEVICE,
122 BOOTSTAGE_ID_NAND_HDR_READ = 55,
123 BOOTSTAGE_ID_NAND_AVAILABLE = 55,
124 BOOTSTAGE_ID_NAND_TYPE = 57,
125 BOOTSTAGE_ID_NAND_READ,
127 /* Boot stages related to loading a kernel from an network device */
128 BOOTSTAGE_ID_NET_CHECKSUM = 60,
129 BOOTSTAGE_ID_NET_ETH_START = 64,
130 BOOTSTAGE_ID_NET_ETH_INIT,
132 BOOTSTAGE_ID_NET_START = 80,
133 BOOTSTAGE_ID_NET_NETLOOP_OK,
134 BOOTSTAGE_ID_NET_LOADED,
135 BOOTSTAGE_ID_NET_DONE_ERR,
136 BOOTSTAGE_ID_NET_DONE,
138 BOOTSTAGE_ID_FIT_FDT_START = 90,
139 /*
140 * Boot stages related to loading a FIT image. Some of these are a
141 * bit wonky.
142 */
143 BOOTSTAGE_ID_FIT_KERNEL_START = 100,
145 BOOTSTAGE_ID_FIT_CONFIG = 110,
146 BOOTSTAGE_ID_FIT_TYPE,
147 BOOTSTAGE_ID_FIT_KERNEL_INFO,
149 BOOTSTAGE_ID_FIT_COMPRESSION,
150 BOOTSTAGE_ID_FIT_OS,
151 BOOTSTAGE_ID_FIT_LOADADDR,
152 BOOTSTAGE_ID_OVERWRITTEN,
154 /* Next 10 IDs used by BOOTSTAGE_SUB_... */
155 BOOTSTAGE_ID_FIT_RD_START = 120, /* Ramdisk stages */
157 /* Next 10 IDs used by BOOTSTAGE_SUB_... */
158 BOOTSTAGE_ID_FIT_SETUP_START = 130, /* x86 setup stages */
160 BOOTSTAGE_ID_IDE_FIT_READ = 140,
161 BOOTSTAGE_ID_IDE_FIT_READ_OK,
163 BOOTSTAGE_ID_NAND_FIT_READ = 150,
164 BOOTSTAGE_ID_NAND_FIT_READ_OK,
166 BOOTSTAGE_ID_FIT_LOADABLE_START = 160, /* for Loadable Images */
167 /*
168 * These boot stages are new, higher level, and not directly related
169 * to the old boot progress numbers. They are useful for recording
170 * rough boot timing information.
171 */
172 BOOTSTAGE_ID_AWAKE,
173 BOOTSTAGE_ID_START_TPL,
174 BOOTSTAGE_ID_END_TPL,
175 BOOTSTAGE_ID_START_SPL,
176 BOOTSTAGE_ID_END_SPL,
177 BOOTSTAGE_ID_START_UBOOT_F,
178 BOOTSTAGE_ID_START_UBOOT_R,
179 BOOTSTAGE_ID_USB_START,
180 BOOTSTAGE_ID_ETH_START,
181 BOOTSTAGE_ID_BOOTP_START,
182 BOOTSTAGE_ID_BOOTP_STOP,
183 BOOTSTAGE_ID_BOOTM_START,
184 BOOTSTAGE_ID_BOOTM_HANDOFF,
185 BOOTSTAGE_ID_MAIN_LOOP,
186 BOOTSTAGE_ID_ENTER_CLI_LOOP,
187 BOOTSTAGE_KERNELREAD_START,
188 BOOTSTAGE_KERNELREAD_STOP,
189 BOOTSTAGE_ID_BOARD_INIT,
190 BOOTSTAGE_ID_BOARD_INIT_DONE,
192 BOOTSTAGE_ID_CPU_AWAKE,
193 BOOTSTAGE_ID_MAIN_CPU_AWAKE,
194 BOOTSTAGE_ID_MAIN_CPU_READY,
196 BOOTSTAGE_ID_ACCUM_LCD,
197 BOOTSTAGE_ID_ACCUM_SCSI,
198 BOOTSTAGE_ID_ACCUM_SPI,
199 BOOTSTAGE_ID_ACCUM_DECOMP,
200 BOOTSTAGE_ID_ACCUM_OF_LIVE,
201 BOOTSTAGE_ID_FPGA_INIT,
202 BOOTSTAGE_ID_ACCUM_DM_SPL,
203 BOOTSTAGE_ID_ACCUM_DM_F,
204 BOOTSTAGE_ID_ACCUM_DM_R,
205 BOOTSTAGE_ID_ACCUM_FSP_M,
206 BOOTSTAGE_ID_ACCUM_FSP_S,
207 BOOTSTAGE_ID_ACCUM_MMAP_SPI,
209 /* a few spare for the user, from here */
210 BOOTSTAGE_ID_USER,
211 BOOTSTAGE_ID_ALLOC,
212 };
214 /*
215 * Return the time since boot in microseconds, This is needed for bootstage
216 * and should be defined in CPU- or board-specific code. If undefined then
217 * you will get a link error.
218 */
219 ulong timer_get_boot_us(void);
221 #if defined(USE_HOSTCC)
222 #define show_boot_progress(val) do {} while (0)
223 #else
224 /**
225 * Board code can implement show_boot_progress() if needed.
226 *
227 * @param val Progress state (enum bootstage_id), or -id if an error
228 * has occurred.
229 */
230 void show_boot_progress(int val);
231 #endif
233 #if !defined(USE_HOSTCC)
234 #if CONFIG_IS_ENABLED(BOOTSTAGE)
235 #define ENABLE_BOOTSTAGE
236 #endif
237 #endif
239 #ifdef ENABLE_BOOTSTAGE
241 /* This is the full bootstage implementation */
243 /**
244 * Relocate existing bootstage records
245 *
246 * Call this after relocation has happened and after malloc has been initted.
247 * We need to copy any pointers in bootstage records that were added pre-
248 * relocation, since memory can be overwritten later.
249 * @return Always returns 0, to indicate success
250 */
251 int bootstage_relocate(void);
253 /**
254 * Add a new bootstage record
255 *
256 * @param id Bootstage ID to use (ignored if flags & BOOTSTAGEF_ALLOC)
257 * @param name Name of record, or NULL for none
258 * @param flags Flags (BOOTSTAGEF_...)
259 * @param mark Time to record in this record, in microseconds
260 */
261 ulong bootstage_add_record(enum bootstage_id id, const char *name,
262 int flags, ulong mark);
264 /**
265 * Mark a time stamp for the current boot stage.
266 */
267 ulong bootstage_mark(enum bootstage_id id);
269 ulong bootstage_error(enum bootstage_id id);
271 ulong bootstage_mark_name(enum bootstage_id id, const char *name);
273 /**
274 * Mark a time stamp in the given function and line number
275 *
276 * See BOOTSTAGE_MARKER() for a convenient macro.
277 *
278 * @param file Filename to record (NULL if none)
279 * @param func Function name to record
280 * @param linenum Line number to record
281 * @return recorded time stamp
282 */
283 ulong bootstage_mark_code(const char *file, const char *func,
284 int linenum);
286 /**
287 * Mark the start of a bootstage activity. The end will be marked later with
288 * bootstage_accum() and at that point we accumulate the time taken. Calling
289 * this function turns the given id into a accumulator rather than and
290 * absolute mark in time. Accumulators record the total amount of time spent
291 * in an activty during boot.
292 *
293 * @param id Bootstage id to record this timestamp against
294 * @param name Textual name to display for this id in the report (maybe NULL)
295 * @return start timestamp in microseconds
296 */
297 uint32_t bootstage_start(enum bootstage_id id, const char *name);
299 /**
300 * Mark the end of a bootstage activity
301 *
302 * After previously marking the start of an activity with bootstage_start(),
303 * call this function to mark the end. You can call these functions in pairs
304 * as many times as you like.
305 *
306 * @param id Bootstage id to record this timestamp against
307 * @return time spent in this iteration of the activity (i.e. the time now
308 * less the start time recorded in the last bootstage_start() call
309 * with this id.
310 */
311 uint32_t bootstage_accum(enum bootstage_id id);
313 /* Print a report about boot time */
314 void bootstage_report(void);
316 /**
317 * Add bootstage information to the device tree
318 *
319 * @return 0 if ok, -ve on error
320 */
321 int bootstage_fdt_add_report(void);
323 /**
324 * Stash bootstage data into memory
325 *
326 * @param base Base address of memory buffer
327 * @param size Size of memory buffer
328 * @return 0 if stashed ok, -1 if out of space
329 */
330 int bootstage_stash(void *base, int size);
332 /**
333 * Read bootstage data from memory
334 *
335 * Bootstage data is read from memory and placed in the bootstage table
336 * in the user records.
337 *
338 * @param base Base address of memory buffer
339 * @param size Size of memory buffer (-1 if unknown)
340 * @return 0 if unstashed ok, -ENOENT if bootstage info not found, -ENOSPC if
341 * there is not space for read the stashed data, or other error if
342 * something else went wrong
343 */
344 int bootstage_unstash(const void *base, int size);
346 /**
347 * bootstage_get_size() - Get the size of the bootstage data
348 *
349 * @return size of boostage data in bytes
350 */
351 int bootstage_get_size(void);
353 /**
354 * bootstage_init() - Prepare bootstage for use
355 *
356 * @first: true if this is the first time bootstage is set up. This causes it
357 * to add a 'reset' record with a time of 0.
358 */
359 int bootstage_init(bool first);
361 #else
362 static inline ulong bootstage_add_record(enum bootstage_id id,
363 const char *name, int flags, ulong mark)
364 {
365 return 0;
366 }
368 /*
369 * This is a dummy implementation which just calls show_boot_progress(),
370 * and won't even do that unless CONFIG_SHOW_BOOT_PROGRESS is defined
371 */
373 static inline int bootstage_relocate(void)
374 {
375 return 0;
376 }
378 static inline ulong bootstage_mark(enum bootstage_id id)
379 {
380 show_boot_progress(id);
381 return 0;
382 }
384 static inline ulong bootstage_error(enum bootstage_id id)
385 {
386 show_boot_progress(-id);
387 return 0;
388 }
390 static inline ulong bootstage_mark_name(enum bootstage_id id, const char *name)
391 {
392 show_boot_progress(id);
393 return 0;
394 }
396 static inline ulong bootstage_mark_code(const char *file, const char *func,
397 int linenum)
398 {
399 return 0;
400 }
402 static inline uint32_t bootstage_start(enum bootstage_id id, const char *name)
403 {
404 return 0;
405 }
407 static inline uint32_t bootstage_accum(enum bootstage_id id)
408 {
409 return 0;
410 }
412 static inline int bootstage_stash(void *base, int size)
413 {
414 return 0; /* Pretend to succeed */
415 }
417 static inline int bootstage_unstash(const void *base, int size)
418 {
419 return 0; /* Pretend to succeed */
420 }
422 static inline int bootstage_get_size(void)
423 {
424 return 0;
425 }
427 static inline int bootstage_init(bool first)
428 {
429 return 0;
430 }
432 #endif /* ENABLE_BOOTSTAGE */
434 /* Helper macro for adding a bootstage to a line of code */
435 #define BOOTSTAGE_MARKER() \
436 bootstage_mark_code(__FILE__, __func__, __LINE__)
438 #endif