1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3 * Copyright (C) 2018 Álvaro Fernández Rojas <noltari@gmail.com>
4 * Copyright (C) 2015 - 2018 Texas Instruments Incorporated <www.ti.com>
5 * Written by Mugunthan V N <mugunthanvnm@ti.com>
6 *
7 */
9 #ifndef _DMA_H_
10 #define _DMA_H_
12 #include <linux/bitops.h>
13 #include <linux/errno.h>
14 #include <linux/types.h>
16 struct udevice;
18 /*
19 * enum dma_direction - dma transfer direction indicator
20 * @DMA_MEM_TO_MEM: Memcpy mode
21 * @DMA_MEM_TO_DEV: From Memory to Device
22 * @DMA_DEV_TO_MEM: From Device to Memory
23 * @DMA_DEV_TO_DEV: From Device to Device
24 */
25 enum dma_direction {
26 DMA_MEM_TO_MEM,
27 DMA_MEM_TO_DEV,
28 DMA_DEV_TO_MEM,
29 DMA_DEV_TO_DEV,
30 };
32 #define DMA_SUPPORTS_MEM_TO_MEM BIT(0)
33 #define DMA_SUPPORTS_MEM_TO_DEV BIT(1)
34 #define DMA_SUPPORTS_DEV_TO_MEM BIT(2)
35 #define DMA_SUPPORTS_DEV_TO_DEV BIT(3)
37 /*
38 * struct dma_dev_priv - information about a device used by the uclass
39 *
40 * @supported: mode of transfers that DMA can support, should be
41 * one/multiple of DMA_SUPPORTS_*
42 */
43 struct dma_dev_priv {
44 u32 supported;
45 };
47 #ifdef CONFIG_DMA_CHANNELS
48 /**
49 * A DMA is a feature of computer systems that allows certain hardware
50 * subsystems to access main system memory, independent of the CPU.
51 * DMA channels are typically generated externally to the HW module
52 * consuming them, by an entity this API calls a DMA provider. This API
53 * provides a standard means for drivers to enable and disable DMAs, and to
54 * copy, send and receive data using DMA.
55 *
56 * A driver that implements UCLASS_DMA is a DMA provider. A provider will
57 * often implement multiple separate DMAs, since the hardware it manages
58 * often has this capability. dma_uclass.h describes the interface which
59 * DMA providers must implement.
60 *
61 * DMA consumers/clients are the HW modules driven by the DMA channels. This
62 * header file describes the API used by drivers for those HW modules.
63 *
64 * DMA consumer DMA_MEM_TO_DEV (transmit) usage example (based on networking).
65 * Note. dma_send() is sync operation always - it'll start transfer and will
66 * poll for it to complete:
67 * - get/request dma channel
68 * struct dma dma_tx;
69 * ret = dma_get_by_name(common->dev, "tx0", &dma_tx);
70 * if (ret) ...
71 *
72 * - enable dma channel
73 * ret = dma_enable(&dma_tx);
74 * if (ret) ...
75 *
76 * - dma transmit DMA_MEM_TO_DEV.
77 * struct ti_drv_packet_data packet_data;
78 *
79 * packet_data.opt1 = val1;
80 * packet_data.opt2 = val2;
81 * ret = dma_send(&dma_tx, packet, length, &packet_data);
82 * if (ret) ..
83 *
84 * DMA consumer DMA_DEV_TO_MEM (receive) usage example (based on networking).
85 * Note. dma_receive() is sync operation always - it'll start transfer
86 * (if required) and will poll for it to complete (or for any previously
87 * configured dev2mem transfer to complete):
88 * - get/request dma channel
89 * struct dma dma_rx;
90 * ret = dma_get_by_name(common->dev, "rx0", &dma_rx);
91 * if (ret) ...
92 *
93 * - enable dma channel
94 * ret = dma_enable(&dma_rx);
95 * if (ret) ...
96 *
97 * - dma receive DMA_DEV_TO_MEM.
98 * struct ti_drv_packet_data packet_data;
99 *
100 * len = dma_receive(&dma_rx, (void **)packet, &packet_data);
101 * if (ret < 0) ...
102 *
103 * DMA consumer DMA_DEV_TO_MEM (receive) zero-copy usage example (based on
104 * networking). Networking subsystem allows to configure and use few receive
105 * buffers (dev2mem), as Networking RX DMA channels usually implemented
106 * as streaming interface
107 * - get/request dma channel
108 * struct dma dma_rx;
109 * ret = dma_get_by_name(common->dev, "rx0", &dma_rx);
110 * if (ret) ...
111 *
112 * for (i = 0; i < RX_DESC_NUM; i++) {
113 * ret = dma_prepare_rcv_buf(&dma_rx,
114 * net_rx_packets[i],
115 * RX_BUF_SIZE);
116 * if (ret) ...
117 * }
118 *
119 * - enable dma channel
120 * ret = dma_enable(&dma_rx);
121 * if (ret) ...
122 *
123 * - dma receive DMA_DEV_TO_MEM.
124 * struct ti_drv_packet_data packet_data;
125 *
126 * len = dma_receive(&dma_rx, (void **)packet, &packet_data);
127 * if (ret < 0) ..
128 *
129 * -- process packet --
130 *
131 * - return buffer back to DAM channel
132 * ret = dma_prepare_rcv_buf(&dma_rx,
133 * net_rx_packets[rx_next],
134 * RX_BUF_SIZE);
135 */
137 struct udevice;
139 /**
140 * struct dma - A handle to (allowing control of) a single DMA.
141 *
142 * Clients provide storage for DMA handles. The content of the structure is
143 * managed solely by the DMA API and DMA drivers. A DMA struct is
144 * initialized by "get"ing the DMA struct. The DMA struct is passed to all
145 * other DMA APIs to identify which DMA channel to operate upon.
146 *
147 * @dev: The device which implements the DMA channel.
148 * @id: The DMA channel ID within the provider.
149 *
150 * Currently, the DMA API assumes that a single integer ID is enough to
151 * identify and configure any DMA channel for any DMA provider. If this
152 * assumption becomes invalid in the future, the struct could be expanded to
153 * either (a) add more fields to allow DMA providers to store additional
154 * information, or (b) replace the id field with an opaque pointer, which the
155 * provider would dynamically allocated during its .of_xlate op, and process
156 * during is .request op. This may require the addition of an extra op to clean
157 * up the allocation.
158 */
159 struct dma {
160 struct udevice *dev;
161 /*
162 * Written by of_xlate. We assume a single id is enough for now. In the
163 * future, we might add more fields here.
164 */
165 unsigned long id;
166 };
168 # if CONFIG_IS_ENABLED(OF_CONTROL) && CONFIG_IS_ENABLED(DMA)
169 /**
170 * dma_get_by_index - Get/request a DMA by integer index.
171 *
172 * This looks up and requests a DMA. The index is relative to the client
173 * device; each device is assumed to have n DMAs associated with it somehow,
174 * and this function finds and requests one of them. The mapping of client
175 * device DMA indices to provider DMAs may be via device-tree properties,
176 * board-provided mapping tables, or some other mechanism.
177 *
178 * @dev: The client device.
179 * @index: The index of the DMA to request, within the client's list of
180 * DMA channels.
181 * @dma: A pointer to a DMA struct to initialize.
182 * @return 0 if OK, or a negative error code.
183 */
184 int dma_get_by_index(struct udevice *dev, int index, struct dma *dma);
186 /**
187 * dma_get_by_name - Get/request a DMA by name.
188 *
189 * This looks up and requests a DMA. The name is relative to the client
190 * device; each device is assumed to have n DMAs associated with it somehow,
191 * and this function finds and requests one of them. The mapping of client
192 * device DMA names to provider DMAs may be via device-tree properties,
193 * board-provided mapping tables, or some other mechanism.
194 *
195 * @dev: The client device.
196 * @name: The name of the DMA to request, within the client's list of
197 * DMA channels.
198 * @dma: A pointer to a DMA struct to initialize.
199 * @return 0 if OK, or a negative error code.
200 */
201 int dma_get_by_name(struct udevice *dev, const char *name, struct dma *dma);
202 # else
203 static inline int dma_get_by_index(struct udevice *dev, int index,
204 struct dma *dma)
205 {
206 return -ENOSYS;
207 }
209 static inline int dma_get_by_name(struct udevice *dev, const char *name,
210 struct dma *dma)
211 {
212 return -ENOSYS;
213 }
214 # endif
216 /**
217 * dma_request - Request a DMA by provider-specific ID.
218 *
219 * This requests a DMA using a provider-specific ID. Generally, this function
220 * should not be used, since dma_get_by_index/name() provide an interface that
221 * better separates clients from intimate knowledge of DMA providers.
222 * However, this function may be useful in core SoC-specific code.
223 *
224 * @dev: The DMA provider device.
225 * @dma: A pointer to a DMA struct to initialize. The caller must
226 * have already initialized any field in this struct which the
227 * DMA provider uses to identify the DMA channel.
228 * @return 0 if OK, or a negative error code.
229 */
230 int dma_request(struct udevice *dev, struct dma *dma);
232 /**
233 * dma_free - Free a previously requested DMA.
234 *
235 * @dma: A DMA struct that was previously successfully requested by
236 * dma_request/get_by_*().
237 * @return 0 if OK, or a negative error code.
238 */
239 int dma_free(struct dma *dma);
241 /**
242 * dma_enable() - Enable (turn on) a DMA channel.
243 *
244 * @dma: A DMA struct that was previously successfully requested by
245 * dma_request/get_by_*().
246 * @return zero on success, or -ve error code.
247 */
248 int dma_enable(struct dma *dma);
250 /**
251 * dma_disable() - Disable (turn off) a DMA channel.
252 *
253 * @dma: A DMA struct that was previously successfully requested by
254 * dma_request/get_by_*().
255 * @return zero on success, or -ve error code.
256 */
257 int dma_disable(struct dma *dma);
259 /**
260 * dma_prepare_rcv_buf() - Prepare/add receive DMA buffer.
261 *
262 * It allows to implement zero-copy async DMA_DEV_TO_MEM (receive) transactions
263 * if supported by DMA providers.
264 *
265 * @dma: A DMA struct that was previously successfully requested by
266 * dma_request/get_by_*().
267 * @dst: The receive buffer pointer.
268 * @size: The receive buffer size
269 * @return zero on success, or -ve error code.
270 */
271 int dma_prepare_rcv_buf(struct dma *dma, void *dst, size_t size);
273 /**
274 * dma_receive() - Receive a DMA transfer.
275 *
276 * @dma: A DMA struct that was previously successfully requested by
277 * dma_request/get_by_*().
278 * @dst: The destination pointer.
279 * @metadata: DMA driver's channel specific data
280 * @return length of received data on success, or zero - no data,
281 * or -ve error code.
282 */
283 int dma_receive(struct dma *dma, void **dst, void *metadata);
285 /**
286 * dma_send() - Send a DMA transfer.
287 *
288 * @dma: A DMA struct that was previously successfully requested by
289 * dma_request/get_by_*().
290 * @src: The source pointer.
291 * @len: Length of the data to be sent (number of bytes).
292 * @metadata: DMA driver's channel specific data
293 * @return zero on success, or -ve error code.
294 */
295 int dma_send(struct dma *dma, void *src, size_t len, void *metadata);
297 /**
298 * dma_get_cfg() - Get DMA channel configuration for client's use
299 *
300 * @dma: The DMA Channel to manipulate
301 * @cfg_id: DMA provider specific ID to identify what
302 * configuration data client needs
303 * @cfg_data: Pointer to store pointer to DMA driver specific
304 * configuration data for the given cfg_id (output param)
305 * @return zero on success, or -ve error code.
306 */
307 int dma_get_cfg(struct dma *dma, u32 cfg_id, void **cfg_data);
308 #endif /* CONFIG_DMA_CHANNELS */
310 #if CONFIG_IS_ENABLED(DMA)
311 /*
312 * dma_get_device - get a DMA device which supports transfer
313 * type of transfer_type
314 *
315 * @transfer_type - transfer type should be one/multiple of
316 * DMA_SUPPORTS_*
317 * @devp - udevice pointer to return the found device
318 * @return - will return on success and devp will hold the
319 * pointer to the device
320 */
321 int dma_get_device(u32 transfer_type, struct udevice **devp);
323 /*
324 * dma_memcpy - try to use DMA to do a mem copy which will be
325 * much faster than CPU mem copy
326 *
327 * @dst - destination pointer
328 * @src - souce pointer
329 * @len - data length to be copied
330 * @return - on successful transfer returns no of bytes
331 transferred and on failure return error code.
332 */
333 int dma_memcpy(void *dst, void *src, size_t len);
334 #else
335 static inline int dma_get_device(u32 transfer_type, struct udevice **devp)
336 {
337 return -ENOSYS;
338 }
340 static inline int dma_memcpy(void *dst, void *src, size_t len)
341 {
342 return -ENOSYS;
343 }
344 #endif /* CONFIG_DMA */
345 #endif /* _DMA_H_ */