]> Gitweb @ Texas Instruments - Open Source Git Repositories - git.TI.com/gitweb - ti-u-boot/ti-u-boot.git/blob - include/membuff.h
Prepare v2024.04
[ti-u-boot/ti-u-boot.git] / include / membuff.h
1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3  * Copyright (c) 2015 Google, Inc
4  * Written by Simon Glass <sjg@chromium.org>
5  *
6  * Copyright (c) 1992 Simon Glass
7  */
9 #ifndef _MEMBUFF_H
10 #define _MEMBUFF_H
12 /**
13  * @struct membuff: holds the state of a membuff - it is used for input and
14  * output buffers. The buffer extends from @start to (@start + @size - 1).
15  * Data in the buffer extends from @tail to @head: it is written in at
16  * @head and read out from @tail. The membuff is empty when @head == @tail
17  * and full when adding another character would make @head == @tail. We
18  * therefore waste one character in the membuff to avoid having an extra flag
19  * to determine whether (when @head == @tail) the membuff is empty or full.
20  *
21  * xxxxxx  data
22  * ......  empty
23  *
24  * .............xxxxxxxxxxxxxxxx.........................
25  *              ^               ^
26  *              tail            head
27  *
28  * xxxxxxxxxxxxx................xxxxxxxxxxxxxxxxxxxxxxxxx
29  *              ^               ^
30  *              head            tail
31  */
32 struct membuff {
33         char *start;            /** the start of the buffer */
34         char *end;              /** the end of the buffer (start + length) */
35         char *head;             /** current buffer head */
36         char *tail;             /** current buffer tail */
37 };
39 /**
40  * membuff_purge() - reset a membuff to the empty state
41  *
42  * Initialise head and tail pointers so that the membuff becomes empty.
43  *
44  * @mb: membuff to purge
45  */
46 void membuff_purge(struct membuff *mb);
48 /**
49  * membuff_putraw() - find out where bytes can be written
50  *
51  * Work out where in the membuff some data could be written. Return a pointer
52  * to the address and the number of bytes which can be written there. If
53  * @update is true, the caller must then write the data immediately, since
54  * the membuff is updated as if the write has been done,
55  *
56  * Note that because the spare space in a membuff may not be contiguous, this
57  * function may not return @maxlen even if there is enough space in the
58  * membuff. However, by calling this function twice (with @update == true),
59  * you will get access to all the spare space.
60  *
61  * @mb: membuff to adjust
62  * @maxlen: the number of bytes we want to write
63  * @update: true to update the membuff as if the write happened, false to not
64  * @data: the address data can be written to
65  * @return number of bytes which can be written
66  */
67 int membuff_putraw(struct membuff *mb, int maxlen, bool update, char **data);
69 /**
70  * membuff_getraw() - find and return a pointer to available bytes
71  *
72  * Returns a pointer to any valid input data in the given membuff and
73  * optionally marks it as read. Note that not all input data may not be
74  * returned, since data is not necessarily contiguous in the membuff. However,
75  * if you call this function twice (with @update == true) you are guaranteed
76  * to get all available data, in at most two installments.
77  *
78  * @mb: membuff to adjust
79  * @maxlen: maximum number of bytes to get
80  * @update: true to update the membuff as if the bytes have been read (use
81  * false to check bytes without reading them)
82  * @data: returns address of data in input membuff
83  * @return the number of bytes available at *@data
84  */
85 int membuff_getraw(struct membuff *mb, int maxlen, bool update, char **data);
87 /**
88  * membuff_putbyte() - Writes a byte to a membuff
89  *
90  * @mb: membuff to adjust
91  * @ch: byte to write
92  * @return true on success, false if membuff is full
93  */
94 bool membuff_putbyte(struct membuff *mb, int ch);
96 /**
97  * @mb: membuff to adjust
98  * membuff_getbyte() - Read a byte from the membuff
99  * @return the byte read, or -1 if the membuff is empty
100  */
101 int membuff_getbyte(struct membuff *mb);
103 /**
104  * membuff_peekbyte() - check the next available byte
105  *
106  * Return the next byte which membuff_getbyte() would return, without
107  * removing it from the membuff.
108  *
109  * @mb: membuff to adjust
110  * @return the byte peeked, or -1 if the membuff is empty
111  */
112 int membuff_peekbyte(struct membuff *mb);
114 /**
115  * membuff_get() - get data from a membuff
116  *
117  * Copies any available data (up to @maxlen bytes) to @buff and removes it
118  * from the membuff.
119  *
120  * @mb: membuff to adjust
121  * @Buff: address of membuff to transfer bytes to
122  * @maxlen: maximum number of bytes to read
123  * @return the number of bytes read
124  */
125 int membuff_get(struct membuff *mb, char *buff, int maxlen);
127 /**
128  * membuff_put() - write data to a membuff
129  *
130  * Writes some data to a membuff. Returns the number of bytes added. If this
131  * is less than @lnehgt, then the membuff got full
132  *
133  * @mb: membuff to adjust
134  * @data: the data to write
135  * @length: number of bytes to write from 'data'
136  * @return the number of bytes added
137  */
138 int membuff_put(struct membuff *mb, const char *buff, int length);
140 /**
141  * membuff_isempty() - check if a membuff is empty
142  *
143  * @mb: membuff to check
144  * @return true if empty, else false
145  */
146 bool membuff_isempty(struct membuff *mb);
148 /**
149  * membuff_avail() - check available data in a membuff
150  *
151  * @mb: membuff to check
152  * @return number of bytes of data available
153  */
154 int membuff_avail(struct membuff *mb);
156 /**
157  * membuff_size() - get the size of a membuff
158  *
159  * Note that a membuff can only old data up to one byte less than its size.
160  *
161  * @mb: membuff to check
162  * @return total size
163  */
164 int membuff_size(struct membuff *mb);
166 /**
167  * membuff_makecontig() - adjust all membuff data to be contiguous
168  *
169  * This places all data in a membuff into a single contiguous lump, if
170  * possible
171  *
172  * @mb: membuff to adjust
173  * @return true on success
174  */
175 bool membuff_makecontig(struct membuff *mb);
177 /**
178  * membuff_free() - find the number of bytes that can be written to a membuff
179  *
180  * @mb: membuff to check
181  * @return returns the number of bytes free in a membuff
182  */
183 int membuff_free(struct membuff *mb);
185 /**
186  * membuff_readline() - read a line of text from a membuff
187  *
188  * Reads a line of text of up to 'maxlen' characters from a membuff and puts
189  * it in @str. Any character less than @minch is assumed to be the end of
190  * line character
191  *
192  * @mb: membuff to adjust
193  * @str: Place to put the line
194  * @maxlen: Maximum line length (excluding terminator)
195  * @return number of bytes read (including terminator) if a line has been
196  *         read, 0 if nothing was there
197  */
198 int membuff_readline(struct membuff *mb, char *str, int maxlen, int minch);
200 /**
201  * membuff_extend_by() - expand a membuff
202  *
203  * Extends a membuff by the given number of bytes
204  *
205  * @mb: membuff to adjust
206  * @by: Number of bytes to increase the size by
207  * @max: Maximum size to allow
208  * @return 0 if the expand succeeded, -ENOMEM if not enough memory, -E2BIG
209  * if the the size would exceed @max
210  */
211 int membuff_extend_by(struct membuff *mb, int by, int max);
213 /**
214  * membuff_init() - set up a new membuff using an existing membuff
215  *
216  * @mb: membuff to set up
217  * @buff: Address of buffer
218  * @size: Size of buffer
219  */
220 void membuff_init(struct membuff *mb, char *buff, int size);
222 /**
223  * membuff_uninit() - clear a membuff so it can no longer be used
224  *
225  * @mb: membuff to uninit
226  */
227 void membuff_uninit(struct membuff *mb);
229 /**
230  * membuff_new() - create a new membuff
231  *
232  * @mb: membuff to init
233  * @size: size of membuff to create
234  * @return 0 if OK, -ENOMEM if out of memory
235  */
236 int membuff_new(struct membuff *mb, int size);
238 /**
239  * membuff_dispose() - free memory allocated to a membuff and uninit it
240  *
241  * @mb: membuff to dispose
242  */
243 void membuff_dispose(struct membuff *mb);
245 #endif