1 /* SPDX-License-Identifier: GPL-2.0+ */
2 /*
3 * Copyright 2010-2011 Calxeda, Inc.
4 */
6 #ifndef __MENU_H__
7 #define __MENU_H__
9 struct menu;
11 struct menu *menu_create(char *title, int timeout, int prompt,
12 void (*display_statusline)(struct menu *),
13 void (*item_data_print)(void *),
14 char *(*item_choice)(void *),
15 void *item_choice_data);
16 int menu_default_set(struct menu *m, char *item_key);
17 int menu_get_choice(struct menu *m, void **choice);
18 int menu_item_add(struct menu *m, char *item_key, void *item_data);
19 int menu_destroy(struct menu *m);
20 int menu_default_choice(struct menu *m, void **choice);
22 /**
23 * menu_show() Show a boot menu
24 *
25 * This shows a menu and lets the user select an option. The menu is defined by
26 * environment variables (see README.bootmenu).
27 *
28 * This function doesn't normally return, but if the users requests the command
29 * problem, it will.
30 *
31 * @bootdelay: Delay to wait before running the default menu option (0 to run
32 * the entry immediately)
33 * @return If it returns, it always returns -1 to indicate that the boot should
34 * be aborted and the command prompt should be provided
35 */
36 int menu_show(int bootdelay);
38 #endif /* __MENU_H__ */